Cornell Dubilier Electronics

Cornell Dubilier Electronics

Cornell Dubilier is the supplier of condensers which turn your applications into success tales. It stands out with electrolytic aluminum, mica, engine running and plastic AC and DC condensers for film. Cornell Dubilier produces condensers exclusively and does so for over 100 years. More than 33,000 client groups include the global leaders in solderers, UPS, engines, drives, avionics, electronics, power and military equipment and medical lasers.

Manufacturers introduction

This video will show you the introduction of the company from the CEO of Cornell Dubilier, Jim Kaplan.

Jim Kaplan, CEO, Cornell Dubilier

Cornell Dubilier Electronics, Inc. is an American privately held company that has won a global reputation for manufacturing high-quality high-end capacitors. Almost all of the company's capacitors are used in demanding industrial applications and stand out from the competition.


Catalog

Ⅰ Cornell Dubilier Company Profile

Ⅱ Cornell Dubilier Products

Ⅲ Cornell Dubilier Applications

Ⅳ A Piece Of News about the product

Ⅴ Cornell Dubilier Locations

Ⅵ Cornell Dubilier Alternate Names


Ⅰ Cornell Dubilier Company Profile

Introduction

Cornell Dubilier Electronics, Inc. is an American privately held company that has won a global reputation for manufacturing high-quality high-end capacitors. Almost all of the company's capacitors are used in demanding industrial applications and stand out from the competition.

Cornell Dubilier Electronics provides the best capacitor solutions and insights. In applications ranging from fighter jets to radar systems, from welding machines to wind turbines, Cornell Dubilier provides the highest quality capacitors.

Cornell Dubilier's capacitors are known for their uncompromising reliability. Each capacitor line has undergone rigorous testing. The company takes all factors into consideration, including application conditions, capacitor wear rates, reliability models, etc. . As the largest power capacitor company in North America, Cornell Dubilier offers one of the world's widest selections of aluminum electrolytic capacitors, mica capacitors, AC film capacitors  and DC film capacitors. Cornell Dubilier is also the only manufacturer of high-quality mica capacitors in the United States.

Before the CDE name was used on a capacitor, it was thoroughly tested to meet all key electrical characteristics. Depending on the type of capacitor, further thermal, electrical and mechanical tests (pulse, shock and vibration, humidity) may be performed. Cornell Dubilier is advancing new applications of capacitor technology and driving recent innovations. Cornell Dubilier's expansion of the Flatpack aluminum electrolytic capacitor product line now includes designs to handle high-vibration packages up to 80g.

The company provides more personalized sales, products and technical support. The company has established a global team composed of capacitor experts, distribution partners and sales support personnel to provide timely and thoughtful services. Cornell Dubilier hopes to become the world's most respected supplier of power capacitors. 


Cornell Dubilier History

The roots of Cornell Dubilier can be traced back to 1909, when founder William Dubilier first used a glassy mineral called mica to help form a "condenser" (now called a "capacitor"). Although the success of mica capacitors in its intended application is limited, it continues to revolutionize radio broadcast communications to achieve better transmission over longer distances.

Soon after inventing the mica capacitor, Dubilier began manufacturing capacitors and contributed to the  First World War  by developing a system for detecting submarines. Dubilier Company was the earliest commercial manufacturer of capacitors and merged with Cornell Radio in 1933 to form Cornell Dubilier Electronics (CDE).

Driven by the rise of radio and television broadcasting, the company has experienced astonishing development. By 1966, it had more than 350 patents in the fields of radio and electrical science. Over time, the company further developed into one of the largest capacitor manufacturers in the world.


Ⅱ Cornell Dubilier Products

Cornell Dubilier Supercapacitors

                          Image                          Products                                           Description

106DCR2R3SGU.png

                    106DCR2R3SGU                           Radial Leaded Super Capacitors.

226DCR2R3STU.png

                     226DCR2R3STU                            Radial Leaded Super Capacitors.

306DCR2R3STV.png

                     306DCR2R3STV                            Radial Leaded Super Capacitors.

407DCR2R3SDG.png

                     407DCR2R3SDG                            Radial Leaded Super Capacitors.

227DCR2R3SNI.png

                     227DCR2R3SNI                             Radial Leaded Super Capacitors.

Cornell Dubilier Capacitors

                              Image                         Products                                        Description

CMR03E220DOYR.png

                   CMR03E220DOYR              Type CMR, High-Reliability, Mica Capacitors

CMR03E240DOYR.png

                   CMR03E240DOYR              Type CMR, High-Reliability, Mica Capacitors

CMR03E430JOYR.png

                    CMR03E430JOYR               Type CMR, High-Reliability, Mica Capacitors

CMR03E470JOYR.png

                    CMR03E470JOYR                Type CMR, High-Reliability, Mica Capacitors

CMR03E510JOYR.png

                    CMR03E510JOYR                  Type CMR, High-Reliability, Mica Capacitors

Aluminum Polymer Capacitors

                              Image                     Products                                             Description

107XMPL002MG19.png

              107XMPL002MG19                                Aluminum Polymer Capacitors

337XMPL002MG28R.png

              337XMPL002MG28R                               Aluminum Polymer Capacitors

AVE107M16E16T-F.png

               AVE107M16E16T-F          Type AVE –40 °C to 85 °C General Purpose SMT Capacitors

AFK337M2AR44T-F.png

             AFK337M2AR44T-F                                 Type AFK –55 °C to 105 °C
      SMT Aluminum Electrolytic Capacitors - Lowest E.S.R., 105 °C

AFK476M50X16T-F.png

             AFK476M50X16T-F                                 Type AFK –55 °C to 105 °C
       SMT Aluminum Electrolytic Capacitors - Lowest E.S.R., 105 °C


Ⅲ Cornell Dubilier Applications

• AC Resonant and Harmonic Filter

• Hid and Ballast Lighting Capacitors

• Motor Run Capacitors

• Resonant Capacitors

• Battery, Battery Backup & SupercapAcitors

• High Energy Storage Pulse Discharge

• Motor Start Capacitors

• RF Capacitors

• DC Link, DC Filtering

• Inverter Capacitors

• Mounting Hardware

• Snubber Capacitors

• Defibrillator Capacitors

• Microwave Oven Capacitors

• Photo Flash and Strobe

• X2 and ARC Suppression

• Harsh Environments

• Military/Aerospace Capacitors

• Power Factor Correction and Harmonic



Ⅳ A Piece Of News about the product

AC HARMONIC FILTER CAPACITORS HAVE DUAL-END OPEN CIRCUIT PROTECTION

Patented design safely expands mounting possibilities.

Cornell Dubilier has introduced the PCD line of high-current AC harmonic filter capacitors, which feature two built-in fail-safe protection devices, one at each end of the capacitor.

Similar capacitors in this category feature one open-circuit pressure device situated under the top cover, which necessitates mounting the capacitor from the bottom stud. The PCD  's terminals can be fastened to a rigid busbar with the addition of a bottom pressure device, allowing the bottom safety device to be activated when appropriate space is supplied at the bottom. When the bottom pressure device is turned on, it expands outward like a bellows.

While these fail-safe devices are meant to avoid case rupture at the end of their service life, PCD  series capacitors are built to be extremely dependable, with a service life of over 60,000 hours at rated voltage and temperature. Their dependability is enhanced by their self-healing, metalized dielectric architecture.

Capacitance ratings of 20 F to 125 F are available in the PCD  series, with voltage ratings ranging from 240 Vac to 600 Vac 50/60Hz. The diameters of the cases range from 63.5mm to 116mm. Capacitance and voltage ratings, as well as sizes and performance characteristics, can all be customized. To properly size capacitors for peak performance, specific application characteristics, particularly harmonic content profiles, are required. M6x1 threaded, tin-plated brass terminations are standard. Other methods of termination are possible.

PCD capacitors are also durable, allowing them to be used in high-humidity conditions. The series has been tested for 1000 hours at 85°C/85 percent RH, putting them in the highest climatic category of Class III-B, according to IEC 60384.

UPS, AC-tuned filters,  AC input filtering, line conditioning, noise suppression, variable-speed drives, and wind turbine monitoring are some of the applications. The PCD  is a step up from European AC power film capacitors, which typically simply include a downward expanding interruption mechanism. When a fail-safe operation is critical, the PCD  series' dual pressure interrupter allows the operator maximum mounting options.



Ⅴ Cornell Dubilier Locations

Corporate Headquarters

South Carolina, United States


Ⅵ Cornell Dubilier Alternate Names

Cornell Dubilier has several brands around the world that distributors may use as alternate names. Cornell Dubilier may also be known as the following names:

CORNELL
CDE
Cornell Dubilier Electronics
CORNELL DUBLIER
DUBILIER
CDC
COR
Cornell Dubilier Electronics (CDE)
CORNELL DUB
CORNEL
CAP
CORNELL DUBILIE
DUB
CORNELL DUBILIER ELECTRONICS INC
Cornell Dubilier - CDE
CORNELL DUBI
ELMENCO
CORN DUB
Cornell Dubilier Electron
CORNELL DUBILIER MARKETING
CORNELL DUBLIER ELECTRONICS
DUBIL
CORNELL DUBILIER ELE
CORNELL-DUBILER
CORNEL DUBLIER
CDE


Frequently Asked Questions

1. Where are Cornell Dubilier capacitors made?

Cornell Dubilier's strength is in the design and manufacture of electrolytic, AC and DC film, and mica capacitors for power electronics. They have facilities in New Bedford, MA, Liberty, SC, Mexicali, Mexico and Shanghai, China.

2. Where is Cornell Dubilier located?

1605 East Rodney French Blvd. The New Bedford, MA facility overlooks the Acushnet River where it enters Buzzard's Bay and is a one-hour drive from Cape Cod. It occupies 70,000 square feet (6,500 square meters) of a 450,000 square foot (41,800 square meters) 1910 textile mill.

3. What does Cornell Dubilier make?

Company Description: Cornell Dubilier Electronics (CDE) makes capacitors, including aluminum electrolytic, clad mica, film, pulse, and high-voltage capacitors. Capacitors are used in virtually all electronic devices to store, filter, and regulate electrical energy.