Cornell Dubilier Electronics
Cornell Dubilier is the supplier of condensers which turn your applications into success tales. It stands out with electrolytic aluminum, mica, engine running and plastic AC and DC condensers for film. Cornell Dubilier produces condensers exclusively and does so for over 100 years. More than 33,000 client groups include the global leaders in solderers, UPS, engines, drives, avionics, electronics, power and military equipment and medical lasers.
Capacitors
Resistors
Kits
Connectors, Interconnects
Barrel - Audio ConnectorsModular Connectors - Wiring BlocksRectangular Connectors - ContactsModular Connectors - Jacks With MagneticsTerminal Blocks - SpecializedUSB, DVI, HDMI ConnectorsCircular ConnectorsTerminal Blocks - Panel MountTerminal Blocks - Barrier BlocksTerminals - PC Pin Receptacles, Socket ConnectorsSockets for ICs, TransistorsFilters
Battery Products
Hardware, Fasteners, Accessories
Discrete Semiconductor Products
Tools
Circuit Protection
Inductors, Coils, Chokes
Optoelectronics
Potentiometers, Variable Resistors
Switches
RF/IF and RFID
Audio Products
Boxes, Enclosures, Racks
Relays
Test and Measurement
Transformers
Cables, Wires
Cables, Wires - Management
Development Boards, Kits, Programmers
Fans, Thermal Management
Integrated Circuits (ICs)
Labels, Signs, Barriers, Identification
Power Supplies - Board Mount
Prototyping, Fabrication Products
Sensors, Transducers
Tapes, Adhesives, Materials

Jim Kaplan, CEO, Cornell Dubilier
Cornell Dubilier Electronics, Inc. is an American privately held company that has won a global reputation for manufacturing high-quality high-end capacitors. Almost all of the company's capacitors are used in demanding industrial applications and stand out from the competition.
Catalog
Ⅰ Cornell Dubilier Company Profile
Ⅲ Cornell Dubilier Applications
Ⅳ A Piece Of News about the product
Ⅵ Cornell Dubilier Alternate Names
Ⅰ Cornell Dubilier Company Profile
Introduction
Cornell Dubilier Electronics, Inc. is an American privately held company that has won a global reputation for manufacturing high-quality high-end capacitors. Almost all of the company's capacitors are used in demanding industrial applications and stand out from the competition.
Cornell Dubilier Electronics provides the best capacitor solutions and insights. In applications ranging from fighter jets to radar systems, from welding machines to wind turbines, Cornell Dubilier provides the highest quality capacitors.
Cornell Dubilier's capacitors are known for their uncompromising reliability. Each capacitor line has undergone rigorous testing. The company takes all factors into consideration, including application conditions, capacitor wear rates, reliability models, etc. . As the largest power capacitor company in North America, Cornell Dubilier offers one of the world's widest selections of aluminum electrolytic capacitors, mica capacitors, AC film capacitors and DC film capacitors. Cornell Dubilier is also the only manufacturer of high-quality mica capacitors in the United States.
Before the CDE name was used on a capacitor, it was thoroughly tested to meet all key electrical characteristics. Depending on the type of capacitor, further thermal, electrical and mechanical tests (pulse, shock and vibration, humidity) may be performed. Cornell Dubilier is advancing new applications of capacitor technology and driving recent innovations. Cornell Dubilier's expansion of the Flatpack aluminum electrolytic capacitor product line now includes designs to handle high-vibration packages up to 80g.
The company provides more personalized sales, products and technical support. The company has established a global team composed of capacitor experts, distribution partners and sales support personnel to provide timely and thoughtful services. Cornell Dubilier hopes to become the world's most respected supplier of power capacitors.
Cornell Dubilier History
The roots of Cornell Dubilier can be traced back to 1909, when founder William Dubilier first used a glassy mineral called mica to help form a "condenser" (now called a "capacitor"). Although the success of mica capacitors in its intended application is limited, it continues to revolutionize radio broadcast communications to achieve better transmission over longer distances.
Soon after inventing the mica capacitor, Dubilier began manufacturing capacitors and contributed to the First World War by developing a system for detecting submarines. Dubilier Company was the earliest commercial manufacturer of capacitors and merged with Cornell Radio in 1933 to form Cornell Dubilier Electronics (CDE).
Driven by the rise of radio and television broadcasting, the company has experienced astonishing development. By 1966, it had more than 350 patents in the fields of radio and electrical science. Over time, the company further developed into one of the largest capacitor manufacturers in the world.
Ⅱ Cornell Dubilier Products
Cornell Dubilier Supercapacitors
| Image | Products | Description |
| 106DCR2R3SGU | Radial Leaded Super Capacitors. |
| 226DCR2R3STU | Radial Leaded Super Capacitors. |
| 306DCR2R3STV | Radial Leaded Super Capacitors. |
| 407DCR2R3SDG | Radial Leaded Super Capacitors. |
| 227DCR2R3SNI | Radial Leaded Super Capacitors. |
Cornell Dubilier Capacitors
| Image | Products | Description |
| CMR03E220DOYR | Type CMR, High-Reliability, Mica Capacitors |
| CMR03E240DOYR | Type CMR, High-Reliability, Mica Capacitors |
| CMR03E430JOYR | Type CMR, High-Reliability, Mica Capacitors |
| CMR03E470JOYR | Type CMR, High-Reliability, Mica Capacitors |
| CMR03E510JOYR | Type CMR, High-Reliability, Mica Capacitors |
Aluminum Polymer Capacitors
| Image | Products | Description |
| 107XMPL002MG19 | Aluminum Polymer Capacitors |
| 337XMPL002MG28R | Aluminum Polymer Capacitors |
| AVE107M16E16T-F | Type AVE –40 °C to 85 °C General Purpose SMT Capacitors |
| AFK337M2AR44T-F | Type AFK –55 °C to 105 °C SMT Aluminum Electrolytic Capacitors - Lowest E.S.R., 105 °C |
| AFK476M50X16T-F | Type AFK –55 °C to 105 °C SMT Aluminum Electrolytic Capacitors - Lowest E.S.R., 105 °C |
Ⅲ Cornell Dubilier Applications
• AC Resonant and Harmonic Filter | • Hid and Ballast Lighting Capacitors | • Motor Run Capacitors | • Resonant Capacitors |
• Battery, Battery Backup & SupercapAcitors | • High Energy Storage Pulse Discharge | • Motor Start Capacitors | • RF Capacitors |
• DC Link, DC Filtering | • Inverter Capacitors | • Mounting Hardware | • Snubber Capacitors |
• Defibrillator Capacitors | • Microwave Oven Capacitors | • Photo Flash and Strobe | • X2 and ARC Suppression |
• Harsh Environments | • Military/Aerospace Capacitors | • Power Factor Correction and Harmonic |
Ⅳ A Piece Of News about the product
AC HARMONIC FILTER CAPACITORS HAVE DUAL-END OPEN CIRCUIT PROTECTION
Patented design safely expands mounting possibilities.
Cornell Dubilier has introduced the PCD line of high-current AC harmonic filter capacitors, which feature two built-in fail-safe protection devices, one at each end of the capacitor.
Similar capacitors in this category feature one open-circuit pressure device situated under the top cover, which necessitates mounting the capacitor from the bottom stud. The PCD 's terminals can be fastened to a rigid busbar with the addition of a bottom pressure device, allowing the bottom safety device to be activated when appropriate space is supplied at the bottom. When the bottom pressure device is turned on, it expands outward like a bellows.
While these fail-safe devices are meant to avoid case rupture at the end of their service life, PCD series capacitors are built to be extremely dependable, with a service life of over 60,000 hours at rated voltage and temperature. Their dependability is enhanced by their self-healing, metalized dielectric architecture.
Capacitance ratings of 20 F to 125 F are available in the PCD series, with voltage ratings ranging from 240 Vac to 600 Vac 50/60Hz. The diameters of the cases range from 63.5mm to 116mm. Capacitance and voltage ratings, as well as sizes and performance characteristics, can all be customized. To properly size capacitors for peak performance, specific application characteristics, particularly harmonic content profiles, are required. M6x1 threaded, tin-plated brass terminations are standard. Other methods of termination are possible.
PCD capacitors are also durable, allowing them to be used in high-humidity conditions. The series has been tested for 1000 hours at 85°C/85 percent RH, putting them in the highest climatic category of Class III-B, according to IEC 60384.
UPS, AC-tuned filters, AC input filtering, line conditioning, noise suppression, variable-speed drives, and wind turbine monitoring are some of the applications. The PCD is a step up from European AC power film capacitors, which typically simply include a downward expanding interruption mechanism. When a fail-safe operation is critical, the PCD series' dual pressure interrupter allows the operator maximum mounting options.
Ⅴ Cornell Dubilier Locations
Corporate Headquarters
South Carolina, United States
Ⅵ Cornell Dubilier Alternate Names
Cornell Dubilier has several brands around the world that distributors may use as alternate names. Cornell Dubilier may also be known as the following names:
| CORNELL CDE Cornell Dubilier Electronics CORNELL DUBLIER DUBILIER CDC COR Cornell Dubilier Electronics (CDE) CORNELL DUB | CORNEL CAP CORNELL DUBILIE DUB CORNELL DUBILIER ELECTRONICS INC Cornell Dubilier - CDE CORNELL DUBI ELMENCO CORN DUB | Cornell Dubilier Electron CORNELL DUBILIER MARKETING CORNELL DUBLIER ELECTRONICS DUBIL CORNELL DUBILIER ELE CORNELL-DUBILER CORNEL DUBLIER CDE |
1. Where are Cornell Dubilier capacitors made?
Cornell Dubilier's strength is in the design and manufacture of electrolytic, AC and DC film, and mica capacitors for power electronics. They have facilities in New Bedford, MA, Liberty, SC, Mexicali, Mexico and Shanghai, China.
2. Where is Cornell Dubilier located?
1605 East Rodney French Blvd. The New Bedford, MA facility overlooks the Acushnet River where it enters Buzzard's Bay and is a one-hour drive from Cape Cod. It occupies 70,000 square feet (6,500 square meters) of a 450,000 square foot (41,800 square meters) 1910 textile mill.
3. What does Cornell Dubilier make?
Company Description: Cornell Dubilier Electronics (CDE) makes capacitors, including aluminum electrolytic, clad mica, film, pulse, and high-voltage capacitors. Capacitors are used in virtually all electronic devices to store, filter, and regulate electrical energy.


Product
Brand
Articles
Tools