Nexperia

Nexperia

Nexperia is dedicated to Discretes, Logic and MOSFETs devices. This new company became independent at the beginning of 2017.

Manufacturers introduction

This video will show you the information of Nexperia.

Nexperia company video - The global expert in essential semiconductors

Nexperia is a world leader in the high-volume production of critical semiconductors, which are crucial components in every electronic design. The company has approximately 12,000 personnel spanning Asia, Europe, and the United States, with decades of experience providing the world's largest firms. The manufacturing locations of Nexperia are in Nexperia Hamburg, Nexperia Malaysia and so on. NXP Nexperia.



What is Nexperia NXP: Nexperia, the former Standard Products division of NXP.


Catalog

Ⅰ Nexperia Company Profile

Ⅱ Nexperia Products

Ⅲ Nexperia Applications

Ⅳ Nexperia Share Price

Ⅴ Nexperia News

Ⅵ Nexperia Locations

Ⅶ Nexperia Alternate Names


Ⅰ Nexperia Company Profile

Introduction


Nexperia is a world leader in the high-volume production of critical semiconductors, which are crucial components in every electronic design. Diodes, bipolar transistors ESD  protection devices MOSFETs , GaN FETs, and analog & logic ICs are among the company's many products. Nexperia, based in Nijmegen, the Netherlands, In Hamburg, Germany, and Greater Manchester, England, it has front-end factories. It is the former NXP Semiconductors Standard Products business unit. It exports more than 100 billion items each year, adhering to the automotive industry's demanding criteria. These products are industry-leading tiny packages that conserve energy and space and are acknowledged as efficiency benchmarks in process, size, power, and performance.

Nexperia has approximately 12,000 personnel spanning Asia, Europe, and the United States, with decades of experience providing the world's largest firms. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949,  ISO  9001, ISO 14001 and ISO 45001.

Nexperia Jobs

• Design Manager Power ICs
• Senior/Principal Design Engineer (Power IC)
• Principal Analog Design Engineer
• Senior/Principal Design Engineer - Signal Chain
• Senior Principal Analog Design Engineer
• R&D Project Manager for Analog Semiconductor Devices
• Senior Principal Test Engineer
• Senior Validation Engineer
• Principal Validation Engineer
• Device Engineer
• International Product Marketing Manager (m/f/d)
• Techniker Wafertest (m/w/d)
• Environment, Social & Governance Expert (m/f/d)
• Senior Principal Design Engineer Gate Drives (Design Architect)
• Process Engineer
• Corporate Recruiter US


Ⅱ Nexperia Products

                            Image                 Product                                                       Description

BZB784-C10.png

             BZB784-C10                                       Voltage regulator double diodes

1N4746A.png

                1N4746A                                               Voltage regulator diodes

BAS17.png

                  BAS17                                                  Low-voltage stabistor

BZX84-A10-Q.png

            BZX84-A10-Q                                                Voltage regulator diodes

1PS300.png

                 1PS300                                          Dual high-speed switching diode

74AUP1G18GM.png

           74AUP1G18GM                Low-power 1-of-2 demultiplexer with 3-state deselected output

XS3A1T5157GS.png

           XS3A1T5157GS                          Low-ohmic single-pole double-throw analog switch

NXS0104PW-Q100.png

         NXS0104PW-Q100              Dual supply translating transceiver; open-drain; auto direction sensing

LSF0102DP.png

              LSF0102DP             2-bit bidirectional multi-voltage level translator; open-drain; push-pull

LFPAK88.png

                LFPAK88                             MOSFETs, Driving power-density to the next level

DFN0606.png

                DFN0606         MOSFETs, Ultra-small footprint, increased power efficiency, 0.35 mm pitch


Ⅲ Nexperia Applications

                   Name                                                                                              Aspect
              Automotive• Adaptive Front LED lights
• ADAS radar sensor module
• Automatic HVAC - BLDC blower motor
• Cooling Fan
• Electronic Fuel Injection
• Electronic Power Steering
• Anti-locking braking systems
• High power, high-efficiency DC/DC converter
• Step-down DC/DC converter
• Constant current source for interior LED lighting
• In-Vehicle Network (CAN / LIN / FlexRay) protection
• Multimedia/infotainment bus protection
• LED backlight for touch screens and cameras
    Computing and Consumer• E-Bike
• High-performance computing / Server
• Hot-swap for blade server
• Solid-state drive (SSD)
• Unmanned aerial vehicles (UAVs)
• Smoke / Fire detector
• Medical diagnostics and therapy
        Industrial and Power• 12–48 V power tools and cordless equipment
• 48/12 V DC/DC conversion (Telecoms / Server)
• 80 PLUS Titanium Industrial PSU (GaN-based)
• 5G marco / micro-cell power supplies
• AC EV wallbox / Bidirectional DC wallbox
• Electric forklift truck
• Photovoltaic (PV) single-phase string inverter
• Industrial Power Supply Units (PSUs)
• Hot-swap for communications infrastructure
• Power Sourcing Equipment / Power over Ethernet
       Mobile and Wearables• AR / VR glasses
• Earbuds
• GPS tracker
• Smartwatch/fitness tracker
• Smartphone
• USB-Type-C AC/DC Wall Charger
• Wired and wireless fast charging
             Sub-systems• Antenna protection (NFC / Bluetooth)
• Constant current source
• I2C voltage translation
• Shift register-based LED driver
• Solenoid driver
• USB4 connectivity and compatibility
• DC/DC conversion for MCU core supply
• Battery-powered motor control drive (25-100 V)
• Asynchronous step-down DC/DC
• Synchronous step-down DC/DC
         Reference designs• H-bridge motor controller power supply circuit• Broadcom GAN039-650NBB half-bridge evaluation board


Ⅳ Nexperia Share Price

share price.png

Stock

Ⅴ Nexperia News

news.jpg


Nexperia introduces a range of A-selection Zener diodes for precise voltage reference with the industry’s lowest tolerance of ±1%

Nijmegen -- The comprehensive product range covers every application from 1.8 V to 75 V

Nexperia, a leader in critical semiconductors, today revealed the first A-selection Zener diodes in the industry. The BZT52H-A (SOD123F) and BZX384-A (SOD323) series give a higher accuracy voltage reference than the B (±2%) and C (±5%) variations, with a tolerance of just ±1%. The two series are also available as Q-portfolio devices to address the increased demands of mobile, portable/wearable, automotive, and industrial applications, as well as increasing regulatory requirements.

According to Paula Stümer, product manager at Nexperia, "Nexperia's A-selection Zener diode range covers every application from 1.8 V to 75 V while delivering an accurate voltage reference with the lowest possible tolerance." "Engineers can go to the limitations of the MOSFET, if applied to limit voltage for the gate-source path or drain-gate path, or choose from a wider variety of acceptable MOSFETs, by substituting B- or C-selection devices with pad compatible A-selection Zener devices."

The nominal working voltage range of A-selection Zener diodes is 1.8 V to 75 V. (E24 range). The devices feature a non-repetitive peak reverse power dissipation of ≤40W, total power dissipation ≤250mW and low differential thermal resistance. The low tolerance allows engineers to substitute more expensive voltage reference devices with greater accuracy voltages, which is especially useful for test and measurement applications. Instead of directly safeguarding the MOSFET.  a Zener diode connected in parallel to the drain-gate line is a more cost-effective option. The MOSFET turns on when the Zener breaks through, preventing the drain source from avalanche breakdown.

AEC-Q101 and  ISO/TS16949  automotive quality standards are met by the A-selection Zeners, which are also available as Q-portfolio devices. These standards are designed to meet the requirements of automotive OEMs for Stress Test Qualification and quality management systems. Customer demands, on the other hand, are evolving, and more non-automotive applications are requiring quality-related services like  PPAP  (Production Part Approval Process) and increased durability. Another distinction between standard and Q-portfolio devices is the  Product Change Notifications  (PCN) term, which has been increased from 90 days to 180 days in accordance with  JEDEC  guidelines. Furthermore, all parts are guaranteed for a minimum of 10 years and have a shelf life of more than two years.

Nexperia continues to invest in technology and in-house manufacturing capacity. The A-selection Zeners are already available as samples and in volume production quantities.


Ⅵ Nexperia Locations

locations.jpg

Sales offices

Nexperia is headquartered in Nijmegen and has a global presence (Netherlands). We have offices in Asia (Beijing, Shanghai, Shenzhen, Hong Kong, Taipei, Singapore, Seoul, Osaka, and Tokyo), Europe (Hamburg, München, Budapest, Milan, and Courbevoie), and the Americas (Detroit, Durham, and Santa Clara), all of which are close to our important customers.

Manufacturing locations

Nexperia's manufacturing facilities are vertically integrated and produce high-volume products at optimal efficiency. These include our own wafer fabs in Hamburg (Germany, Nexperia Hamburg), Manchester and Newport (UK), as well as three assembly centers in Guangdong (China), Seremban (Nexperia Malaysia) and Cabuyao (Phillipes). We have the industry's largest capacity for diverse packages and are constantly investing in new capacity. We're ensuring the long-term availability of our production methods and goods so that our customers may be certain in their supply.


Nexperia USA Inc.



Ⅶ Nexperia Alternate Names

Nexperia has several brands around the world that distributors may use as alternate names. Nexperia may also be known as the following names:

Nexperia USA Inc
Nexperia BV
NXP/NEXPERIA
Nexperia USA
NEXP
NEXPERIA / NXP
Nexperia Inc
NEXPER
Nexperia/NXP Semiconductors
Nexperi

Manufacturers Alias

  • Nexperia USA Inc
  • Nexperia BV
  • NXP/NEXPERIA
  • Nexperia USA
  • NEXP
  • NEXPERIA / NXP
  • Nexperia Inc
  • NEXPER
  • Nexperia/NXP Semiconductors
  • Nexperi
Frequently Asked Questions

1. Is Nexperia a Chinese company?

Currently, it is owned by Chinese based 'Wingtech Group'. Before becoming the company name for the Standards Products business spun-off from NXP, Nexperia was a brand for NXP's media processors range.

2. Is Nexperia same as NXP?

Nexperia, the former Standard Products division of NXP, today announced the formal completion of its launch as a separate entity. Headquartered in Nijmegen, Netherlands and backed by a consortium of financial investors consisting of Beijing Jianguang Asset Management Co.

3. Who is the owner of Nexperia?

Wingtech Technology.

4. Is NXP a good buy?

NXPI has an Overall Score of 80. ... NXPI has an average analyst ranking of Strong Buy with an average price target of $238.318.

5. When was NXP founded? Where is NXP based?

2006, Eindhoven, Netherlands. Headquartered in Eindhoven, Netherlands and with locations throughout the globe, our dedicated team of ~29,000 employees are united by a passion to build solutions—not just products—that enhance the capabilities of people, organizations and society at large.