Sort by
VRAM (Video RAM) Explained03 June 2021
VRAM (video RAM), also known as a frame buffer, is used to store the rendering data processed or about to be extracted by the graphics chip. Like computer memory, VRAM is a component used to store graphics information to be processed.
Introduction to Optical Amplifier27 March 2025
An optical amplifier is a subsystem product that can amplify optical signals in optical fiber communication systems. The principle of the optical amplifier is basically based on the stimulated radiation of the laser, which realizes the amplification effect by converting the energy of the pump light into the energy of the signal light.
Solid State Relay Basics: Working, Features and Structure17 September 2020
Solid State Relay (SSR) is a non-contact switch composed of microelectronic circuits, discrete electronic devices, and power electronic power devices. The isolation device is used to realize the isolation between the control end and the load end. The input terminal of the solid state relay uses a tiny control signal to directly drive a large current load.
What are Graphene Transistors?21 October 2025
Graphene is a two-dimensional crystal. Its structure is very stable because carbon atoms are arranged in hexagons and connected to each other to form a carbon molecule.
Bearing: Features, Types and Uses08 February 2022
Hello everyone, I am Rose. Today I will introduce bearing to you. Bearing is an important component in contemporary mechanical equipment. Its main function is to support the mechanical rotating body, reduce the friction coefficient during its movement, and ensure its rotation accuracy.
A Guide to AVR Microcontroller [PDF]15 October 2025
AVR microcontroller is an enhanced RISC (Reduced Instruction Set CPU) high-speed 8-bit microcontroller with built-in Flash developed by ATMEL in 1997.
Design and Implementation of High Frequency Inverter for Printer Based on IR211013 April 2022
Hello everyone, I am Rose. Welcome to the new post today.In this article, the design of an independent inverter power supply based on SPWM technology is completed by combining the principle of the inverter circuit with the single-chip technology.
Silicon Carbide (SiC): The Third-generation Semiconductor Material30 August 2021
Silicon carbide (SiC) is the main development direction of the power semiconductor industry. It is the semiconductor material to make power devices. In the foreseeable future, new energy vehicles are the main application for silicon carbide power devices.
Introduction to Flash Memory31 October 2025
Flash memory is a non-volatile computer memory storage medium that allows multiple erases or writes during operation. This technology is mainly used for general data storage, as well as the exchange and transmission of data between computers and other digital products, such as memory cards and USB flash drives.
Introduction to Top Sensor Manufacturers in the World15 February 2022
The modern industrial system cannot be separated from sensors. In this article, we will introduce you to 10 world-renowned sensor companies.
NPN Transistors and PNP Transistors29 October 2020
NPN and PNP are two types of transistors. Transistors are semiconductor devices made of doped p-type and n-type junctions. This article mainly introduces the differences between this two kinds of transistors, the methods of distinguishing them, and the application of them.
An Overview of Photoelectric Sensors27 October 2025
The photoelectric sensor is a key component of photoelectric conversion in various photoelectric detection systems. It is a device that converts optical signals (visible and ultraviolet laser light) into electrical signals. There are many types of photoelectric sensors that use photoelectric elements as sensitive elements, and they are widely used. Photoelectric devices include photocells, photomultiplier tubes, photoresistors, photodiodes, phototransistors, photocells, etc.


Product
Brand
Articles
Tools