NPN Transistors and PNP Transistors

Transistors - NPN & PNP - Basic Introduction
Catalog
I. Differences
The transistor is consisted of a three-part semiconductor forming two PN junctions, and its composition forms are PNP type and NPN type. Most of the germanium transistors are of PNP type, and most of the silicon transistors are of NPN type. Their structural principles are the same. The triode has three regions and three electrodes. Among them, the base region (a thin layer of semiconductor in the middle of the triode) leads to the base b; there are emitter regions leading to the emitter e and collector regions leading to the collector c on both sides. The PN junction between the transmitting area and the base area is called the transmitting junction, and the PN junction between the collecting area and the base area is called the collecting junction. On the circuit symbol, the PNP tube emitter arrow points inward, and the NPN tube emitter arrow points outward, indicating the current direction.
NPN and PNP transistors are mainly different because the direction of current is different from the positive and negative of voltage. To be professional, it is the "polarity" issue. NPN uses the B-E current (IB) to control the C-E current (IC), the E pole has the lowest potential, and usually, the C pole has the highest potential during normal amplification, namely VC>VB>VE. PNP uses the E-B current (IB) to control the E-C current (IC). The E pole has the highest potential, and usually, the C pole has the lowest potential during normal amplification, that is, VC<VB<VE.

The circuit configuration of NPN and PNP transistors
1. Difference in definitions
NPN transistor: It is consisted of two N-type semiconductors and one P-type semiconductor, with the P-type semiconductor in the middle and two N-type semiconductors on both sides. The triode is the most important device in electronic circuits, and its main function is the amplification and switching of current.
PNP transistor: A triode composed of two P-type semiconductors sandwiched between an N-type semiconductor, so it is called the PNP type triode. It can also be described as a transistor in which current flows from the emitter E.
2. Difference in circuit controlling
NPN: Use the current (IB) of B→E to control the current (IC) of C. The E pole has the lowest potential, and the C pole has the highest potential during normal amplification, that is, VC> VB> VE
PNP: Use E&B current (IB) to control E&C current (IC). The E pole has the highest potential, and the C pole has the lowest potential during normal amplification, that is, VC <VB <VE.
3. Other differences
The Output states of PNP and NPN sensors are different. They actually use the saturation and cut-off of the transistor to output two states, which are switch-type sensors. But the output signal is completely opposite, namely high level and low level. NPN output is low level 0, PNP output is a high level 1.
NPN transistors and PNP transistors are different in structure: NPN transistors consist of a p-type semiconductor sandwiched between two n-type semiconductors, while PNP transistors consist of n-type semiconductors sandwiched between two p-type semiconductors.
The majority of the carriers in NPN transistors are electrons, while most carriers in PNP transistors are electron holes.
When being used as switches, NPN transistors are faster to switch. When the triode is being used as a switch, it works in two states: cut-off and saturation. Generally, the conduction and disconnection of the transistor are controlled by controlling the base voltage Ub of the transistor.
II. Methods of distinguishing NPN transistors and PNP transistors
1. Identifying Base B
Set the digital multimeter to the diode position, connect the red test lead to a certain pin, and use the black test lead to touch the other two pins in turn. If the two displayed values are both less than 1V or the overflow symbol "1" is displayed, The connected pin that connects to the red test lead is base B. If in the two tests, one display value is less than 1V, another displays overflow symbol "1", it indicates that the pin connected to the red test lead is not base B. Then you should change to other pins and measure them again until base B is found.
Then, use the diode file of the digital multimeter. After identifying base B according to the above operation, connect the red test lead to base B, and touch the other two pins with the black test lead. If both display 0.500~0.800V, the tested tube is of NPN type; if the overflow symbol "1" is displayed both times, it means that the tested tube is of PNP type.
2. Identifying Base
Use a multimeter R×100 or R×1k to measure the forward and reverse resistance values between every two of the three electrodes of the tube. When the first test lead is connected to a certain electrode, and the second test lead successively touches the other two electrodes and the low resistance values are measured, the electrode connected to the first test lead is base b. At this time, pay attention to the polarity of the test lead of the multimeter. If the red test lead is connected to base b, and the measured resistance of the black test lead connected to the other two poles is small, then the tested tube can be determined to be a PNP transistor; If the black test lead is connected to the base electrode b and the red test lead is connected to the other two electrodes, and the measured value of resistance is small, then the tested transistor is an NPN transistor, such as 9013, 9014, 9018.
Notes
Use the diode gear of the digital multimeter to measure the forward voltage drop of the diode. At this time, the unit of reading is mV. For example, use this file to detect the forward voltage drop of a 2AP3 diode, and the display is "352", which means 352mV or 0.352V (this tube is a germanium tube). When detecting the IN4007 diode with this gear, the forward display is "509", which means that the forward voltage drop is 509mV or 0.509V (this tube is a silicon tube). The diode file of the digital multimeter can also be used to detect whether the circuit is short-circuited.
III. Application
There are PNP and NPN type of sensors (switch type), and they are divided into six categories:
1. NPN-NO (normally open type)
2. NPN-NC (normally closed type)
3. NPN-NC+NO (common type of normally open and normally closed)
4. PNP-NO (normally open type)
5. PNP-NC (normally closed type)
6. PNP-NC+NO (common type of normally open and normally closed)
PNP and NPN sensors generally have three lead wires, namely the power line VCC, the 0V line, and the OUT signal output line.
1. PNP type
When a signal is triggered, the signal output line OUT is connected to the power line VCC, and the PNP type of sensors is equivalent to a power line that outputs a high level.
For the PNP-NO type, when the signal is not triggered, the output line is suspended, that is, the VCC power line and the OUT line are disconnected. When the signal is triggered, the same voltage as the VCC power line is issued, that is, the OUT line is connected to the power line VCC, and a high-level VCC is output.
For the PNP-NC type, when the signal is not triggered, the same voltage as the VCC power line is sent, that is, the OUT line is connected to the power line VCC, and the high level VCC is output. When the signal is triggered, the output line is suspended, that is, the VCC power line is disconnected from the OUT line.
For the PNP-NC+NO type, there is actually an extra output line OUT, which can be selected according to needs.
2. NPN type
When a signal is triggered, the signal output line OUT is connected to the 0v line, and the PNP type of sensors are equivalent to outputting a low level of 0V.
For the NPN-NO type, when the signal is not triggered, the output line is floating, that is, the 0v line and the OUT line are disconnected. When the signal is triggered, the same voltage as 0V is issued, that is, the OUT line is connected to the 0V line, and the output is low level OV.
For the NPN-NC type, when the signal is not triggered, the same voltage as the 0V line is sent, that is, the OUT line is connected to the 0V line, and the low level 0V is output. When the signal is triggered, the output line is suspended, that is, the 0V line is disconnected from the OUT line.
The PNP-NC+NO type is similar to the NPN-NC+NO type. There is one more output line OUT, and two output lines with inverted signals. They need to be chosen according to needs.
What is a NPN transistor made of?
The npn transistor is made up of three semiconductor layers: one p-type semiconductor layer and two n-type semiconductor layers. The p-type semiconductor layer is sandwiched between two n-type semiconductor layers. The npn transistor has three terminals: emitter, base and collector.
How does an NPN transistor work?
The NPN transistor is designed to pass electrons from the emitter to the collector (so conventional current flows from collector to emitter). The emitter "emits" electrons into the base, which controls the number of electrons the emitter emits.
Can I use NPN instead of PNP?
NPN and PNP transistors are interchangeable if you remember one simple rule: A bipolar transistor is essentially two back-to-back diodes with the base being the common connection.
MOSFET vs IGBT: Structure, Switching Behavior, and How to ChooseUTMEL21 September 202624573With the rise of new energy in recent years, the market demand for MOSFETs and IGBTs is increasing steeply. Generally used as switching devices, they are widely used in electronic circuits. MOSFETs and IGBTs are relatively similar in appearance and characteristics parameters. So what is the difference between MOSFETs and IGBTs?
Read More
Introduction to FinFETUTMEL18 March 202131317The full name of FinFET is Fin Field-Effect Transistor. It is a new complementary metal oxide semiconductor transistor. The FinFET name is based on the similarity between the shape of the transistor and the fin.
Read More
What Is a MOSFET? Working Principle, Types, and Selection GuideUTMEL15 July 20268147This guide walks through how a MOSFET works, how it differs from an ordinary bipolar transistor, the four standard types, the roles it plays in a circuit, and a practical, parameter-driven way to choose one. Because this topic invites a lot of numbers, the discussion stays qualitative on purpose. Any exact voltage, resistance, current, or thermal figure belongs to the specific part you are using, so treat the manufacturer datasheet as the final word on every number.
Read More
NPN Transistors and PNP TransistorsUTMEL29 October 202010159NPN and PNP are two types of transistors. Transistors are semiconductor devices made of doped p-type and n-type junctions. This article mainly introduces the differences between this two kinds of transistors, the methods of distinguishing them, and the application of them.
Read More
An Overview of Bipolar TransistorsUTMEL27 August 20209421Bipolar Transistor, full name bipolar junction transistor(BJT), is an electronic device with three terminals, made of three parts of semiconductors with different levels of doping. The charge flow in the transistor is mainly due to the diffusion and drift movement of carriers at the PN junction.
Read More
Subscribe to Utmel !
7BB-35-3Murata Electronics
PKM22EPPH2001-B0Murata Electronics
BLM18PG330SN1DMurata Electronics
ENW-89847A3KFPanasonic Electronic Components
BLM03AX102SN1DMurata Electronics
TP88Fluke Electronics
BLM15AG121SN1DMurata Electronics
01050003HLittelfuse Inc.
DX0505/RD/12Bulgin
7BB-12-9Murata Electronics


Product
Brand
Articles
Tools