web counter

What Is an Electrical Connector? Types and Selection Checklist

Published: 01 August 2020 | Last Updated: 14 July 202610255
This guide walks through the parts that actually matter, the main connector families and how to tell them apart, the locking methods that keep a mate secure, the role of contact plating, and a practical checklist you can apply when selecting one. It closes with the failure modes worth knowing and a short set of frequently asked questions.
This video illustrates various types of electrical connectors or "Terminals" how they are used and how to connect them.

Electrical Connectors and WireTerminals

An electrical connector is the electromechanical interface that joins one part of a circuit to another so that signal or power can pass across a separable joint. Unlike a soldered or crimped permanent bond, a connector is built to mate and unmate, which means it has to stay electrically clean and mechanically stable through every cycle. That single requirement, holding a reliable contact across a separable interface, is what drives almost every design decision behind the thousands of connector styles on the market.


What a connector is and the parts that matter

Most connectors come down to four functional regions, and reading any datasheet becomes easier once you can name them.

The contacts are the conductive elements that actually touch when the connector is mated, usually a pin and a socket or a blade and a beam. They carry the current and create the electrical path, and their normal force and contact geometry decide how stable that path stays over time.

The housing, sometimes called the shell or body, holds the contacts in fixed positions, sets the spacing between them, and provides mechanical protection and polarization so the halves can only join one way. Housings are plastic for most signal and board-level parts and metal where shielding or ruggedness is needed.

The plating is the thin metal finish applied over the base contact metal. It is not cosmetic; it controls how easily the surface corrodes, how it wears across repeated mating, and how low and stable the contact resistance remains. Gold and tin finishes behave very differently, which is why plating gets its own section below.

The termination and strain relief is where the connector meets the rest of the world, whether that is a crimp barrel, a solder tail, an insulation-displacement slot, or a printed-circuit footprint. Strain relief keeps mechanical load off the contact joint so that pulling or flexing the cable does not slowly degrade the connection.

When any of these four regions is mismatched to the application, the connector tends to fail there first, so it helps to evaluate each one separately rather than judging a connector by its outward shape.

Exploded diagram of an electrical connector showing contacts, housing, plating, termination and strain relief..jpg

A reliable connector depends on more than its outer shape: contacts, housing, plating, termination and strain relief all affect long-term performance.

The main connector families and how to tell them apart

Connectors are easiest to navigate by family, because each family clusters around a typical use, a typical locking style, and a typical environment. The table below is a starting map rather than a rulebook, and exact ratings always belong to the specific series datasheet.

FamilyTypical useCommon locking styleTypical environmentHow to recognize it
CircularIndustrial, instrumentation, harsh-environment cablingThreaded, bayonet, or push-pullOutdoor, vibration-prone, splash to submersion depending on seriesRound shell, keyed insert, often metal
RectangularMulti-pin power and signal harnesses, panelsLatch, lever, or jackscrewIndustrial enclosures and machineryBoxy housing, high contact count, modular inserts
Board-to-boardStacking or mating two printed circuit boardsFriction fit or board-mounted latchInside enclosed assembliesLow-profile headers and receptacles facing each other
Wire-to-boardBringing a cable onto a printed circuit boardFriction lock or positive latchGeneral electronics, appliancesSmall housing on the cable, header on the board
PowerHigher-current distribution and battery linksThreaded, latch, or bolt-down lugPower systems, energy storage, motorsHeavier contacts, fewer poles, larger spacing
RF / coaxialAntennas, radio, high-frequency signal pathsThreaded, bayonet, or snap-onAnywhere a controlled impedance line is neededSingle central contact in a coaxial shell

The practical way to tell families apart is to look at contact count, contact size, and shell shape together. A round metal shell with a coupling nut is almost always circular; a single center pin inside a coaxial body points to RF; a wide flat housing with dozens of small contacts is usually rectangular or a board-level part. Once the family is clear, the search narrows to a manageable set of series.

Comparison chart of common electrical connector families including circular, rectangular, board-to-board, wire-to-board, powe.png

Connector families are easiest to recognize by shell shape, contact count, contact size, locking style and typical application.

Locking and retention methods

Retention is how a connector resists unmating from vibration, cable tension, or accidental pulls, and the right method depends on how often the joint is serviced and how rough the environment is.

  • Threaded coupling uses a screw nut to draw the halves together. It resists vibration well and is common on circular and RF connectors, at the cost of slower mating and the need for clearance to turn the nut.

  • Bayonet coupling locks with a quarter-turn against pins or slots. It mates faster than a thread and gives a tactile confirmation, which suits parts that are connected and disconnected often.

  • Push-pull latches on insertion and releases when an outer sleeve is pulled, allowing quick, blind, or densely packed mating without tools.

  • Latch or clip retention is the snap-fit found on most wire-to-board and rectangular signal connectors; it is light and cheap but relies on the plastic latch staying intact.

  • Jackscrews are the small screws on the flanges of many rectangular connectors that hold the housing firmly and prevent partial unmating under load.

A good rule is to match retention to the worst mechanical event the joint will see, not the average one. A latch that survives gentle handling on a bench can still walk loose under continuous machine vibration, where a threaded or jackscrew design would hold.

Contact plating: gold, tin, and why mixing them causes trouble

Plating choice is one of the most consequential and most overlooked parts of connector selection, because it sets the long-term stability of the contact joint.

Gold plating is favored for low-level signal contacts and high-reliability work. It does not form an insulating oxide, so the contact resistance stays low and stable even when the current is too small to break through a surface film. That stability is why gold tends to appear on critical signal lines, low-voltage logic, and connectors that must stay dependable over long service.

Tin plating is the cost-effective default for general-purpose and many power contacts. Tin does form a thin oxide, but a sufficiently high contact force and a small wiping motion during mating break through that film and establish a solid metal-to-metal joint. Tin works very well when the design provides that force and when the joint is not disturbed by constant micro-motion.

The trouble starts when dissimilar plating is mated across a pair, for example a tin contact against a gold contact. The mismatch can accelerate localized corrosion and unstable resistance over time, especially in the presence of micro-motion and humidity. The practical takeaway is to keep both halves of a mated pair on a compatible plating system and to follow the connector maker's stated finish for the application. The exact thickness and underplate that make a given finish suitable belong to the series datasheet, so treat plating as a qualitative selection rule and confirm the numbers against the manufacturer.

PlatingWhere it fits bestStrengthPractical limitation
GoldLow-level signals, logic, high-reliability linksNo insulating oxide, stable low resistanceHigher cost; thin flash finishes wear with many cycles
TinGeneral-purpose and many power contactsEconomical, reliable with adequate contact forceForms oxide; sensitive to micro-motion and fretting
Mixed gold-to-tin pairNot recommended as a deliberate choiceNoneEncourages localized corrosion and unstable contact

How to choose an electrical connector

A connector is chosen by working through a short set of questions in order. Each one narrows the field, and skipping one is the usual reason a connector that looked fine on paper fails in service.

Electrical connector selection flowchart based on current, voltage, mating cycles, plating, termination, sealing, environment.png

A good connector choice starts with electrical load, then checks durability, plating, termination, environment and retention before final datasheet confirmation.

  1. Current and voltage with headroom. Start from the highest steady and peak load the joint will carry, then choose a series rated comfortably above it rather than at the edge. The exact rating depends on contact size, wire gauge, and the number of energized contacts, so read it from the chosen series datasheet.

  2. Mating cycles for the duty. Estimate how many times the joint will be connected over its life. A connector mated once at assembly has very different needs from one a technician services weekly, and plating and contact design must match that count.

  3. Plating for the signal level. Use a stable finish such as gold for low-level signals and high-reliability paths, and a cost-effective finish such as tin where the contact force and use case support it. Keep both halves compatible.

  4. Wire and termination compatibility. Confirm the connector accepts your conductor size and your preferred termination, whether crimp, solder, insulation-displacement, or board mount, and that the tooling for that termination is available to you.

  5. Sealing and environment. Decide whether the joint faces dust, splash, immersion, vibration, or temperature extremes, and pick a sealed series with the appropriate ingress protection where needed. Verify the specific protection grade against the maker's documentation.

  6. Retention method. Match the locking style to the mechanical environment and service frequency, favoring threaded or jackscrew designs under heavy vibration and latches where quick, frequent mating matters.

Selection factorQuestion to answerWhere the exact figure lives
Current / voltageWhat are the peak and continuous loads, plus headroom?Series datasheet rating tables
Mating cyclesHow often is the joint connected over its life?Series durability specification
PlatingWhat signal level and reliability does the contact serve?Manufacturer plating options
TerminationWhat conductor and joining method is used?Connector wire-accommodation data
SealingWhat dust, water, or vibration is present?Series ingress-protection rating
RetentionWhat is the worst mechanical event expected?Series mechanical documentation

Working top to bottom gives a shortlist of series, after which the final pick is a matter of reading datasheets and confirming availability through normal sourcing channels.

Common connector problems

Most connector failures trace back to a handful of mechanisms, and recognizing them early saves a great deal of intermittent-fault chasing.

Fretting corrosion is the slow buildup of insulating debris when two contacts make tiny repeated movements against each other, typically from vibration or thermal cycling. It mostly affects tin surfaces and shows up as rising or erratic contact resistance. Stable retention, adequate contact force, and an appropriate finish all reduce it.

Exceeding the mating-cycle limit wears the plating thin until the base metal is exposed and corrodes. A connector chosen for a few assembly mates will degrade quickly if it is actually serviced often, so the duty estimate in the checklist matters.

Under-rated current and heating occurs when a connector runs near or above its rating; the contact resistance turns load current into heat, which raises resistance further and can damage the housing. Headroom on the current rating is the simple defense.

Poor termination covers under-crimped barrels, cold solder joints, and missing strain relief. These often pass an initial test and then fail after handling or vibration, which is why strain relief and correct tooling are part of selection rather than an afterthought.

Frequently asked questions

What is an electrical connector in simple terms?
It is a separable joint between two parts of a circuit that lets signal or power pass while still allowing the halves to be connected and disconnected. The whole design exists to keep that separable contact electrically reliable.

What are the main types of electrical connectors?
The common families are circular, rectangular, board-to-board, wire-to-board, power, and RF or coaxial. They differ mainly in shell shape, contact count and size, locking style, and the environment they are built for.

What are the basic parts of a connector?
A connector has contacts that carry the current, a housing that positions and protects them, a plating finish on the contacts, and a termination with strain relief that joins it to the cable or board.

How do I choose a connector for a power application?
Begin with the peak and continuous current and voltage, add headroom, choose a power-oriented series with suitably sized contacts and spacing, confirm the termination and wire size, and verify the rating in the series datasheet rather than assuming it from the shell size.

Why does plating matter so much, and can I mix gold and tin?
Plating sets how stable the contact resistance stays over time; gold suits low-level and high-reliability signals while tin suits cost-sensitive general and power use. Mating a gold contact against a tin contact is best avoided because the mismatch encourages corrosion and unstable contact.

Why do connectors fail intermittently?
Intermittent faults usually come from fretting corrosion, worn plating after too many mating cycles, contacts running hot from under-rated current, or a weak termination that loosens with handling. Each leaves the contact path unstable rather than fully open.

How many times can a connector be mated and unmated?
That depends entirely on the series and its plating, so there is no universal number; the durability figure is published in the manufacturer's specification for the specific part you select.

Sources and references

  • TE Connectivity connector products and documentation confirms how a major manufacturer organizes connector families and the contact, housing, and termination data it publishes per series, though its figures are specific to TE parts and should not be read as universal ratings.

  • Molex connector product resources supports the wire-to-board and board-to-board framing and shows the kind of mating and durability data a datasheet provides, while remaining limited to Molex's own catalog and conventions.

  • Amphenol connector offerings reinforces how circular, rectangular, and ruggedized families map to industrial and harsh environments, but it is a vendor source whose specifications describe its products rather than industry-wide minimums.

  • Hirose connector technical pages help confirm the compact board-level and signal connector descriptions used here, with the caveat that detailed plating and cycle figures live in each individual product datasheet rather than the overview.

  • IEC reference for the ingress-protection (IP) code is the standards body behind the IP sealing concept referenced in the environment step, though the formal grade for any connector must be taken from that connector's own rating rather than the standard alone.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Related Articles

  • High-speed Connectors Shortage Outlook 2026: Supply, Lead Times, and Sourcing Options
    High-speed Connectors Shortage Outlook 2026: Supply, Lead Times, and Sourcing Options
    UTMEL16 July 20261426

    Entering 2026, the electronics supply chain faces a bifurcated market. While standard connectors remain stable, high-speed interconnects, RF modules, and optical transceivers experience severe shortages driven by rapid AI infrastructure growth. To mitigate these bottlenecks, engineering and procurement teams must adopt proactive design-for-availability strategies, utilize multi-footprint layouts, and leverage alternative global sourcing channels like UTMEL to secure critical BOM components.

    Read More
  • Crimp Connector Failures: Strip Length, Tooling, and Pull-Test Checks
    Crimp Connector Failures: Strip Length, Tooling, and Pull-Test Checks
    UTMEL20 October 20261099

    This technical guide diagnoses wire crimp connector failures and outlines a complete shop-floor verification workflow. It covers matching conductor and insulation barrels to wire specifications, distinguishing strip-length errors from insertion-depth mistakes, and inspecting bellmouths and anvil impressions. Finally, it pairs non-destructive crimp height measurements with IPC/WHMA-A-620 tensile pull-force testing and a three-stage sampling protocol to prevent latent field failures.

    Read More
  • The Introduction to USB Type-C Pin Signal and PCB Layout
    The Introduction to USB Type-C Pin Signal and PCB Layout
    UTMEL03 December 202127933

    Hello everyone. Welcome to the new post today. USB Type-C is a smaller-volume USB interface standard than Type-A and Type-B. It can be used on a PC (master device) as well as external devices (slave devices, such as mobile phones).

    Read More
  • Everything You Need to Know about Connectors
    Everything You Need to Know about Connectors
    UTMEL07 September 20218914

    Electrical connectors, as key components for current or signal connections, are also an important part of the industrial system. Connectors can be as huge as airplanes and rockets or as small as mobile phones and televisions, forming bridges between circuits or other components and serving as electric current or signal links.

    Read More
  • Network Interface Card: Types, Functions and Buying Guide
    Network Interface Card: Types, Functions and Buying Guide
    UTMEL17 August 202111286

    Network Interface Card (NIC, also known as a network interface controller) is one of the most basic components in the local area network. It is the hardware device connecting the computer and the network. Whether it is a twisted pair connection, a coaxial cable connection, or an optical fiber connection, data communication must be realized with the help of a network interface card.

    Read More

Subscribe to Utmel !

Featured Parts More