A/D Converter: Basic Principle and Types

Published: 06 November 2020 | Last Updated: 06 November 202017871
An analog-to-digital converter, or A/D converter, or ADC for short, is usually an electronic component that converts an analog signal into a digital signal. A typical analog-to-digital converter converts an input voltage signal into an output digital signal.
This Tutorial describes basic characteristics of analog to digital converters and covers the most common errors.

Analog-to-Digital Converters (ADC) - Basics

Catalog

Ⅰ Introduction

Ⅱ Basic Principle

Ⅲ Types

 

1 Flash ADC

2 Successive approximation ADC (SAR ADC)

3 Dual Slope ADC

Ⅳ Technical parameters

 

Ⅰ Introduction

Analog signal refers to the information expressed by continuously changing physical quantities, such as temperature, humidity, pressure, length, current, voltage, etc. We usually call the analog signal a continuous signal, which can have infinitely many different values in a certain time range. The digital signal is a discrete and discontinuous signal in terms of values.

The circuit that converts an analog signal into a digital signal is called an analog-to-digital converter (referred to as A/D converter or ADC). Therefore, generally, there are 4 processes during A/D conversion: sampling, holding, and Quantization, and Coding. In the actual circuit, some of these processes are combined, for example, sampling, and holding. Quantizing and Encoding are often achieved simultaneously in the conversion process.

Now the software, radio, digital image acquisition are required to have high-speed A/D sampling to ensure effectiveness and accuracy, general measurement, and control systems also want to make a breakthrough in accuracy. The wave of digitization of mankind has driven the continuous transformation of the A/D converter, and the A/D converter is the pioneer of mankind to achieve digitalization. A/D converter has undergone many technological innovations since more than 30 years ago from flash ADC, SAR ADC, integrating ADC, and the newly developed sigma-delta ADC and flow line ADC in recent years. They have their own advantages and disadvantages and can meet the use of different applications.

Ⅱ Basic Principle

ADC (analog to digital converter) conversion process

ADC (analog to digital converter) conversion process

ADC conversion process

The basic conversion principle of the ADC is divided into four processes.

(1) Anti-aliasing, which can be understood as a low-pass filter.

(2) Sampling and holding circuit.

(3) Quantizing

(4) Encoding

Sampling and Holding

Sampling is the process of replacing the original signal that was continuous in time with a sequence of signal sample values at regular intervals, i.e., discretizing the analog signal in time. The results of the sampling are stored until the next sampling, and this process called holding.

Quantizing and Encoding

Quantizing is to convert the continuous amplitude of the analog signal into a finite number of discrete values with a certain interval using a finite number of amplitude values that approximate the original continuous changing amplitude value. Encoding is in accordance with certain rules, to represent the quantized value with binary numbers and then convert it into a binary or multi-valued digital signal stream. The digital signals thus obtained can be transmitted over digital lines such as cables, microwave trunks, satellite channels, etc.

This process of an analog signal converted into a digital signal through the ADC is called quantizing. Due to the quantization of the output digital signal is limited to a number of bits, the output digital signal and the analog signal you sample will have an error, known as quantization error. For an N-bit ADC, assuming that its full-scale voltage Vref, Vref ADC is divided into 2N intervals, the width of the interval with LSB ( (last significant bit) indicates LSB=Vref/2N.

For example, Vref=8V, ADC is 3 bits, LSB=1, so each interval is 1V. The resolution of this ADC is 1V.

000 means voltage 0 &le; V < 1

001 means voltage 1 &le; V < 2

010 means voltage 2 &le; V < 3

011 means voltage 3 &le; V < 4

100 means voltage 4 &le; V < 5

101 means voltage 5 &le; V < 6

110 represents voltage 6 &le; V < 7

111 represents voltage 7 &le; V < 8

 ADC output and error

ADC output and error

Ⅲ Types

There are many types of analog-to-digital converters, which can be divided into indirect ADCs and direct ADCs according to the different working principles.

Indirect ADC is to first convert the input analog voltage into time or frequency, and then convert these intermediate quantities into digital quantities, the commonly used indirect ADC is Dual Slope ADC whose intermediate quantity is the time.

1 Flash ADC 

As a result of the flash ADC using the magnitude of the parallel comparison, the output code is also generated in parallel at the same time, so the conversion speed is its outstanding advantage, while the conversion speed and the number of output code bits independent. Flash ADC&rsquo;s disadvantages are high cost and high power consumption. Because of the n-bit output ADC, which requires 2n resistors, (2n-1) comparators and D flip-flops, and a complex coding network, the number of its components increases geometrically with the number of bits. Therefore, this kind of ADC is suitable for situations where high speed and low resolution are required.

 Circuit diagram of flash ADC

Circuit diagram of flash ADC

2 Successive approximation ADC (SAR ADC)

The successive approximation ADC is another kind of direct ADC, which also generates a series of comparative voltages VR. Unlike the flash ADC, it generates comparative voltages one by one, and compares them with the input voltages one by one, and performs the analog-to-digital conversion in the way of gradual approximation. The successive approximation ADC is bit by bit comparison for each conversion, and needs (n + 1) beat pulse to complete, so it is slower than the conversion speed of the parallel comparison ADC, much faster than the double fractional product ADC, which belongs to the medium-speed ADC device. In addition, it needs to use much fewer components than the flash type, so it is one of the more widely used integrated ADC.

 Circuit diagram of successive approximation ADC

Circuit diagram of successive approximation ADC

3 Dual Slope ADC

Dual Slope ADC belongs to indirect ADC, which integrates the input sampling voltage and reference voltage twice to get a time interval proportional to the average value of the sampling voltage. At the same time, it counts the standard clock pulse (CP) with a counter in this time interval, and the counter output result is the corresponding digital quantity. The advantages of double-integral ADC are strong anti-interference ability, good stability, and can realize high-precision analog-to-digital conversion. The main disadvantage is the low conversion speed, so this type of converter is mostly used in instrumentation which requires high precision but not high conversion speed, such as multi-bit high-precision digital DC voltmeter.

Dual Slope ADC schematic diagram 

Dual Slope ADC schematic diagram

Ⅳ Technical parameters

1 Conversion accuracy

(1) Resolution

The resolution of an A/D converter is expressed in bits of the output binary (or decimal) number. It indicates the ability of the A/D converter to distinguish between input signals. Theoretically speaking, the n-bit output of the A/D converter can distinguish between 2n different levels of input analog voltage, and the minimum value that can distinguish between input voltages is 1/2n of the full-scale input. For example, if the output of the A/D converter is 8 binary digits and the maximum value of the input signal is 5V, then the converter should be able to distinguish the minimum voltage of the input signal is 19.53mV.

(2) Conversion error

The conversion error is usually given in the form of the maximum value of the output error. It represents the difference between the actual digital output of the A/D converter and the theoretical output of digital quantity. It is commonly expressed as a multiple of the lowest effective bit. For example, the relative error is given as no greater than ±LSB/2, which indicates that the error between the actual output digital quantity and the theoretically desirable output digital quantity is less than half a word of the lowest effective bit.

2 Conversion time

The conversion time is the time it takes for an A/D converter to convert the control signal from the time it arrives at the time it gets a stable digital signal at the output.

The conversion speed varies considerably between different types of converters. Parallel comparative A/D converters have the highest conversion speed. Single-chip integrated A/D converters with 8-bit binary output have a conversion time of less than 50ns, followed by successive approximation A/D converters, most of which have a conversion time of less than 10-50&mu;s. Indirect A/D converters are the slowest, such as dual slope A/D converters with conversion times mostly in the tens of milliseconds to hundreds of milliseconds. In practical applications, the selection of A/D converters should be considered from the total number of bits of system data, accuracy requirements, the range of the input analog signal, and the polarity of the input signal.

3 Selection of ADC

Sampling accuracy - i.e. resolution, typically 8, 10, 12, 16 bits, etc..

Conversion time - i.e., the time required for each sample, characterizing the ADC's conversion speed, which is related to the ADC's clock frequency, sampling period, and conversion period.

Data output methods - e.g. parallel output, serial output.

ADC types - as mentioned above, there are many types of ADCs, and different types have different performance limits.

Operating voltage - attention needs to be paid to the operating voltage range of the ADC, the ability to measure negative voltages directly, etc.

Chip packaging - whether the chip package meets product design requirements.

Value for money - controlling costs.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What does an A D converter do?

In electronics, an analog-to-digital converter (ADC, A/D, or A-to-D) is a system that converts an analog signal, such as a sound picked up by a microphone or light entering a digital camera, into a digital signal.

2.What is the main function of a D or ADC converter?

The main purpose of the A/D converters within a data acquisition system is to convert conditioned analog signals into a stream of digital data so that the data acquisition system can process them for display, storage, and analysis.

3.What is the difference between ADC and DAC?

A DAC essentially does the opposite of an ADC, converting digital inputs to analog output signals. The analog signals are generated at the sampling frequency applied to the DAC clock. As with an ADC, the key spectral-performance parameters for a DAC include SNR and SFDR.

4.What is the advantage of using Flash Type A D converter?

Flash type ADC has the advantage of high speed as the conversion takes place simultaneously rather than sequentially. The typical conversion time is 100nanosecond or less. Explanation: The number of comparators required almost doubles for each added bit.

5.Why we use ADC & DAC?

Analog to Digital Converter (ADC) and Digital to Analog Converter (DAC) are very important components in electronic equipment. Since most real-world signals are analog, these two converting interfaces are necessary to allow digital electronic equipment to process the analog signals.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242212

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 2025798

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • A Comprehensive Guide to FPGA Development Boards
    A Comprehensive Guide to FPGA Development Boards
    UTMEL11 September 2025659

    This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.

    Read More
  • The Ultimate Guide to Microchip MCUs: From Selection to Real-World Applications
    The Ultimate Guide to Microchip MCUs: From Selection to Real-World Applications
    UTMEL13 September 2025295

    Are you an aspiring electronics enthusiast, a seasoned engineer, or a hobbyist looking to bring your next project to life? If so, you've likely encountered the term Microchip MCU. But what exactly is a Microchip MCU, and how do you choose the right one from their vast portfolio? This comprehensive guide will walk you through everything you need to know about Microchip's powerful microcontrollers, from selection and programming to real-world applications.

    Read More
  • Lattice FPGA: The Ultimate Guide to Low-Power, Small Form Factor Solutions
    Lattice FPGA: The Ultimate Guide to Low-Power, Small Form Factor Solutions
    UTMEL19 September 2025191

    Comprehensive review of Lattice FPGAs. Discover why their low-power, small-size, and cost-effective solutions are dominating the edge AI, IoT, and automotive markets. Compare Lattice vs. Xilinx and Intel to make the right choice.

    Read More