web counter

Results: ( 333,019 )

Box & Enclosure Products

Box & Enclosure Products definition

Box and enclosure products are used for physical containment, organization and protection of electronic devices, computer systems, small items, instruments, test equipment, and similar items. Examples include organizing drawers for resistor assortments, enclosures for custom guitar pedals, airline-resistant transport cases, 19- and 21-inch equipment racks, and more. Included within the category in addition to the enclosures themselves are a variety of related products commonly used with them, such as handles, locks, mounting rails, fan trays, interconnect panels, and others.

What types of enclosures are there?

Certain types of enclosures are specifically designed for a product in particular (such as Arduino cases for Arduino boards, or Raspberry Pi cases), while general purpose enclosures offer more versatility in terms of applications and normally feature a simpler structure. They are most commonly made of plastic, metal or PVC and they may feature doors, which can be transparent to reveal the contents. Depending on their application, size and structure, enclosures can be: Floor standing, Hand Held and Wall Mounted.

Floor Standing

These freestanding structures can house several racks to store equipment. They can have one or two doors depending on their dimensions, and they’re perfect to store large electrical components.

Hand held

Hand Held Enclosures are the perfect solution on the go when carrying small devices, such as batteries and PCBs, or tools like screwdrivers. Their modular structure makes it easy to store and protect different kinds of electrical components in the same box.

Wall mounted

Wall Mounted Enclosures are also called wall boxes, they come in handy when the space for storage is too narrow for standing enclosures.

What do you need for enclosure mounting and installation?

Wall mounting enclosures are being increasingly used to provide the double function of saving space and protecting components at the same time. Several accessories and fittings are available in our range to make the job easier: to name some, mounting rails and plates, brackets, screws, in addition to a choice of screwdrivers and drills to complete the installation in the safest way possible. We offer enclosures and accessories from the top brands worldwide, such as ABB, Schneider Electric, Rittal and Fibox, as well as RS Pro.

What are IP Ratings for enclosures?

Most enclosures feature an IP (Ingress Protection) rating which is an international standard used as a measure of the protection offered by the structure against foreign bodies and moisture. IP ratings are made of two digits which indicate the degree of protection on two progressive scales: the first digit indicates the effectiveness of isolation against intrusive bodies, whereas the second digit indicates protection against several moisture agents such as sprays, condensation or strong water jets.

Related to the manufacturers

Recommended Manufacturers

3MAavidABB Embedded PowerAdafruitAdapteva, Inc.Advantech