web counter

Results: ( 181,083 )

Thermal Management

Thermal Management definition

Here at Utmel Electronic, we have a wide range of HVAC and thermal management solutions in stock to suit your needs.

The fan and thermal management category includes products and materials used to facilitate heat transfer and/or air movement, and thermal accessories related to such products. Along with AC and DC fans and heat sinks, thermally-conductive adhesives, thermal interface products, heat pipes, and thermoelectric (peltier) modules are included. In context of electronic devices and systems, such products are commonly used to maintain the temperatures of power-dissipationg components within acceptable operating limits.

Thermal Management

Thermal management uses passive or active methods to keep machinery, equipment, electronics, batteries and other devices within a specified temperature range. Passive methods simply attach to the device or machine and work through natural radiation, convection or conduction. These include heat sinks, cold plates and heat pipes. Active methods use another device to speed up the cooling such as a fan or pump.

Thermal management is a key element within electronic design and keeping components cool is a key consideration. Over-heating is one of the primary causes of malfunction of modern devices. For example, modern computers will generally use both active and passive cooling methods with a heat sink and fan on the processor to provide the necessary cooling.

DC Brushless Fans

DC Brushless motors (BLDC motors) with a cross pattern arrangement of four permanent magnets positioned on the sides of the rotor are used in brushless DC fans. BLDC motors, unlike brushed DC motors, do not require a commutator or brushes to function.

A strong BLDC motor, shaft, and fan blades make up the DC Brushless Cooling Fan. These fans are long-lasting, dependable, and energy-efficient. They don't cause any sparks in the circuit and are completely silent.

DC Brushless fans achieve their full capability quickly due to the strong initial torque provided by DC motors. Increasing or reducing the voltage input is all it takes to adjust their speed. Brushless DC fans may be divided into two types: Sensor-driven BLDC fans and sensor-less BLDC fans are available.

Thermal Accessories

Thermal Accessories can help you attach your thermal solution with hardware, increase heat dispersion, transmission, or dissipation, or provide electrical insulation to improve device safety.

What is a Temperature Heat Sink?

Heat Sink, namely heatsink, is able to transfer the heat from the high temperature electrical component like transistor to the low temperature electronic parts such as oil, air or water through conduction and convection. And the active heat sink and the passive heat sink are the two types of heat sinks. And if you would like to calculate the the junction temperature of power components, here is a online calculation tool (Heat Sink Temperature Calculator) for you.

Related to the manufacturers

Recommended Manufacturers

3G Shielding Specialties3MAavidABB Embedded PowerAdafruitAdvanced Thermal Solutions, Inc.
Frequently Asked Questions

Is heat sink better than fan?

The fan maintains a consistent stream of air for the heatsink to distribute the heat to while the heatsink takes heat away from the CPU. However, choosing a heatsink and fan entails more than just shopping for a good deal or one that looks cool.

How do brushless DC fans work?

When an electric current is applied to the armature of a brushed DC motor, the rotor rotates 180 degrees. Permanent magnets are on the rotor while electromagnets are on the stator in brushless DC motors. The electromagnets in the stator are then charged by a computer to rotate the rotor 360 degrees.

How Do Thermoelectric Coolers (TECs) Work?

The Peltier effect governs the operation of thermoelectric coolers. By transmitting heat between two electrical connections, the effect causes a temperature differential. To generate an electric current, a voltage is supplied across linked conductors. Heat is evacuated from one junction and cooling occurs when current travels across the junctions of the two conductors. At the other end of the circuit, heat is deposited.

The Peltier effect is most commonly used for cooling. The Peltier effect, on the other hand, may be utilized to heat or regulate temperature. A DC voltage is necessary in all cases.

What is an example of thermoelectric?

Biomass cooking stoves, camping stoves, and barbecues are all examples of thermoelectric generator uses. Sun thermal applications focus solar energy onto the hot side of a thermoelectric generator at extremely high temperatures. The heat sink is made of ambient air.

What are Peltier modules?

A Peltier module (thermoelectric module) is a thermal control module that can both warm and cool. It is possible to adjust the surface temperature and maintain it at the target temperature by running an electric current through the module.

What are Peltier modules used for?

Peltier modules are electrical devices that use controlled heating and cooling to chill items to below ambient temperatures or to keep objects at a specified temperature.

What is thermoelectric cooler module?

A thermoelectric (TE) module, also known as a thermoelectric cooler or Peltier cooler, is an electrical component made of semiconductors that acts as a miniature heat pump, transporting heat from one side of the device to the other.

What does a thermoelectric module do?

A Peltier module (thermoelectric module) is a thermal control module that can both warm and cool. It is possible to adjust the surface temperature and maintain it at the target temperature by running an electric current through the module.