Sort by
Supercapacitors Explained: How EDLC, Pseudo, and Hybrid Capacitors Store Power14 July 2026
Supercapacitors, also known as electrochemical capacitors, electric double-layer capacitors, gold capacitors, and farad capacitors, are developed between the 1970s and 1980s, which is an electrochemical element that uses polarized electrolytes to store energy. The supercapacitor is different from the traditional chemical power supply. It is a power supply with special performance between the traditional capacitor and battery, which mainly relies on the electric double layer and redox pseudo capacitor charge to store electrical energy. However, no chemical reaction occurs during the energy storage process. This energy storage process is reversible, for which supercapacitors can be repeatedly charged and discharged hundreds of thousands of times.
An Overview of JFET19 August 2020
JFET is a Junction field-effect transistor. Regular transistor is a current-controlled device that requires biasing power, while JFET is a voltage-controlled device. The JFET is an active electronic component that is one of the electronics industry's workhorses that offers a reasonable compromise between cost and efficiency.
An Overview of Digital Signal Processor31 October 2025
A digital signal processor (DSP) is a processor composed of large-scale integrated circuit chips to complete digital signal processing tasks. Digital signal processing is the theory and technology of representing and digitally processing signals. Digital signal processing and analog signal processing are a subset of signal processing.
Basic Introduction to the Types of Capacitors16 October 2025
A variety of capacitors are used in the manufacture of electronic devices, and they play different roles in the circuit. There are many types of capacitors, such as fixed capacitors, variable capacitors, and trimmer capacitors, and fixed capacitors can be divided into ceramics, mica, paper, film, and electrolytic capacitors according to the different dielectric.
Tunnel Diode: Definition, Features and Tunneling Process25 August 2020
Tunnel diode, also known as Ezaki diode, is a crystal diode with tunnel effect current as the main current component. The tunnel diode is a semiconductor diode made of a mixture of gallium arsenide (GaAs) and gallium antimonide (GaSb).
Capacitor Signs: Decoding Symbols & Markings14 August 2025
Capacitor signs, symbols, and markings with our ultimate guide. Learn to identify polarity, decode value codes, and avoid common mistakes for safe and effective circuit work.
Toggle Switches: Features, Types and Applications23 January 2021
Toggle switch adopts integrated circuit technology and SMT appearance device technology to manufacture a new generation of photoelectric switch devices. It has intelligent functions such as delay, expansion, external synchronization, anti-interference, high reliability, stable working area, and self-diagnosis. This novel photoelectric switch is an active photoelectric detection system electronic switch that uses pulse modulation. The cold light source used is infrared light, red light, green light and blue light, etc., which can be quickly and without contact and damage Control the state and action of various solid, liquid, transparent, black, soft, smoke and other substances.
Lattice FPGA vs Competitors A Comprehensive Comparison09 June 2025
Compare Lattice FPGA with competitors like Xilinx and Intel. Discover its low power, compact size, and cost-effective solutions for IoT and automation.
What is a Capacitive Sensor?31 October 2025
Capacitive sensors use various types of capacitors as sensing elements. It is a conversion device that converts the measured physical or mechanical quantities into changes in capacitance which is actually a capacitor with variable parameters. Capacitive sensors are widely used for measurement of displacement, angle, vibration, speed, pressure, composition analysis, medium characteristics, etc.
What is AMOLED?25 April 2021
AMOLED is an active-matrix organic light-emitting diode. AMOLED is a display technology for mobile devices, digital cameras, media players, and television. It uses active matrices to address pixels and uses a special type of film technology, wherein the organic compound forms an electroluminescent material.
What are Types and Application of Gas Sensors?18 November 2025
The gas sensor is the core of the gas detection system and is usually installed in the detection head. Essentially, a gas sensor is a converter that converts a certain gas volume fraction into a corresponding electrical signal. The probe uses the gas sensor to adjust the gas sample, which usually includes filtering out impurities and interfering gases, drying or refrigeration treatment, sample pump, and even chemical treatment of the sample, so that the chemical sensor can make faster measurements. In the following, we’ll mainly discuss the properties, typical types and application fields of gas sensors.
Introduction to Mass Air Flow Sensor15 September 2020
Mass air flow sensor is one of the important sensors of EFI engines. It converts the inhaled air flow into an electric signal and sends it to the electronic control unit (ECU). As one of the basic signals for determining fuel injection, it is a sensor that measures the air flow into the engine.


Product
Brand
Articles
Tools