Sort by
What Is a Shunt (Resistor)? How Current Sensing Works and How to Choose17 July 2026
A shunt is a measuring element that uses voltage to indicate current. It is made according to the principle of generating voltage at both ends of the resistor when DC current passes through the resistor. It is connected in parallel with the current circuit of measuring instruments to expand its measurement range; or An element on which voltage is measured, thereby indirectly measuring current.
What is An Optoisolator?09 January 2021
An optoisolator, also called optical coupler, optocoupler, and opto-isolator, is a device that encapsulates the infrared light-emitting device, the infrared light receiving device, and the signal processing circuit in the same tube socket.
Function and Application of Laser Sensors28 October 2025
Laser sensors are sensors that use laser technology for measurement. It consists of laser, laser detector and measuring circuit. The laser sensor is a new type of measuring instrument.
What is a Transformer: Definition, Principle and Applications03 November 2021
Hi, fellas. I am Rose. Today I will introduce the transformer to you. The device that increases or decreases the voltage in an AC circuit is known as a transformer. The transformer is an AC voltage converter that works on the mutual inductance concept.
ARM, FPGA, DSP and CPLD: Connection and Difference15 March 2022
Hello everyone, I am Rose. Welcome to the new post today. I am sure you know what is ARM, FPGA, DSP and CPLD. But do you know their connection and difference? Let me introduce to you.
What is UWB (Ultra-wideband)?04 June 2021
UWB (Ultra-wideband) technology is a wireless carrier communication technology, which does not use a sinusoidal carrier, but uses the non-sinusoidal narrow pulse of the nanosecond level, so the spectrum range is wide.
What is Cat 7 Cable?04 January 2022
Cat 7 cable is the latest twisted pair in the ISO/IEC 11801 Cat 7 / Class F standard, which is designed to accommodate the application and development of 10 Gigabit Ethernet technology.
What is a Semiconductor?22 October 2025
Semiconductor refers to a material whose conductivity is between a conductor and an insulator at room temperature. Semiconductors are used in integrated circuits, consumer electronics, communication systems, photovoltaic power generation, lighting applications, and high-power power conversion.
Comparison of Advantages and Disadvantages of Common Switch Mode Power Supply(SMPS)21 January 2022
This article mainly describes the characteristics and advantages and disadvantages of common switching power supply topologies. Common topologies include Buck Buck, Boost Boost, Buck-Boost Buck-Boost, Flyback Flyback, Forward Forward, Two-Transistor Forward, etc.
Japan's Three-Stage Strategy to Revive the Semiconductor Industry01 April 2022
Continuing chip shortages and the high risk of disruptions in the semiconductor supply chain remain major challenges for governments around the world, and Japan is under tremendous pressure to find solutions to revitalize the semiconductor industry. In recent years, the global market share of Japanese semiconductor companies has been declining, from 50.3% in 1988 to less than 10%. To develop an effective industry revitalization strategy, the Japanese government and domestic semiconductor companies are now reflecting on why Japan's semiconductor industry has been losing ground to foreign competitors in the global market.
What is Graphics Processing Unit (GPU)?18 October 2021
Hello everyone, I am Rose. Welcome back to the new post today. The graphics processing unit (GPU), also known as the visual processor, display core, or display chip, is a type of microprocessor that specializes in image processing on personal computers, workstations, gaming consoles, and mobile devices (such as tablets and smartphones). After reading this article, you will have a clear understanding of GPU.
What are Fiber Optic Patch Cables?11 February 2022
Hello everyone, I am Rose. Today I will introduce fiber optic patch cables to you. Optical fiber communication, as an emerging technology, has become one of the main pillars of modern communication and plays a critical role in modern telecommunication networks, thanks to the rapid growth of traffic data.


Product
Brand
Articles
Tools