Sort by
4680 Battery - Upgrade of Battery Technology17 December 2021
This paper introduces the 4680 battery introduced by Tesla, mainly including its structure, characteristics, and process principle.
What is a Wireless Network Adapter?01 June 2021
The wireless network adapter is actually a terminal wireless network device, which needs to be used for Internet access through the wireless connection network under the wireless coverage of the wireless local area network. With a wireless network adapter, it also needs a wireless network that can be connected, so it needs to be used with a wireless router or wireless AP.
What is PLL(Phase Locked Loop)?29 November 2021
PLL (Phase Locked Loop): It is a phase-locked loop or a phase-locked loop, which is used to unify and integrate clock signals to make high-frequency devices work normally, such as memory access data. PLL is used for feedback technology in oscillators. For many electronic devices to work normally, the external input signal is usually synchronized with the internal oscillating signal. Ordinary crystal oscillators cannot achieve very high frequencies due to process and cost reasons. When high frequency applications are required, the corresponding device VCO can be converted to high frequency, but it is not stable, so the phase-locked loop can be used. Realize a stable and high-frequency clock signal.
The Different Types of Circuit Breakers and Their Applications11 April 2023
Electricity, electrical equipment, electronics and powered devices have become an integral part of modern society. From getting a cup of coffee from the coffee machine to running an entire plant, electricity is used. Electricity can thus be defined as an energy that enables us to power many devices and systems that we heavily depend on in the day to day lives.
What Size Wire for a 60 Amp Breaker? The Complete NEC Guide22 May 2026
Selecting the right wire size for a 60-amp breaker requires evaluating conductor materials, insulation, and distance. While 6 AWG copper THHN or 4 AWG aluminum in conduit is standard, NM-B Romex limits 6 AWG to 55 amps, requiring 4 AWG copper. Additionally, installers must account for continuous load limits, ground wire sizing, and voltage drop over long runs.
Lattice FPGA: The Ultimate Guide to Low-Power, Small Form Factor Solutions19 September 2025
Comprehensive review of Lattice FPGAs. Discover why their low-power, small-size, and cost-effective solutions are dominating the edge AI, IoT, and automotive markets. Compare Lattice vs. Xilinx and Intel to make the right choice.
Amorphous Silicon Solar Cells: Features, Structure and Applications22 August 2022
Hello everyone, I am Rose. Welcome to the new post today. Today I will introduce Amorphous Silicon Solar Cells to you. Including its definition, structures, characteristics and applications.
Commonly Used Circuit Protection Components: How to Match the Right Device to Each Threat14 July 2026
This guide organizes the commonly used components by threat and lays out a selection path for your own input stage. Exact numbers such as clamping voltage, interrupting current, and trip points always belong to the manufacturer datasheet, and each section points you there.
Utmel Attends the PCIM Europe 2023– Excelling in Power Electronics20 June 2023
Utmel Electronics, a professional independent distributor of electronic components, recently announced that it will attend PCIM Europe.
Aluminum Electrolytic Capacitor Basis: Definition, Characteristics and Life03 March 2022
Hello everyone, I am Rose. Welcome to the new post today. Aluminum electrolytic capacitors are made of an aluminum cylinder as the negative electrode, which is filled with liquid electrolyte and inserted into a bent aluminum strip as the positive electrode.
What is a USB Type-C Connector?28 October 2025
The USB connector has three interfaces with different appearances, namely Type-A, Type-B, and Type-C. A Type-C connector has a much smaller volume than Type-A and Type-B and is the latest USB interface appearance standard. Also, Type-C is an interface type that can be applied to both PCs (master devices) and external devices (slave devices, such as mobile phones).
Hydrogen Fuel Cell: Features, Working and Applications21 June 2021
A hydrogen fuel cell is a power generation device that directly converts the chemical energy of hydrogen and oxygen into electrical energy. The basic principle is the reverse reaction of electrolyzed water. Hydrogen and oxygen are supplied to the anode and the cathode respectively. After the hydrogen diffuses out through the anode and reacts with the electrolyte, electrons are released to the cathode through an external load.


Product
Brand
Articles
Tools