web counter

Analog-to-Digital Converters (ADCs): Decrypting Resolutions and Sampling Rates

Published: 24 February 2022 | Last Updated: 24 February 20225636
Resolution and sample rate are two important factors to consider when choosing an analog-to-digital converter (ADC). To fully understand these, concepts such as quantization and the Nyquist criterion must be understood to some extent.
This video introduces analog-to-digital converters and discusses how different sampling rate factors affect accuracy. It also highlights the Nyquist frequency.

ADC and Sampling

Topics covered in this article:
Ⅰ. Quantisation
Ⅱ. Quantization Error
Ⅲ. Sampling
Ⅳ. The Nyquist Criterion and Shannon’s Theorem


Resolution and sample rate are perhaps the two most significant factors to consider when choosing an analog-to-digital converter  (ADC). Before making a decision, these two factors should be carefully weighed. They'll have an impact on everything from the price to the underlying architecture of the required analog-to-digital converter during the selection process. A reasonable comprehension of these features is required in order to appropriately identify the correct resolution and sampling rate for a given application.

Some mathematical definitions of terminology relevant to analog-to-digital conversion are provided here. Although math is vital, the concepts it depicts are far more so. You will be able to limit the number of  ADC s that fit your application and make a much easier selection if you can live with the arithmetic and comprehend the principles offered.

 

 Ⅰ. Quantisation

A continuous signal (voltage or current) is converted into a sequence of numbers represented by discrete logic levels via an analog-to-digital converter,  The process of transforming a large number of values into a smaller or discrete set of values is known as quantization. An  ADC can be represented mathematically as quantizing a large-domain function to yield a smaller-domain function.

Analog to digital conversion process.png

Analog to Digital Conversion Process

The analog-to-digital conversion process is mathematically described by the equation above. The input voltage Vin is described as a series of bits b N-1...b 0. The number of quantization levels is represented by 2 N in this formula. More quantization levels, on the surface, appear to result in a more accurate digital reproduction of the original analog signal. Because each quantization level reflects a lower amplitude range, if we can represent the signal with 1024 quantization levels instead of 256, we can improve the ADC's accuracy.

The greatest input voltage that can be effectively translated to an accurate digital representation is represented by Vref. As a result, it's critical that V ref be more than or equal to V in's maximum value. However, take in mind that a value substantially higher than V will result in fewer quantization levels representing the original signal. If we knew our signal would never rise over 2.4 V, for example, having a voltage reference of 5 V would be inefficient because we would be utilizing more than half of the quantization level.

Quansisation of a continuous signal.png

Quantization of a Continuous Signal

 

Ⅱ. Quantization Error

The disparity between the original signal and the discrete representation of the signal is referred to as quantization error.

Quantum description.png

Quantum description

A quantum can be defined as shown above, with A denoting amplitude and the signal spanning A to -A. The number N denotes the number of bits that the signal is quantized to.

It's time to look at what quantization means for ADCs now that we've looked at quantization. We'll need to do more math to do this. The quantization error is described by the equation below.

Quantisation Error.png

Quantization Error

As a result, the quantization error's power can be characterized as follows.

Definition of power in quantization error.png

Definition of Power in Quantization Error

Quantisation of a shine wave.png

Quantization of a Shine Wave

Take a look at the signal in the illustration above. The following equation can be used to calculate the signal's power.

Power Definition of Signal.png

Power Definition of Signal

As a result, the  Signal Quantization Noise Ratio  (SQNR) can be expressed in decibels. This equation shows that having more quantization levels in an ADC enhances the SQNR ratio.

Definition of SQNR.png

Definition of SQNR

The signal-to-noise ratio (SNR) of an ideal ADC will equal the SQNR value. Other sources of noise are unfortunately related to the analog-to-digital conversion process. Nonetheless, careful examination and consideration of the analog signal to identify the SQNR required for your application will help with the decision. The resolution of an analog-to-digital converter is the number of bits of quantization.

Feature 1: Resolution  - The number of bits of quantization in the ADC.

In most cases, it is preferable to have the highest resolution available. Other factors, such as resources and cost in the digital arena, often limit its resolution. As a result, determining the minimum resolution required for your application is critical.

 

Ⅲ. Sampling

Signals in the continuous-time domain must be quantized not only in amplitude but also in time. Consider the following series of pulses, where Ts is the sample period.

Ts is defined as sampling time period.png

Ts is Defined as Sampling Time Period

impulse train and analog signal.png

Impulse Train and Analog Signal

The sampled signal y(t) can be formally characterized as stated in the equation below.

Sampled Signal Definition.png

Sampled Signal Definition

This produces the pulse train seen in the image below for the pulse train and analog signal in the image above.

sampled data.png

Sampled Data

When looking at signals in the frequency domain, the  Dirac delta function is useful for mathematically explaining the concept of sampling. However, it's important to note that these characteristics don't exist in real-world devices. Instead, virtually rectangular pulses take their place.

 

Ⅳ. The Nyquist Criterion and Shannon’s Theorem

The frequency-domain of the analog signal must be examined in order to identify the desired sampling rate. This, too, necessitates some math knowledge. The Fourier transform of w(t) can be calculated using the equation below.

Fourier transform definition of W(t).png

Fourier Transform Definition of W(t)

This equation essentially states that the  Dirac delta function is repeated at each harmonic of its frequency Fs. Let's take a look at an analog signal with a spectrum like the one below. The spectrum of the sampled signal Y(f) turns out to be the convolution of X(f) and W. (f).

Two sided frequency spectrum of X(f).png

Two Sided Frequency Spectrum of X(f)

This signifies that the signal repeats for all multiples of the sampling frequency after sampling. If the sampling frequency is not high enough, the spectrum pictures of the signal will overlap, as seen in the diagram below. The Nyquist rate is defined as the minimum frequency equal to twice the bandwidth of the signal to be sampled.

minimum spectrum.png

Minimum Spectrum

Spectrum of signal sampled at different Hz.png

Spectrum of Signal Sampled at Different Hz

As a result of the Nyquist criterion, it is evident that we must know the spectrum content of the analog signal in order to accurately specify the correct ADC for an application.

Filtering the analog signal before digitization is one approach to ensure that the Nyquist requirement is met.

Looking at the above image again, it's clear that the spectrum after filtering using a proper filter is identical to that of the original signal. There is no data loss, and the original signal can be recovered. Shannon's theorem is the name for this.

Feature 2: Sampling  Rate - The sampling frequency of the analog signal.

When determining the ADC necessary for an application, the sampling rate and resolution of the ADC must be carefully examined. In order to accurately digitize an analog signal, a compromise between sample rate and resolution is frequently required. It's crucial to determine the sample rate and resolution you want before choosing an ADC. In order to appropriately specify the needed resolution and sample rate, careful examination of analog signals and the digital resources required to process digital data is required.

 


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. What is the difference between resolution and accuracy of an analog to digital converter?

"Precision" is used to describe how accurate a physical quantity is, while "resolution" is used to describe scale division.

2. What is the resolution of an analog-to-digital converter?

Resolution refers to the ability of the ADC to resolve the smallest signal quantized.
Resolution is expressed in binary digits.

3. How to interpret the unit SPS of the sampling rate in the ADC?

Sps is the sampling rate, which is the number of sampling points per second, and Sp represents the number of sampling points. When sampling, 1 Sample is one cycle of sampling.
Therefore, the two units should be equal in value, the difference is that the frequency Hz can be a decimal and the sampling rate S/s must be an integer.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242876

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20255582

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    UTMEL30 April 20261867

    A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.

    Read More
  • AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    UTMEL15 May 20261005

    The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.

    Read More
  • The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    UTMEL29 May 2026799

    This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.

    Read More

Subscribe to Utmel !

Featured Parts More