Graphics Card Explained: Classification, Working and Structure

Published: 27 May 2021 | Last Updated: 27 May 202111949
A Graphics card (Video card, Display card, Video adapter) is one of the basic components of personal computers. It converts the display information required by the computer system to drive the display, which is an important component that connects the monitor and the PC motherboard, and is one of the important equipment of "human-machine". Its built-in parallel computing capability is also used for deep learning and other operations.
Use a computer? Game on a PC? Ever wonder how those graphics get so pretty? Let's go inside your high-end graphics card with this animation.

What's Inside Your GRAPHICS CARD?

Catalog

 Overview
 Graphics card working principle and mode
 Graphics card classification 1.Integrated graphics
2.Dedicated graphics
3.Core graphics
 Graphics card structure
 Bus interface types


Ⅰ Overview

The graphics card is responsible for the task of outputting and displaying graphics. For those who like to play games and engage in professional graphics design, the video card is very important. The display chips of mainstream graphics cards are mainly manufactured by NVIDIA and AMD. Graphics cards that use NVIDIA display chips are usually called N cards, and those that use AMD display chips are called A cards. Computers with higher configurations all contain graphics card computing cores. In scientific computing, the graphics card is called a display accelerator card.

The video chipset is the main processing unit of the graphics card, so it is also called the Graphics Processing Unit (GPU). The GPU is the first concept proposed by NVIDIA when it released the GeForce 256 graphics processing chip. Especially when dealing with 3D graphics, the GPU enables the graphics card to reduce the dependence on the CPU and complete part of the work originally belonging to the CPU. The core technologies used by the GPU include hardware T&L (geometric conversion and lighting processing), cubic environment texture mapping and vertex blending, texture compression and bump mapping, dual texture four-pixel 256-bit rendering engine, etc...

The various 3D special effects supported by the graphics card are determined by the performance of the display chip. The type of display chip used roughly determines the grade and basic performance of the graphics card, such as NVIDIA's GT series and AMD's HD series.

Ⅱ Graphics card working principle and mode

The graphics card is inserted into the expansion slot on the motherboard (usually a PCI-E slot, before there were AGP, PCI, ISA, and other slots). It is mainly responsible for converting the display signal sent by the host to the display into a general electrical signal so that the display can understand what the personal computer is making it do. The graphics card is mainly composed of a graphics card motherboard, display chip, display memory, radiator (heat sink, fan), and other parts. The main chip of the graphics card is called "Video chipset" (also called GPU or VPU, graphics processor or visual processor), which is the main processing unit of the graphics card. The graphics card also has a memory similar to the computer memory, called "display memory".

Early graphics cards were purely graphics cards, which only played the role of signal conversion. The graphics cards we generally use have 3D graphics calculations and graphics acceleration functions, so they are also called "graphics acceleration cards" or "3D acceleration cards." The earliest graphics cards on the PC were the MDA and CGA 2D accelerator cards that were installed on the 5150 personal computer launched by IBM in 1981.

Graphics card is usually composed of bus interface, PCB board, display chip, video memory, RAMDAC, VGA BIOS, VGA function pins, D-sub socket, and other peripheral components. Most graphics cards also have a VGA, DVI display interface or HDMI interface and S-Video Terminal and Display Port interface.

Ⅲ Graphics card classification

1.Integrated graphics

The integrated graphics card is a component that integrates the display chip, video memory, and related circuits on the motherboard. The display chip of the integrated graphics card is almost integrated into the northbridge chip of the motherboard. The display effect and processing performance of the integrated graphics card are relatively weak, and hardware upgrades of the graphics card cannot be performed. However, you can use CMOS to adjust the frequency or flash a new BIOS file to achieve software upgrades to tap the potential of the display chip. The advantages of integrated graphics are low power consumption and low heat. The performance of some integrated graphics can be comparable to entry-level discrete graphics, so many people who like to assemble computers by themselves can get themselves without spending the extra money to buy dedicated graphics.

Integrated graphics.jpg

Integrated graphics

The disadvantage of the integrated graphics card is that the performance is relatively low, and it is solidified on the motherboard or CPU. It cannot be replaced by itself. If it must be replaced, the motherboard can only be replaced.

2.Dedicated graphics

Dedicated graphics.png

Dedicated graphics

A dedicated graphics card means that the display chip, video memory, and related circuits are separately built on a circuit board, which is self-contained and exists as an independent board card. It needs to occupy the expansion slot of the motherboard (ISA, PCI, AGP, or PCI- E). The advantage of a dedicated graphics card is that it has a separate installation of video memory, generally does not occupy system memory. It is technically much more advanced than integrated graphics, but its performance is certainly not worse than that of integrated graphics, and it is easy to upgrade the hardware of the graphics card. The disadvantage of the dedicated graphics card is that the power consumption of the system has increased, the heat generation is also larger. It needs to spend extra money to buy the graphics card, and at the same time (especially for notebook computers) takes up more space. As the performance of the graphics card has different requirements for the graphics card, dedicated graphics cards are actually divided into two categories, one type is graphics cards designed specifically for games, and the other is professional graphics cards used for graphics and 3D rendering.

3.Core graphics

The Core Graphics is the new generation graphics processing core of Intel products. Unlike previous graphics cards, Intel relies on its advanced processor manufacturing process and new architecture design to integrate the graphics core and the processing core on the same substrate. The design integration of the intelligent processor architecture greatly reduces the data turnaround time between the processing core, graphics core, memory, and memory controller, effectively improving processing efficiency and greatly reducing the overall power consumption of the chipset, which helps to reduce the cost of core components. The size provides more options for the design of notebooks, all-in-ones, and other products.

Core graphics.jpg

Core graphics

It should be noted that the core graphics card is not the same as the integrated graphics card in the traditional sense. The graphics solutions adopted by the notebook platform are mainly "dedicated" and "integrated". The former has a separate graphics core and independent video memory, which can meet the complex and huge graphics processing needs and provide efficient video encoding applications. The graphics core of integrated graphics cards is integrated on the motherboard as a separate chip, and part of the system memory is dynamically shared as video memory, so it can provide simple graphics processing capabilities and smoother coding applications.

Core Graphics architecture.png

Core Graphics architecture

Compared with the first two, core Graphics integrates the graphics core in the processor, further enhancing the efficiency of graphics processing, and integrates the "processor + south bridge + northbridge (graphic core + memory control + display output)" in the integrated graphics card. The three-chip solution is reduced to a dual-chip mode of "processor (processing core + graphics core + memory control) + motherboard chips (display output)", which effectively reduces the overall power consumption of core components and is more conducive to extending the battery life of the notebook time.

Low power consumption is the main advantage of the core graphics card. Due to the new streamlined architecture and integrated design, the core graphics card has better control of the overall energy consumption. The efficient processing performance greatly reduces the computing time and further reduces the consumption of the system platform. High performance is also its main advantage: core graphics cards have many advantageous technologies, which can bring sufficient graphics processing capabilities, and their performance is very obvious compared with the previous generation of products.

Ⅳ Graphics card structure

The structure of a general graphics card is as follows:

Capacitors: Capacitors are very important components in graphics cards, because the quality of the display image mainly depends on the quality of the capacitors, and the quality of the capacitors directly affects the quality of the graphics card circuit.

Video memory: Video memory is responsible for storing various data that the display chip needs to process. Its capacity and performance directly affect the display effect of the computer. The new graphics cards all use DDR6/DDR5 video memory, and the mainstream video memory capacity is generally 2GB ~ 4GB.

GPU and fan: GPU is the graphics chip, it is responsible for most of the calculation work of the graphics card, which is equivalent to the role of the CPU in the computer. The function of the GPU fan is to dissipate heat to the GPU.

Graphics card interface: It can be divided into three types: PCI, AGP, and PCI Express. PCI and AGP graphics card interfaces are basically eliminated. The mainstream graphics cards on the market use PCI Express graphics cards.

Peripheral interface: The peripheral interface of the graphics card is responsible for the output task of the graphics card. The new graphics card includes a traditional VGA analog interface and one or more digital interfaces (DVI, HDMI, and DP).

Bridge interface: Mid-to-high-end graphics cards can support multiple works at the same time, and the bridge interface is connected through a bridge between them.

Ⅴ Bus interface types

ISA graphics card

The ISA graphics card is an old graphics card that the most commonly used VGA monitor can support.

VESA graphics card

VESA is the abbreviation of "Video Electronic Standards Association", co-founded in 1989 by a number of computer chip manufacturers. At the end of 1994, VESA published the 64-bit architecture "VESA Local Bus" standard. Most of the 80486 personal computers use this standard graphics card.

PCI graphics card

PCI (Peripheral Component Interconnect) graphics cards are usually used in earlier or streamlined computers. Such computers must rely on PCI interface graphics cards due to the removal of the AGP standard slot. Known to be used mostly from 486 to the early era of Pentium II. But until the display chip cannot directly support AGP, some manufacturers continue to manufacture graphics cards based on AGP to PCI. The latest known PCI interface graphics cards are GeForce GT 610 PCI (SPARKLE system) model GRSP610L1024LC, ATI HD 4350 PCI (HIS system) and HIS HD 5450 PCI (HIS system) HIS 5450 Silence 512MB DDR3 PCI DVI/HDMI/VGA Product number H545H512P.

AGP graphics card

AGP (Accelerated GraphicsPort) is a 32-bit bus interface developed by Intel Corporation in 1996 to enhance the display performance of computer systems. There are AGP 1X, AGP 2X, AGP 4X, and finally AGP 8X, with bandwidths of 266MB/s, 533MB/s, 1066MB/s, and 2133 MB/s. Among them, AGP 4X is not compatible with the previous voltage. Among them, "Wildcat4 7210" of 3DLABS is the strongest professional-grade AGP graphics accelerator card, while ATI's RadeonHD 4670 and HD3850 are the most powerful consumer-grade AGP graphics accelerator cards of the year (2007).

PCI Express graphics card

PCI Express (also known as PCI-E) is the latest graphics interface for graphics cards. It is used to replace AGP graphics cards. Faced with the continuous advancement of 3D display technology in the future, the bandwidth of AGP is no longer sufficient to handle huge data operations. The PCI-Express graphics cards with the highest performance are nVidia's "NVIDIA Titan V" and AMD's "Radeon Pro Duo (Fiji)". At present, the graphics cards produced after 2007 can support dual graphics technology (nVIDIA's SLi and nvlink and AMD's CrossFire).

External PCI Express graphics card

Use a USB or Thunderbolt high-bandwidth cable to connect to an external PCI Express graphics card box, which requires an independent power supply.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is a graphic card in a PC?

The graphics processing unit (GPU), also called a graphics card or video card, is a specialized electronic circuit that accelerates the creation and rendering of images, videos, and animations. It performs fast math calculations while freeing the CPU to perform other tasks.

2.Which graphic card is best for gaming?

Best Graphics Cards for Gaming 2021
1.GeForce RTX 3080. Best Graphics Card Overall, for 4K and More.
2.Radeon RX 6800 XT. Best AMD GPU, Forget About DLSS.
3.GeForce RTX 3090. Fastest Graphics Card, Great for Creators.
4.GeForce RTX 3060 Ti.
5.GeForce RTX 3070.
6.Radeon RX 6700 XT.
7.Radeon RX 6800.
8.GeForce RTX 3060 12GB.

3.What is the graphic card used for?

A graphics card is an expansion card for your PC that is responsible for rendering images to the display. High-end GPUs are used for gaming, ray tracing, graphics production, and even mining cryptocurrency.

4.Can a graphics card die?

Today, graphics cards have several innovative features and cooling components that protect their hardware during rigorous gaming sessions. If crucial components inside the video card get too hot, they can fry up and cause the video card to die over time.

5.Is a graphics card only for gaming?

Not all computers need a graphics card and it's completely 100% possible to get by without one – especially if you're not gaming. But, there are some stipulations. Since you still need a way to render what you see on your monitor, you'll need a processor with an Integrated Graphics Processing Unit (or iGPU for short).
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242202

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 2025742

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • A Comprehensive Guide to FPGA Development Boards
    A Comprehensive Guide to FPGA Development Boards
    UTMEL11 September 2025530

    This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.

    Read More
  • The Ultimate Guide to Microchip MCUs: From Selection to Real-World Applications
    The Ultimate Guide to Microchip MCUs: From Selection to Real-World Applications
    UTMEL13 September 2025258

    Are you an aspiring electronics enthusiast, a seasoned engineer, or a hobbyist looking to bring your next project to life? If so, you've likely encountered the term Microchip MCU. But what exactly is a Microchip MCU, and how do you choose the right one from their vast portfolio? This comprehensive guide will walk you through everything you need to know about Microchip's powerful microcontrollers, from selection and programming to real-world applications.

    Read More
  • Lattice FPGA: The Ultimate Guide to Low-Power, Small Form Factor Solutions
    Lattice FPGA: The Ultimate Guide to Low-Power, Small Form Factor Solutions
    UTMEL19 September 2025104

    Comprehensive review of Lattice FPGAs. Discover why their low-power, small-size, and cost-effective solutions are dominating the edge AI, IoT, and automotive markets. Compare Lattice vs. Xilinx and Intel to make the right choice.

    Read More