What are the Types of Phone Displays?

OLED vs LCD: Smartphone Display Teardown and Comparison
Catalog
| Ⅰ Overview |
| Ⅱ Phone display types |
| Ⅲ Phone display innovation trend |
Ⅰ Overview
The global mobile phone display market has grown and technological innovation has accelerated in recent years, as a result of the rapid promotion and popularization of smartphones, and the industry's scale has continued to develop. In terms of product composition, today's phone displays are mostly touch screens, consisting of a cover glass, touch modules, display modules, and other components. However, as the demand for light and small mobile phones grows, as does the demand for high-definition displays and the maturation of embedded touch technology, the mobile phone screen sector is transitioning from traditional single-component supply to integrated module manufacture. And there's no denying that vertical industrial chain integration is on the rise.
Mobile phone color screens vary due to variances in LCD quality and R&D technologies. TFT, TFD, UFB, STN, and OLED phone screens are the most common. In general, the more colors displayed, the more complex images may be displayed, and the amount of richness of the image grows.

smartphone display
Cover glass: The phone's display's outermost protective component is the cover glass. High investment thresholds and production technology requirements characterize the upstream glass substrate business.
Touch module: A crucial connection in improving mobile phone human-computer interaction. TDDI (Touch with Display Driver Integration), which combines touch and panel driver ICs, is currently the most popular approach.
Display module: LCD and OLED display modules are the two types of display modules available. Polarizer, color filter, liquid crystal, TFT (glass), backlight, and other components make up the LCD display module. The polarizer, Encap (glass), organic self-luminous layer, TFT (glass), and other components make up the OLED display module. It has self-luminescence, a straightforward production process, low energy consumption, ultra-thinness, and flexibility.
Ⅱ Phone display types
TFT material, SLCD material, AMOLED material, SuperAMOLED material, SuperAMOLEDPlus material, ASV technology material, IPS technology material, and NOVA technology material are the most common types of mobile phone display screen materials. Their differences may be seen in their respective traits, which are as follows:
1. TFT phone display
TFT displays are currently the most common type of display on mobile phones. The thin-film transistor (TFT) is a form of active-matrix liquid crystal display (AM-LCD). On the rear of the LCD, TFT has a unique light tube. It can actively manipulate each individual pixel on the screen, resulting in a significant reduction in response time.
The liquid crystal configuration can be recalled because the TFT is an active matrix LCD. And once the current is gone, it will not return to its previous state. TFT additionally improves the STN flicker (water ripple)-blur phenomena, allowing for more dynamic picture playback.
Each pixel in a TFT liquid crystal is equipped with a semiconductor switch. Dot pulses can control each pixel individually. As a result, each node is largely self-contained and may be regulated indefinitely. It not only enhances the display screen's response time but also allows for fine color gradation management. As a result, TFT liquid crystal color is more realistic. The TFT liquid crystal display is bright, layers well, and has vibrant colors.
2. SLCD material phone display
Splice Liquid Crystal Display (SLCD) is an abbreviation for a specific LCD screen used for splicing. It is a high-end LCD variant. The SLCD is a complete splicing display device that may be used as a monitor or spliced together to create a super-sized screen. Depending on the requirements, it may do single-screen split display, single-screen independent display, arbitrary combination display, full-screen splicing, vertical-screen presentation, image frame correction or covering, as well as real-time processing of full HD data.

mobile phone display sizes
SLCD can be used for a variety of purposes and with a variety of signal inputs. It has a service life of over 50,000 hours and has never been burned or damaged. A complete picture can be displayed by combining any number of pieces. Any signal can be moved on the splicing screen wall with a screen as a unit using the software. Additionally, the screen's viewing angle is excellent.
3. AMOLED material phone display
It's a sort of OLED display. AMOLED (Active Matrix Organic Light Emitting Diode) is an organic light-emitting diode panel with an active matrix. AMOLED displays have a faster response time, greater contrast, and a wider viewing angle than standard liquid crystal displays. Fast response time, self-illumination, outstanding display effect, and low power consumption are all advantages of AMOLED screens.
With the help of continued innovation, the early AMOLED panels' limited panel size and lower TFT life cycle have also narrowed the gap. The panel of an AMOLED is self-luminous. AMOLED displays provide richer, brighter effects, and we can see the screen easily outside during the day. The most crucial factor is that AMOLED consumes significantly less energy.
4.SuperAMOLED material phone display
SuperAMOLED stands for Super Active Matrix/Organic Light Emitting Diode. It abandons the prior touch sensing layer + display layer architecture design, as opposed to the typical AMOLED dazzling screen. The control has a higher sensitivity. Furthermore, the removal of the glass cover improves the display effects in direct sunlight.
mDNIe (Mobile Digital Natural Image Engine) technology is also included in SuperAMOLED. It responds swiftly and can be viewed from any angle. The AMOLED screen, touch screen panel, and glass that protects the outside are the three layers of the structure. Because the Touch Sensor is on the AMOLED, Super AMOLED lacks the middle layer of the Touch Screen Panel.

phone display
The SuperAMOLED panel is a native touch display that is thinner than the AMOLED panel. Because the SuperAMOLED display does not require a touch sensor or an air layer, it is more sensitive to touch. The color is brighter due to the lack of a barrier. In terms of viewing angle, display sharpness, and vibrant color saturation, SuperAMOLED excels.
5. SuperAMOLEDPlus phone display
It's Samsung's most recent display. SuperAMOLEDPlus is presently only found on I9100 phones, but I expect it will become more common in the future. By adjusting the RGB primary color distribution in the pixel and extending the pixel range, the brand-new SuperAMOLEDPlus material screen effectively decreases the graininess of the material screen.
Samsung presently exclusively employs the newest SuperAMOLEDPlus display on the Samsung I9100. More phones with such screens will arrive as time goes on.
6. ASV technology material phone display
Sharp's ASV (AdvancedSuper-V) technology improves the TFT display's response speed and viewing angle. ASV is a novel technique for aligning crystalline material between two thin glass sheets.
There are various enhancements, the most noticeable of which is the viewing angle. Users can read the content clearly from an angle of 140 degrees vertically and 110 degrees horizontally on the present display, but ASV improves this angle to 170 degrees.
Furthermore, most displays now have a default state in which all pixels remain white until they are changed to various colors when the display is turned on. It signifies that the damaged pixels are still black and hard to see. The response time of ASV has been reduced from 45 milliseconds to less than 25 milliseconds, which is the third improvement.
7. IPS technology material phone display
To enhance the viewing angle, the IPS panel employs the liquid crystal molecular plane switching technology. The screen has a stronger sensation of transparency and a more delicate hue because it is made without an additional compensation layer. However, the panel's short response time and difficulties in enhancing contrast are two main drawbacks that limit its popularity.
The obvious benefit of the IPS screen is that it has a wider viewing angle, brighter and more vibrant colors, and the squeeze water ripple is less noticeable. Of course, the IPS screen's response time is slower, and its power consumption is higher.
Furthermore, since LG acquired the technology, LG screens are now found in the majority of key consumer items including cell phones, monitors, and televisions. When it comes to IPS, the iPhone4 is a must-have. IPS hard screens are used in the iPhone4, which has a cult following and universal appeal.
8. NOVA technology material phone screen
NOVA is a brand-new sort of display technology on the market right now. The most significant advantage of NOVA over other panels is that it uses less electricity at the same brightness and performs exceptionally well in black color systems.
The most notable aspect of NOVA is that it consumes very little energy at a brightness of 700 Nit. It also has the ability to give a crisp reading experience. The screen contrast has been substantially increased, and a real black and white display effect has been created. When compared to a typical LCD, the brightness is less than 280Nit, which saves up to 50% of the electricity. Under the pure white screen, it saves twice the power of AMOLED.
Ⅲ Phone display innovation trend
1. Embedded touch technology
The development trend of full-fit touch and display integration is clear, with the continual improvement of customers' needs for the visual effects of mobile phone screens and the constant expansion of the product lines of touch and display firms. On/in-cell technology is also being accelerated by touch makers and other leading panel firms. In-cell laminating technique is one of them, and it's tough and expensive. In-cell technology will become widespread as traditional OGS, on-cell screen technology, and production efficiency reach a bottleneck. As expected, the market will continue to grow in the future. In 2016, nearly 50% of mobile phones worldwide used on/in-cell touch panels.
2. OLED display technology
After CRT (Cathode Ray Tube) and FPD (Field Programmable Display), OLED is the most promising new display technology (Flat Panel Display). It offers ultra-thinness, high brightness, a wide viewing angle, low power consumption, high definition, and flexibility, allowing it to efficiently fulfill new product demands. Wide viewing angles, thinner, lighter, softer, and high color saturation are among the new needs. Samsung, Gionee, ZTE, and other brand manufacturers have recently produced flagship models with AMOLED displays.
3. 3D glass
The curved design of 3D glass fits ergonomic requirements. It has a high heat dissipation capacity, good elasticity, and is not fragile. The use of 3D glass as the back panel of phones can efficiently overcome the problem of radio signals being shielded by standard metal phone casings. Wireless charging and high-bandwidth, high-speed next-generation mobile communication technology uses are also possible. In recent years, mobile phone manufacturers have paid close attention to it. Currently, 3D glass coverings may be found on a variety of high-end models. The 3D glass may usher in an era of rapid progress in the future.
4. Application of sapphire material
The sapphire material has a high dielectric constant and high hardness. It has a gorgeous appearance, good thermal conductivity, scratch resistance, sensitive fingerprint identification, and a glass cover built of it. At this time, firms have succeeded in mass-producing sapphire phone covers, which are widely utilized in electronic consumer areas such as smartphones and wearable gadgets. Sapphire displays have been used on some flagship models. Sapphire screens will become increasingly common in the future as the sapphire manufacturing process becomes more refined and production costs continue to plummet.
1.How does phone display work?
In the capacitive system, a layer of an electroconductive material (most often indium-tin-oxide) that stores an electrical charge is placed on the glass panel of the monitor. When a user touches the monitor with his finger, some of the charges are transferred to the user, so the charge on the capacitive layer decreases.
2.What is a phone display?
Smartphone display is the main thing a user sees when buying a new mobile device. There are quite a lot of display types used in mobile phones. TFT LCD – (Thin Film Transistor technology) TFT LCDs are supposedly the most common type of display unit found in mobile devices.
3.Which phone display is best?
Most display experts and consumers agree that OLED displays are the world's best smartphone displays. The best smartphone OLED displays are the Super AMOLED displays produced by Samsung Display, but other OLED producers (such as LG and BOE Display) are also producing high-quality OLEDs.
4.Which display is best for the eyes?
Use High-Resolution screens Most people don't have to use CRT screens anymore. Those are the old computer screens with low refresh rates that created a noticeable flicker that made your eyes feel uncomfortable. Today, screens typically offer refresh rates of 75Hz or more. The higher the better.
5.What is the difference between touch and display?
When you tap your fingertip or swipe it across the screen, the digitizer senses it and sends data to the phone processor. The digitizer pasted to the front glass together is called a "Touch Screen". The display is the visual component underneath the glass that displays the image on the screen.
The Introduction to Common Tools and Using Methods of Fiber OpticUTMEL07 January 20227106The building and maintenance of optical cables in the intelligent industry has gradually expanded with the rapid expansion of the Internet of Things and 5G technologies, resulting in an increase in demand for various optical fiber tools. Cutting shears, for example, come in a variety of shapes and sizes, and each tool serves a different purpose. Do you have any experience with them? When should you utilize certain fiber optic tools?
Read More
What are Fiber Optic Patch Cables?UTMEL11 February 20228155Hello everyone, I am Rose. Today I will introduce fiber optic patch cables to you. Optical fiber communication, as an emerging technology, has become one of the main pillars of modern communication and plays a critical role in modern telecommunication networks, thanks to the rapid growth of traffic data.
Read More
Basis of Fiber Optic and Fiber Optic CommunicationUTMEL22 October 20215091Hello everyone, I am Rose. Today I will introduce fiber optic to you. Fiber Optic is a type of glass or plastic fiber that can be utilized to transmit light. It is mostly used for communication. This article will show you the basic knowledge of fiber optic and fiber optic communication.
Read More
The History of MicroscopeUTMEL21 October 20217973Hello, everyone. I am Rose. Today I will show you the history of microscopes. The microscope is used to magnify tiny objects into instruments that can be seen by human eyes. Microscopes are divided into optical microscopes and electron microscopes.
Read More
What is VCSEL?UTMEL28 October 202111731Hello everyone, I am Rose. I welcome you on board, today I will introduce VCSEL to you. The Vertical-Cavity Surface-Emitting Laser (VCSEL, or Vertical-Cavity Surface-Emitting Laser) is a semiconductor whose laser is emitted perpendicular to the top surface. It differs from an edge-fired laser, which emits the laser from the edge.
Read More
Subscribe to Utmel !
5988160107FDialight
17-21UYC/S530-A3/TR8Everlight Electronics Co Ltd
OP245ATT Electronics/Optek Technology
C10333_LEDILSTAR-SUBLedil
26-21SURC/S530-A3/TR8Everlight Electronics Co Ltd
OP295ATT Electronics/Optek Technology
APHCM2012CGCK-F01Kingbright
C10781_IRISLedil
CC56-12SURKWAKingbright
SLR-343MGT32ROHM Semiconductor


Product
Brand
Articles
Tools