OLED, QLED, MicroLED: Who is the Next Generation Display Technology?

Best Display Tech - QLED/OLED/MicroLED
| Topics covered in this article: |
| Ⅰ. Burn-in OLED |
| Ⅱ. QLED living in the lab |
| Ⅲ. Expensive MicroLED |
| Ⅳ. Who is the next generation display technology? |
Everyone will almost certainly think of LCD and OLED when discussing display panels. The former is a technology that has gained a lot of traction and is frequently utilized in many different display devices. The latter is a new display technology, also referred to as the next-generation display technology, that has progressively gained popularity in recent years. In addition, QLED and MicroLED are now the leading display technologies of the future.
What distinguishes OLED, QLED, and MicroLED from one another and who is the next generation of display technology?
Ⅰ. Burn-in OLED
The term "OLED," which stands for organic light-emitting diode, describes the process whereby an electric field-driven carrier injection and recombination in organic semiconductor materials and light-emitting materials results in the emission of light. Instead than discussing the theory, let's discuss the benefits of OLED over conventional LCD.
One of the main benefits of OLEDs is their ability to illuminate themselves. OLEDs, which can emit light on their own, can make TVs exceedingly thin, in contrast to liquid crystals, which cannot emit light and must rely on the backlight. OLED TVs from LG have an astounding 2.57 mm thickness, with the thickest component measuring no more than 5 mm. Additionally, as the OLED is self-illuminated by the pixel, it may implement pixel-level partitioned lighting, perform pixel switching, and possibly achieve infinite contrast.
OLED also provides a wider viewing angle and uses less electricity than LCD with a backlight module because to its self-luminous features. The color performance of OLED is also significantly superior than LCD, with a larger color spectrum, at the same time. In order to create soft screens, OLED can be generated on a variety of flexible substrate materials, including polymers and resins. This property of OLED is utilized by phones with curved screens and foldable phones.
The organic materials used in OLED age more quickly than the inorganic materials used in LCD, and OLED will leave afterimages when displaying a static image for an extended period of time, which is OLED. These are fatal faults. distinctive burn-in phenomena Although there are numerous methods that can reduce the occurrence of screen burn-in, the problem still isn't very well solved.

Figure. 1
Ⅱ. QLED living in the lab
Let's talk about QLED after discussing OLED. The quantum dot light-emitting diode is another name for QLED. OLED benefits from QLED's self-illumination, slow response time, wide color range, and other features. Since QLED uses inorganic quantum dot materials, which have a longer lifespan than OLED organic materials and won't burn the screen, its advantages over OLED are incomparable.
However, the same technology as OLED cannot be employed due to the drawbacks of quantum dots of quantum dot light-emitting diodes that are easily damaged by heat and moisture, and a new approach needs to be devised. Since QLED technology is still in its infancy, there are still limitations including low reliability and efficiency, unstable component life, and challenges in the research and development of solution processes. As a result, QLED is now only available in laboratories, and its commercial application is still some time off.

Figure. 2
Someone will now inquire, "Hasn't Samsung already launched a QLED TV?" In actuality, the QLED TVs now on the market are an improved version of LCD TVs rather than true QLEDs. LCD TVs can be made to perform better than conventional LCD TVs by placing a quantum dot film layer in front of the backlight of the TVs. better color performance and image quality.
Because of this, the QLED TVs currently on the market are photoluminescent and require a backlight, whereas the true QLED is electroluminescent and can achieve pixel self-illumination.

Figure. 3
Ⅲ. Expensive MicroLED
In essence, MicroLED is an LED light-emitting billboard, but it produces each tiny lamp bead to the micron level, unlike the LED light-emitting billboards we see on the road. MicroLED is similarly self-luminous at the pixel level like OLED. The conventional inorganic LED array is reduced in size. With a 10 micron LED pixel size, each one may be separately addressed and lighted.

Figure. 4
Compared to current OLED technology, microLEDs are more efficient and brighter while using less electricity. However, the manufacturing of MicroLEDs is challenging, with "mass transfer technology" posing the greatest challenge.
The high cost of MicroLED is a result of the manufacture's severe production challenges and low yield. Large-screen MicroLED TVs are now too expensive for the average person to afford.

Figure. 5
Ⅳ. Who is the next generation display technology?
OLED, QLED, and MicroLED are the next-generation display technologies. The pixels are self-illuminating and function well, not scorching the screen. OLED is clearly inferior than QLED and MicroLED, which have longer lives. However, things change when you take into account how various technologies are currently developing. In contrast to MicroLED, which has a low yield rate and high cost and currently has no genuine civilian product, OLED has been able to accomplish mass manufacturing, even if the cost is often greater than QLED. QLED is still in the laboratory stage, and mass production is still in the future. Although the LCD is somewhat higher, it is still within the permitted limit.

Figure. 6
As of now, OLED may be anticipated to displace LCD as the next-generation display technology if the cost can be further reduced. OLED is a transitional technology as well, and QLED and MicroLED are the ultimate forms, in the long term. In terms of the present, LCD is still the big brother when it comes to TVs, despite OLED starting to displace LCD in the sector of small screens like those seen in smartphones.
In actuality, choosing a display technology is not a big concern for us consumers. Cheap and simple are paramount. Even if QLED and MicroLED can be commercialized, if the price does not go down, it still cannot shake the status of LCD.
1. Which is better QLED or OLED?
OLED is better. In terms of picture quality, OLED is the clear winner when QLED is compared to OLED, especially when the lights are dimmed, OLED is a more attractive option. When it comes to color, OLED once ruled the field, but by improving the purity of the backlight, quantum dots have given QLED TVs a huge boost in color standard, color brightness and color volume, putting them on a par with OLED TVs.
2. Which technology is more powerful, QLED or OLED?
QLED. Since QLED technology uses very mature inorganic materials, the fluorescence lifetime is longer, and there will be no color attenuation problem after long-term use. At the same time, QLED technology will save more power. OLED power saving is when the black field is displayed, but under normal use, the power consumption of QLED of the same size is lower.
3. Is MicroLED about to replace OLED?
Not possible in the near future. At present, the manufacturing process of Micro LED is immature, the yield rate is low, and the price is high. Although manufacturers such as Samsung have demonstrated prototypes, it is still difficult to achieve commercialization. However, with the improvement of technology, Micro LED is indeed one of the development directions of future display technology, it depends on how manufacturers overcome the difficulties.
Improving the Energy Conversion Efficiency of Triboelectric NanogeneratorsSaumitra Jagdale19 November 20243276There is a huge growth in demand for self-sustaining electronic devices, as the traditional power-generating devices fail in remote and harsh environments due to the periodic requirement of battery changes. Also, these devices are frequency specific; some work only in high frequency and some in low frequency. Triboelectric nanogenerators (TENGs) provide a promising solution by efficiently converting mechanical energy into electricity as they are versatile, compact, and cheap, making them a popular choice.
Read More
Methodologies for Increasing Efficiency of Fuel Stack Technology for Energy GenerationSaumitra Jagdale19 November 20243125Presently, power companies are moving towards renewable energy systems. Conventional energy sources are more expensive because they require a vast network to be maintained and huge human resources. Also, they harm the environment by releasing several harmful gases. As the industry’s focus shifts toward renewable energy sources, energy systems powered by Proton Exchange Membrane Fuel Stacks (PEMFS) are gaining traction.
Read More
VSC Light Meaning, Causes, and Step-by-Step DiagnosticsUTMEL19 May 20263797A VSC (Vehicle Stability Control) light indicates the system is disabled, often as a fail-safe triggered by unrelated engine faults like a loose gas cap. While the stability system prevents lateral skidding, it shuts down when sensor data is unreliable. Proper diagnosis requires an ABS-capable OBD2 scanner. Resolving the root engine code, checking wheel speed sensors, or performing a zero-point calibration usually restores system function.
Read More
What JEDEC JEP203 and JEP204 Actually Change for SiC Qualification Engineers and Component BuyersUTMEL29 July 2026524Summary: When JEDEC published JEP203 and JEP204 on June 3, 2026[1], most coverage treated them as an announcement. They are better understood as the first shared language the silicon carbide industry has had for two problems that have quietly consumed engineering hours since the first commercial SiC MOSFETs shipped: short-circuit evaluation that produces numbers you can compare across suppliers, and a consolidated reference of stress procedures so qualification engineers stop reinventing test plans from scratch. This article explains what changes on Monday morning and what to ask suppliers for now.
Read More
2nm vs 3nm Chips: What the Latest Process Nodes Mean for PerformanceUTMEL19 August 20261757The shift from 3nm to 2nm process nodes marks a fundamental change in transistor architecture, moving from FinFET to Gate-All-Around (GAA) nanosheets. This transition delivers meaningful improvements in performance, power, and density, but also introduces new challenges like SRAM scaling limits, thermal density, and backside power delivery. The article compares TSMC, Samsung, and Intel approaches, offering a practical decision framework for engineering teams.
Read More
Subscribe to Utmel !


Product
Brand
Articles
Tools