web counter

Improving the Energy Conversion Efficiency of Triboelectric Nanogenerators

Published: 19 November 2024 | Last Updated: 19 November 20243270
There is a huge growth in demand for self-sustaining electronic devices, as the traditional power-generating devices fail in remote and harsh environments due to the periodic requirement of battery changes. Also, these devices are frequency specific; some work only in high frequency and some in low frequency. Triboelectric nanogenerators (TENGs) provide a promising solution by efficiently converting mechanical energy into electricity as they are versatile, compact, and cheap, making them a popular choice.

A commonly used configuration of TENGs is a free-standing mode with 6 electrolytes which gives a power output of 14.84mW. This setup is preferable for powering small-scale electronic devices and is very useful in IoT applications. Triboelectric nanogenerators operate on the principle of triboelectricity. It works on the principle of frictional sliding, triboelectric charges are generated on the surfaces between the two dielectrics, causing a potential difference between the two electrodes.

The simplicity of the mechanism allows the use of TENGs in various power harvesting sources such as human movement, vibrations, wind, and water flow. After a lot of research, the average power density of TENGs was calculated to be raised to 87.26 W m−2 Hz−1, which is sufficient to meet the power requirements of most electronic devices in IoTs, making it a potential game-changer for small-scale, renewable energy generation.

Use of TENG as power harvesters.png

Figure 1: Use of TENG as power harvesters

Due to its usage on a large scale, there is always a demand for increasing the efficiency of performance. Researchers have developed various effective strategies, including charge excitation local discharge, space charge accumulation, charge migration, etc., to boost the output performance of TENGs. However, it possesses several limitations but the major problem that affects the performance of TENG is its high intrinsic impedance this leads to a mismatch of output energy from TENG to the input energy required by the applications they are powering.

Solution to Irregular Power Supply

TENGs provide irregular power output because they generate energy from unstable mechanical energy sources. These irregular inputs occur because TENGs take energy from mechanical sources which can be highly irregular some TENGs use water flow or wind flow, but the flow is highly irregular as it depends upon a lot of other natural factors.

In real-world applications, these energy sources rarely provide a constant, smooth mechanical input, instead, they come in bursts or fluctuating cycles, creating inconsistent power output from the TENG. This irregularity poses challenges for directly powering devices, as most electronics require stable, continuous energy to function effectively. To overcome this problem, integration of TENGs with an energy management circuit, helps with the output regulations and comes with an energy storage system. When the power consumption of a device is lower than the input power from the TENG, the output terminal can maintain a constant voltage, allowing for consistent load operation. Excess energy is stored in the input capacitor (Cin) for future use, which is crucial for applications where the mechanical energy harvested may be intermittent.

The energy storage system enables continuous power output even when the mechanical energy input is unstable. It was also found that using this mechanism a rotating TENG that only works for 21s can make a hygrothermograph run for 417s which is significantly higher than normally used TENGs. Also, hand-driven TENG which have irregular inputs can be used to run small systems such as mini game consoles and calculators using these EM circuits. Even though theoretically the power efficiency seemed to increase in practical use the power efficiency increased only by 5%.

Overcoming the Limitations by Resolving the Topologies in TENGs

To tackle the limitations of TENG, the need for optimization so synergistic optimization was suggested for both the TENG itself and the energy management circuit. Here the main focus was to reduce the charge loss and voltage loss caused by the switches used in the TENGs for controlling the energy flow. By optimizing the TENG’s switching configuration the current and voltage losses are significantly reduced. This increased the conversion efficiency by 42.5% which is 8.5 times higher than the EM circuits.

The power losses can be further minimized by designing an efficient energy management circuit. Zener diode is generally used to stabilize the voltage, but this approach affects the energy loss when the power exceeds the required power level because the diode dissipates the extra energy as heat, which reduces the overall efficiency of the TENG system. Recognizing this issue the researchers came up with a special chip LTC-3588-1 which is essential for regulating voltage and could be a potential solution. The direct integration of the chip with TENGs initially showed low energy utilization rates, largely due to inefficiencies in the energy transfer process between the TENG and the input capacitor which is the basic energy storage component. To tackle this problem, chip was integrated with the TENG system to optimize the performance. 3588 is a newer version of the chip which can maintain stable output voltage when the load resistance exceeds 60 kΩ, with an output power of 56.8 μW. By applying the EM strategy, the system improves energy conversion efficiency by 121.5 times, reaching an RMS output power of 6.9 mW under a 500 Ω load.


Figure 2.png

Figure 2

The improved efficiency of TENGs makes them more usable across different applications such as for real-time applications where we need to replace batteries which is both costly and inconvenient. Optimized TENGs can be used in environmental monitoring, smart cities, and portable electronics where there is abundant mechanical energy. By continuing to optimize TENG configurations and integrating more advanced energy management circuits, researchers believe that the energy utilization efficiency of TENGs can be further enhanced, making them a core component in the future of sustainable energy solutions.

Saumitra Jagdale

Saumitra Jagdale is a Backend Developer, Freelance Technical Author, Global AI Ambassador (SwissCognitive), Open-source Contributor in Python projects, Leader of Tensorflow Community India, and Passionate AI/ML Enthusiast

Related Articles

  • Improving the Energy Conversion Efficiency of Triboelectric Nanogenerators
    Improving the Energy Conversion Efficiency of Triboelectric Nanogenerators
    Saumitra Jagdale19 November 20243270

    There is a huge growth in demand for self-sustaining electronic devices, as the traditional power-generating devices fail in remote and harsh environments due to the periodic requirement of battery changes. Also, these devices are frequency specific; some work only in high frequency and some in low frequency. Triboelectric nanogenerators (TENGs) provide a promising solution by efficiently converting mechanical energy into electricity as they are versatile, compact, and cheap, making them a popular choice.

    Read More
  • Methodologies for Increasing Efficiency of Fuel Stack Technology for Energy Generation
    Methodologies for Increasing Efficiency of Fuel Stack Technology for Energy Generation
    Saumitra Jagdale19 November 20243116

    Presently, power companies are moving towards renewable energy systems. Conventional energy sources are more expensive because they require a vast network to be maintained and huge human resources. Also, they harm the environment by releasing several harmful gases. As the industry’s focus shifts toward renewable energy sources, energy systems powered by Proton Exchange Membrane Fuel Stacks (PEMFS) are gaining traction.

    Read More
  • VSC Light Meaning, Causes, and Step-by-Step Diagnostics
    VSC Light Meaning, Causes, and Step-by-Step Diagnostics
    UTMEL19 May 20263701

    A VSC (Vehicle Stability Control) light indicates the system is disabled, often as a fail-safe triggered by unrelated engine faults like a loose gas cap. While the stability system prevents lateral skidding, it shuts down when sensor data is unreliable. Proper diagnosis requires an ABS-capable OBD2 scanner. Resolving the root engine code, checking wheel speed sensors, or performing a zero-point calibration usually restores system function.

    Read More
  • What JEDEC JEP203 and JEP204 Actually Change for SiC Qualification Engineers and Component Buyers
    What JEDEC JEP203 and JEP204 Actually Change for SiC Qualification Engineers and Component Buyers
    UTMEL29 July 2026505

    ​Summary: When JEDEC published JEP203 and JEP204 on June 3, 2026[1], most coverage treated them as an announcement. They are better understood as the first shared language the silicon carbide industry has had for two problems that have quietly consumed engineering hours since the first commercial SiC MOSFETs shipped: short-circuit evaluation that produces numbers you can compare across suppliers, and a consolidated reference of stress procedures so qualification engineers stop reinventing test plans from scratch. This article explains what changes on Monday morning and what to ask suppliers for now.

    Read More
  • 2nm vs 3nm Chips: What the Latest Process Nodes Mean for Performance
    2nm vs 3nm Chips: What the Latest Process Nodes Mean for Performance
    UTMEL19 August 20261682

    The shift from 3nm to 2nm process nodes marks a fundamental change in transistor architecture, moving from FinFET to Gate-All-Around (GAA) nanosheets. This transition delivers meaningful improvements in performance, power, and density, but also introduces new challenges like SRAM scaling limits, thermal density, and backside power delivery. The article compares TSMC, Samsung, and Intel approaches, offering a practical decision framework for engineering teams.

    Read More