web counter

Basis of Fiber Optic and Fiber Optic Communication

Published: 22 October 2021 | Last Updated: 22 October 20215471
Hello everyone, I am Rose. Today I will introduce fiber optic to you. Fiber Optic is a type of glass or plastic fiber that can be utilized to transmit light. It is mostly used for communication. This article will show you the basic knowledge of fiber optic and fiber optic communication.
This video will show you how fiber optics carry datas.

How Does LIGHT Carry Data? - Fiber Optics Explained

Topics covered in this article:
Ⅰ. What is Fiber Optic
Ⅱ. The Working Principle of Fiber Optic
Ⅲ. The Development History of Fiber Optic Communication
Ⅳ. The Characteristics of Fiber Optic Communication


Ⅰ. What is Fiber Optic

Fiber Optic is a type of glass or plastic fiber that can be utilized to transmit light. 

微信图片_20211022152548.jpg

It is mostly used for communication. The fiber optic utilized in communication today is essentially a silica optical fiber, with high-purity silica glass, especially silicon dioxide, as its principal component (SiO2). 

2.jpg

Fiber optic communication systems use light waves to transfer information via optical fibers to achieve the goal of communication.

▎Dispersion of fiber optic

Causes of fiber dispersion

The optical signal in an optical fiber is made up of several different components. Because each frequency component or mode component of the signal propagates at a different speed, there will be a time delay difference between the different components after a certain distance along with the optical fiber, causing the transmission signal waveform to change. Fiber dispersion is a phenomenon that causes pulse broadening and distortion.

Influence of fiber dispersion

Inter-symbol interference is caused by fiber dispersion, which distorts and broadens the transmitted signal pulse. The inter-symbol interval must be raised to ensure communication quality, which means the signal's transmission rate must be reduced, limiting the optical fiber system's communication capacity and transmission distance.

Classification of fiber dispersion

Fiber dispersion can be classified as modal dispersion, material dispersion, waveguide dispersion, and polarization dispersion based on the sources of dispersion.

 

▎The electromagnetic spectrum of fiber optic

 8.jpg

 

▎The loss of fiber optic

After the optical signal has been carried through the optical fiber, the loss of optical power occurs owing to absorption, scattering, and other factors.

 10.jpg


Schematic diagram of the attenuation of ordinary single-mode fiber with wavelength

▎The classification of fiber optic

11.png

Step fiber

The refractive index distributions in the core and cladding areas are uniform, n1 and n2, respectively. The refractive index changes gradually (n2n1) at the boundary between the core and the cladding.

12.jpg

13.jpg

Graded fiber

The refractive index is highest (n1) along the fiber axis, but it gradually falls as the radial direction of the cross-section increases. It simply lowers to the refractive index n2 with the cladding region at the boundary between the core and the cladding.

14.jpg

MMF, multimode fiber

Multiple light modes can be transmitted. However, inter-mode dispersion is rather high, limiting the frequency of digital signal transmission, and it becomes more serious as distance increases.

SMF, single-mode fiber

Because just one mode of light may be communicated, the inter-mode dispersion is extremely low, making it ideal for long-distance communication.

 15.png

16.jpg

17.png

MMF VS SMF

▎Fiber optic interface

Optical fiber interfaces are classified as follows:

FC threaded circle (most used on patch panels)

ST circular snap-on type

square type SC card-connected SC card-connected SC card-connected SC card-connected SC (most used on router switches)

The LC connector has a similar design to the SC connector, although it is smaller. MT-RJ square type, integrated one-head dual fiber transceiver

MPO/MTP type

BFOC type

DIN type

FDDI type

MU type

19.jpg

What exactly do terms like "FC/PC," "SC/PC," and "SC/APC" mean?

The part before "/" denotes the pigtail connector type; FC and SC are, as previously said, omitted; the part following "/" denotes the optical fiber connector cross-section process, i.e. the grinding method.

“PC: Physical Contact”:

It has a flat joint cross-section; in fact, it is micro-spherical grinding and polishing, which is the most extensively used in telecom equipment.

“APC”:

It grinds and polishes micro-spherical surfaces at an angle of 8 degrees. It is the most common model in radio and television, as well as early CATV. Its pigtail head has an angled end face that helps increase TV signal quality. The fundamental reason is that because the TV signal is analog light modulation, the reflected light returns along the original path when the coupling surface of the connector is vertical.

“UPC”:

The attenuation is lower than that of "PC," therefore it is commonly utilized for special-purpose equipment. For internal fiber jumpers in ODF racks, some foreign manufacturers employ FC/UPC, mostly to improve the ODF equipment's own indications.

▎Fiber optic module

Optical transceiver, or optical transceiver in full, is a critical component in optical fiber communication systems.

The following types of network equipment are typically included:

SFP(Small Form-factor Pluggable transceiver ):

SFP is a small package pluggable transceiver (LC interface) that can transmit data at speeds of 100, 155, 622, 1000, 1250, and 2500 Mbps.

GBIC (Gigabit Interface Converter):

Gigabit Ethernet interface converter (SC interface)

XFP(10-Gigabit small Form-factor Pluggable transceiver ): 

10 Gigabit Ethernet interface small package pluggable transceiver (LC interface)

XENPAK(10 Gigabit EtherNet Transceiver PAcKage ):

10 Gigabit Ethernet interface transceiver package (SC interface)

 20.jpg

▎Fiber splicing

Fusion splicing is a wiring technique that melts the optical fiber into a single piece using the heat created by the discharge between the electrode rods. It's broken down into two sections:

Fiber core alignment method

This is a fusion method in which the optical fiber's core wire is examined under a microscope, image processing is used to place the core wire's center axis, and the fiber is then discharged. For placement from two directions, a fusion splicing machine with a two-way observation camera is employed.

32.jpg

Fiber Fusion Splicer

22.png

Fixed V-groove alignment method

This is a fusion process in which the fibers are organized in a high-precision V-groove and the outer diameter is aligned using the aligning effect created by the surface tension of the melted fiber. The dimensional accuracy of the position of the optical fiber core has recently improved as a result of advancements in manufacturing technology, allowing for low-loss wiring to be produced.

This method is mostly used for one-time multi-core wiring.

23.png

Ⅱ. The Working Principle of Fiber Optic

Principle of Total Reflection

The angle of refraction is greater than the angle of incidence when the light beam is directed from the optically dense media to the optically thin medium, as illustrated in the picture.

If 0 is increased constantly, the refraction angle 1 can reach 90°, at which point 1 is referred to as the critical angle.

Total reflection occurs when light is directed from an optically dense media to an optically thin medium with an incidence angle larger than the critical angle.

Total reflection is used in fiber optics to convey optical signals.

7.png

Ⅲ. The Development History of Fiber Optic Communication

The "optical telephone" was invented by Alexander Graham Bell in 1880.

Charles Vernon Boys, a British physicist, created the first optical fiber in the laboratory in 1887.

Long glass strands were first produced in 1938 by the American Owens Illinois Glass Company and the Japanese Nitto Textiles Company.

Brian O'Brian, an optical physicist, invented the notion of cladding in 1951.

The first glass-clad fiber was created in 1956 by a University of Michigan student. To melt a glass tube with a low refractive index onto a glass rod with a high refractive index, he used a low refractive index glass tube.

Theodore Maiman demonstrated the first laser in 1960. People's interest in optical communication has been piqued as a result of this. Laser appears to be a very promising communication method that can solve the bandwidth problem. Experiments have begun in a number of laboratories.

Gao Kun, a British-Chinese researcher, first suggested the feasibility and technological technique of employing optical fiber for data transmission in 1966, laying the groundwork for modern optical communication—optical fiber communication.

Corning, a company based in the United States, created a quartz optical fiber with a loss of 20dB/km in 1970.

Bell Laboratories in the United States improved on this in 1973, lowering optical fiber loss to 2.5dB/km.

The optical fiber loss was lowered to 0.47 dB/km (wavelength 1.2m) by Nippon Telegraph and Telephone (NTT) in 1976.

 

Ⅳ. The Characteristics of Fiber Optic Communication

Huge communication capacity

An optical cable may theoretically transport 10 billion voice channels at once. Currently, the simultaneous testing of 500,000 voice channels has been successful, which is thousands or even hundreds of thousands of times greater than typical coaxial cables and microwaves.

Long Relay Distance

Optical fiber has a very low attenuation coefficient, which, when combined with appropriate optical transmission, optical receiving equipment, optical amplifier, forward error correction, and RZ code modulation technology, can achieve relay distances of thousands of kilometers, whereas traditional cable can only transmit 1.5 kilometers and microwave 50 kilometers, respectively.

Good confidentiality

Adaptable

It has the benefits of not being affected by powerful external electromagnetic fields, corrosion resistance, and so on.

Small size and lightweight

Rich sources of raw materials and low prices

 4.jpg




UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. Which fiber has better performance?

The core of the single-mode fiber is thin, so that the light can be directly launched to the center. It is recommended to use it when the distance is long; the optical signal in the multi-mode fiber propagates through multiple channels, and it is usually recommended to be used when the distance is short. In addition, the distance loss of single-mode signals is smaller than that of multi-mode signals.

2. What are the main advantages of optical fiber communication?

Optical fiber communication has many advantages: its transmission frequency bandwidth, large communication capacity; low transmission loss, long relay distance; thin wire diameter, light weight, raw material made of quartz, saving metal materials, conducive to the rational use of resources; insulation, anti-electromagnetic interference Strong performance; it also has the advantages of strong corrosion resistance, strong radiation resistance, good circumvention, no electric spark, small leakage, and strong confidentiality. It can be used in special environments or military.

3. What does splicing mean in optical fiber communication?

Fusion fiber is fusion splicing optical fibers, that is, welding optical fibers together.
The optical fiber fusion splicing technology mainly uses a fiber fusion machine to connect the optical fiber and the optical fiber or the optical fiber and the pigtail, and fuse the bare fiber and the fiber pigtail in the optical cable into a whole, and the pigtail has a separate optical fiber head.
Related Articles

  • Optical Transceiver Guide: How It Works, Types, Form Factors, and Selection
    Optical Transceiver Guide: How It Works, Types, Form Factors, and Selection
    UTMEL24 June 2026684

    An optical transceiver is the replaceable interface between electronic network equipment and an optical fiber link. It converts electrical data from a switch, router, server, storage system, or transport platform into modulated light, then converts received light back into electrical data.

    Read More
  • Transceivers Shortage Outlook 2026: Supply, Lead Times, and Sourcing Options
    Transceivers Shortage Outlook 2026: Supply, Lead Times, and Sourcing Options
    UTMEL09 July 20262325

    The 2026 transceiver market is defined not by a broad, systemic silicon crisis, but by a highly targeted, structural constraint driven by AI data center build-outs. Figure 3: Power connectors on server racks designed for intense workloads.

    Read More
  • The Introduction to Common Tools and Using Methods of Fiber Optic
    The Introduction to Common Tools and Using Methods of Fiber Optic
    UTMEL07 January 20227499

    The building and maintenance of optical cables in the intelligent industry has gradually expanded with the rapid expansion of the Internet of Things and 5G technologies, resulting in an increase in demand for various optical fiber tools. Cutting shears, for example, come in a variety of shapes and sizes, and each tool serves a different purpose. Do you have any experience with them? When should you utilize certain fiber optic tools?

    Read More
  • What are Fiber Optic Patch Cables?
    What are Fiber Optic Patch Cables?
    UTMEL11 February 20228494

    Hello everyone, I am Rose. Today I will introduce fiber optic patch cables to you. Optical fiber communication, as an emerging technology, has become one of the main pillars of modern communication and plays a critical role in modern telecommunication networks, thanks to the rapid growth of traffic data.

    Read More
  • Basis of Fiber Optic and Fiber Optic Communication
    Basis of Fiber Optic and Fiber Optic Communication
    UTMEL22 October 20215471

    Hello everyone, I am Rose. Today I will introduce fiber optic to you. Fiber Optic is a type of glass or plastic fiber that can be utilized to transmit light. It is mostly used for communication. This article will show you the basic knowledge of fiber optic and fiber optic communication.

    Read More

Subscribe to Utmel !

Featured Parts More