web counter

What is a Knock Sensor?

Published: 27 October 2021 | Last Updated: 08 January 202621597
Hello everyone, I am Rose. Welcome back to the new post today. I will introduce Knock Sensor to you. The knock sensor is a small "listening" device in or on the engine that detects abnormal vibrations and sounds coming from the engine block.
This video will tell you how to test knock sensor.

HOW TO TEST KNOCK SENSOR

Executive Summary (2026 Update)

What is a Knock Sensor? A knock sensor is a piezoelectric listening device mounted on the engine block that detects irregular combustion (detonation or "pinging"). It sends real-time voltage signals to the Engine Control Unit (ECU), allowing the computer to retard ignition timing and prevent catastrophic engine damage.

Key Takeaway: Modern knock sensors are critical for fuel efficiency and engine longevity. Symptoms of failure include a Check Engine Light (codes P0325/P0332), reduced acceleration, and audible metallic clicking sounds.

Topics covered in this article:
Ⅰ. What is Engine Knock? (Detonation)
Ⅱ. What is a Knock Sensor & How Does It Work?
Ⅲ. Where is the Knock Sensor Located?
Ⅳ. Technical Operation Principles
Ⅴ. Top 5 Causes of Engine Knocking
Ⅵ. How to Test and Detect Faults


An automobile engine is a complex system where millisecond-precise timing is essential.

In the past, drivers had to rely on their ears to detect engine "pings," often realizing too late that internal damage had occurred. In 2026, modern vehicles utilize advanced sensor networks to self-diagnose issues before they become catastrophic.

While sensors like O2 and Mass Air Flow monitor chemical ratios, the Knock Sensor (KS) acts as the engine's microphone, continuously monitoring acoustic vibration levels to prevent piston damage.

The knock sensor serves a critical role in the Engine Management System (EMS).

 Illustration comparing normal spark plug ignition versus uncontrolled engine knocking detonation

Ⅰ. What is Engine Knock? (Detonation)

Engine knock, technically known as detonation, is the sharp sound and physical shockwave produced when pockets of air-fuel mixture ignite spontaneously (uncontrolled) rather than being ignited smoothly by the spark plug.

In a healthy combustion cycle, the spark plug creates a flame front that moves predictably through the cylinder. However, if heat or pressure becomes excessive, a second, unintended ignition point can form. When the two flame fronts collide, they create a massive spike in cylinder pressure. This collision causes the characteristic "pinging" or "knocking" sound.

Why is this dangerous?    Continued knocking can shatter pistons, bend connecting rods, and destroy cylinder heads. Modern ECUs rely on knock data to prevent this by adjusting timing immediately.

 

Ⅱ. What is a Knock Sensor & How Does It Work?

A knock sensor is a piezoelectric acoustic sensor mounted directly to the engine block that "listens" for specific vibrational frequencies associated with detonation (typically 5–15 kHz).

When the sensor detects these specific vibrations, it converts the mechanical stress into an electrical voltage signal and sends it to the Engine Control Unit (ECU). The car's computer immediately retards (delays) the ignition timing to stop the knocking, protecting the engine.

It may also trigger the Check Engine Light (CEL) with codes like P0325 (Malfunction) or P0330 (Sensor 2 Circuit) if the sensor itself fails.

Knock Sensor Architecture

While older resources may list confusing categories, in 2026, we classify sensors into three distinct technologies based on how they detect frequency:

1. Inductive Knock Sensor

The inductive sensor utilizes electromagnetic induction. It consists of an induction coil, iron core, shell, and permanent magnet (see Figure 1). When the engine block vibrates, the movement of the iron core changes the magnetic flux through the coil, generating an electromotive force. This sensor is tuned to output maximum voltage when the engine vibration matches the sensor's natural frequency.

2. Piezoelectric Resonant Knock Sensor

Cross-section diagram of a piezoelectric resonant knock sensor showing vibrator and base

Piezoelectric resonance type structure

This type uses a vibrator plate and a piezoelectric element. The vibrator is designed to resonate at the exact frequency of engine knock for that specific engine model. When knock occurs, the vibrator resonates, exerting pressure on the piezoelectric element, which generates a high-voltage signal. This type is highly sensitive but engine-specific.

3. Piezoelectric Non-Resonant Knock Sensor

Diagram of a broad-band non-resonant knock sensor typically used in modern vehicles

Piezoelectric non-resonant structure

Also known as "broadband" sensors, these are the standard in 2026. They use a seismic mass and a piezoelectric crystal to detect a wide range of vibration frequencies (not just one). The ECU then uses digital filters to isolate the "knock" frequency from background engine noise. This allows one sensor design to be used across many different vehicle models.

4. Spark Plug Seat Sensor

Washer-style knock sensor that fits under a spark plug

 Spark plug holder metal pad knock sensor 

This specialized sensor is shaped like a washer and installed directly under the spark plug. It measures combustion pressure directly from the cylinder head. While less common in mass-production cars, it offers extremely precise cylinder-specific data.

 

Ⅲ. Where is the Knock Sensor Located?

The knock sensor is bolted directly to the engine block to ensure maximum acoustic transfer.

  • V-Configuration Engines (V6, V8): Commonly located deep in the "valley" of the engine, underneath the intake manifold.

  • Inline Engines (4-cylinder): Typically found on the side of the engine block, below the intake manifold, between cylinders 2 and 3.

Because it detects physical vibration, it must be torqued to exact manufacturer specifications during installation. A loose sensor cannot detect knock; an overtightened sensor may be too sensitive.

 

Ⅳ. Technical Operation: How Knock Sensors Detect Vibration

Graphic showing how piezoelectric ceramics convert vibration into voltage

Knock sensors operate on the Piezoelectric Effect. Inside the sensor are piezoelectric crystals or ceramics. When these crystals are mechanically stressed (squeezed or shaken by vibration), they generate a small AC voltage.

Unlike position sensors (which use magnets), the knock sensor is essentially a microphone.

  1. Detection: Engine knock creates a high-frequency pressure wave (shockwave).

  2. Conversion: The sensor vibrates, and the internal crystal produces a voltage spike relative to the intensity of the vibration.

  3. Transmission: This voltage (signal) travels to the PCM/ECU.

  4. Action: The ECU recognizes the frequency (e.g., 6kHz) as "knock" and instantly retards the ignition timing in steps (e.g., -2 degrees) until the knocking stops.

This creates a "closed-loop" feedback system, allowing the engine to run on the verge of knock for maximum power and efficiency, correcting itself only when necessary.

 

Ⅴ. Top 5 Causes of Engine Knocking in 2026

Engine knocking indicates abnormal combustion. While the sensor detects it, the root cause usually lies elsewhere. Common culprits include:

  • 1) Low Octane Fuel: High-compression engines require high-octane fuel (91/93). Using 87 octane can cause the fuel to ignite prematurely due to compression heat.

  • 2) Carbon Deposits: Over time, carbon builds up on pistons and valves. This decreases cylinder volume (increasing compression) and can retain heat, creating "hot spots" that ignite fuel early.

  • 3) Incorrect Spark Plugs: Using plugs with the wrong heat range can cause the tip to overheat and ignite the fuel before the spark fires (Pre-ignition).

  • 4) Overheating Engine: If the cooling system fails, high cylinder head temperatures promotes detonation.

  • 5) Lean Air/Fuel Mixture: A vacuum leak or bad fuel injector causes a lean mixture (too much air, not enough gas). Lean mixtures burn hotter and are more prone to knocking.

 

Ⅵ. How to Test a Faulty Knock Sensor (Step-by-Step)

A faulty knock sensor can cause poor fuel economy, sluggish acceleration, and a lit Check Engine Light. Here is a professional workflow for testing (Reference: VW/Audi/General applications):

Schematic for testing knock sensor resistance and voltage with a multimeter

Standard Multimeter Testing Procedure

Method 1: Resistance Check (Static Test)    
1. Disconnect the sensor harness.    
2. Set your multimeter to Ohms (Ω).    
3. Measure the resistance between the signal wire and ground (or between pins if 2-wire).    
4. Expected Result: Most modern sensors should read as an "Open Circuit" (Infinite resistance) or a specific high resistance (e.g., 200kΩ - 10MΩ depending on the car). If it reads Zero (0Ω) or very low continuity, the sensor is shorted and failed. Note: Consult your specific service manual for the exact spec.

Method 2: AC Voltage Check (Active Test)    
1. Back-probe the sensor connector while it is still plugged in.    
2. Set multimeter to AC Volts (millivolts range).    
3. With the engine idling, tap the engine block near the sensor with a wrench (lightly).    
4. Expected Result: You should see a spike in AC voltage corresponding to your taps. If the voltage stays flat at 0V, the sensor is not generating a signal.

Method 3: Oscilloscope (Professional)    
Connect an oscilloscope to the signal wire. Rev the engine or tap the block. A healthy sensor will produce a messy, jagged "grass-like" waveform that spikes instantly with vibration. A flat line indicates a dead sensor.


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. What is the phenomenon of knock sensor failure?

When the knock sensor fails, the vehicle cannot ignite, cannot control the deflagration, the air conditioner in the vehicle is not cooled, the compressor does not work, and the engine check indicator light flashes.

2. How many knock sensors does the car have?

Only one.

3. How to look at the waveform of a knock sensor?

1. Disconnect the sensor plug and connect the oscilloscope to the signal line
2. Knock the cylinder near the sensor to generate an AC signal
3. The normal waveform is displayed, the heavier the knock, the greater the amplitude
Related Articles

  • The Key Role of Electronic Components in IoT Devices
    The Key Role of Electronic Components in IoT Devices
    UTMEL01 September 20236514

    The article discusses the pivotal role of electronic components in Internet of Things (IoT) devices. IoT devices work by capturing real-world data using sensors, processing it through a microcontroller, and then sending it to the cloud for further analysis.

    Read More
  • Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and Applications
    Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and Applications
    UTMEL25 June 20261505

    A practical accelerometer sensor guide covering working principles, MEMS and piezoelectric types, datasheet specifications, circuit design, mounting, applications, and selection.

    Read More
  • 2026 ADAS Sensors: Supply Outlook and Alternative Sourcing
    2026 ADAS Sensors: Supply Outlook and Alternative Sourcing
    UTMEL18 July 20261618

    Automotive cleanroom assembly integrating advanced driver assistance systems. The automotive industry faces a structural semiconductor deficit in 2026, driven not by pandemic-era demand shocks but by AI data centers absorbing global foundry capacity on legacy nodes (40nm-90nm) where 95% of automotive-grade components are manufactured. Video demonstrations of these systems show a "machine view" overlay with red crosshairs tracking pedestrian movement and sudden cut-ins before traditional collision thresholds are triggered.

    Read More
  • Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering Guide
    Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering Guide
    UTMEL21 August 2026950

    This guide compares Hall effect, AMR, and TMR magnetic sensors for position detection in motor control and robotics. It explains their physical principles, key performance metrics, and selection criteria. Hall effect suits low-cost commutation, AMR offers high-speed angle sensing, and TMR provides maximum precision and low power, with practical integration advice.

    Read More
  • Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection Guide
    Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection Guide
    UTMEL17 August 2026802

    This comprehensive selection guide compares thermocouples, platinum RTDs, and semiconductor ICs across measurement range, accuracy limits, and signal conditioning complexity. It covers fundamental operating physics, mathematical transfer functions, lead-wire compensation topologies, and power budgets. Engineers will find practical design checklists, benchtop multimeter diagnostic techniques, and an architectural decision workflow to optimize system performance and bill-of-materials cost.

    Read More

Subscribe to Utmel !

Featured Parts More