Optoelectronics definition
What is Optoelectronics Devices?
Optoelectronics are devices which combine both electronics and light technologies. Optoelectronic devices are the smaller components that are found in PCBs (printed circuit boards) and emit and/or detect light in particular wavelengths. Optoelectronics devices are used by engineers and hobbyists during both the design phase through to manufacturing.
Examples of Optoelectronics
Optoelectronics is a rapidly developing technology discipline that involves the use of electronic devices to source, detect, and manipulate light. Military services, automatic access control systems, telecommunications, medical equipment, and other applications can all benefit from these gadgets.
Because optoelectronics is such a large topic, it encompasses a wide range of devices, including image capture devices, LEDs and elements, information displays, optical storages, remote sensing systems, and optical communication systems.
There are some examples of optoelectronic devices, such as Solar cells, Blue laser, Optical Fibre, Telecommunication laser, Photodiodes and LED traffic lights.
Types of Optoelectronic Devices and Their Applications
On the basis of the structure of the energy bandgap in the material, optoelectronic devices are generally based on semiconductors like silicon (Si), which display electronic characteristics that are intermediate between those of a conductor and an insulator.
Though optoelectronics and semiconductors are not mutually exclusive, they are the foundation of the majority of optoelectronic systems utilized in consumer, industrial, and military applications. Optoelectronics devices types include Encoder sensor integrated circuits (ICs), LEDs (Light-emitting diodes), Laser diodes, Optical fibres, Photovoltaics/solar cells, Photoresistors, Photodiodes and more.
Encoder sensor integrated circuits (ICs)
These are a full system-on-chip (SoC) IC sensor used in optical encoders to translate rotational or linear motion into electrical signals that may be used to calculate speed, rate, velocity, distance, location, or direction. In a motion control system, one or more of these sensors will be used as feedback to the controller.
Encoder Sensors ICs have a monolithic array of active photodiodes that convert light impulses into electrical signals, as well as the majority of the peripheral circuitry to condition and modify the electrical analog signals. Some of the most complicated encoder Integrated Circuits can have up to ten subsystems working together to produce a unified system for precise motion detection.
LEDs (Light-emitting diodes)
A light-emitting diode, short for LED, is a P-N semiconductor diode in which electrons and holes recombine to generate a photon, a phenomenon known as electroluminescence.
LEDs have a wide range of applications since they emit less heat, use less energy, and last longer than incandescent bulbs. Computer components and medical equipment are only a few examples of typical uses, which also include instrument panels, home appliances, watches, and more.
Laser diodes
Laser diodes are semiconductor laser devices that convert electrical energy into light energy. They are very similar in form and operation to LEDs.
Optical fibres
Optical fibre is a type of optical fiber that is used in optoelectronic devices to transport information via modulated light. Optical fibres are commonly used in fibre lasers, sensors, biomedical applications, and telecommunications.
Photovoltaics/Solar Cells
A photovoltaic cell, often known as a solar cell, is a device that transforms sunlight directly into electricity. When photons from the sun collide with a solar cell, they produce a voltage and a current. So this process generates electricity. Applications of Photovoltaics are rural electrification, ocean navigation aids, Telecommunication systems, etc.
Photoresistors
Photoresistors are largely employed in light-sensitive switching devices in terms of application. Light-controlled variable resistors, also known as light-dependent resistors, are the devices in question (or LDRs).
A photoresistor's resistance is particularly high when it is put somewhere very dark (in the megaohms). When lighted, however, its resistance drops dramatically (up to hundreds of ohms depending on the intensity of the light).
Photodiodes
As a form of light sensor, a photodiode is a type of semiconductors. And photodiode circuit is able to convert light energy/protons into electrical energy (current/voltage). Photodiode sensor consists of a P-N junction. Meanwhile, the N layer is negative with an abudance of electrons, while the P layer is positive with an abundance of holes. Typical photodiode materials are Silicon, Germanium, Indium Gallium Arsenide Phosphide and Indium gallium arsenide.
Optoelectronics vs. Electro-Optics vs. Photonics: What's the Difference?
Optoelectronics is a term used to describe the science of using light to make electronic devices ""Any device that functions as an electrical-to-optical or optical-to-electrical transducer" or "any device that responds to optical power, emits or modifies optical radiation, or uses optical radiation for its internal operation."
"Use of applied electrical fields to create and regulate optical radiation" is what electro-optics is called ". It's also worth mentioning that this phrase comes with a caution because the term electro-optic (E-O) is sometimes used interchangeably with optoelectronic, which is erroneous.
Photonics is defined as "technology for creating and harnessing light, using the photon as its quantum unit." This is the fullest definition of the three words listed.