Next-Generation Flexible Display Technology - QLED

OLED vs QLED - With a Microscope! - What is the best TV?
Topics covered in this post: |
What is QLED?
QLED (Quantum Dot Light Emitting Diodes) refers to quantum dots named by Yale University Mark Rid. It specifically refers to some semiconductor nanocrystals that cannot be seen by naked eyes. In general, quantum dots are combined with zinc, cadmium, selenium, and sulfur atoms. It is a particle having a particle diameter below 10 nm. If it is made into a quantum dot layer, the layer is placed in a backlight module of the liquid crystal display (LCD). This makes it possible to reduce the color crosstalk of backlight luminance and RGB color filter (CROSS TALK), which is better than the advantage of lifting the display color gamut. Applications of this method are also used in white light, blue, or ultraviolet (UV) organic light-emitting diodes (OLED) display or television devices with color filter design.
What are the advantages of QLED?
In many next-generation light-emitting display devices, QLEDs have unique advantages, such as color gadget width, high purity, high brightness, low voltage, and extremely thin appearance.
Because of its potential application prospects in mobile and wearable electronic products such as smartphones, car displays, and wearable smart devices, the flexible display is greatly concerned. The flexible display is thin, light, not easy to break, and the shape can be used, which can be used on the surface.
Although the non-planar display has been promoted, most commercial displays are mostly curved, and their shape cannot be changed. Next-generation displays should be displayed in various forms.
In the study of the next-generation display, the main technical objectives are LEDs with mechanical deformation capability and excellent device performance. The brightness of the inorganic LEDs is high (106 ~ 108 cd m-2) and the high-level voltage is low (<2V), which has been used to develop flexible LED arrays. However, its active layer thickness (micron) and fragile disadvantages limit their flexibility, and the point array design cannot achieve high resolution.
The characteristics of QLEDs are excellent color purity (FWHM 30 nm), high brightness (up to 200,000 CD M 2), low operating voltage (opening voltage <2V), and easy processing. The thermal stability and air stability of inorganic quantum dots (QDS) can enhance the life and durability of the display.
QLED structure and principle
The device structure of flexible/wearable QLEDs is largely used in general QLEDs. The general structure of QLEDS includes an anode, an electron transport layer (ETLS), a QD layer, a hole transport layer (HTLS), and a cathode.
In 1983, the Scientists in Bell Labs in the United States first studied QLEDs, but "forgot" to give it a name. After years, the physicist Mark Rid, Yale University, officially named this semiconductor microcontroller "Quantum dots "and use it so far.
Quantum dot has an unusual characteristic: Whenever by light or electrical stimulation, quantum dots will be issued colored light. Light color and size determine the shape of the constituent material of the quantum dots. This feature enables quantum points to change the light color from the light source.
Notably, the blue quantum dot LED light source can be completely converted to white light, rather than the YAG phosphor that absorbs a part only. This means that under the same light bulb brightness, the blue light required for quantum point LED lights are less, and the electric power required in electro-optical conversion is less. More efficient performance makes it better in energy conservation and emission reduction.
The QLED's work is as follows:
1. Electronic and holes are injected from the electrodes into the charge transport layer (CTLS);
2. Inject the carrier into the QDS from the CTLs;
3. Inject carriers in the QDS layer for radiation composite.
The performance and stability of QLEDs depend to a large extent on the choice of CTL material. Good CTLs should have high carrier mobility and can balance electronic / hole injection.
Depending on the CTLS type used, the structure of QLEDs can be divided into four different types: (i) organic / QD double layer; (ii) all-organic type; (iii) full-inorganic (IV) organic-inorganic hybrid type.
Since the structure I is very simple, it is first used in the QLEDS device. However, because there is no ETLS, and the physical separation of QDS and CTLs is difficult to control, the electronic injection is difficult to control, the leakage current is large so that the maximum brightness of the device is only 100 Cd m-2, EQE <0.01%. In order to solve these problems, structural II is proposed, so that the QD layer is sandwiched between the organic HTLS and ETLs to form a sandwich structure. The earliest structure II device peak EQE is 0.5% and has been increased to 6%.
Inorganic CTLS (Structure III) has high electrical conductivity and environmental stability (such as oxygen-resistant moisture). Early, the QD layer is sandwiched between the P-type and N-type GaN (EQE <0.01%). Later, the QLLDS of all inorganic CTLs composed of metal oxides such as ZnO, SnO2, ZnS, NIO, and WO3 occurred. These devices exhibit strong stability under long-term use and high current density conditions, which is extremely advantageous for future flexible display applications.
However, due to the degradation of QDS during the harsh deposition of the inorganic layer, the overall equipment performance is poor. This type (IV) structure (usually organic HTLS and inorganic ETLS) is developed in order to use the advantages of inorganic and organic CTLs. Despite the initial work, their performance did not increase significantly (0.2% of EQE), but the ZnO nanoparticles were introduced into ETLs as an important breakthrough. Even in the form of nanoparticles, ZnO also exhibits good electron migration capabilities. When these nanoparticles are introduced into the device, the QD layer of the underlying layer does not undermine significantly.
At present, due to the excellent performance of ZnO nanoparticles, it has become a standard for QLED research, including flexible devices. Another important advantage of these devices is the ultra-thin overall layer (hundreds of nanometers), which makes them suitable for flexible displays. For example, a recent study showed that the total thickness of such a highly deformable wearable luminescent diode is less than 3 μm, including device components and a double layer package layer.
Existing Problems
The quantum dot of QLED is susceptible to the disadvantage of heat and moisture, and cannot achieve the same vapor deposition method as self-exhibiting OLED. So we can only develop an inkjet printing process. QLED technology is still in its initial stage. There is a constraint between reliability/efficiency, unstable blue component is unstable, and has difficult solutions. The industry believes that at least 10 years ago at least 10 years.

QLED 8K TV
The "QLED TV" that has already begun is a quantum dot liquid crystal TV with backlight illuminating, which is not called a real QLLD TV (self-luminous). It just adds the quantum dot film on the LCD TV backlight to improve the color gamut. There is still a restriction on the inherent light leakage light, low contrast, poor viewing angle, and slow response speed, etc.
QLED TV
Quantum dot TV is a television that applies a quantum dot technology backlight, a liquid crystal TV.
It is different from traditional LCD TVs in that it uses a different backlight to bring a much different performance. It is more advantageous than traditional LED backlight traditional LCD TVs in screen quality and energy saving. QLED TV has become a new direction of development.

QLED TV
The QLED TV is a television product class with high color gamut, pure chromaticity, and color long. QLED TV is proposed by TCL, and the efficiency and life problem of red green blue three-primary quantum point material developed by QLED technology is broken by TCL.
The quantum dot material used by the QLED TV is an inorganic nanocrystalline, wherein the color gamut coverage rate is 157%, which shows the number of color numbers of 1 billion. QLED TV is 58.3% compared to the color purity of traditional TV. The QLED TV has a long-lasting amount of more than 600,000 hours due to inorganic nanocrystalline material. It is 2 times that of organic material life.
1.Is QLED better than 4K?
If you see a 4K LED TV and a 4K QLED TV, the rule of thumb says that the QLED TV is going to be better in terms of colour accuracy. Although most QLED TVs are sold by Samsung, it does also supply them to TCL and Hisense.
2.Is it worth getting a QLED TV?
QLED TVs are worth buying if you stream movies, games, or shows regularly. If you are looking for a TV with an enhanced brightness display, the layer of quantum dots helps to achieve additional vibrancy compared to a traditional LCD image. Opt for models Q70T and up for the best value for your money.
3.What is the difference between QLED and LED TV?
LED and QLED TVs are similar to each other as they each use LCD panels with LED backlights; the only difference is that QLED TVs use a quantum dot layer that allows them to produce a wider range of colors. LED TVs use the same backlight as QLEDs, but they don't have the quantum dot layer.
Optical Transceiver Guide: How It Works, Types, Form Factors, and SelectionUTMEL24 June 2026774An optical transceiver is the replaceable interface between electronic network equipment and an optical fiber link. It converts electrical data from a switch, router, server, storage system, or transport platform into modulated light, then converts received light back into electrical data.
Read More
Transceivers Shortage Outlook 2026: Supply, Lead Times, and Sourcing OptionsUTMEL09 July 20262623The 2026 transceiver market is defined not by a broad, systemic silicon crisis, but by a highly targeted, structural constraint driven by AI data center build-outs. Figure 3: Power connectors on server racks designed for intense workloads.
Read More
The Introduction to Common Tools and Using Methods of Fiber OpticUTMEL07 January 20227596The building and maintenance of optical cables in the intelligent industry has gradually expanded with the rapid expansion of the Internet of Things and 5G technologies, resulting in an increase in demand for various optical fiber tools. Cutting shears, for example, come in a variety of shapes and sizes, and each tool serves a different purpose. Do you have any experience with them? When should you utilize certain fiber optic tools?
Read More
What are Fiber Optic Patch Cables?UTMEL11 February 20228562Hello everyone, I am Rose. Today I will introduce fiber optic patch cables to you. Optical fiber communication, as an emerging technology, has become one of the main pillars of modern communication and plays a critical role in modern telecommunication networks, thanks to the rapid growth of traffic data.
Read More
Basis of Fiber Optic and Fiber Optic CommunicationUTMEL22 October 20215531Hello everyone, I am Rose. Today I will introduce fiber optic to you. Fiber Optic is a type of glass or plastic fiber that can be utilized to transmit light. It is mostly used for communication. This article will show you the basic knowledge of fiber optic and fiber optic communication.
Read More
Subscribe to Utmel !
19-217/R6C-AL1M2VY/3TEverlight Electronics Co Ltd
AFBR-2418TZBroadcom Limited
SFH 4713AOSRAM Opto Semiconductors Inc.
SML-S13RTT86ROHM Semiconductor
MSL0104RGBU1ROHM Semiconductor
LUW GVCP-EBFB-GMKM-1-140-R18-ZOSRAM Opto Semiconductors Inc.
SMLP36RGB1W3ROHM Semiconductor
120PSB-Visual Communications Company - VCC
SLI-343P8G3FROHM Semiconductor
SLI-343P8C3FROHM Semiconductor


Product
Brand
Articles
Tools