Capacitor Energy and Time Constant Calculator Overview
The Capacitor Energy and Time Constant Calculator helps calculate two common capacitor values: the energy stored in a capacitor and the RC time constant of a resistor-capacitor circuit. By entering voltage, capacitance, and resistance, users can estimate stored energy in joules and the time response of a capacitor during charging or discharging.
This calculator is useful for power supply design, timing circuits, pulse circuits, capacitor discharge checks, backup energy estimates, filter design, and general electronics troubleshooting. It is also helpful when comparing capacitor sizes, resistor values, and expected charge or discharge times.
Use this tool as a first-pass design aid. Real circuits may also be affected by capacitor tolerance, equivalent series resistance, leakage current, dielectric absorption, temperature, voltage rating, resistor tolerance, and the source or load impedance around the RC network.

What This Calculator Can Calculate
Capacitor energy, the electrical energy stored in the capacitor at a given voltage.
RC time constant, the time scale that describes how quickly a capacitor charges or discharges through a resistor.
Charge and discharge behavior, using standard exponential RC circuit relationships.
Approximate time to near-full charge or discharge, often estimated as about five time constants.
Input Parameters Explained
| Input | Meaning | Typical Unit |
|---|---|---|
| Voltage | The voltage across the capacitor or the final charging voltage. | V |
| Capacitance | The capacitance value of the capacitor. | F, mF, uF, nF, or pF |
| Resistance | The series resistance or load resistance through which the capacitor charges or discharges. | Ohm, kOhm, or MOhm |
Output Parameters Explained
| Output | Meaning |
|---|---|
| Energy | The amount of electrical energy stored in the capacitor at the entered voltage. |
| Time Constant | The RC value that describes how fast the capacitor voltage changes. |
| 5 Time Constants | A common estimate for practical full charge or discharge, about 99.3% complete. |
Capacitor Energy Formula
The energy stored in a capacitor is:
E = 0.5 * C * V2
Equivalent forms are:
E = Q * V / 2
E = Q2 / (2 * C)
Where:
E = stored energy in joules
C = capacitance in farads
V = capacitor voltage in volts
Q = charge in coulombs
Energy increases with the square of voltage. Doubling the voltage stores four times as much energy in the same capacitor, so voltage rating and discharge safety are important in real circuits.
RC Time Constant Formula
The RC time constant is:
tau = R * C
Where:
tau = time constant in seconds
R = resistance in ohms
C = capacitance in farads
One time constant is the time required for a charging capacitor to reach about 63.2% of its final voltage, or for a discharging capacitor to fall to about 36.8% of its initial voltage.

Capacitor Charging and Discharging Equations
For a capacitor charging from 0 V toward a supply voltage:
VC(t) = VS * (1 - e-t/RC)
For a capacitor discharging from an initial voltage:
VC(t) = V0 * e-t/RC
Where:
VC(t) = capacitor voltage at time t
VS = source voltage
V0 = initial capacitor voltage
t = elapsed time in seconds
RC = time constant in seconds

Example Calculation
Suppose a circuit uses:
Voltage: 12 V
Capacitance: 1000 uF = 0.001 F
Resistance: 10 kOhm = 10000 Ohm
The capacitor energy is:
E = 0.5 * 0.001 * 122 = 0.072 J
The time constant is:
tau = 10000 * 0.001 = 10 s
The capacitor will reach about 63.2% of the final voltage after 10 seconds and about 99.3% after 50 seconds.
RC Charging Table
| Time | RC Value | Capacitor Voltage During Charging | Charging Current |
|---|---|---|---|
| 0.5 time constant | 0.5 tau | 39.3% | 60.7% |
| 0.7 time constant | 0.7 tau | 50.3% | 49.7% |
| 1.0 time constant | 1 tau | 63.2% | 36.8% |
| 2.0 time constants | 2 tau | 86.5% | 13.5% |
| 3.0 time constants | 3 tau | 95.0% | 5.0% |
| 4.0 time constants | 4 tau | 98.2% | 1.8% |
| 5.0 time constants | 5 tau | 99.3% | 0.7% |
RC Discharging Table
| Time | RC Value | Capacitor Voltage During Discharge | Discharge Current |
|---|---|---|---|
| 0.5 time constant | 0.5 tau | 60.7% | 39.3% |
| 0.7 time constant | 0.7 tau | 49.7% | 50.3% |
| 1.0 time constant | 1 tau | 36.8% | 63.2% |
| 2.0 time constants | 2 tau | 13.5% | 86.5% |
| 3.0 time constants | 3 tau | 5.0% | 95.0% |
| 4.0 time constants | 4 tau | 1.8% | 98.2% |
| 5.0 time constants | 5 tau | 0.7% | 99.3% |
How to Use This Calculator
Enter the capacitor voltage in volts.
Enter the capacitance value and convert it to the unit expected by the calculator.
Enter the resistance value through which the capacitor charges or discharges.
Calculate stored energy and RC time constant.
Use one time constant for the 63.2% charge point or 36.8% discharge point.
Use five time constants for a practical full charge or discharge estimate.
Check the capacitor voltage rating, discharge current, and resistor power rating before using the circuit.
Unit Conversion Tips
| Quantity | Conversion |
|---|---|
| 1 mF | 0.001 F |
| 1 uF | 0.000001 F |
| 1 nF | 0.000000001 F |
| 1 pF | 0.000000000001 F |
| 1 kOhm | 1000 Ohm |
| 1 MOhm | 1000000 Ohm |
How to Read the Results
| Result | What It Means | Design Check |
|---|---|---|
| Energy | The stored energy available in the capacitor at the entered voltage. | Check discharge safety and pulse current requirements. |
| Time constant | The RC response time of the circuit. | Compare it with the required timing, delay, or filter response. |
| 5 tau | Approximate practical full charge or discharge time. | Use this when estimating reset delays, discharge wait time, or startup behavior. |
| Initial current | For charging or discharge through a resistor, the initial current is approximately V/R. | Check resistor power and source or switch current rating. |
Practical Design Notes
Capacitor voltage rating should be higher than the maximum expected circuit voltage.
Electrolytic capacitors have polarity and should not be reverse-biased unless designed for it.
Capacitance tolerance can be wide, especially for electrolytic and ceramic capacitors.
Ceramic capacitance can decrease significantly under DC bias.
Equivalent series resistance affects ripple current, heating, and pulse behavior.
Leakage current affects long time constants and energy storage over long periods.
Discharge resistors need suitable voltage and power ratings.
Large capacitors can store hazardous energy even after power is removed.
Common Mistakes to Avoid
Forgetting to convert microfarads to farads before using the formula.
Assuming a capacitor is fully charged after only one time constant.
Ignoring capacitor tolerance and leakage current in long-delay circuits.
Using a resistor with insufficient power rating during discharge.
Ignoring the initial surge current when charging a large capacitor.
Assuming the capacitor voltage rating can equal the operating voltage with no margin.
Touching or shorting a charged capacitor without verifying it is safely discharged.
When This Calculator Is Not Enough
This calculator is best for simple RC timing and stored-energy estimates. More detailed analysis is needed for high-voltage capacitor banks, pulsed power circuits, switching power supplies, supercapacitor backup systems, precision timing circuits, high-frequency filters, and circuits where ESR, ESL, leakage, or dielectric absorption matters.
For final designs, verify capacitor ratings, resistor power, thermal behavior, discharge safety, and circuit behavior with datasheet values and bench measurements.
Helpful Video Reference
How To Calculate The Energy Stored In a Capacitor
Frequently Asked Questions
What is the energy stored in a capacitor?
It is the electrical energy stored in the capacitor's electric field. It is calculated with E = 0.5 * C * V2.
What does the RC time constant mean?
The RC time constant is the product of resistance and capacitance. It describes how quickly the capacitor voltage rises or falls in a resistor-capacitor circuit.
Why is one time constant 63.2%?
Capacitor charging follows an exponential curve. After one time constant, the capacitor voltage reaches 1 - e-1, or about 63.2% of its final value.
How long does a capacitor take to fully charge?
In theory, it approaches the final voltage asymptotically. In practical electronics, five time constants is commonly treated as nearly fully charged.
Can a charged capacitor be dangerous?
Yes. Large or high-voltage capacitors can store hazardous energy. Always discharge and verify the voltage before handling the circuit.
Does capacitor energy depend on resistance?
Stored energy depends on capacitance and voltage. Resistance affects how quickly the capacitor charges or discharges, not the final stored energy for a given voltage.


Product
Brand
Articles
Tools