web counter
Inductance Conversion

The inductance conversion tool converts the measurement of inductance between units of differing scale, from picohenries (pH) to kilohenries (kH), and units in between. Enter value into any box of unit scale. The conversion results will immediately show in all boxes.

Inductance Conversion

Picohenry
pH
Nanohenry
nH
Microhenry
µH
Millihenry
mH
Henry
H
Kilohenry
kH

pH, nH and µH Conversion Chart

Introduction

What is Inductor - An inductor is a passive electronic component that storesenergy in the form of a magnetic field.

What is Inductor? What is inductance?

Inductance Conversion Overview

The Inductance Conversion tool converts inductance values between henries and units with SI prefixes, including kilohenries, henries, millihenries, microhenries, nanohenries, and picohenries. Enter a value in any supported unit to display the equivalent values in the other units.

Inductance describes the relationship between changing current, magnetic flux linkage, and induced voltage. The SI unit of inductance is the henry, symbol H. In electronic circuits, mH, µH, and nH are much more common than whole henries.

How to Use the Inductance Converter

  1. Find the input field for the inductance unit you already know.

  2. Enter the numerical value.

  3. Confirm the prefix and symbol, including uppercase and lowercase letters.

  4. Read the converted results in the other units.

  5. Keep enough significant digits for the component tolerance and intended calculation.

  6. When selecting a real inductor, also verify the datasheet's measurement frequency, current, tolerance, and temperature conditions.

General Inductance Conversion Formula

Each inductance unit can be represented by a factor in henries. To convert from one unit to another:

Target value = Source value × Source factor in H / Target factor in H

For example, one millihenry equals 0.001 H and one microhenry equals 0.000001 H. Therefore:

1 mH = 0.001 / 0.000001 = 1000 µH

What Is Inductance?

An inductor stores energy in a magnetic field when current flows through it. A changing current produces a voltage across the inductance. Using the passive sign convention for an ideal inductor:

v(t) = L × di(t) / dt

Where:

  • v(t) = voltage across the inductor in volts

  • L = inductance in henries

  • di(t)/dt = rate of change of current in amperes per second

If induced electromotive force is written with a reference polarity opposing the current change, the same physical relationship may appear with a negative sign according to Lenz's law. The sign depends on the selected voltage and current reference directions.

Inductance voltage and current-change formula

Definition of the Henry

One henry is the inductance for which a current changing at one ampere per second corresponds to one volt across the inductor under the stated reference convention.

The henry can be expressed using other SI units:

  • 1 H = 1 Wb/A

  • 1 H = 1 V·s/A

  • 1 H = 1 Ω·s

Wb/A is not a different-sized unit. One weber per ampere is exactly one henry.

SI Inductance Units and Prefixes

UnitSymbolEquivalent in Henries
ExahenryEH1018 H
PetahenryPH1015 H
TerahenryTH1012 H
GigahenryGH109 H
MegahenryMH106 H
KilohenrykH103 H
HectohenryhH102 H
DekahenrydaH10 H
HenryH1 H
DecihenrydH10-1 H
CentihenrycH10-2 H
MillihenrymH10-3 H
MicrohenryµH10-6 H
NanohenrynH10-9 H
PicohenrypH10-12 H
FemtohenryfH10-15 H
AttohenryaH10-18 H

Common Inductance Relationships

Starting UnitEquivalent Values
1 H1000 mH = 1000000 µH = 1000000000 nH = 1000000000000 pH
1 mH0.001 H = 1000 µH = 1000000 nH
1 µH0.001 mH = 1000 nH = 1000000 pH
1 nH0.001 µH = 1000 pH
1 pH0.001 nH = 0.000001 µH

pH, nH, and µH Conversion Chart

The following original chart provides a visual reference for commonly used small inductance units.

Picohenry nanohenry and microhenry conversion chart

Prefix Capitalization Matters

SI symbols are case-sensitive. A change in capitalization can represent an enormous difference in value.

SymbolsMeaningsDifference
MH and mHMegahenry and millihenryMH is 1000000000 times mH.
PH and pHPetahenry and picohenryPH is 1027 times pH.
H and hHHenry and hectohenry1 hH = 100 H.
µH and uHMicrohenry and an ASCII substituteµH is the proper SI form; uH is often used when µ is unavailable.

In an inductance context, pH means picohenry. It should not be confused with pH as a measure of acidity in chemistry.

Worked Inductance Conversion Examples

Millihenries to Microhenries

Convert 4.7 mH to microhenries:

4.7 × 1000 = 4700 µH

The same value is 0.0047 H or 4700000 nH.

Microhenries to Millihenries

Convert 220 µH to millihenries:

220 / 1000 = 0.22 mH

The same value is 0.00022 H or 220000 nH.

Nanohenries to Picohenries

Convert 68 nH to picohenries:

68 × 1000 = 68000 pH

The same value is 0.068 µH.

Kilohenries to Henries

Convert 2.5 kH to henries:

2.5 × 1000 = 2500 H

Historical Non-SI Inductance Units

UnitApproximate SI EquivalentUse
Abhenry, abH1 abH = 10-9 HHistorical electromagnetic CGS unit
Stathenry, stH1 stH ≈ 8.987552 × 1011 HHistorical electrostatic CGS unit
Weber per ampere1 Wb/A = 1 HEquivalent SI expression

Historical CGS units are rarely used in current component specifications. Confirm the original unit system before converting archival material.

Inductance Is Not Inductive Reactance

Inductance L is a component property measured in henries. Inductive reactance XL is the frequency-dependent opposition to AC and is measured in ohms:

XL = 2 × π × f × L

A unit conversion changes how the same inductance is expressed. It does not calculate reactance unless frequency is also provided.

Reactance Example

A 10 mH inductor has L = 0.01 H. At 1 kHz:

XL = 2 × π × 1000 × 0.01 = 62.832 Ω

At 10 kHz, the same ideal inductance has ten times the reactance, approximately 628.319 Ω.

Energy Stored in an Inductor

The ideal magnetic energy stored at current I is:

E = 0.5 × L × I2

Where E is energy in joules, L is inductance in henries, and I is current in amperes. Convert the inductance to henries before applying this equation.

Stored Energy Example

For L = 100 µH = 0.0001 H and I = 2 A:

E = 0.5 × 0.0001 × 22 = 0.0002 J = 0.2 mJ

Series and Parallel Inductors

For ideal uncoupled inductors in series:

LTOTAL = L1 + L2 + ... + LN

For ideal uncoupled inductors in parallel:

1 / LTOTAL = 1 / L1 + 1 / L2 + ... + 1 / LN

These simple formulas do not apply unchanged when the inductors are magnetically coupled. Mutual inductance and winding polarity must then be included.

Reading Inductor Datasheets

A converted nominal value is only one part of inductor selection. Check the datasheet for:

  • Tolerance: the permitted range around nominal inductance.

  • Test frequency: the frequency at which inductance is specified.

  • Test signal level: the small-signal voltage or current used for measurement.

  • DC resistance: winding resistance and copper loss.

  • Rated current: current associated with temperature rise or another stated criterion.

  • Saturation current: current at which inductance falls by a specified amount.

  • Self-resonant frequency: the frequency where parasitic capacitance changes behavior.

  • Q factor: a frequency-dependent measure related to reactance and loss.

  • Temperature range: operating and storage limits.

Manufacturers may define rated current and saturation current differently. Compare the stated test methods rather than relying only on the current number.

Why Measured Inductance Can Change

  • Core permeability changes with frequency, temperature, and DC bias.

  • Magnetic saturation reduces incremental inductance at high current.

  • Parasitic capacitance affects the measured result near self-resonance.

  • Fixture and lead inductance matter when measuring very small values.

  • Winding geometry and nearby conductive or magnetic materials can affect inductance.

  • Instrument test frequency and equivalent-circuit mode can change the reported value.

Typical Inductance Ranges and Applications

Inductance ScaleCommon Examples
pH to low nHPackage, lead, PCB trace, and interconnect parasitic inductance
nH to µHRF matching, high-frequency chokes, and compact power inductors
µH to mHSwitching converters, filters, EMI chokes, and energy storage
mH to HAudio filters, low-frequency chokes, sensors, relays, and transformers

These ranges are broad orientation only. The correct value and construction depend on frequency, current, loss, size, voltage, and application requirements.

Common Inductance Conversion Mistakes

  • Confusing MH with mH or PH with pH.

  • Reading µH as mH.

  • Moving the decimal three places in the wrong direction.

  • Confusing inductance in henries with reactance in ohms.

  • Using a converted nominal value without considering tolerance.

  • Ignoring the frequency and current conditions used to specify inductance.

  • Using the uncoupled-inductor formula for magnetically coupled windings.

  • Assuming measured inductance remains constant near saturation or self-resonance.

  • Ignoring fixture and trace inductance when measuring nH or pH values.

  • Comparing current ratings from different manufacturers without reading their definitions.

Frequently Asked Questions

What is the SI unit of inductance?

The SI unit of inductance is the henry, symbol H.

How many microhenries are in one millihenry?

One millihenry equals 1000 microhenries.

How many nanohenries are in one microhenry?

One microhenry equals 1000 nanohenries.

How many picohenries are in one nanohenry?

One nanohenry equals 1000 picohenries.

Is Wb/A the same as H?

Yes. One weber per ampere is exactly one henry.

Is inductance the same as impedance?

No. Inductance is measured in henries. An ideal inductor's impedance is j2πfL and depends on frequency.

Why does an inductor value change with current?

Magnetic core permeability can change with DC bias, and the core may approach saturation. Datasheets commonly specify how much inductance decreases at a stated saturation current.

Why is measurement frequency important?

Core behavior, winding resistance, and parasitic capacitance are frequency-dependent. The measured inductance may therefore differ when test frequency changes.

Can I add inductors directly?

Uncoupled ideal inductors in series add directly. Magnetically coupled inductors require mutual-inductance and polarity analysis.

Related Online Calculation Tools

Frequently Asked Questions

What is the value of 1 Henry?

Henry, unit of either self-inductance or mutual inductance, abbreviated H, and named for the American physicist Joseph Henry. One henry is the value of self-inductance in a closed circuit or coil in which one volt is produced by a variation of the inducing current of one ampere per second.

How do you convert Henry to ohms?

Inductance is frequently expressed as micro-Henries, which represents 1,000,000 Henries. To convert to Henries, you would divide the number of micro-Henries by 1,000,000. Calculate reactance, in ohms, by using the formula: Reactance = 2 * pi * Frequency * Inductance. Pi is simply a constant, measured as 3.14.

What is mH inductance?

The henry (symbolized H) is the Standard International ( SI ) unit of inductance. In audio-frequency ( AF ) and radio-frequency ( RF ) applications, units of millihenrys (mH), where 1 mH = 10 -3 H, and microhenrys (µH), where 1 µH = 10 -6 H, are common.

How do you calculate inductance?

The formula is: The micro henrys of inductance in a coil = (N^2)(D^2)/(18D + 40L) where "N" equals the number of rings in the coil, "D" equals the diameter of the coil and "L" equals the length of the coil.

Why is inductance measured in Henrys?

Inductance is measured in units called henrys. The definition of one henry is simple: One henry is the amount of inductance necessary to induce one volt when the current in coil changes at a rate of one ampere per second.

How do you convert inductance to ohms?

The unit of a inductance is a 1H - henry. So, to get Ohms divide by one second. That's only after you divide the applied voltage by the measured inductor current for a period of one second.

What is the SI unit of self inductance of a coil?

Henry Henry (symbol H) is the SI derived unit of self-inductance.

What is mH Electrical?

Inductance. An inductor is a passive electronic component that stores energy in the form of a magnetic field. The standard unit of inductance is the henry abbreviated H. This is a large unit and more commonly used units are the microhenry abbreviated μH (1 μH =10-6H) and the millihenry abbreviated mH (1 mH =10-3 H).

What is the unit of inductance 1 point?

The unit of inductance in the SI system is the henry (H), named after American scientist Joseph Henry, which is the amount of inductance which generates a voltage of one volt when the current is changing at a rate of one ampere per second.

What is XL in inductance?

XL = inductive reactance on ohms, Ω π = Greek letter Pi, 3.142. f = frequency in Hz. L = inductance in henries.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

TP3420AV309TP3420AV309Texas InstrumentsInterface - Telecom20-LCC (J-Lead)IC TELECOM INTERFACE 20PLCC-

In stock

Minimum: 1

19-217/R6C-AL1M2VY/3T19-217/R6C-AL1M2VY/3TEverlight Electronics Co LtdLED Indication - Discrete0603 (1608 Metric)LED RED CLEAR 2SMD-

In stock : 6070

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock : 10000

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP
  • 1:$0.521267
  • 10:$0.491761
  • 100:$0.463925
  • 500:$0.437666

In stock : 1000

Minimum: 1

HMC588LC4BTRHMC588LC4BTRAnalog Devices Inc.RF Misc ICs and Modules24-TFQFN Exposed PadIC OSC VCO WIDEBAND 24SMD-

In stock : 5

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

DS21Q48NDS21Q48NMaxim IntegratedInterface - Telecom144-BBGAIC LIU E1/T1/J1 4X 5V LONG144BGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

EEF-CS1E150REEF-CS1E150RPanasonic Electronic ComponentsAluminum - Polymer Capacitors2917 (7343 Metric)Aluminum Organic Polymer Capacitors 15uF 25volt
  • 1:$0.597914
  • 10:$0.564069
  • 100:$0.532141
  • 500:$0.502020

In stock : 28000

Minimum: 1

AFBR-2418TZAFBR-2418TZBroadcom LimitedFiber Optics - Receivers-Fiber Optic Transmitters, Receivers, Transceivers RX DC-50MBd ML 820nm ST Thrd-

In stock : 660

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock : 6000

Minimum: 1

TZY2Z060AC01R00TZY2Z060AC01R00Murata ElectronicsTrimmers, Variable Capacitors-2.5 ~ 6pF Trimmer Capacitor 25V Top Adjustment-

In stock : 4636

Minimum: 1

SML-S13RTT86SML-S13RTT86ROHM SemiconductorInfrared, UV, Visible Emitters1206 (3216 Metric)EMITTER IR 850NM 30MA 1206-

In stock : 1

Minimum: 1

TZY2Z100AC01R00TZY2Z100AC01R00Murata ElectronicsTrimmers, Variable Capacitors-3 ~ 10pF Trimmer Capacitor 25V Top Adjustment-

In stock : 22000

Minimum: 1

DGD2136S28-13DGD2136S28-13Diodes IncorporatedPMIC - Gate Drivers28-SOIC (0.295, 7.50mm Width)HV GATE DRIVER SO-28-

In stock : 2799

Minimum: 1

TEN-HS5TEN-HS5Traco PowerAccessoriesAluminumTRACOPOWER TEN-HS5 Power Supply Accessory, Heat Sink, DC/DC Converter, TEN25, TEN25WI Series
  • 1:$3.817981
  • 10:$3.601869
  • 100:$3.397990
  • 500:$3.205651

In stock : 255

Minimum: 1

HEF4044BT,652HEF4044BT,652NXP USA Inc.Logic - Latches16-SOIC (0.154, 3.90mm Width)IC R/S LATCH 3-STATE QUAD 16SOIC-

In stock

Minimum: 1

T9GV5L14-22T9GV5L14-22TE ConnectivityRelays-Power Relays, Standard, Monostable, DC, 900 mW Coil Power Rating DC, 538 Ω Coil Resistance, UL Coil Insulation Class F, Potter & Brumfield T9G-

In stock : 31

Minimum: 1