Series and Parallel Capacitor Calculator Overview
The Series and Parallel Capacitor Calculator calculates the equivalent capacitance of multiple capacitors connected in series or in parallel. It is useful when you need to combine available capacitor values, estimate timing capacitance, increase total capacitance, or reduce equivalent capacitance in a circuit.
Enter the capacitor values you want to combine and leave unused fields blank. The calculator can then return the total capacitance for the selected connection type. If you need to calculate more capacitors than the input fields allow, calculate a group first, then use that equivalent value as one input in the next calculation.

Capacitors in Series Formula
For capacitors connected in series:
1 / Ctotal = 1 / C1 + 1 / C2 + 1 / C3 + ... + 1 / Cn
For two capacitors in series, the formula can be simplified to:
Ctotal = (C1 × C2) / (C1 + C2)
In a series connection, the equivalent capacitance is always smaller than the smallest individual capacitor in the chain. Series connection is often used when designers need a lower capacitance value or a higher total voltage rating, but voltage sharing must still be checked carefully.
Capacitors in Parallel Formula
For capacitors connected in parallel:
Ctotal = C1 + C2 + C3 + ... + Cn
In a parallel connection, all capacitors share the same voltage, and the total capacitance is the sum of the individual capacitances. Parallel connection is commonly used to increase capacitance, reduce equivalent series resistance, improve ripple-current capability, or provide both bulk storage and high-frequency decoupling.
Series vs Parallel Capacitors
| Connection | Total Capacitance | Voltage Behavior | Common Use |
|---|---|---|---|
| Series | Less than the smallest capacitor. | Voltage divides across the capacitors. | Reducing capacitance or increasing voltage capability with proper balancing. |
| Parallel | Sum of all capacitor values. | Each capacitor sees the same voltage. | Increasing capacitance, reducing ESR, or adding decoupling over a wider frequency range. |
Supported Capacitance Units
| Unit | Name | Value in Farads |
|---|---|---|
| F | farad | 1 F |
| mF | millifarad | 0.001 F |
| µF | microfarad | 0.000001 F |
| nF | nanofarad | 0.000000001 F |
| pF | picofarad | 0.000000000001 F |
Example: Capacitors in Series
Suppose three capacitors are connected in series:
C1 = 10 µF, C2 = 22 µF, C3 = 47 µF
The reciprocal calculation is:
1 / Ctotal = 1 / 10 + 1 / 22 + 1 / 47
1 / Ctotal ≈ 0.1667
Ctotal ≈ 6.0 µF
The result is lower than 10 µF, which is the smallest capacitor in the series string.
Example: Capacitors in Parallel
Suppose the same three capacitors are connected in parallel:
C1 = 10 µF, C2 = 22 µF, C3 = 47 µF
Ctotal = 10 + 22 + 47 = 79 µF
In this case, the equivalent capacitance is the sum of the individual capacitance values.
How to Use the Calculator
First choose whether the capacitors are connected in series or in parallel. Enter each capacitance value and select the correct unit. Leave unused input fields blank. The calculator converts the entered values to a common unit, applies the correct formula, and returns the equivalent capacitance.
If you are combining capacitor values from different unit scales, such as 0.1 µF and 100 nF, make sure the unit selected for each value is correct. Those two values are equal, so entering the wrong unit can create a large error.
Voltage Rating and Safety Notes
Equivalent capacitance is only one part of capacitor selection. You must also check voltage rating, ripple current, leakage current, temperature rating, ESR, dielectric type, tolerance, polarity, and safety certification when the circuit requires it.
In a series capacitor string, voltage does not always divide equally. Leakage current and capacitance tolerance can cause one capacitor to see more voltage than another. High-voltage series strings often require balancing resistors or an active balancing method. Always follow the capacitor manufacturer's recommendations.
Capacitors can store dangerous energy after power is removed. Discharge high-voltage or large-value capacitors safely before handling the circuit.
Practical Effects Beyond Capacitance
| Parameter | Why It Matters |
|---|---|
| Tolerance | The actual capacitance may differ from the marked value, especially for electrolytic and Class 2 ceramic capacitors. |
| ESR | Equivalent series resistance affects ripple current, heating, filtering, and transient response. |
| ESL | Equivalent series inductance affects high-frequency behavior and decoupling performance. |
| Leakage current | Leakage affects long timing circuits, sample-and-hold circuits, and voltage sharing in series strings. |
| DC bias effect | Some ceramic capacitors lose effective capacitance when a DC voltage is applied. |
| Polarity | Polarized capacitors must be connected with the correct polarity unless the circuit and part type allow otherwise. |
Common Mistakes to Avoid
| Mistake | Correct Approach |
|---|---|
| Adding capacitor values in series. | Use the reciprocal formula for series capacitors. |
| Using the reciprocal formula for parallel capacitors. | Parallel capacitance is the direct sum of the values. |
| Assuming series capacitors share voltage equally. | Check leakage, tolerance, and balancing requirements. |
| Ignoring units. | Convert mF, µF, nF, and pF correctly before comparing values. |
| Ignoring real capacitor behavior. | Check ESR, ESL, ripple current, dielectric, and DC bias effects. |
FAQ
Why is total capacitance smaller in series?
In a series connection, each capacitor carries the same charge, and the total voltage is divided among the capacitors. The equivalent capacitance therefore follows the reciprocal sum and becomes smaller than any individual capacitor.
Why does capacitance add in parallel?
In a parallel connection, all capacitors share the same voltage. The total stored charge is the sum of the charge on each capacitor, so the equivalent capacitance is the sum of their capacitances.
Can I increase voltage rating by putting capacitors in series?
It can be done, but voltage sharing must be controlled. Use capacitors with suitable ratings and follow manufacturer guidance for balancing resistors or active balancing, especially in high-voltage circuits.
Can I mix different capacitor types in parallel?
Yes, when the voltage, polarity, ripple current, and frequency behavior are suitable. Designers often place a large bulk capacitor in parallel with smaller ceramic capacitors for decoupling over a wider frequency range.
Related Online Calculation Tools
Capacitor Energy and Time Constant Calculator - calculates capacitor energy and RC time constant values.
Parallel and Series Resistor Calculator - calculates equivalent resistance for series and parallel resistor networks.
Ohm's Law Calculator - calculates voltage, current, resistance, and power.
Capacitor Conversion Calculator - converts capacitance values between common units.


Product
Brand
Articles
Tools