web counter
Length Conversion

Use this length conversion tool to convert between commonly used length units. Select the current unit in the upper column, the desired unit in the lower column, and enter a value in the upper column to generate the resulting conversion. You can choose multiple units from kilometers (km), miles (mi), nautical miles (nmi), meter (m), yards (yd), inches (in), feet (ft) centimeters (cm) up to nanometers.

Length Conversion

Input Type
To
Output Type

Conversion

1 cm = 0.393701 in

Introduction

Convert Metric Units of Length with mm, cm, m, and km conversions?

How do you convert metric lengths?

Length Conversion Overview

The Length Conversion tool converts values between metric, SI, U.S. customary, Imperial, nautical, and selected engineering length units. Enter a value in one supported unit to calculate its equivalent in kilometers, meters, centimeters, millimeters, micrometers, nanometers, inches, feet, yards, miles, nautical miles, and other units.

Length describes the distance between two points or the linear extent of an object. The metre, symbol m, is the SI base unit of length. Other metric units are related to the metre by powers of ten, while the international inch, foot, yard, and mile are defined by exact relationships to the metre.

How to Use the Length Converter

  1. Select the unit of the value you already know.

  2. Enter the length or distance.

  3. Select the unit required for the result.

  4. Read the converted value.

  5. Keep extra digits during calculation and round the final result appropriately.

  6. For survey or legacy data, confirm whether the original measurement used the international foot or the former U.S. survey foot.

General Length Conversion Formula

Each unit can be represented by a conversion factor in metres. To convert from one unit to another:

Target value = Source value × Source factor in metres / Target factor in metres

For example, one inch equals exactly 0.0254 m. To convert 20 inches to centimeters:

20 in × 0.0254 m/in × 100 cm/m = 50.8 cm

SI and Metric Length Units

UnitSymbolEquivalent in Metres
MegametreMm1000000 m
Kilometrekm1000 m
Hectometrehm100 m
Dekametredam10 m
Metrem1 m
Decimetredm0.1 m
Centimetrecm0.01 m
Millimetremm0.001 m
Micrometreµm0.000001 m
Nanometrenm0.000000001 m
Picometrepm0.000000000001 m

SI symbols are case-sensitive. Mm means megametre, while mm means millimetre. The difference is a factor of one billion.

Common Metric Relationships

Starting UnitEquivalent Values
1 km1000 m = 100000 cm = 1000000 mm
1 m100 cm = 1000 mm = 1000000 µm
1 cm10 mm = 10000 µm
1 mm1000 µm = 1000000 nm
1 µm1000 nm

International Inch, Foot, Yard, and Mile

UnitSymbolExact DefinitionMetric Equivalent
Inchin1/12 ft25.4 mm
Footft12 in0.3048 m
Yardyd3 ft = 36 in0.9144 m
Statute milemi5280 ft = 1760 yd1609.344 m

These international definitions are used for ordinary modern U.S. customary and Imperial length conversion. The names U.S. customary and Imperial describe different measurement traditions, but the modern international inch, foot, yard, and mile share these same defined lengths.

Common Cross-System Conversions

Starting UnitEquivalent Values
1 mm0.1 cm = 0.001 m = 0.0393700787 in
1 cm10 mm = 0.01 m = 0.3937007874 in
1 m1000 mm = 100 cm = 39.37007874 in = 3.280839895 ft = 1.093613298 yd
1 km1000 m = 0.6213711922 mi = 0.5399568035 nmi
1 in25.4 mm = 2.54 cm = 0.0254 m
1 ft12 in = 30.48 cm = 0.3048 m
1 yd3 ft = 36 in = 0.9144 m
1 mi5280 ft = 1760 yd = 1.609344 km

Nautical Length Units

UnitSymbolEquivalent LengthTypical Use
International nautical milenmi1852 m exactlyMarine and aviation distance
Fathom based on the international footftm6 ft = 1.8288 mWater depth and nautical use
Cable length based on 120 fathomscable720 ft = 219.456 mSelected nautical and legacy contexts

A knot is not a length unit. It is a speed equal to one nautical mile per hour.

Statute Mile vs. Nautical Mile

UnitMetresKilometres
1 statute mile1609.344 m1.609344 km
1 nautical mile1852 m1.852 km

One nautical mile is approximately 1.15078 statute miles. Use mi for a statute mile and nmi for a nautical mile to prevent ambiguity.

Former U.S. Survey Foot

The former U.S. survey foot was defined as exactly 1200/3937 m, approximately 0.304800609601 m. It is slightly longer than the international foot of exactly 0.3048 m.

Beginning January 1, 2023, NIST guidance says the U.S. survey foot should be avoided except for historical and legacy applications. Modern work should use the international foot unless a source dataset explicitly states that it uses the former survey definition.

DefinitionMetresRecommended Use
International foot0.3048 m exactlyCurrent general and surveying applications
Former U.S. survey foot1200/3937 m exactlyHistorical and legacy data only

Engineering and Precision Length Units

UnitSymbolEquivalent LengthCommon Context
Thousandth of an inchmil or thou0.001 in = 0.0254 mm = 25.4 µmPCB, wire, machining, and material thickness
Micrometreµm0.001 mm = 0.000001 mManufacturing, coatings, and semiconductor features
Nanometrenm0.001 µm = 0.000000001 mOptics, wavelengths, and nanoscale features
AngstromÅ0.1 nm = 0.0000000001 mAtomic dimensions and spectroscopy

In engineering, mil means one thousandth of an inch. It must not be confused with millimetre, abbreviated mm. One mil is 0.0254 mm, not 1 mm.

Selected Survey and Legacy Units

Unit Based on the International FootDefinitionMetric Equivalent
Link0.66 ft0.201168 m
Rod, pole, or perch16.5 ft5.0292 m
Chain66 ft20.1168 m
Furlong660 ft201.168 m
League3 mi4828.032 m

Legacy survey records may use definitions based on the former U.S. survey foot. Do not apply the international-foot factors blindly when reproducing historical coordinates or legal descriptions.

Worked Length Conversion Examples

Inches to Metres

Convert 72 inches to metres:

72 × 0.0254 = 1.8288 m

Kilometres to Miles

Convert 5 km to statute miles:

5 / 1.609344 = 3.10686 mi

Nautical Miles to Kilometres

Convert 10 nautical miles to kilometres:

10 × 1.852 = 18.52 km

Nanometres to Micrometres

Convert 250 nm to micrometres:

250 / 1000 = 0.25 µm

Feet and Inches to Centimetres

Convert 6 ft 4 in to centimetres. First convert the feet to inches:

6 × 12 + 4 = 76 in

Then convert inches to centimetres:

76 × 2.54 = 193.04 cm

Length, Area, and Volume Are Different

A linear conversion factor applies only to length. For area, square the length factor. For volume, cube the length factor.

QuantityInch-to-Metre Relationship
Length1 in = 0.0254 m
Area1 in2 = 0.02542 m2 = 0.00064516 m2
Volume1 in3 = 0.02543 m3 = 0.000016387064 m3

Significant Digits and Rounding

Some conversion relationships, such as 1 in = 25.4 mm, are exact. However, a measured input still has limited accuracy. The converted result should reflect the precision of the original measurement rather than displaying every available calculator digit.

Keep additional digits during intermediate calculations, especially when converting through more than one unit. Round only the final result according to the intended engineering, commercial, or educational use.

Common Length Conversion Mistakes

  • Confusing mm with Mm because SI symbols are case-sensitive.

  • Confusing mil, one thousandth of an inch, with millimetre.

  • Using a statute mile factor for a nautical mile.

  • Using the former U.S. survey foot for new work.

  • Applying a length factor directly to area or volume.

  • Assuming foot and inch values are decimal parts of the same unit.

  • Using micron instead of the preferred unit name micrometre without confirming the symbol.

  • Rounding intermediate values before the final result.

  • Reporting more digits than the original measurement supports.

  • Ignoring thermal expansion or measurement uncertainty in precision work.

Applications

  • Converting PCB dimensions between millimetres and mils.

  • Comparing wire, cable, connector, and enclosure dimensions.

  • Translating mechanical drawings between metric and inch units.

  • Converting road, aviation, and marine distances.

  • Working with optical wavelengths in micrometres or nanometres.

  • Converting construction and surveying measurements.

  • Checking product dimensions for international specifications.

Frequently Asked Questions

What is the SI unit of length?

The metre, symbol m, is the SI base unit of length.

How many millimetres are in one inch?

One international inch equals exactly 25.4 mm.

How many metres are in one foot?

One international foot equals exactly 0.3048 m.

How many kilometres are in one mile?

One statute mile equals exactly 1.609344 km when based on the international foot.

What is the difference between a mile and a nautical mile?

A statute mile is 1609.344 m, while an international nautical mile is 1852 m.

Is the U.S. survey foot still used?

It should be avoided for new work beginning January 1, 2023. It remains relevant when interpreting historical and legacy survey data.

What does mil mean in electronics?

A mil is one thousandth of an inch, equal to 0.0254 mm or 25.4 µm.

Is a micron the same as a micrometre?

Yes. Micron is an older name for the micrometre. The preferred SI name and symbol are micrometre and µm.

Can I use the same factor for square or cubic units?

No. Square the linear factor for area and cube it for volume.

Related Online Conversion Tools

Frequently Asked Questions

How do you convert measurements?

There are just two simple steps: 1.Find a conversion factor between the given units and the desired units, and write it as an equation. 2.Convert that equation to a fraction with the desired units on top and the given units on the bottom.

What length is 1m?

one meter 1m (one meter) is approximately equal to one yard. About 39 inches.

What is length and width?

Definition: Length is the distance from one end to the other end of an object, while width is the distance from side to side. Length is a type of measurement that shows how tall or long an object is.

Is a meter smaller than a foot?

Feet are smaller than meters, so there should be more feet than meters. The conversion is 1 ft = 0.3048 meters.

Is length a height?

The difference between length and height is very precise, as length denotes how long a shape is and height denotes how tall it is. Length is the horizontal measurement in a plane whereas height is the vertical measurement.

What are the examples of length?

The definition of length is how long something is, or the amount of vertical space or time it takes up. An example of length is two hours for a movie. An example of length is 12 inches.

What does 1 cm look like?

1 centimeter is equal to 0.3937 inches, or 1 inch is equal to 2.54 centimeters. ... In other words, 1 centimeter is less than half as big as an inch, so you need about two-and-a-half centimeters to make one inch.

What things are 25 cm?

It's about two-thirds as tall as a Bowling Pin. It's about two-fifths as long as a Woman's Footstep. It's about one-third as long as a Man's Footstep. It's about three-tenths as tall as Verne Troyer. It's about one-fourth as tall as General Tom Thumb. It's about one-fourth as tall as Kenny Baker.

How many times is 1 mm longer than 1cm?

Metric units use a base numbering system of 10. Thus a centimeter is ten times larger than a millimeter.

How many cm go into an inch?

2.54 centimeters The value of 1 inch is approximately equal to 2.54 centimeters. To convert inches to the centimeter values, multiply the given inch value by 2.54 cm.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

TP3420AV309TP3420AV309Texas InstrumentsInterface - Telecom20-LCC (J-Lead)IC TELECOM INTERFACE 20PLCC-

In stock

Minimum: 1

19-217/R6C-AL1M2VY/3T19-217/R6C-AL1M2VY/3TEverlight Electronics Co LtdLED Indication - Discrete0603 (1608 Metric)LED RED CLEAR 2SMD-

In stock : 6070

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock : 10000

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP
  • 1:$0.465882
  • 10:$0.439511
  • 100:$0.414633
  • 500:$0.391163

In stock : 1000

Minimum: 1

HMC588LC4BTRHMC588LC4BTRAnalog Devices Inc.RF Misc ICs and Modules24-TFQFN Exposed PadIC OSC VCO WIDEBAND 24SMD-

In stock : 5

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

DS21Q48NDS21Q48NMaxim IntegratedInterface - Telecom144-BBGAIC LIU E1/T1/J1 4X 5V LONG144BGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

EEF-CS1E150REEF-CS1E150RPanasonic Electronic ComponentsAluminum - Polymer Capacitors2917 (7343 Metric)Aluminum Organic Polymer Capacitors 15uF 25volt
  • 1:$0.593588
  • 10:$0.559988
  • 100:$0.528291
  • 500:$0.498388

In stock : 28000

Minimum: 1

AFBR-2418TZAFBR-2418TZBroadcom LimitedFiber Optics - Receivers-Fiber Optic Transmitters, Receivers, Transceivers RX DC-50MBd ML 820nm ST Thrd-

In stock : 660

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock : 6000

Minimum: 1

TZY2Z060AC01R00TZY2Z060AC01R00Murata ElectronicsTrimmers, Variable Capacitors-2.5 ~ 6pF Trimmer Capacitor 25V Top Adjustment-

In stock : 4636

Minimum: 1

SML-S13RTT86SML-S13RTT86ROHM SemiconductorInfrared, UV, Visible Emitters1206 (3216 Metric)EMITTER IR 850NM 30MA 1206-

In stock : 1

Minimum: 1

TZY2Z100AC01R00TZY2Z100AC01R00Murata ElectronicsTrimmers, Variable Capacitors-3 ~ 10pF Trimmer Capacitor 25V Top Adjustment-

In stock : 22000

Minimum: 1

DGD2136S28-13DGD2136S28-13Diodes IncorporatedPMIC - Gate Drivers28-SOIC (0.295, 7.50mm Width)HV GATE DRIVER SO-28-

In stock : 2799

Minimum: 1

TEN-HS5TEN-HS5Traco PowerAccessoriesAluminumTRACOPOWER TEN-HS5 Power Supply Accessory, Heat Sink, DC/DC Converter, TEN25, TEN25WI Series
  • 1:$3.808917
  • 10:$3.593318
  • 100:$3.389922
  • 500:$3.198040

In stock : 255

Minimum: 1

HEF4044BT,652HEF4044BT,652NXP USA Inc.Logic - Latches16-SOIC (0.154, 3.90mm Width)IC R/S LATCH 3-STATE QUAD 16SOIC-

In stock

Minimum: 1

T9GV5L14-22T9GV5L14-22TE ConnectivityRelays-Power Relays, Standard, Monostable, DC, 900 mW Coil Power Rating DC, 538 Ω Coil Resistance, UL Coil Insulation Class F, Potter & Brumfield T9G-

In stock

Minimum: 1