web counter
Reflection Attenuator Calculator

This reflection attenuator calculator is designed to help in calculating the correct values of the resistor R1 in a reflection attenuator.

Reflection Attenuator Calculator

ATTENUATION (DB)
DB
IMPEDANCE
Ω
R1 > Z0
Ω
R1 < Z0
Ω

FORMULAS

reflection-attenuator-formula-update
reflection-attenuator-chart
Introduction

Learn how to use the Attenuation Interactive Calculator to determine signal power loss for electromagnetic, acoustic, and optical waves through transmission media.

Attenuation Interactive Calculator

Reflection Attenuator Calculator Overview

The Reflection Attenuator Calculator helps calculate the two possible resistor values for a reflection attenuator. Unlike a standard T-pad or pi-pad attenuator, a reflection attenuator uses controlled reflection from matched termination elements to reduce signal level.

Enter the desired attenuation in decibels and the system impedance Z0. The calculator returns two possible values for R1: one value greater than Z0 and one value smaller than Z0. Both solutions can produce the same attenuation magnitude when used in the correct reflection attenuator structure.

Reflection attenuator calculator circuit

What Is a Reflection Attenuator?

A reflection attenuator is an attenuator topology that uses a coupler, hybrid, or similar RF network together with reflective terminations. The attenuation is controlled by the reflection coefficient of the termination resistors. This is different from a purely absorptive attenuator, where resistors dissipate the signal in a direct pad network.

Reflection attenuators are often used in variable attenuator or phase-control circuits because the termination resistance can be switched, varied, or electronically controlled. The practical circuit must be designed so that reflected power is routed correctly by the coupler or hybrid instead of returning to the source in an uncontrolled way.

Reflection Attenuator Formulas

For a desired attenuation entered as a positive dB value:

K = 10^(AdB / 20)

The resistor solution greater than Z0 is:

R1 high = Z0 × (K + 1) / (K - 1)

The resistor solution smaller than Z0 is:

R1 low = Z0 × (K - 1) / (K + 1)

Reflection attenuator resistor equations

SymbolMeaningTypical Unit
R1 highTermination resistor solution greater than the system impedance.Ω
R1 lowTermination resistor solution smaller than the system impedance.Ω
Z0Characteristic impedance of the RF system.Ω
AdBRequired attenuation, entered as a positive loss value.dB
KVoltage loss ratio used to calculate the reflection termination.unitless

Why There Are Two R1 Values

The reflection coefficient of a purely resistive termination depends on how far the resistor is from the system impedance. A resistor above Z0 and a resistor below Z0 can have the same reflection magnitude but opposite reflection sign. That is why the calculator gives two possible resistor values.

When the two values are normalized to Z0, they are reciprocal solutions. For example, in a 50 Ω system, one solution may be much larger than 50 Ω while the other is much smaller than 50 Ω.

Example Calculation

Suppose the desired attenuation is 10 dB in a 50 Ω system.

K = 10^(10 / 20) ≈ 3.162

R1 high = 50 × (3.162 + 1) / (3.162 - 1) ≈ 96.3 Ω

R1 low = 50 × (3.162 - 1) / (3.162 + 1) ≈ 26.0 Ω

Either resistor value can represent the same reflection magnitude in the proper circuit. The correct choice depends on the attenuator architecture, switching device, biasing method, power handling, and the desired phase behavior.

Common Values for a 50 Ω System

AttenuationR1 HighR1 Low
3 dB292.4 Ω8.55 Ω
6 dB150.5 Ω16.6 Ω
10 dB96.3 Ω26.0 Ω
20 dB61.1 Ω40.9 Ω
30 dB53.3 Ω46.9 Ω

These values assume ideal resistive terminations and a matched 50 Ω environment. At high attenuation, both solutions move closer to 50 Ω because the reflected signal becomes smaller.

How to Use the Calculator

Enter the target attenuation as a positive dB value. Then enter the characteristic impedance of the system. The calculator returns both resistor solutions. Use the solution that matches the intended circuit topology, switching arrangement, and phase requirement.

After selecting a resistor value, verify the complete attenuator with the coupler, hybrid, switching element, PCB layout, and load conditions included. The resistor alone does not define the complete reflection attenuator performance.

Applications

ApplicationWhy Reflection Attenuation Is Useful
RF variable attenuatorsAllows attenuation to be changed by varying or switching reflective terminations.
Phase shiftersReflection-based networks can be used in variable phase-control designs.
Receiver front endsCan reduce signal level before sensitive mixer, amplifier, or detector stages.
Test fixturesProvides controlled signal reduction when integrated with a suitable RF coupler or hybrid.
Switched attenuation banksDiscrete resistor states can create selectable attenuation steps.

Reflection Attenuator vs Resistive Pad

TypeMain IdeaTypical Design Concern
Reflection attenuatorUses reflected signal energy from controlled terminations.Requires the coupler or hybrid behavior to be included in the design.
T-pad or pi-padUses a direct resistor network to absorb signal power.Requires correct resistor values, power rating, and impedance match.
Bridged-T attenuatorUses a bridge and shunt resistor network to set attenuation.Useful when attenuation is adjusted by two main resistor values.

Design Notes

Reflection attenuators are sensitive to the quality of the RF coupler, hybrid balance, resistor accuracy, switching device parasitics, and PCB layout. A resistor value that is mathematically correct can still produce poor performance if the hybrid has limited bandwidth or if the termination is not a clean real impedance at the operating frequency.

For practical RF work, verify insertion loss, attenuation range, phase variation, input match, output match, bandwidth, and power handling. If the circuit uses PIN diodes, FETs, or other active switching elements, also check bias isolation and nonlinear distortion.

Common Mistakes to Avoid

MistakeWhy It Matters
Using a reflection attenuator formula for a T-pad or pi-padThe topologies are different and require different resistor equations.
Ignoring the two possible R1 solutionsThe high and low values can have the same reflection magnitude but different implementation behavior.
Using dB directly as a linear valueConvert attenuation to K with K = 10^(AdB / 20).
Assuming the resistor is purely resistive at RFPackage parasitics and layout can make the termination complex at high frequency.
Ignoring power dissipationReflected and absorbed power can heat the termination resistors and switching devices.

FAQ

Why does the calculator return two resistor values?

A resistor above the system impedance and a resistor below the system impedance can produce the same reflection magnitude. The two values correspond to the two possible real terminations for the same attenuation level.

Can I use this as a normal inline attenuator?

Not by itself. A reflection attenuator normally works with a coupler or hybrid network that routes reflected power correctly. For a simple inline attenuator, use a T-pad, pi-pad, or bridged-T calculator.

What does Z0 mean?

Z0 is the characteristic impedance of the RF system, such as 50 Ω or 75 Ω. The resistor values are calculated relative to this impedance.

Which solution should I choose, the high value or the low value?

Choose the value required by your circuit architecture. The high and low values may differ in power dissipation, switching practicality, phase behavior, and device parasitic sensitivity.

Related Online Calculation Tools

Tee Attenuator Calculator - calculates resistor values for a matched T-pad attenuator.

Pi Attenuator Calculator - calculates resistor values for a matched pi-pad attenuator.

Bridged-Tee Attenuator Calculator - calculates resistor values for a bridged-T attenuator.

dBm to Watts Calculator - converts RF power between dBm and watts.

Frequently Asked Questions

1.How does attenuator work?

As signal at the input of the attenuator will experience a 3 dB reduction in power by the time it reaches the load. That 3 dB less power will be 100% reflected by the load and experience another 3 dB reduction in power by the time is returns back to the input, for a total loss of 6 dB.

2.How do you calculate reflection attachment?

Enter Attenuation and Zo to solve for R1 and R2. R1 = Zo * ((10 ^ (dB / 20) - 1) / (10 ^ (dB / 20) + 1)) for R1 < Zo. R1 = Zo * ((10 ^ (dB / 20) + 1) / (10 ^ (dB / 20) - 1)) for R1 > Zo.

3.How do you calculate attenuator loss?

Enter values for R1 and R2 to calculate attenuator loss and impedance. Alternatively, generate R1 and R2 for a wanted attenuation. *Strictly, a loss quantity when expressed in dB should be positive. However, convention and some literature quote return loss as a negative value akin to an S (1,1) measurement on a Network analyser.

4.What is the formula for attenuator resistance?

The power level at various points in the RF circuit is chosen based on the 1dB compression points of the devices in transmit or receive chain. The most popular values of PI attenuator pads are 3dB and 6dB. Following equation or formula is used for PI attenuator resistance values calculation.

5.What are the functions of attenuator?

An attenuator is an electronic device that reduces the power of a signal without appreciably distorting its waveform. An attenuator is effectively the opposite of an amplifier, though the two work by different methods. While an amplifier provides gain, an attenuator provides loss, or gain less than 1.

6.How to find the emf of an attenuator?

After selecting preferred values, simple series and parallel resistor calculations are used to find the attenuator input impedance, input voltage and output voltage. The source EMF is again assumed to be 2 Volts.

7.What is a 3 dB attenuator?

Insert a 3 dB attenuator in front of the load. Now the incident signal is referenced to the input of the attenuator. As signal at the input of the attenuator will experience a 3 dB reduction in power by the time it reaches the load.

8.Does an attenuator affect the tone?

Yep, attenuators do affect the tone. While I don't have an attenuator, I have played amps that have had built-in attenuators. If you didn't adjust the controls after engaging the attenuators, the amps (even the overpriced THD Univalve) sounded muddy.

9.What is the best attenuator?

Best Guitar Amp Attenuators Comparison Table: S.No. Model Ratings #1 Weber Mass III 4.8 #2 Rivera RockCrusher 5.0 #3 Panama Guitars Conqueror 4.5 #4 THD Electronics HP8 4.1 1 more rows.

10. What are the different types of attenuators?

There are essentially six different kinds of RF designs: fixed, step, continuously variable, programmable, dc bias and dc blocking. Key specifications of an attenuator to consider include the attenuation measured in decibels (dB), frequency range (MHz), power handling (W), and impedance (Ohms).
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, &#177; 25%-

In stock : 355131

Minimum: 1

AD9364BBCZAD9364BBCZAnalog Devices Inc.RF Transceiver ICs144-LFBGA, CSPBGARF Transceiver 1.3V 144-Pin CSP-BGA Tray-

In stock

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock : 10000

Minimum: 1

CYBL10162-56LQXICYBL10162-56LQXICypress Semiconductor CorpRF Transceiver ICs56-UFQFN Exposed PadMCU 32-Bit CYBL10X6X ARM Cortex M0 RISC 128KB Flash 1.8V/2.5V/3.3V/5V 56-Pin QFN EP Tray-

In stock : 48

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP
  • 1:$0.465882
  • 10:$0.439511
  • 100:$0.414633
  • 500:$0.391163

In stock : 1000

Minimum: 1

HSMS-282P-TR1GHSMS-282P-TR1GBroadcom LimitedDiodes - RF6-TSSOP, SC-88, SOT-363Diode Schottky 15V 6-Pin SOT-363 T/R-

In stock

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

SI8261BBD-C-ISSI8261BBD-C-ISSilicon LabsIsolators - Gate Drivers6-SOIC (0.295, 7.50mm Width)4A Gate Driver Capacitive Coupling 5000Vrms 1 Channel 6-SDIP
  • 1:$7.623102
  • 10:$7.191606
  • 100:$6.784534
  • 500:$6.400503

In stock : 9020

Minimum: 1

SI8261BAD-C-ISSI8261BAD-C-ISSilicon LabsIsolators - Gate Drivers6-SOIC (0.295, 7.50mm Width)Gate Drivers 5kV Opto input Sgl channel 4.0A driver
  • 1:$4.558766
  • 10:$4.300723
  • 100:$4.057286
  • 500:$3.827628

In stock : 100000

Minimum: 1

CSR8510A06-ICXR-RCSR8510A06-ICXR-RQualcommRF Transceiver ICs6-XFBGAIC RF TXRX BLUETOOTH 6XFBGA-

In stock

Minimum: 1

FOD8333FOD8333ON SemiconductorIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)Optocoupler AC/DC-IN 1-CH DC-OUT 16-Pin SO Rail
  • 1:$7.142559
  • 10:$6.738263
  • 100:$6.356852
  • 500:$5.997030

In stock : 50

Minimum: 1

FOD8332R2FOD8332R2ON SemiconductorIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)OPTOISO 4.243KV GATE DRIVER 16SO-

In stock : 11

Minimum: 1

SP1004U-ULC-04UTGSP1004U-ULC-04UTGLittelfuse Inc.TVS - Diodes10-XFDFNTVS DIODE 9.2V 1004/10DFN-

In stock : 2633

Minimum: 1

ISM303DACTRISM303DACTRSTMicroelectronicsMultifunction-HIGH PERFORMANCELOW POWER COMPAC-

In stock : 4138

Minimum: 1

SLD8S36ASLD8S36ALittelfuse Inc.TVS - DiodesNonstandard SMDTVS DIODE 36.5V 58.1V SMTO-263-

In stock : 20

Minimum: 1

ACPL-302J-500EACPL-302J-500EBroadcom LimitedIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)OPTOISO 5KV 1CH GATE DRIVER 16SO
  • 1:$6.873772
  • 10:$6.484691
  • 100:$6.117633
  • 500:$5.771352

In stock : 36800

Minimum: 1

UR020-006-RAUR020-006-RATripp LiteUSB Cables-TRIPP-LITE UR020-006-RACOMPUTER CABLE, USB, 6FT, BLACK-

In stock

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock : 6000

Minimum: 1