web counter
Bridged-Tee Attenuator Calculator

This Bridged-Tee Attenuator Calculator will help you figure out what values to use for the resistors R1 and R2 in a bridged-tee attenuator.

Bridged-Tee Attenuator Calculator

ATTENUATION (DB)
IMPEDANCE
Ω
R 1
Ω
R 2
Ω
R 2 Z 0 Z 0 R 1
Introduction

It consists of a basics of Symmetrical Bridge T-Attenuator and derivation of design equation of Symmetrical Bridge T-Attenuator.

Bridge T-Attenuator

Bridged-Tee Attenuator Calculator Overview

The Bridged-Tee Attenuator Calculator helps calculate the resistor values for a bridged-T attenuator. A bridged-T attenuator reduces signal level while maintaining a matched impedance between the source and load, which is especially useful in RF, audio, communication, and test-measurement circuits.

Enter the required attenuation in decibels and the system impedance, such as 50 Ω, 75 Ω, or 600 Ω. The calculator returns the values of R1 and R2 used in the bridged-T network.

Bridged-tee attenuator circuit

What Is a Bridged-T Attenuator?

A bridged-T attenuator, also called a bridged-tee attenuator, is a passive resistor network derived from the T-pad and pi-pad attenuator families. It uses a bridge resistor across the signal path and a shunt resistor to ground to set the attenuation.

In many bridged-T diagrams, the two horizontal arms of the network are fixed at the characteristic impedance Z0. The two calculated parts are the bridge resistor R1 and the shunt resistor R2. This makes the topology convenient when a designer wants to vary attenuation by changing only two resistor values while keeping the same nominal impedance.

Bridged-Tee Attenuator Formulas

For a matched bridged-T attenuator with equal source and load impedance:

K = 10^(AdB / 20)

R1 = Z0 × (K - 1)

R2 = Z0 / (K - 1)

Bridged-tee attenuator equations

SymbolMeaningTypical Unit
R1Bridge resistor connected across the signal path in the bridged-T network.Ω
R2Shunt resistor connected from the center node to ground.Ω
Z0Characteristic impedance of the source, load, and attenuator ports.Ω
AdBRequired attenuation, entered as a positive loss value.dB
KVoltage loss ratio, equal to Vin / Vout for matched ports.unitless

Example Calculation

Suppose you need a 10 dB bridged-T attenuator in a 50 Ω system.

K = 10^(10 / 20) ≈ 3.162

R1 = 50 × (3.162 - 1) ≈ 108.1 Ω

R2 = 50 / (3.162 - 1) ≈ 23.1 Ω

These are ideal resistor values. In a real circuit, choose the nearest standard resistor values or combine resistors to get closer values, then verify attenuation, return loss, and power dissipation.

Common Bridged-T Values for 50 Ω Systems

AttenuationR1, Bridge ResistorR2, Shunt Resistor
3 dB20.6 Ω121.2 Ω
6 dB49.8 Ω50.2 Ω
10 dB108.1 Ω23.1 Ω
20 dB450 Ω5.56 Ω
30 dB1.53 kΩ1.63 Ω

These values assume a matched 50 Ω source and 50 Ω load. For other impedances, use the calculator with the required Z0 value.

How to Use the Calculator

Enter the desired attenuation as a positive dB value. Then enter the system impedance. For RF test equipment, this is commonly 50 Ω. For video systems, it may be 75 Ω. For some audio systems, it may be 600 Ω.

After calculation, confirm the physical resistor values, tolerance, power rating, voltage rating, temperature coefficient, and package parasitics. In RF layouts, the calculated resistor values are only part of the design; grounding, trace length, component package, and board material can also affect performance.

Why Use a Bridged-T Attenuator?

BenefitDesign Meaning
Matched impedanceMaintains the intended source and load impedance when designed correctly.
Two calculated resistor valuesAttenuation is set by R1 and R2 while the line arms can remain tied to Z0.
Useful for variable attenuationCan be implemented with variable or switched resistor values in lab and audio controls.
Good for signal reductionReduces signal level before a sensitive receiver, amplifier, mixer, or measurement input.

Applications

ApplicationWhy It Helps
RF signal level controlReduces a strong signal while preserving the nominal impedance of the signal path.
Receiver or analyzer protectionPrevents excessive input power from damaging sensitive equipment.
Stage isolationReduces interaction between adjacent amplifier or filter stages.
Audio level matchingAttenuates a line-level signal while maintaining a predictable impedance environment.
Switchable attenuation padsProvides fixed attenuation steps in test fixtures or front-end circuits.

Bridged-T vs Tee and Pi Attenuators

TopologyStructureTypical Advantage
Bridged-TBridge resistor plus shunt resistor with matched line arms.Convenient for changing attenuation with two active resistor values.
T-padTwo series resistors and one shunt resistor.Simple and common for fixed attenuation pads.
Pi-padTwo shunt resistors and one series resistor.Often convenient in RF layouts with strong ground reference points.

Power and Layout Notes

A passive attenuator converts part of the signal power into heat. Check the power dissipated in each resistor, especially when the pad is used near transmitters, signal generators, or power amplifiers. A resistor that is correct in value but too small in power rating can overheat, drift, or fail.

For RF and microwave work, use components with suitable frequency behavior. Keep the layout compact, give the shunt resistor a low-inductance ground path, and avoid long traces that add parasitic inductance or capacitance. Verify the final design with S-parameter measurements when return loss or flatness matters.

Common Mistakes to Avoid

MistakeWhy It Matters
Using dB directly as KConvert attenuation to the voltage ratio K with K = 10^(AdB / 20).
Swapping R1 and R2 without checking the diagramDifferent references may name the bridge and shunt resistors differently.
Using a 50 Ω design in a 75 Ω systemThe impedance match and attenuation will not be as intended.
Ignoring resistor parasiticsAt high frequency, package inductance and capacitance can change attenuation and return loss.
Ignoring power dissipationThe attenuator may overheat even if the calculated resistance values are correct.

FAQ

Is a bridged-T attenuator the same as a T-pad attenuator?

No. A T-pad uses two series resistors and one shunt resistor. A bridged-T attenuator adds a bridge-style resistor path and uses a different relationship between attenuation and resistor values.

Can a bridged-T attenuator be used at RF?

Yes, but only if the resistor technology, package size, PCB layout, grounding, and power rating are suitable for the target frequency and power level.

Why do some formulas label R1 and R2 differently?

Attenuator diagrams are not always labeled consistently. Always match the formula to the specific diagram. In this page, R1 is the bridge resistor and R2 is the shunt resistor.

Can this calculator match unequal impedances?

This calculator is intended for equal source and load impedance. For unequal impedances, use a matching attenuator design specifically derived for those two impedance values.

Related Online Calculation Tools

Tee Attenuator Calculator - calculates resistor values for a matched T-pad attenuator.

Pi Attenuator Calculator - calculates resistor values for a pi-pad attenuator.

dBm to Watts Calculator - converts RF power between dBm and watts.

Ohm's Law Calculator - calculates voltage, current, resistance, and power.

Frequently Asked Questions

1.Why we use the bridged T circuits?

A bridged-T attenuator is required to reduce the level of an 8Ω audio signal line by 4dB. Calculate the values of the resistors required. Then resistors R1 are equal to the line impedance of 8Ω, resistor R2 is equal to 13.7Ω and the bridging resistor R3 is equal to 4.7Ω, or the nearest preferred values.

2.What is matching network explain bridged T network?

A T network with a fourth branch bridging the two series arms of the T from input to output terminal, used to control the ratio of the magnitude of the output to input voltage, their relative phase, or both, such magnitudes or phase relations trips in many cases depending on signal frequency.

3.How does an RF attenuator work?

As the name implies RF attenuators reduce the level of the signal, i.e. they attenuate the signal. Typically the attenuation is defined in decibels, and fixed attenuators may be available in a variety of levels. This attenuation may be required to protect a circuit stage from receiving a signal level that is too high.

4.What is the function of attenuator?

Attenuators are electrical components designed to reduce the amplitude of a signal passing through the component, without significantly degrading the integrity of that signal. They are used in RF and optical applications.

5.What does a 3db attenuator do?

The FAM-3 in-line attenuator can be inserted to coaxial cable feeds to reduce signal levels. Combinations of attenuators may be used together to create the exact signal loss needed.

6.What are the different types of attenuator?

Types of Attenuator Fixed Type.  Step Type.  Continuously Variable Type.  Programmable Type.  DC Bias Type.  DC Blocking Type.  Optical Attenuators.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

TP3420AV309TP3420AV309Texas InstrumentsInterface - Telecom20-LCC (J-Lead)IC TELECOM INTERFACE 20PLCC-

In stock

Minimum: 1

19-217/R6C-AL1M2VY/3T19-217/R6C-AL1M2VY/3TEverlight Electronics Co LtdLED Indication - Discrete0603 (1608 Metric)LED RED CLEAR 2SMD-

In stock : 6070

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock : 10000

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP
  • 1:$0.465882
  • 10:$0.439511
  • 100:$0.414633
  • 500:$0.391163

In stock : 1000

Minimum: 1

HMC588LC4BTRHMC588LC4BTRAnalog Devices Inc.RF Misc ICs and Modules24-TFQFN Exposed PadIC OSC VCO WIDEBAND 24SMD-

In stock : 5

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

DS21Q48NDS21Q48NMaxim IntegratedInterface - Telecom144-BBGAIC LIU E1/T1/J1 4X 5V LONG144BGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

EEF-CS1E150REEF-CS1E150RPanasonic Electronic ComponentsAluminum - Polymer Capacitors2917 (7343 Metric)Aluminum Organic Polymer Capacitors 15uF 25volt
  • 1:$0.593588
  • 10:$0.559988
  • 100:$0.528291
  • 500:$0.498388

In stock : 28000

Minimum: 1

AFBR-2418TZAFBR-2418TZBroadcom LimitedFiber Optics - Receivers-Fiber Optic Transmitters, Receivers, Transceivers RX DC-50MBd ML 820nm ST Thrd-

In stock : 660

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock : 6000

Minimum: 1

TZY2Z060AC01R00TZY2Z060AC01R00Murata ElectronicsTrimmers, Variable Capacitors-2.5 ~ 6pF Trimmer Capacitor 25V Top Adjustment-

In stock : 4636

Minimum: 1

SML-S13RTT86SML-S13RTT86ROHM SemiconductorInfrared, UV, Visible Emitters1206 (3216 Metric)EMITTER IR 850NM 30MA 1206-

In stock : 1

Minimum: 1

TZY2Z100AC01R00TZY2Z100AC01R00Murata ElectronicsTrimmers, Variable Capacitors-3 ~ 10pF Trimmer Capacitor 25V Top Adjustment-

In stock : 22000

Minimum: 1

DGD2136S28-13DGD2136S28-13Diodes IncorporatedPMIC - Gate Drivers28-SOIC (0.295, 7.50mm Width)HV GATE DRIVER SO-28-

In stock : 2799

Minimum: 1

TEN-HS5TEN-HS5Traco PowerAccessoriesAluminumTRACOPOWER TEN-HS5 Power Supply Accessory, Heat Sink, DC/DC Converter, TEN25, TEN25WI Series
  • 1:$3.808917
  • 10:$3.593318
  • 100:$3.389922
  • 500:$3.198040

In stock : 255

Minimum: 1

HEF4044BT,652HEF4044BT,652NXP USA Inc.Logic - Latches16-SOIC (0.154, 3.90mm Width)IC R/S LATCH 3-STATE QUAD 16SOIC-

In stock

Minimum: 1

T9GV5L14-22T9GV5L14-22TE ConnectivityRelays-Power Relays, Standard, Monostable, DC, 900 mW Coil Power Rating DC, 538 Ω Coil Resistance, UL Coil Insulation Class F, Potter & Brumfield T9G-

In stock

Minimum: 1