web counter
Pressure Conversion

​Use this tool to calculate equivalent pressure values across a variety of measurement units. Enter the value you want to convert in any input box to solve the other results.

Pressure Conversion

Pascal
Pa (N/m2)
Bar
Bar
Kilogram per Square Centimeter
kg/cm2
Inches of Mercury
in Hg
Pound per Square Inch
psi
Pound per Square Foot
psf
Millimeters of Water Column at 4°C
mm H2O
Inches of Water Column at 4°C
in H2O
Atmospheric Pressure
atm
Introduction

A simple technique to convert between the pressure units of atm, mmHg, torr, kPa, and psi.

Converting Between Pressure Units

Pressure Conversion Overview

The Pressure Conversion tool converts pressure values between common engineering, laboratory, HVAC, hydraulic, pneumatic, meteorological, and vacuum units. Enter a value in one unit and the calculator displays the equivalent pressure in the other supported units.

Supported units include pascal, kilopascal, megapascal, bar, psi, psf, atmosphere, torr, millimeter of mercury, inch of mercury, millimeter of water column, inch of water column, and kilogram-force per square centimeter.

Pressure unit conversion table

What Is Pressure?

Pressure is force applied perpendicular to a surface divided by the area over which that force is applied.

Pressure = Force / Area

The SI unit of pressure is the pascal. One pascal equals one newton per square meter:

1 Pa = 1 N/m²

Common Pressure Units

UnitSymbolEquivalent in PascalsCommon Use
pascalPa1 PaSI pressure unit, scientific and engineering calculations.
kilopascalkPa1000 PaGeneral engineering, HVAC, tire pressure in some regions.
megapascalMPa1000000 PaHydraulics, materials, high-pressure systems.
barbar100000 PaIndustrial pressure, compressors, pneumatics.
standard atmosphereatm101325 PaReference atmospheric pressure.
pound per square inchpsi6894.757 PaTires, hydraulics, compressed air, US customary systems.
torrTorr133.322 PaVacuum measurement and laboratory pressure.
millimeter of mercurymmHg133.322 PaBlood pressure, vacuum, barometric pressure.
inch of mercuryinHg3386.389 PaWeather, aviation, vacuum gauges.
inch of water columninH2O249.089 PaHVAC, low-pressure gas systems, airflow measurement.

Pressure Unit Conversion Formula

Most pressure conversions can be handled by converting the input value to pascals first, then converting from pascals to the desired output unit.

Value in Pa = Input Value × Unit Factor

Output Value = Value in Pa / Output Unit Factor

For example, because 1 psi = 6894.757 Pa:

30 psi = 30 × 6894.757 Pa = 206842.71 Pa = 206.843 kPa

Example Conversions

InputConversionResult
1 bar1 bar = 100000 Pa100 kPa
1 atm1 atm = 101325 Pa101.325 kPa
14.6959 psi14.6959 psi ≈ 101325 Pa1 atm
760 Torr760 Torr = 101325 Pa1 atm
100 inH2O100 × 249.089 Pa24.909 kPa

How to Use the Pressure Conversion Tool

Enter the pressure value in the unit you already know. The calculator converts the value into equivalent pressure values across the available units. Use enough significant digits for engineering work, especially when converting calibration values, sensor ranges, or safety limits.

If the result will be used for equipment selection, compare the converted value with the sensor datasheet, valve rating, gauge range, pipe rating, or applicable safety code. Unit conversion does not replace pressure-system design review.

Absolute, Gauge, and Differential Pressure

Pressure TypeMeaningExample Label
Absolute pressureMeasured relative to a perfect vacuum.psia, kPa absolute
Gauge pressureMeasured relative to local atmospheric pressure.psig, bar gauge
Differential pressureMeasured as the difference between two pressure points.psid, Pa differential

Unit conversion changes the unit, not the pressure reference. For example, converting 30 psig to kPa gives a gauge pressure in kPa, not an absolute pressure. To convert between gauge and absolute pressure, you must account for local atmospheric pressure.

Water Column and Mercury Column Units

Units such as mmH2O, inH2O, mmHg, and inHg come from manometer measurements. They express pressure as the height of a liquid column. These units depend on reference density and gravity assumptions, so high-accuracy work should use the exact standard or calibration reference required by the application.

Water column units are often used for low pressure in HVAC and gas systems. Mercury column units are common in barometry, vacuum measurement, and medical pressure measurement.

Common Mistakes to Avoid

MistakeCorrect Approach
Confusing psi and psf.psi is pound-force per square inch; psf is pound-force per square foot.
Mixing gauge and absolute pressure.Keep the same reference type unless you intentionally add or subtract atmospheric pressure.
Rounding too early.Keep enough significant digits during intermediate conversions.
Assuming water-column units are universal constants.Check the temperature and density reference for precision calibration work.
Using conversion results as equipment ratings.Always check manufacturer ratings and safety factors.

Applications

Pressure conversion is used in pneumatic systems, hydraulic systems, vacuum systems, compressors, HVAC, barometers, weather data, tire pressure, medical devices, industrial sensors, process control, gas regulators, and laboratory measurement.

The most common engineering workflow is to convert a sensor range or specification into the unit used by the rest of the design. For example, a pressure transducer may be rated in psi, while the controller expects kPa or bar.

FAQ

What is the SI unit of pressure?

The SI unit of pressure is the pascal, symbol Pa. One pascal equals one newton per square meter.

Is bar the same as atmosphere?

No. One bar is exactly 100000 Pa. One standard atmosphere is 101325 Pa, so one atmosphere is slightly higher than one bar.

Why are psi and kPa both used?

psi is common in US customary applications, while kPa is a metric unit used in many engineering and scientific contexts. The calculator converts between them.

Can I convert gauge pressure to absolute pressure with this tool?

The tool converts units. To convert gauge pressure to absolute pressure, add the local atmospheric pressure first, then convert units if needed.

Related Online Calculation Tools

Temperature Conversion - converts common temperature units.

Force Conversion - converts force values between engineering units.

Length Conversion - converts length and distance units.

Ohm's Law Calculator - calculates voltage, current, resistance, and power.

Frequently Asked Questions

1.What are the 5 units of pressure?

The most frequently used units of pressure are pascal (Pa), kilopascal (kPa), megapascal (MPa), psi (pound per square inch), torr (mmHg), atm (atmospheric pressure), and bar.

2.What is the unit of pressure?

For pressure, the SI system's basic unit is Pascal (Pa), which is N/m² (Newton per square meter, while Newton is kgm/s²). Pascal is a very small pressure unit and for example, the standard atmospheric pressure is 101325 Pa absolute.

3.How do you convert psi to LBS force?

PSI is a unit of measure for pressure, and pressure (PSI) is the amount of force (lbf) applied per unit of area (in2). The equations below illustrate this. To convert PSI to lbs, simply multiply the pressure by the area over which the force is applied.

4.How much pressure is a Newton?

The SI unit of the pressure is the pascal with the formula sign Pa. 1 Pascal is equal to the pressure of 1 newton per square meter. 1 Pa = 1 N / m2 ≡ 1 kg / m · s2.

5.How vacuum pressure is measured?

Vacuum pressure is measured relative to ambient atmospheric pressure. It is referred to as pounds per square inch (vacuum) or PSIV. The electrical output of a vacuum pressure transducer is 0 VDC at 0 PSIV (14.7 PSIA) and full-scale output (typically 5 VDC) at full-scale vacuum, 14.7 (0 PSIA).

6.What is meant by Pascal?

A pascal is a unit of pressure, where one pascal is equal to the force of one newton exerted on one square meter. A pascal is a unit of pressure, where one pascal is equal to the force of one newton exerted on one square meter.

7.What is the SI unit of force and pressure?

Pressure—the effect of a force applied to a surface—is a derived unit, obtained from combining base units. The unit of pressure in the SI system is the pascal (Pa), defined as a force of one Newton per square meter. The conversion between atm, Pa, and torr is as follows: 1 atm = 101325 Pa = 760 torr.

8.How much psi can a human take?

The body is a lot more resilient than you think. The human body can withstand 50 psi (pounds per square inch) and that's if it's a sudden impact. However if it's sustained pressure, the body can withstand up to 400 psi if the weight is gradually increased.

9.What is pressure and how is it calculated?

Pressure and force are related, and so you can calculate one if you know the other by using the physics equation, P = F/A. Because pressure is force divided by area, its meter-kilogram-second (MKS) units are newtons per square meter or N/m2. If you convert an atmosphere to pounds per square inch, it's about 14.7 psi.

10.What is a perfect vacuum in PSI?

At atmospheric pressure, the value 0 in. -Hg is equivalent to 14.7 psia. At the opposite reference point, 0 psia, — a perfect vacuum (if it could be attained) — would have a value equal to the other extreme of its range, 29.92 in. -Hg.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

TP3420AV309TP3420AV309Texas InstrumentsInterface - Telecom20-LCC (J-Lead)IC TELECOM INTERFACE 20PLCC-

In stock

Minimum: 1

19-217/R6C-AL1M2VY/3T19-217/R6C-AL1M2VY/3TEverlight Electronics Co LtdLED Indication - Discrete0603 (1608 Metric)LED RED CLEAR 2SMD-

In stock : 6070

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP-

In stock

Minimum: 1

HMC588LC4BTRHMC588LC4BTRAnalog Devices Inc.RF Misc ICs and Modules24-TFQFN Exposed PadIC OSC VCO WIDEBAND 24SMD-

In stock

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

DS21Q48NDS21Q48NMaxim IntegratedInterface - Telecom144-BBGAIC LIU E1/T1/J1 4X 5V LONG144BGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

EEF-CS1E150REEF-CS1E150RPanasonic Electronic ComponentsAluminum - Polymer Capacitors2917 (7343 Metric)Aluminum Organic Polymer Capacitors 15uF 25volt-

In stock

Minimum: 1

AFBR-2418TZAFBR-2418TZBroadcom LimitedFiber Optics - Receivers-Fiber Optic Transmitters, Receivers, Transceivers RX DC-50MBd ML 820nm ST Thrd-

In stock

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock

Minimum: 1

TZY2Z060AC01R00TZY2Z060AC01R00Murata ElectronicsTrimmers, Variable Capacitors-2.5 ~ 6pF Trimmer Capacitor 25V Top Adjustment-

In stock

Minimum: 1

SML-S13RTT86SML-S13RTT86ROHM SemiconductorInfrared, UV, Visible Emitters1206 (3216 Metric)EMITTER IR 850NM 30MA 1206-

In stock : 1

Minimum: 1

TZY2Z100AC01R00TZY2Z100AC01R00Murata ElectronicsTrimmers, Variable Capacitors-3 ~ 10pF Trimmer Capacitor 25V Top Adjustment-

In stock

Minimum: 1

DGD2136S28-13DGD2136S28-13Diodes IncorporatedPMIC - Gate Drivers28-SOIC (0.295, 7.50mm Width)HV GATE DRIVER SO-28-

In stock

Minimum: 1

TEN-HS5TEN-HS5Traco PowerAccessoriesAluminumTRACOPOWER TEN-HS5 Power Supply Accessory, Heat Sink, DC/DC Converter, TEN25, TEN25WI Series
  • 1:$3.795684
  • 10:$3.580834
  • 100:$3.378146
  • 500:$3.186930

In stock : 255

Minimum: 1

HEF4044BT,652HEF4044BT,652NXP USA Inc.Logic - Latches16-SOIC (0.154, 3.90mm Width)IC R/S LATCH 3-STATE QUAD 16SOIC-

In stock

Minimum: 1

T9GV5L14-22T9GV5L14-22TE ConnectivityRelays-Power Relays, Standard, Monostable, DC, 900 mW Coil Power Rating DC, 538 Ω Coil Resistance, UL Coil Insulation Class F, Potter & Brumfield T9G-

In stock

Minimum: 1