Sort by
Analysis of SiP (System in Package)12 January 2022
SiP (System in Package) is a packaging concept in which all or most of the electronic functions of a system or subsystem are configured in an integrated substrate, and the chips are bonded to the integrated substrate in 2D or 3D.
How to Choose MOSFET for Switching Power Supply?02 March 2022
A metal-oxide semiconductor field-effect transistor (MOSFET) is a field-effect transistor that can be widely used in analog circuits and digital circuits.This article will help you to select MOSFET for switching power supply.
How Many do You Know About the 12 Components Included in the Circuit Board?12 February 2022
We are lucky to live in an era where electronic devices are readily available. These electronic devices, on the other hand, come to us thanks to the incredible components on the circuit board, and we frequently wonder what makes electronic devices operate, how they achieve such massive success, and how they accomplish it. Electronic devices are incredible things; you can't see what's going on within them, but you can see what they're capable of. We'll talk about the wonders of PCBs and how to get past them to construct the circuit board in this article.
What is a 18650 Lithium Battery?15 December 2021
18650 battery is the originator of lithium-ion batteries-a standard lithium-ion battery model set by SONY in Japan in order to save costs, where 18 means a diameter of 18mm, 65 means a length of 65mm, and 0 means a cylindrical battery.
What is a Baseband Processor?11 November 2021
A baseband processor is used to synthesize the baseband signal to be transmitted or to decode the received baseband signal. Specifically, when transmitting, the audio signal is compiled into the baseband code used to transmit. When receiving a signal, the received baseband code is decoded into the audio signal. It is also responsible for compiling address information (cell phone number, website address), text information (SMS text, website text), and picture information.
Parallel Plate Capacitor: Features, Working Principle and Applications30 January 2021
A parallel plate capacitor is defined as a capacitor that can be created using the arrangement of electrodes and insulating material such as a dielectric. Two conducting plates that are separated by a dielectric material are included in the capacitor. The conducting plates here act as electrodes.
Basics of Phase Change Memory05 February 2021
Phase change memory (PCM) is an advanced non-volatile memory technology recently sold in a computer system as storage-class memory. For non-von Neumann computing, such as in-memory computing and neuromorphic computing, PCM is also being investigated.
Classification and Characteristics of Microwave Filter14 December 2021
This article analyzes the main characteristics of various microwave filters in detail according to the classification of transmission lines.
LDO vs Buck Converter: Which Power Regulator Is Best For Your Application?28 August 2026
A comprehensive guide to understanding, comparing, and choosing between Low Dropout Regulators and Buck Converters for optimal power management.
What is Brushless DC Motors (BLDC) ?03 April 2025
Brushless DC (BLDC) motors represent a significant advancement in electric motor technology, combining high efficiency with superior performance characteristics. Unlike their brushed counterparts, BLDC motors eliminate mechanical commutation components in favor of electronic commutation systems, resulting in enhanced reliability and operational longevity. These motors have become increasingly prevalent across various industries due to their excellent torque-to-weight ratio, improved electrical efficiency, and precise control capabilities (Miller & Hendershott, 2022).
What is SMT (Surface Mount Technology)?02 December 2021
SMT (Surface Mount Technology) refers to the abbreviation of a series of technological processes that are processed on the basis of PCB. SMT is the most popular technology and process in the electronic assembly industry.
What is a Schmitt Trigger?09 December 2021
Schmitt triggers have two stable states, but unlike general triggers, Schmitt triggers use a potential trigger mode, and their state is maintained by the input signal potential. Schmitt triggers have different threshold voltages for input signals with two different changing directions, negatively decreasing and positively increasing.


Product
Brand
Articles
Tools