web counter

Parallel Plate Capacitor: Features, Working Principle and Applications

Published: 30 January 2021 | Last Updated: 30 January 20219109
A parallel plate capacitor is defined as a capacitor that can be created using the arrangement of electrodes and insulating material such as a dielectric. Two conducting plates that are separated by a dielectric material are included in the capacitor. The conducting plates here act as electrodes.
This video introduces you to Features, Working Principle and Applications of the Parallel Plate Capacitor.

THE PARALLEL PLATE CAPACITOR

Catalog

I. Features1. Construction
2. Circuit
3. Capacitance
4. Derivation
II. Working Principle
III. Applications
IV. FAQ

One kind of electrical component is the capacitor and the main purpose of this is to store the energy in an electrical charging form and produce a potential difference similar to a mini rechargeable battery between its two plates. Capacitors are available from very small to large in various shapes, but the purpose of all these is the same as electrical charge storage. Two metal plates that are isolated electrically through the air or good insulating material such as ceramic, plastic, mica, etc. are used in a capacitor. It is known as a dielectric for this insulating material. A description of the parallel plate capacitor and its operation is discussed in this article.

I. Features

1. Construction

The construction of this capacitor can be done with the help of metal plates otherwise metalized foil plates. These are arranged at an equal distance in parallel with each other. The two parallel plates are attached to the power supply in the capacitor. If the capacitor's primary plate is attached to the battery's +Ve terminal, then it gets a positive charge. Similarly, it receives a negative charge when the second plate of the capacitor is attached to a negative battery terminal. So, due to the attraction charges, it stores the energy between the plates.

 

2. Circuit

For charging the capacitor, the following circuit of the parallel plate capacitor is used. 'E' is the capacitor in this circuit,' V0'is the potential discrepancy, and' K 'is the switch. 

Once the main such as 'K' is closed, the electron flow begins flowing in the direction of the battery's +Ve terminal. But the electron flow will be from the end of the battery to the end of + Ve.

The electrons flow into the battery in the direction of the positive end, after which they continue to flow into the plate2. These two plates will receive charges like this, where one plate will receive a positive charge and the second plate will receive a negative charge. 

Once the capacitor receives a potential change in the exact quantity of the battery, this process will proceed. Once this method ceases, the capacitor stores electrical charge, including the potential difference, as well. The charge can be written as Q = CV in the capacitor.

3. Capacitance

The direction of the electrical field is nothing but the flow of the positive test charge. The weakness of the body is known as capacitance and can be used to store electric energy. Similarly, a capacitor includes its capacitance, two metal plates with area 'A' are included in the parallel plate capacitor, and these are separated by the 'width.' It is possible to display the parallel plate capacitor formula below.

C = k*ϵ0*A*d

Where,

‘ϵo’ is the permittivity of space

‘k’ is the dielectric material’s relative permittivity

‘d’ is the partition between the two plates

‘A’ is the area of two plates

4. Derivation

The capacitor with two plates arranges in parallel is shown below.

The first plate has a charge of '+ Q' in the capacitor and the second plate has a charge of '- Q'. With 'A' and the width, the area between these plates can be denoted (d). In this case,' d' is smaller than the plate area (d<<A). If the whole charge on the first plate is 'Q' & 'A' is the plate field, then the surface charge density can be extracted as:

σ =Q/A

Similarly, if the entire charge is'-Q 'on the second plate & the area of the plate is' A 'on the second plate, then the surface charge density can be extracted as:

σ = -Q/A

You may break the regions of this capacitor into three divisions, such as area1, area2, and area3. Area 1 is on the right of the second plate, area 2 is between the planes, and area 3 is on the right of the second plate. In the region around the capacitor, the electric field can be measured. The electric field is consistent here & its direction is from the plate +Ve to the plate-Ve. 

The potential difference is determined in the condenser by multiplying the space between the electric field planes, which can be derived as:

V = Exd = 1/ε(Qd/A)

The capacitance of the parallel plate can be derived as C = Q/V = εoA/d

The capacitance of a parallel plate capacitor with 2 dielectrics is shown below. Every region of the plate is Am2 and is separated by a d-meter gap. K1 & k2 are the two dielectrics, so the capacitance would be like the following.

The main half of the capacitor width capacitance is d/2 = C1=> K1Aϵ0/ d/2=> 2K1Aϵ0/d

Similarly, the capacitance of the capacitor's next half is C2 = 2K2Aϵ0/d

Once these two capacitors are linked in sequence, the net capacitance:  Ceff= C1C2/C1+C2= 2Aϵ0/d( K1K2/ /K1+K2) will be associated.

II. Working Principle

We know that we can supply a capacitor plate with a certain amount of electric charge. If we give more energy, then the potential increases so that it contributes to an outflow in the charge. Once plate 2 is arranged next to plate 1 that receives a positive charge, this plate 2 will be supplied with a negative charge. 

If we get plate2 and it is put next to plate1, it is possible to supply negative energy through plate2. This negatively charged plate is closer to the plate that has been positively charged. If plate1 & plate2 have charges, the negative charge on plate2 on the first plate would reduce the potential difference.

The positive charge on the second plate would, alternatively, increase the potential variation on the first plate. The negative charge on plate 2 will have an extra effect, however. Therefore, it is possible to charge more on plate 1. Therefore, because of the negative charges on the second plate, the theoretical difference would be smaller.

III. Applications

The following are the applications of the parallel plate capacitor. 

By connecting multiple capacitors in a circuit in parallel, more energy would be stored since the resulting capacitance is the number of individual capacitances of all the capacitor types inside the circuit. 

In DC power supplies, parallel plate capacitors are used to process the O/P signal and eliminate the AC ripple. 

Using inductive loads, the capacitor banks for energy storage can be used in PF(power factor) correction. 

These are used for regenerative braking in large vehicles in the automotive industry. 

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

How does a parallel plate capacitor work?

The simplest design for a capacitor is a parallel-plate, which consists of two metal plates with a gap between them: electrons are placed onto one plate (the negative plate), while an equal amount of electrons are removed from the other plate (the positive plate). Capacitors function a lot like rechargeable batteries.

What is the principle of parallel plate?

The two plates of parallel plate capacitor are of equal dimensions. They are connected to the power supply. The plate, connected to the positive terminal of the battery, acquires a positive charge. On the other hand, the plate, connected to the negative terminal of battery acquires a negative charge.

What happens to the charge on a parallel plate capacitor?

Differentiate between electrical potential and potential difference. potential difference is the change in electric potential between two points in space. What happens to the charge on a parallel-plate capacitor if the potential difference doubles? The charge on each plate doubles.

What is meant by the capacitance of a parallel plate capacitor?

The ability of a capacitor to store electric charge between its plates is its capacity or capacitance. DEFINITION. The capacitance of a capacitor is defined as: "The ratio of electric charge stored on any one of the plates of capacitor to potential difference between the plates.

How do you find the capacitance of a parallel plate capacitor?

The capacitance of a parallel plate capacitor is C=ϵ0Ad C = ϵ 0 A d , when the plates are separated by air or free space.
Related Articles

  • AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    UTMEL02 June 20263584

    Next-generation AI servers like NVIDIA's Rubin architecture require over 600,000 MLCCs per rack due to extreme power densities exceeding 120kW. This transition from GB300 demands high-capacitance, low-ESR capacitors with X7R/X7S dielectrics to handle intense transient responses and thermal loads, forcing procurement teams to navigate extended 24-week lead times for these specialized components.

    Read More
  • MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    UTMEL07 August 2026766

    Facing 2026 MLCC lead times of up to 24 weeks driven by AI server demand, hardware engineers are substituting multi-layer ceramic capacitors with conductive polymer tantalum capacitors. While Class II MLCCs suffer severe DC bias capacitance loss and acoustic noise, polymer tantalums offer voltage stability and low ESR. Implementing a division-of-labor strategy—using polymer tantalums for bulk decoupling and MLCCs for point-of-load—optimizes PDN performance and bypasses supply bottlenecks.

    Read More
  • Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    UTMEL13 August 2026644

    Modern AI hardware requires a hybrid Power Delivery Network (PDN) to maintain low-voltage stability under extreme transient currents. Deep Trench Silicon Capacitors (DTCs) integrate directly into advanced packages to deliver ultra-low ESL and stable performance for high-frequency transient suppression. Meanwhile, Multilayer Ceramic Capacitors (MLCCs) provide essential bulk energy storage on the motherboard, making both technologies complementary across the AI power stack.

    Read More
  • MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    UTMEL11 September 2026645

    Class II ceramic capacitors suffer significant capacitance loss under DC voltage due to ferroelectric domain saturation and high electric field intensity. This comprehensive engineering guide explains how to calculate true worst-case effective capacitance by compounding DC bias, temperature, tolerance, and aging. It provides multi-vendor simulation workflows, benchtop impedance measurement techniques, and practical guidelines to maintain power supply stability and avoid costly design failures.

    Read More
  • Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    UTMEL13 July 2026424

    Explore how the transition from traditional air-cooling to liquid cooling (direct-to-chip and immersion) in high-density AI server racks alters component thermal profiles. Focus on why design engineers are increasingly specifying Class 2 MLCCs (X7R and X7S dielectrics) over standard X5R variants to prevent thermal degradation near the liquid cooling microchannels. Explain how these capacitors mitigate acoustic noise and voltage bias degradation under heavy workloads. Provide sourcing advice for high-reliability passives via UTMEL during this high-demand memory and passive component super-cycle.

    Read More

Subscribe to Utmel !

Featured Parts More