web counter

What is Feedthrough Capacitor?

Published: 06 November 2021 | Last Updated: 06 November 202142309
Hello, everyone. I am Rose. Today I will introduce the feedthrough capacitor to you. The feedthrough capacitor is a three-terminal capacitor that is used to reduce high frequencies. The feedthrough capacitor, unlike regular three-terminal capacitors, is directly installed on the metal panel, resulting in a lower grounding inductance and a negligible effect on the lead inductance.
In this video you will see what is feedthrough capacitor and it’s meaning.

What is FEEDTHROUGH? What does FEEDTHROUGH mean? FEEDTHROUGH meaning, definition & explanation

Topics covered in this article:
Ⅰ. What is Feedthrough Capacitor?
Ⅱ. Where can Feedthrough Capacitor Use?
Ⅲ. What is Filtering?
Ⅳ. How does the Feedthrough Capacitor Filter?
Ⅴ. Several Forms of Feedthrough Filter
Ⅵ. Installation Precautions


Ⅰ. What is Feedthrough Capacitor?

1. Definition

The feedthrough capacitor is a three-terminal capacitor that is used to reduce high frequencies. The feedthrough capacitor, unlike regular three-terminal capacitors, is directly installed on the metal panel, resulting in a lower grounding inductance and a negligible effect on the lead inductance. As a result, the feedthrough capacitor provides good filtering. The better the electromagnetic interference suppression effect, especially for high-frequency electronic equipment, the better.

1.jpg

Feedthrough Capacitor

2. Structure and Selection

One (C type) or two (Pi type) capacitors with inner and outer electrodes and ceramics make up the simpler through-core structure.

The through-core capacitor's medium is ceramic, and the capacity of the ceramic capacitor changes as the ambient temperature changes. The filter cut-off rate will be affected by this change in capacity. Ceramic capacitors' capacity temperature change rate is determined by the ceramic medium itself. As a result, selecting an appropriate ceramic media is critical.

结构图.png

Feedthrough Capacitor structure diagram

3. Classification

Type C

This is a low-self-induction device that shields the ground from high-frequency noise interference. It is low-cost and ideal for high-impedance sources and high-load applications.

Type L

This is a capacitor having both inductive and capacitive components that runs through the core. This capacitor is commonly employed in circuits with low impedance sources and high impedance loads, as well as the other way around. It's important to keep in mind that the inductive component should face the low-impedance source.

Type Pi

The Pi type has a low impedance to both the impedance source and the load because it is made up of two capacitive elements and an inductive element sandwiched between them. The Pi type filter outperforms the C and L type structures in terms of high-frequency filtering.

4. Characteristics and Applications

Welded feedthrough capacitors

The most suited product for a small installation space is welded feedthrough capacitors.

Filtering signals, data lines, and AC power lines are the most common applications.

Components for composite circuit filters, telecommunications equipment, transmission equipment, microwave filters, industrial computers;

Smaller size allows for more efficient use of space;

Up to 1000VDC rated voltage;

Various circuit structures are available, including C-type, Pi-type, and L-type circuits.

Structure with a high-temperature range: prevents backflow during installation.

MIL-F-15733 QPL and MIL-C-11015 (CK99) certified filters are available for certification.

Resin sealed threaded feedthrough capacitor

Through-hole nuts and washers for resin-sealed bolt-type through-core capacitors are simple to install.

To ensure good environmental protection, the two ends of the solid shell are sealed with resin.

Micro-extrusion mounting or screw mounting is the ideal choice when welding is not suitable, suitable for microwave and other high-frequency applications; among them, micro-extrusion mounting or screw mounting is the ideal choice when welding is not suitable, suitable for microwave and other high-frequency applications;

Up to 2500VDC/240VAC voltage

MIL-F-15733 approved goods are eligible for certification.

C type, L type, and Pi type circuit structures

High current and high voltage resin sealed feedthrough capacitors

High-current filters are utilized primarily in high-current switching power supply and DC charging systems.

High-voltage filters are primarily employed in high-voltage power supplies, and their solid bolt-type structure makes them simple to install.

Features: up to 100Amps of high current

Up to 2500VDC and 240VAC@400HZ voltages are possible.

Glass-sealed high-performance feedthrough capacitors

It uses glass sealing packaging and has outstanding EMI filtering performance; this product is the best alternative for people who still demand high dependability filtering in difficult settings. From 10KHz to greater than 10GHz, it can be used for broadband high-performance EMI filtering. Series of glass sealants Moisture-proof, corrosion-resistant, and resistant to other extreme environments encountered in military applications.

Power supply, signal line, rocket ignition device, aircraft, military communications, medical equipment, multi-stage filtering are all examples of applications.

Optimized design: a wide range of sizes and forms, as well as C, L, and Pi-type circuits for selection, as well as instantaneous suppression of Pi, T, and TT circuits;

Reliability: In accordance with QPL regulations, manufactured to MIL-F-15733 and MIL-F-28861 specifications.

Space application “S” level FED/MIL certification based on MIL-F-28861: MIL-F-15733 and MIL-F-28861 criteria are met.

Features: The insertion loss ranges from 0.01MHz to 10GHz.

1pF-1mu; F; NPO, X7R, Z5U, and other capacitance and temperature characteristics

Temperature range: -55°C to +125°C; -40°C to +85°C

400VDC 240VAC@400Hz is the maximum voltage value.

30 amps maximum current

 

Ⅱ. Where can Feedthrough Capacitor Use?

Signals, data lines, and AC power lines, telecommunications equipment, microwave filters, industrial computers, and composite circuit filter components are all examples of where feedthrough capacitors and other filters are employed. A feedthrough capacitor on the computer's CPU high-speed data bus, for example, can successfully reduce noise, while a feedthrough capacitor on the transmitter can effectively suppress interference.

 

Ⅲ. What is Filtering?

We all know that the higher the voltage or current frequency, the easier it is to produce radiation. There are filters in addition to altering the circuit board and installing the requisite magnetic ring. In many circumstances, appropriate filters are added to limit the interference caused by radiation. The high-frequency interference signal can be considerably reduced in this manner. Common interference filters have an effective filtering frequency range of several kHz to tens of MHz, whereas radio frequency interference filters have an effective filtering frequency range of several kHz to above GHz.

Ordinary capacitors cannot effectively filter out high-frequency noise because they are not perfect capacitors. This is because: 1The capacitor lead inductance generates capacitor resonance, which causes high-frequency signals to have a large impedance and weakens the bypass effect; 2The parasitic capacitance between the wires causes the high-frequency signal to be coupled, reducing the filtering effect.

 2.png

Ⅳ. How does the Feedthrough Capacitor Filter?

The use of feedthrough capacitors as bypass capacitors, on the other hand, can produce excellent high-frequency filtering effects. Feedthrough capacitors have very low parasitic inductance and bypass impedance, and the high frequency between the input and output terminals is removed due to the isolation installation method. Frequency coupling is a term used to describe when two frequencies are coupled together. Feedthrough capacitors can be used to provide a wide range of RF filters for high-frequency applications, which we refer to as "feedthrough filters." Even at a frequency of 10GHz, the tubular feedthrough capacitor will not cause obvious self-resonance due to its coaxially.

The feedthrough capacitor's medium is ceramic, and the capacity of the ceramic capacitor changes as the ambient temperature changes. The filter cut-off rate will be affected by this change incapacity. As a result, selecting an appropriate ceramic dielectric for feedthrough capacitors is critical. Because the feedthrough capacitor's shell is the opposite electrode and is connected to "ground," high-frequency electromagnetic interference signals are short-circuited to "ground" while passing through the center conductor, and electromagnetic interference is eliminated. The feedthrough capacitor is what it sounds like. The noise filtering principle.

Insertion loss

Insertion loss is a measure of the filter's key performance index, which indicates the filter's quality of performance. The feedthrough capacitor, as depicted in the diagram, is closer to the ideal capacitor.

 3.png

Ⅴ. Several Forms of Feedthrough Filter

RF filters are another name for feedthrough filters. This filter has a similar shape and construction to feedthrough capacitors, but it also has ferrite cores. This filter usually comes in five different forms to satisfy the needs of different situations: Filters of the C-type, LC-type, -type, T-type, and double T-type types

1. Type C Filter

Type C filters, which are made up of three-terminal or feedthrough capacitors, are designed to reduce high-frequency sounds. It's a low-self-induction device that shields the ground from high-frequency noise. It is low-cost and ideal for high-impedance sources and high-load applications.

4.png

2. Type LC Filter

A feed-through filter made up of inductive and capacitive elements is known as an LC-type filter. This filter is commonly employed in circuits with low-impedance sources and high-impedance loads, as well as the other way around. It's important to keep in mind that the inductive component should face the low-impedance source.

5.png

3. Type π Filter

It is made up of two capacitive elements and an inductance element sandwiched between them, and it has a low impedance to both the impedance source and the load. The -type filter outperforms the C-type and LC-type structures in terms of high-frequency filtering.

6.png

4. Type T filter

Two inductance elements and one capacitance element make up a T-type filter. Its circuit topology reveals that both ends' inputs have high impedance. It has a structure that is similar to that of the -type filter, although it is not generally employed in the -type filter and can be used in switching conversion.

7.png

5. Type double T Filter

The double T filter is made up of two high-performance T-type filters with more stringent circuit requirements.

The simple through-core structure consists of one (C type) or two (type) capacitors made up of inner and outer electrodes and ceramics. This type of capacitor has a capacity of up to 10pF and a working voltage of up to 2000VDC. The plug-in C-type feedthrough filter is shown in the following diagram, however, soldered feedthrough filters are especially crucial for electrical equipment with limited installation space.

 8.png

Ⅵ. Installation Precautions

Due to the unique structure of the feedthrough capacitor and feedthrough filter, the housing of the filter must be suitably connected to the panel's ground in order to provide an effective path for interference to pass through. therefore:

1) A disc-shaped multilayer or tubular ceramic capacitor serves as the through-core filter's core. Sudden temperature changes, mechanical vibration, and excessive voltage will all harm them, just like other ceramic things. When placing the through-core filter on the board, take care when welding the filter's guide pin and shaping it to avoid any tension.

2)When installing threaded through-type filters to a partition or panel, the suggested installation rotation force relative to the housing should be applied. Otherwise, the distortion of the shell may cause harm to the inside capacitor.


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. How many pins does feedthrough capacitor have?

The feedthrough capacitor is a three-terminal capacitor
, Two pins and one grounding terminal, the connection between the two pins is the same as that of ordinary capacitors, but the grounding terminal area is relatively large, and the grounding terminal installation methods include welding type and crimp contact type.

2. What's the Difference Between Feedthrough Capacitors and Ordinary Capacitors?

A three-terminal capacitor is used as a feedthrough capacitor. Because it is directly installed on the metal panel, it has a lower grounding inductance than a standard three-terminal capacitor, and the lead inductance has essentially no effect. As a result, the feedthrough capacitor outperforms standard capacitors. Have a greater self-resonant frequency; in addition, metal plates separate the input and output terminals to prevent high-frequency coupling. Because of these two features, the through-core capacitor provides a filtering effect that is similar to that of the ideal capacitor.

3. Why can Feedthrough Capacitors Effectively Filter Out High-Frequency Noise?

The three-terminal feedthrough capacitor is named after its hollow physical structure. The feedthrough capacitor connects the low-frequency signal (including power supply) output or input from the shielding cavity, which can filter out some of the noise brought in. As a result, feedthrough capacitors are found in a variety of high-frequency, ultra-high-frequency, and microwave devices. This term is frequently used. Because the feedthrough capacitor is directly installed on the metal panel, it has a lower grounding inductance and essentially no influence from lead inductance when compared to typical three-terminal capacitors. Metal plates separate the input and output terminals, and metal plates separate the input and output terminals. The panel serves as a high-frequency isolation device, preventing high-frequency coupling. Because of these two features, the feedthrough capacitor provides a filtering effect that is similar to that of the ideal capacitor.
Related Articles

  • AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    UTMEL02 June 20263839

    Next-generation AI servers like NVIDIA's Rubin architecture require over 600,000 MLCCs per rack due to extreme power densities exceeding 120kW. This transition from GB300 demands high-capacitance, low-ESR capacitors with X7R/X7S dielectrics to handle intense transient responses and thermal loads, forcing procurement teams to navigate extended 24-week lead times for these specialized components.

    Read More
  • MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    UTMEL07 August 2026935

    Facing 2026 MLCC lead times of up to 24 weeks driven by AI server demand, hardware engineers are substituting multi-layer ceramic capacitors with conductive polymer tantalum capacitors. While Class II MLCCs suffer severe DC bias capacitance loss and acoustic noise, polymer tantalums offer voltage stability and low ESR. Implementing a division-of-labor strategy—using polymer tantalums for bulk decoupling and MLCCs for point-of-load—optimizes PDN performance and bypasses supply bottlenecks.

    Read More
  • Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    UTMEL13 August 2026773

    Modern AI hardware requires a hybrid Power Delivery Network (PDN) to maintain low-voltage stability under extreme transient currents. Deep Trench Silicon Capacitors (DTCs) integrate directly into advanced packages to deliver ultra-low ESL and stable performance for high-frequency transient suppression. Meanwhile, Multilayer Ceramic Capacitors (MLCCs) provide essential bulk energy storage on the motherboard, making both technologies complementary across the AI power stack.

    Read More
  • MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    UTMEL11 September 2026928

    Class II ceramic capacitors suffer significant capacitance loss under DC voltage due to ferroelectric domain saturation and high electric field intensity. This comprehensive engineering guide explains how to calculate true worst-case effective capacitance by compounding DC bias, temperature, tolerance, and aging. It provides multi-vendor simulation workflows, benchtop impedance measurement techniques, and practical guidelines to maintain power supply stability and avoid costly design failures.

    Read More
  • Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    UTMEL13 July 2026553

    Explore how the transition from traditional air-cooling to liquid cooling (direct-to-chip and immersion) in high-density AI server racks alters component thermal profiles. Focus on why design engineers are increasingly specifying Class 2 MLCCs (X7R and X7S dielectrics) over standard X5R variants to prevent thermal degradation near the liquid cooling microchannels. Explain how these capacitors mitigate acoustic noise and voltage bias degradation under heavy workloads. Provide sourcing advice for high-reliability passives via UTMEL during this high-demand memory and passive component super-cycle.

    Read More

Subscribe to Utmel !

Featured Parts More