web counter

What is a Power Capacitor?

Published: 20 November 2021 | Last Updated: 20 November 20216650
Power capacitors are capacitors used in power systems and electrical equipment. Any two pieces of metal conductors are separated by an insulating medium to form a capacitor. The size of the capacitor is determined by its size and the characteristics of the insulating medium between the two plates.


Catalog

Ⅰ Power capacitor classification

Ⅱ Application fields

Ⅲ Cause of damage

Ⅳ Precautions

Ⅴ Power capacitor manufacturers

 

Ⅰ Power capacitor classification

Power capacitors can be divided into 8 types according to their purpose:

①Parallel capacitor. Originally called a phase-shifting capacitor. It is mainly used to compensate the reactive power of the inductive load of the power system to increase the power factor, improve the voltage quality, and reduce the line loss.

②Series capacitor. It is connected in series in power frequency high voltage transmission and distribution lines to compensate the distributed inductance of the line, improve the static and dynamic stability of the system, improve the voltage quality of the line, extend the power transmission distance and increase the transmission capacity.

③Coupling capacitor. Mainly used for high-frequency communication, measurement, control, protection of high-voltage power lines, and as components in devices for extracting electrical energy.

④Circuit breaker capacitor. Formerly known as a voltage equalizing capacitor. Parallel connection on the fracture of the ultra-high voltage circuit breaker has the effect of equalizing the voltage, so that the voltage between the fractures is uniform during the breaking process, and can improve the arc extinguishing characteristics of the circuit breaker and increase the breaking capacity.

⑤Electric heating capacitor. It is used in electric heating equipment systems with a frequency of 40 to 24000 Hz to increase the power factor and improve the voltage or frequency characteristics of the loop.

⑥Pulse capacitor. It is mainly used for energy storage and is used as basic energy storage components such as impulse voltage generator, impulses current generator, and oscillating circuit for circuit breaker test.

⑦DC and filter capacitors. Used in high-voltage direct current devices and high-voltage rectifier filter devices.

⑧Standard capacitor. Used in the power frequency high voltage measurement dielectric loss circuit, as a standard capacitor, or as a capacitive voltage divider device for measuring high voltage.

power capacitor.jpg

power capacitor

In the power system, it is divided into high-voltage power capacitors (above 6KV) and low-voltage power capacitors (400V)

Low-voltage power capacitors are classified into oil impregnated paper power capacitors and self-healing power capacitors according to their properties. According to the function, it is divided into ordinary power capacitors and intelligent power capacitors.

Self-healing shunt capacitor.jpg

Self-healing shunt capacitor

Take American Swell products as an example to introduce smart power capacitors.

Smart power capacitors integrate advanced technologies such as modern measurement and control, power electronics, network communications, automation control, and power capacitors. It has changed the backward controller technology of the traditional reactive power compensation device and the backward mechanical contactor or electromechanical integrated switch as the switching technology of switching capacitors. It also changed the bulky and bulky structure of the traditional reactive power compensation device, so that the new generation of low-voltage reactive power compensation equipment has better compensation effect, smaller size, lower power consumption, lower price, more flexible use, and more maintenance. The features of convenience and longer service life meet the higher requirements of modern power grids for reactive power compensation.

Ⅱ Application fields

The main application areas are:

■ Factory Power Distribution System

■ Residential district power distribution system

■ Municipal Commercial Building

■ Traffic Tunnel Power Distribution System

■ Box change, complete cabinet, outdoor distribution box

Ⅲ Cause of damage

In recent years, more and more power capacitors have been put into operation, but due to poor management and other technical reasons, power capacitors are often damaged and exploded. The reasons are as follows:

Breakdown of the internal components of the capacitor: mainly caused by the poor manufacturing process.

The capacitor's insulation damage to the shell: The high-voltage side lead of the capacitor is made of thin copper. If the manufacturing process is poor, the edge is uneven, there are burrs or severely bent, and the tip is prone to corona. Corona will decompose the oil, expand the tank shell, and drop the oil level, causing breakdown. In addition, when the cover is sealed, if the welding time is too long at the corners, the internal insulation will be burned and oil and gas will be generated, which will greatly reduce the voltage and cause damage to the capacitor.

Poor sealing and oil leakage: due to poor sealing of the assembly sleeve, moisture enters the interior, which reduces the insulation resistance; or the oil level drops due to oil leakage, resulting in pole-to-shell discharge or component breakdown.

Bulging and internal dissociation: due to the internal corona, breakdown discharge and internal dissociation, the capacitor will reduce the initial dissociation voltage of the element to below the working electric field strength under the action of overvoltage, which causes physical, chemical, and electrical effects. Accelerate the aging and decomposition of the insulation, generate gas, form a vicious circle, increase the pressure of the box shell, and cause the outer wall of the box to bulge and cause an explosion.

Capacitor explosion caused by charge closing: Any capacitor bank with a rated voltage is prohibited from closing with charge. Each time the capacitor bank is reclosed, the capacitor must be discharged for 3 minutes when the switch is disconnected. Otherwise, it may explode due to the residual charge on the capacitor at the moment of closing. For this reason, it is generally stipulated that capacitor banks with a capacity of more than 160 kvar should be equipped with automatic discharge devices when there is no voltage, and it is stipulated that the switches of the capacitor banks are not allowed to be equipped with automatic closing.

In addition, the capacitor may be damaged and exploded due to excessive temperature, poor ventilation, excessive operating voltage, excessive harmonic components, or operating overvoltage.

Ⅳ Precautions

1 When installing capacitors, the wiring of each capacitor should preferably be connected to the bus with a separate flexible wire. Do not use hard bus connections to prevent assembly stress from damaging the capacitor casing and breaking the seal and causing oil leakage.

2 Any poor contact in the capacitor circuit may cause high-frequency oscillating arcs, which will increase the working electric field strength of the capacitor and generate heat. Therefore, it is necessary to maintain good contact between the electrical circuit and the grounding part during installation.

3 When the capacitors of lower voltage levels are connected in series and run in the higher voltage level network, measures such as installing insulators equivalent to the operating voltage level should be adopted to ensure reliable insulation between the housing of each unit and the ground.

4 After the capacitor is connected in a star shape, it is used for a higher rated voltage and the neutral point is not grounded. The shell of the capacitor should be insulated from the ground.

5 Before the capacitor is installed, the capacitance should be allocated once to balance the phases, and the deviation should not exceed 5% of the total capacity. When a relay protection device is installed, it should also meet the requirement that the balance current error does not exceed the relay protection operating current during operation.

6 The wiring of individual compensation capacitors should be done: for induction motors that are started directly or via a varistor, the power factor-increasing capacitor can be directly connected to the outlet terminal of the motor, and no switchgear or fuse should be installed between the two; For induction motors started with star-delta starters, it is best to use three single-phase capacitors, each capacitor is directly connected in parallel to the two terminals of each phase winding so that the connection of the capacitor is always consistent with the connection of the winding.

7 For the grouping compensation low-voltage capacitor, it should be connected to the outside of the low-voltage grouping bus power switch to prevent self-excitation when the grouping bus switch is disconnected.

8 The low-voltage capacitor bank for centralized compensation should be specially equipped with switches and installed on the outside of the main line switch, not on the low-voltage bus.

Ⅴ Power capacitor manufacturers

The general trend of the development of the electromechanical industry in recent years is to develop toward a large group, merge related majors, and form a multinational company. The power container industry is no exception. The scale of major manufacturers and their main products are introduced as follows:

1 ABB

ABB has capacitor production plants in 11 countries including Sweden, the United Kingdom, Australia, Spain, Belgium, Canada, India and Thailand, with the power capacitor plant in Sweden as its core plant. The total annual output of each plant is above 20 million kvar. In December 2000, it formed a joint venture with Xi'an Power Capacitor Factory to form Xi'an ABB Power Capacitor Co., Ltd. The company has an annual production capacity of 3.5 million kvar. Its main products include 1~25kV, 100~1000kvar parallel capacitors; 1~500kV, 0.6~300Mvar parallel sets of devices; 3~300kV, 1~300Mvar filter sets, SVC, DC transmission series compensation devices, filter capacitors, and sets Devices, etc.

2 Cooper, USA

In May 1985, the original Megaraw-Edison company merged with Cooper, with an annual output of approximately 19 million kvar. According to the American standard, the design field strength in the capacitor medium is low and high, up to 70/80kV/mm, usually without internal fuse. The characteristics of the product are: small size, light weight, and good specific characteristics. The main products include high and low voltage shunt capacitors and complete sets of devices, filter capacitors and complete sets of devices, etc.

3 Nisshin Corporation

Its capacitor production accounts for 95% of Japan's total production, about 8 million kvar. The Kyoto headquarters mainly produces large-capacity box-type shunt capacitors. In 1988, a branch company was established in Thailand and a branch factory in Taiwan Province of my country. In the late 1990s, a joint venture company was established in Wuxi Power Capacitor Factory, which mainly produces capacitive voltage transformers with very good economic benefits. In recent years, it has also fully established a joint venture with Wuxi Plant to produce parallel capacitors and complete sets of devices.

4 Finland Nokia Capacitor Company

Founded in 1957, merged into NOKIAN in 1967, established NOKIAN Capacitor Company in 1990, became a member of the SEHNIDER Group in 1994, and has been a global independent supplier since 2000. The headquarters is located in Tampere, Finland, 85% of the products are exported, and the marketing network covers more than 50 countries. Adopt European standards. The main products include: high and low voltage shunt capacitors and complete sets of devices, thyristor switching capacitor banks (TSC), automatic switching non-tuned filter banks, shunt reactors, static compensation devices (SVC), series compensation devices (SC/ASC) Not source filtering device, etc...

5 American GE Company

American GE mainly produces high-voltage shunt capacitors and large-capacity electric heating capacitors, as well as filter, pulse, DC capacitors and complete sets. Using American standards, the annual output is about 12 million kvar.

6 French Alstom Sant'an Factory

Using European standards, shunt capacitors are equipped with discharge resistors, and those with a single unit above 150kvar have internal fuses. The annual output is about 3.5 million kvar.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. How do power capacitors work?

Stiffing capacitors store electricity, which they can discharge very quickly unlike the vehicles battery and alternator. They give your amplifier quick jolts of power when the bass hits to cover the amount of current it requires for musical transients.

2. When should you use a capacitor?

Capacitors are widely used in electronic circuits for blocking direct current while allowing alternating current to pass. In analog filter networks, they smooth the output of power supplies.
Related Articles

  • AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    UTMEL02 June 20263584

    Next-generation AI servers like NVIDIA's Rubin architecture require over 600,000 MLCCs per rack due to extreme power densities exceeding 120kW. This transition from GB300 demands high-capacitance, low-ESR capacitors with X7R/X7S dielectrics to handle intense transient responses and thermal loads, forcing procurement teams to navigate extended 24-week lead times for these specialized components.

    Read More
  • MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    UTMEL07 August 2026766

    Facing 2026 MLCC lead times of up to 24 weeks driven by AI server demand, hardware engineers are substituting multi-layer ceramic capacitors with conductive polymer tantalum capacitors. While Class II MLCCs suffer severe DC bias capacitance loss and acoustic noise, polymer tantalums offer voltage stability and low ESR. Implementing a division-of-labor strategy—using polymer tantalums for bulk decoupling and MLCCs for point-of-load—optimizes PDN performance and bypasses supply bottlenecks.

    Read More
  • Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    UTMEL13 August 2026644

    Modern AI hardware requires a hybrid Power Delivery Network (PDN) to maintain low-voltage stability under extreme transient currents. Deep Trench Silicon Capacitors (DTCs) integrate directly into advanced packages to deliver ultra-low ESL and stable performance for high-frequency transient suppression. Meanwhile, Multilayer Ceramic Capacitors (MLCCs) provide essential bulk energy storage on the motherboard, making both technologies complementary across the AI power stack.

    Read More
  • MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    UTMEL11 September 2026645

    Class II ceramic capacitors suffer significant capacitance loss under DC voltage due to ferroelectric domain saturation and high electric field intensity. This comprehensive engineering guide explains how to calculate true worst-case effective capacitance by compounding DC bias, temperature, tolerance, and aging. It provides multi-vendor simulation workflows, benchtop impedance measurement techniques, and practical guidelines to maintain power supply stability and avoid costly design failures.

    Read More
  • Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    UTMEL13 July 2026424

    Explore how the transition from traditional air-cooling to liquid cooling (direct-to-chip and immersion) in high-density AI server racks alters component thermal profiles. Focus on why design engineers are increasingly specifying Class 2 MLCCs (X7R and X7S dielectrics) over standard X5R variants to prevent thermal degradation near the liquid cooling microchannels. Explain how these capacitors mitigate acoustic noise and voltage bias degradation under heavy workloads. Provide sourcing advice for high-reliability passives via UTMEL during this high-demand memory and passive component super-cycle.

    Read More

Subscribe to Utmel !

Featured Parts More