Introduction to Types of Oscillator Circuits

Published: 20 February 2021 | Last Updated: 14 January 202616937
The oscillator operates on the theory of the oscillation and it is a mechanical or electronic unit. The periodic difference between the two items is dependent on the variations in the electricity. The oscillations are used in the watches, clocks, metal detectors and in many other applications use the oscillators.
This electronics video tutorial explains how the LC oscillator tank circuit works.

LC Oscillator Tank Circuit

2026 Executive Summary

What is an Oscillator? An electronic circuit that converts DC signal (from a power supply) into a periodic AC signal (sine or square wave). In 2026, oscillators remain the "heartbeat" of modern electronics, essential for CPU clock timing, 5G/6G signal modulation, and IoT sensor data transmission.

Key Takeaway: While the fundamental principles of Armstrong, Hartley, and Colpitts circuits established in the early 20th century remain unchanged, their integration has shifted from vacuum tubes to micro-scale MEMS and precision quartz components in today's high-speed digital infrastructure.

Catalog

I. General Introduction
II. Types1. Armstrong Oscillator
2. Hartley Oscillator
3. Colpitts Oscillator
4. Multi-Wave Oscillator

 

I. What are Oscillator Circuits? (2026 Overview)

An oscillator is an electronic circuit that generates a repetitive periodic waveform, usually a sine wave or a square wave, without a mechanical input. They are the fundamental building blocks of modern electronics, acting as the timekeeping source for quartz watches, the frequency generator for 5G radio transmitters, and the clock signal for computer processors. In AM radio receivers, a specialized oscillator known as a resonator is used to tune into specific stations.

Functionally, the oscillator transforms direct current (DC) from a power supply into an alternating current (AC). These signals are ubiquitous in 2026 technology, found in everything from autonomous vehicle sensors to smart home hubs.

There are two primary categories of electronic oscillators: linear (harmonic) and nonlinear (relaxation) oscillators. Linear oscillators produce sinusoidal inputs. They rely on the principles of resonance, conceptually similar to a mass m acted upon by a restoring force in linear equilibrium. By applying Hooke's Law, the system produces a linear force for small displacements, sustaining oscillation.

The following list details the most significant types of oscillators used in engineering history and modern applications:

  • Armstrong Oscillator: The first tickler-feedback circuit.

  • Crystal Oscillator: Known for high stability (Quartz).

  • Hartley Oscillator: Uses inductive voltage division.

  • RC Phase Shift Oscillator: Used for audio frequencies.

  • Colpitts Oscillator: Uses capacitive voltage division.

  • Cross-Coupled Oscillator: Common in IC design.

  • Dynatron Oscillator: Relies on negative resistance.

  • Meissner Oscillator: A variation of the Armstrong.

  • Optoelectronic Oscillator: Converts light to RF energy.

  • Phase Shift Oscillator: Generates sine waves via phase shift.

  • Wien Bridge Oscillator: Famous for low distortion audio generation.

II. Common Types of Oscillators in Modern Electronics

1. How does the Armstrong Oscillator Work?

The Armstrong oscillator is the original LC electronic oscillator which utilizes a tank circuit (inductor and capacitor) to determine frequency. Invented in 1912 by US engineer Edwin Armstrong, it was the first circuit capable of generating continuous radio-frequency oscillations. By 1913, Austrian engineer Alexander Meissner applied this concept to vacuum tubes.

Often called the "tickler oscillator," its defining characteristic is the use of a "tickler coil"—a small inductor that magnetically couples the feedback signal from the output back to the input (tank circuit). Even if the coupling is weak, it sustains oscillation. The resonant frequency f is calculated using the standard LC formula:

Circuit diagram of an Armstrong Oscillator featuring <a href='https://www.utmel.com/blog/categories/transformers/what-is-a-transformer-definition-principle-and-applications'><strong>a transformer</strong></a> feedback loop

f = 1 / (2&pi;&radic;LC)

To maintain oscillation, the circuit requires a 180-degree phase shift, provided by the transistor (or vacuum tube in vintage models). As shown in the figure above, the output flows through the main transformer coil (with a load resistor), and the input is fed back via the secondary coil. The polarity dots indicate that the secondary coil is reversed to achieve the necessary positive feedback. The operating frequency is strictly determined by capacitor C1 and the main transformer inductance.

2. What distinguishes the Hartley Oscillator?

The Hartley oscillator is an LC circuit distinguished by its use of a tapped inductor to create the feedback path. Invented by Ralph Hartley in 1915, this circuit determines frequency via a tuned circuit consisting of a single capacitor in parallel with two inductors (or a single tapped coil) in series. The feedback signal is drawn from the center tap connection between the two inductors.

Schematic of a Hartley Oscillator showing the tapped inductor configuration

Functionally, the Hartley is the "inductive" counterpart to the Colpitts oscillator. Instead of dividing voltage with capacitors, it divides voltage across the inductors L1 and L2. The feedback network ratio is mathematically expressed as:

Feedback Factor = XL2 / XL1 = L2 / L1

2026 Applications:

  • Tunable Circuits: Ideal for generating a broad spectrum of frequencies using a variable capacitor.

  • RF Generation: Commonly used in Radio Frequency (RF) applications up to 30MHz.

  • Signal Receivers: Used in legacy radio receivers requiring wide-range frequency tuning.

3. Why use a Colpitts Oscillator?

The Colpitts Oscillator, designed by Edwin H. Colpitts in 1918, is renowned for its exceptional frequency stability. Unlike the Hartley, the Colpitts circuit uses a capacitive voltage divider for feedback. The tank circuit consists of an inductor in parallel with two capacitors (C1 and C2) connected in series.

Modern Colpitts circuits utilize gain devices such as Bipolar Junction Transistors (BJTs), FETs, or operational amplifiers. The output connects to the input via a feedback loop, functioning as a band-pass filter that sets the oscillation frequency. It is the electrical dual of the Hartley oscillator.

The diagram below illustrates a typical Colpitts configuration. Inductor L and capacitors C1 & C2 form the resonant tank. The voltage across C2 is applied to the base-emitter junction of the transistor to generate sustained feedback oscillations.

Diagram of a Colpitts Oscillator utilizing capacitive voltage division

Advantages & Applications:

  • High Stability: Produces stable sinusoidal signals even at very high frequencies (VHF/UHF).

  • Communications: Critical for modern mobile radio, microwave, and satellite communications.

  • Surface Acoustic Wave (SAW): Often paired with SAW devices for precision sensors.

4. What is the Multi-Wave Oscillator (MWO)?

The Multi-Wave Oscillator (MWO) was a historical experimental device invented by French engineer Georges Lakhovsky between 1920 and 1940. Lakhovsky theorized that cellular nuclei functioned similarly to electronic resonant circuits and could receive or transmit vibratory information. The MWO utilized a unique "Golden Ratio" antenna (printed circuit board style in modern replicas) to generate a wide spectrum of frequencies simultaneously.

Historical & Alternative Applications:

  • Experimental Therapy: Historically, Lakhovsky claimed the device could revitalize cells by restoring their natural resonant frequency.

  • Holistic Use: In alternative medicine circles, it is used for holistic wellness, though these claims lack mainstream medical validation in 2026.

  • Global Usage: MWO units remain popular among enthusiasts of radionics and historical electro-therapy worldwide.

  • Note: Claims regarding cancer treatment or medical cures associated with the MWO are historical in nature and are not supported by current clinical consensus.

Frequently Asked Questions (2026 Edition)

1. What is the main difference between Linear and Nonlinear oscillators?

Linear oscillators (like Hartley and Colpitts) produce sinusoidal waves using resonance, while Nonlinear (relaxation) oscillators produce non-sinusoidal shapes like square or sawtooth waves, often used in digital timing and function generators.

2. Which oscillator is best for high-frequency RF applications?

The Colpitts oscillator is generally preferred for high-frequency RF applications (VHF and UHF) due to its superior capacitive feedback stability compared to the Hartley oscillator.

3. How are oscillators used in IoT devices in 2026?

In IoT, oscillators (specifically MEMS and Crystal oscillators) provide the precise clock signals required for microcontrollers to wake up, process sensor data, and synchronize wireless data transmission (Bluetooth/Wi-Fi) to the cloud.

4. What defines the frequency of an LC oscillator?

The frequency is primarily determined by the values of the Inductor (L) and Capacitor (C) in the tank circuit, calculated by the formula f = 1 / (2&pi;&radic;LC).

5. Are vacuum tube oscillators still used today?

While rare in digital tech, vacuum tube oscillators are still prized in high-end analog audio equipment and high-power RF transmission for their distinct warm tonal characteristics and durability against electromagnetic pulses.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

What is oscillation circuit?

An oscillator is a circuit which produces a continuous, repeated, alternating waveform without any input. Oscillators basically convert unidirectional current flow from a DC source into an alternating waveform which is of the desired frequency, as decided by its circuit components.

Which type of circuit is used in the oscillator?

Types of Oscillators: Harmonic Oscillators & Crystal Oscillators. Harmonic or linear oscillators produce a sinusoidal output where a signal increases and decreases at a predictable level over time. Two basic types are RC, or resistor/capacitor circuits, as well as LC, or inductor capacitor circuits.

What is the principle of oscillator?

There are many types of electronic oscillators, but they all operate according to the same basic principle: an oscillator always employs a sensitive amplifier whose output is fed back to the input in phase. Thus, the signal regenerates and sustains itself. This is known as positive feedback.

What are the types of oscillator?

Types of Oscillators: Common oscillator technology variations  Crystal Oscillators.  SAW oscillators.  MEMS Oscillators.  Voltage-controlled oscillators.  Voltage-controlled oscillators can operate at higher frequencies but are much less stable than other oscillator signals.

Why do we use oscillator?

Oscillators convert direct current (DC) from a power supply to an alternating current (AC) signal. They are widely used in many electronic devices ranging from simplest clock generators to digital instruments (like calculators) and complex computers and peripherals etc.
Related Articles

  • A Simple Method to Build a Programmable Oscillator
    A Simple Method to Build a Programmable Oscillator
    UTMEL27 May 20227191

    Hello, this is Candy. Nice to meet you. Digital potentiometers (digiPOT) are versatile and can be used for a variety of tasks, including filtering and generating AC signals. However, depending on the application, the frequency must occasionally be able to fluctuate and be altered. Programmable solutions that permit frequency change through the appropriate interface are quite handy and, in some situations, extremely beneficial to the development of such designs. Using digiPOT, this article shows how to make a programmable oscillator in which the oscillation frequency and amplitude may be modified independently of one another.

    Read More
  • Introduction to Types of Oscillator Circuits
    Introduction to Types of Oscillator Circuits
    UTMEL14 January 202616937

    The oscillator operates on the theory of the oscillation and it is a mechanical or electronic unit. The periodic difference between the two items is dependent on the variations in the electricity. The oscillations are used in the watches, clocks, metal detectors and in many other applications use the oscillators.

    Read More
  • What are Resonators?
    What are Resonators?
    UTMEL07 January 202617407

    A resonator is an electronic component that can generate a resonant frequency. It has the characteristics of stability and good anti-interference performance. Like the low-frequency circuit, the resonator is also the basic component of the radio frequency circuit. It is widely used in filters, oscillators, frequency meters and adjustable In circuits such as amplifiers. The commonly used RF/MW resonators are basically transmission line resonators.

    Read More
  • How to Understand the Oscilloscope Bandwidth?
    How to Understand the Oscilloscope Bandwidth?
    UTMEL13 December 202110703

    When a user selects an oscilloscope for essential measurements, the oscilloscope's key characteristics are frequently the only criteria used to determine which oscilloscope to employ. An oscilloscope's most essential index parameters are:Bandwidth, Sampling Rate, Record length

    Read More
  •  Active Electroacoustic Resonator-Silent Speaker
    Active Electroacoustic Resonator-Silent Speaker
    UTMEL10 November 20215687

    Hello everyone, I am Rose. Today I will introduce active electroacoustic resonator to you. The only component of this system is a closed-box dynamic speaker. The surface acoustic impedance of the diaphragm is appropriately changed by connecting an active electrical control system to generate an independently tunable sound absorption coefficient, bandwidth, and resonance frequency.

    Read More