web counter

What Determines the Maximum Operating Frequency of a Diode?

Published: 29 June 2022 | Last Updated: 29 June 202213334
Hello, wish you a wonderful day. In this essay, we first pose the following query: what determines the diode's maximum operating frequency? In regards to the solution, the first thing we need to understand is that the junction capacitance and the reverse recovery time of the diode are two distinct concepts. The charging and discharging times of the junction capacitance cannot match the reverse recovery time. You say that, why? Let's start by taking a look at these facts.
In this video we look at how diodes work, where diodes are used, why diodes are used, the different types.

Diodes Explained - The basics how diodes work working principle pn junction

Topics covered in this article:
Ⅰ. Simple Basics
Ⅱ. Facts
Ⅲ. Answers to Questions


Ⅰ. Simple Basics

1. Junction Capacitance

The diode will have parasitic capacitance, which is mainly the junction capacitance, which is a simple diode model.

Figure. 1.png

Figure. 1

 2. Reverse Recovery Time

When the voltage abruptly reverses, the diode current in actual applications does not drop to zero right away; instead, a relatively substantial reverse current remains, which must be reduced to 0.1 times the maximum value. The reverse recovery time is time.

Figure. 2.png

Figure. 2

 

Ⅱ. Facts

Why can the reverse recovery time never be equal to the charge and discharge time of the junction capacitance?

The junction capacitance and reverse recovery time Trr characteristics for diodes are typically provided by the manufacturer. Now let's compare the characteristics of four distinct diode types: Schottky diodes, and ultra-quick recovery diodes.  rapid recovery diodes, and standard diodes, 

We ensure that the four manufacturers of the four different types of diodes   have the same withstand voltage, packing, and maximum working current in order to make the results more credible. The maximum reverse withstand voltage is 100V, all of the packages are SMA, and the maximum operating current is 1A. The manufacturer chosen here is DIODE Semiconductor.

The models are:

● Schottky diode: B1100-13-F

● Ultra-fast recovery diode: US1B-13-F

● Fast recovery diode: RS1B-13-F

● Ordinary diode: S1B-13-F

Screenshots of these diode parameters are as follows:

Figure. 3.png

Figure. 3

The parameters sorted out are as follows:

Figure. 4.png

Figure. 4

The Schottky diode has the greatest junction capacitance among them, as was previously demonstrated. The Schottky diodes aren't running at the highest frequency, are they? The junction capacitance is the biggest, so why?

Although Schottky diodes' reverse recovery time isn't specified in the standard document, we should all be aware that it is the least.

In a strict sense, the Schottky diode's operation differs from the PN junction diode's in that there is no reverse recovery time. Simply said, because parasitic capacitance exists, there is a maximum operating frequency.

We are aware that various sorts of diodes operate in the following sequence from greatest to lowest operating frequency:

Figure. 5.png

Figure. 5

We now know that Schottky's junction capacitance, which is 80 pF, is the greatest. The reverse recovery times of the other three diodes, which range in capacitance from 10pF to 20pF, differ by an order of magnitude.

We may also determine how long it takes for the junction capacitance to fully charge if we assume that the reverse recovery time also serves as the junction capacitance's charging time.

As an illustration, consider the fast recovery diode RS1B-13F, whose junction capacitance is 15pF and reverse recovery current as depicted in the figure below (extracted from the specification). Given that the typical reverse current is around 0.5A, it is simple to calculate that it will take 1.5ns to charge a 15pF from 0V to -50V, which is substantially less time than the actual reverse recovery time of 150ns.

Figure. 6.png

Figure. 6

So it is certain that the length of the reverse recovery time is not determined by the PN junction capacitance.

 

Ⅲ. Answers to Questions

Returning to the original query, what factor determines the diode's maximum operating frequency?

In fact, it is simple to consider: First off, a high operating frequency cannot be used if the junction capacitance is too large. Because the capacitor's impedance decreases with frequency, the signal passes directly from the capacitor and the diode's reverse cut-off capability is lost.

Second, a high operating frequency is not possible if the reverse recovery time is too long. Because voltage flips more quickly at higher frequencies. The voltage changed again after the reverse bias, the reverse current did not return, and the diode's ability to serve as a reverse cut-off was lost.

Therefore, in general, the maximum operating frequency of the diode will depend on the junction capacitance and reverse recovery time. Exactly who chooses who has more influence.

A Schottky diode's operating frequency is determined by the junction capacitance since the reverse recovery time is so quick.

The reverse recovery time determines the maximum operating frequency of PN junction diodes since it has a far bigger impact than the junction capacitance,  which is typically tens of pF.

We also know that Schottky diodes can operate at higher frequencies and have the quickest Schottky speed when compared to PN junction diodes.

In conclusion, The reverse recovery time is not the charging and discharging time of the junction capacitance.


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

What is the purpose of diode?

A diode is a semiconductor device that essentially acts as a one-way switch for current. It allows current to flow easily in one direction but severely restricts current from flowing in the opposite direction.

Can diode convert AC to DC?

A single diode can transform AC power into an intermittent DC flow, but a bridge rectifier uses four diodes to reverse the direction of both sides of the AC pulse.

What is the difference between a diode and a resistor?

A diode is a type of electrical device that allows the current to move through it in only one direction. It consists of an N-type semiconductor and a P-type semiconductor that are placed together. A resistor is an electric component that is used to provide resistance to current in the circuit.
Related Articles

  • All You Need to Know About Rectifier Circuit
    All You Need to Know About Rectifier Circuit
    UTMEL24 April 202518083

    All You Need to Know About Rectifier Circuit

    Read More
  • 15 Key Elements of Diode Selection
    15 Key Elements of Diode Selection
    UTMEL26 November 202119401

    Hello everyone, I am Rose. Welcome back to the new post today. Diodes are one of the most common components in our circuit boards. So, what factors should be considered when selecting models?

    Read More
  • What is a PIN Diode?
    What is a PIN Diode?
    UTMEL04 February 202110547

    While diodes with a simple PN junction are by far the most common type of diode in operation, in a variety of applications, other forms of diode may be used. The PIN diode is one type that is used for a number of circuits. In a variety of places, this diode type is used. For RF switching, the PIN diode is very fine, and the PIN structure in photodiodes is very useful as well.

    Read More
  • Microwave Diode: Introduction and Types
    Microwave Diode: Introduction and Types
    UTMEL07 January 202126481

    Microwave diodes are diodes that work in the microwave frequency band. It is a solid-state microwave device. Microwave band usually refers to the frequency from 300 MHz to 3000 GHz. After the discovery of the point contact diode effect at the end of the 19th century, microwave diodes such as PIN diodes, varactor diodes, and Schottky diode tubes appeared one after another. Microwave diodes have the advantages of small size and high reliability, and are used in microwave oscillation, amplification, frequency conversion, switching, phase shifting and modulation.

    Read More
  • What Determines the Maximum Operating Frequency of a Diode?
    What Determines the Maximum Operating Frequency of a Diode?
    UTMEL29 June 202213334

    Hello, wish you a wonderful day. In this essay, we first pose the following query: what determines the diode's maximum operating frequency? In regards to the solution, the first thing we need to understand is that the junction capacitance and the reverse recovery time of the diode are two distinct concepts. The charging and discharging times of the junction capacitance cannot match the reverse recovery time. You say that, why? Let's start by taking a look at these facts.

    Read More

Subscribe to Utmel !

Featured Parts More