web counter

A Simple Method to Build a Programmable Oscillator

Published: 27 May 2022 | Last Updated: 27 May 20227774
Hello, this is Candy. Nice to meet you. Digital potentiometers (digiPOT) are versatile and can be used for a variety of tasks, including filtering and generating AC signals. However, depending on the application, the frequency must occasionally be able to fluctuate and be altered. Programmable solutions that permit frequency change through the appropriate interface are quite handy and, in some situations, extremely beneficial to the development of such designs. Using digiPOT, this article shows how to make a programmable oscillator in which the oscillation frequency and amplitude may be modified independently of one another.
This video will introduces the Oscillators to you.

Oscillators explained in 4 minutes


Topics covered in this article:
Ⅰ. How to Build a Programmable Oscillator
Ⅱ. Conclusion


Ⅰ. How to Build a Programmable Oscillator

Figure 1 illustrates a typical diode-stabilized Venturi bridge oscillator that can generate a precise sine wave signal at the output with a frequency range of around 10 kHz to 200 kHz (VOUTPUT). The  Wien Bridge  oscillator is made up of two bridges, one of which is a bandpass filter and the other a voltage divider. This example employs the AD5142 digiPOT, which comprises two independently adjustable potentiometers, each with 256-step resolution, in addition to the ADA4610-1 rail-to-rail precision amplifier. As demonstrated in Figure 2, the resistor value is set via  SPI  programming. The AD5142A, which is controlled by I2C, can also be used. Both 10 kΩ and 100 kΩ potentiometers are offered.

Figure. 1 Amplitude Stable Programmable Wien Bridge Oscillator in which resistors are replaced by digiPOTs.png

Figure. 1 Amplitude Stable Programmable Wien Bridge Oscillator in which Resistors are Replaced by digiPOTs

Figure. 2 Functional block diagram of AD5142.png

Figure. 2 Functional Block Diagram of AD5142

R1A, R1B, C1 and C2 form positive feedback in the traditional oscillator circuit depicted in Figure 1, whereas R2A, R2B, and the two parallel diodes D1 and D2 or their resistor RDIODE form a negative feedback. The formula can be utilized in this scenario:

R2 = R2A||(R2B+RDIODE)

In order to achieve continuous stable oscillation, the phase shift in the loop gain needs to be eliminated. Expressed as a formula, the oscillation frequency:

ω0 = 1/RC or f0 = 1/2πRC

where R represents the programmable resistor value on the AD5142:

R = (256-D)/256*RAB

D represents the decimal equivalent of the programmable digital code in the AD5142, and RAB represents the total resistance of the potentiometer.

The Wien bridge oscillator must be generally balanced in order to maintain oscillation, which means the positive and negative feedback gains must be synchronized. The oscillation amplitude or VOUTPUT will increase until the amplifier saturates if the positive feedback (gain) is too strong. If negative feedback takes precedence, the oscillation amplitude will decrease.

The gain R2/R1 in this circuit should be tuned to roughly 2 or greater. The signal will begin to oscillate as a result of this.

However, turning on and off the diodes in the negative feedback loop alternately reduces the gain to less than 2, stabilizing the oscillations.

Once the desired oscillation frequency is determined, the oscillation amplitude can be tuned independently of frequency via R2. It can be calculated by the following formula:

2/3VOUTPUT = ID*R2B+VD

As a result, the ID of the variable and VD denote the diode forward current and diode forward voltage, respectively, through D1 and D2. If R2B is shorted, the oscillation amplitude will be around ±0.6 V. An equilibrium is attained when the magnitude of R2B is of the correct magnitude, allowing VOUTPUT to converge. For R2B, a single 100 kΩ digiPOT is utilized in the circuit shown in Figure 1.


Ⅱ. Conclusion

The 8.8 kHz, 17.6 kHz, and 102 kHz oscillation frequencies can be tuned with resistance values of 8 kΩ, 4 kΩ, and 670Ω, respectively, using the specified circuit and a 10 kΩ dual digiPOT, with frequency inaccuracies as low as ±3%. The frequency error may be affected by increasing the output frequency. The frequency inaccuracy will increase to 6% at 200 kHz, for example.

When using such circuits in frequency-dependent applications, it's important not to exceed the digiPOT 's bandwidth limit, which is determined by the programmable resistance. Furthermore, the frequency tuning depicted in Figure 1 necessitates the use of the same  R1A  and R1B resistor values. The two channels, on the other hand, can only be set in order, resulting in a temporary critical intermediate state. This scenario is unacceptable for some applications. A digiPOT that supports daisy-chain mode, such as the AD5204, can be used in these circumstances to modify the resistor values at the same time.


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

How do oscillator circuits work?

An electronic oscillator is a circuit that generates a periodic, oscillating electronic signal, which is usually a sine wave, square wave, or triangle wave. Oscillators are devices that transform direct current (DC) from a power source to alternating current (AC).

What is a crystal oscillator?

A crystal oscillator is an electronic oscillator circuit in which the frequency-selective element is a piezoelectric crystal. The oscillator frequency is used to keep time in quartz wristwatches, to generate a stable clock signal for digital integrated circuits, and to stabilize frequencies in radio transmitters and receivers. Because quartz crystals are the most prevalent type of piezoelectric resonator, oscillator circuits that utilize them are known as crystal oscillators. In similar circuits, however, different piezoelectric materials, such as polycrystalline ceramics, are employed.

What is a crystal oscillator used for?

Crystal oscillators are primarily utilized to provide a consistent clock signal in digital integrated circuits and in certain applications that demand a high-frequency reference.
Related Articles

  • A Simple Method to Build a Programmable Oscillator
    A Simple Method to Build a Programmable Oscillator
    UTMEL27 May 20227774

    Hello, this is Candy. Nice to meet you. Digital potentiometers (digiPOT) are versatile and can be used for a variety of tasks, including filtering and generating AC signals. However, depending on the application, the frequency must occasionally be able to fluctuate and be altered. Programmable solutions that permit frequency change through the appropriate interface are quite handy and, in some situations, extremely beneficial to the development of such designs. Using digiPOT, this article shows how to make a programmable oscillator in which the oscillation frequency and amplitude may be modified independently of one another.

    Read More
  • Introduction to Types of Oscillator Circuits
    Introduction to Types of Oscillator Circuits
    UTMEL14 January 202618317

    The oscillator operates on the theory of the oscillation and it is a mechanical or electronic unit. The periodic difference between the two items is dependent on the variations in the electricity. The oscillations are used in the watches, clocks, metal detectors and in many other applications use the oscillators.

    Read More
  • What are Resonators?
    What are Resonators?
    UTMEL07 January 202618447

    A resonator is an electronic component that can generate a resonant frequency. It has the characteristics of stability and good anti-interference performance. Like the low-frequency circuit, the resonator is also the basic component of the radio frequency circuit. It is widely used in filters, oscillators, frequency meters and adjustable In circuits such as amplifiers. The commonly used RF/MW resonators are basically transmission line resonators.

    Read More
  • How to Understand the Oscilloscope Bandwidth?
    How to Understand the Oscilloscope Bandwidth?
    UTMEL13 December 202111235

    When a user selects an oscilloscope for essential measurements, the oscilloscope's key characteristics are frequently the only criteria used to determine which oscilloscope to employ. An oscilloscope's most essential index parameters are:Bandwidth, Sampling Rate, Record length

    Read More
  •  Active Electroacoustic Resonator-Silent Speaker
    Active Electroacoustic Resonator-Silent Speaker
    UTMEL10 November 20216245

    Hello everyone, I am Rose. Today I will introduce active electroacoustic resonator to you. The only component of this system is a closed-box dynamic speaker. The surface acoustic impedance of the diaphragm is appropriately changed by connecting an active electrical control system to generate an independently tunable sound absorption coefficient, bandwidth, and resonance frequency.

    Read More

Subscribe to Utmel !

Featured Parts More