web counter
Resistor Color Code Calculator

Resistor Color Code Calculator is an interactive online Calculator to calculate the resistance value based on color bands or color-coded stripes on a resistor. There are many different types of resistors in electronics today. A resistance calculator for the color code of resistor is an efficient way to help you to find the right one for your needs, whether it is for a circuit or just to know what type of resistor you have in your box. Known as ohmmeter calculator, the Color Code resistor calculator is the integration of 4 Band, 5 Band and 6 Band Resistor Color Code Calculators. So you can use this parallel resistor calculator to make basic and complex electrical circuits for both home and industrial purposes. And the following will show you how to use this tool to read the color code of resistors, calculate the resistor value in Ohms (Ω) for 4-band, 5-band and 6-band resistors based on the color code on the resistor and identify the resistor's value, tolerance, and power rating.

Number of Bands

Resistor Parameters

1st Band of Color
2nd Band of Color
Multiplier
Tolerance
Output
-
-
-
-

Resistor value:

Introduction

How To Calculate Resistor Resistance Value From Resistor Color Code Bands if your new in electronic & you don't know how Resistor Color Code Bands Calculations work. So just watch this Video To learn every thing about  Resistor Resistance Value from  Color Code Bands.

Resistor Color Code | Calculation Resistance From Color Bands

Resistor Color Code Calculator Overview

The Resistor Color Code Calculator helps identify the resistance value, tolerance, and temperature coefficient of axial leaded resistors from their color bands. It supports common 4-band, 5-band, and 6-band resistor markings, so it can be used for quick part identification, repair work, circuit prototyping, and checking values before soldering a resistor into a board.

Color bands are used because many resistors are too small for printed text. The first bands give the significant digits, the next band gives the multiplier, and the tolerance band shows how far the actual resistance may vary from the nominal value. On a 6-band resistor, the final band usually indicates the temperature coefficient in ppm/K.

Standard resistor color code chart

The standard resistor color code chart.

How to Use the Resistor Color Code Calculator

  1. Count the color bands on the resistor body: 4, 5, or 6 bands are the most common.

  2. Find the tolerance band first. It is often separated by a wider gap and may be gold, silver, brown, red, green, blue, or violet.

  3. Read the resistor from the opposite end, starting with the significant digit bands.

  4. Select each band color in the calculator. The tool returns the resistance value in Ω, kΩ, or MΩ, along with the tolerance.

  5. For a 6-band resistor, also select the temperature coefficient band if it is present.

If the band spacing is unclear, compare the result with nearby standard resistor values. A value such as 10 kΩ, 4.7 kΩ, 220 Ω, or 1 MΩ is usually more likely than an unusual value on a general-purpose resistor.

A video guide from the original article is available here: How to read a resistor color code chart.

4-Band, 5-Band, and 6-Band Resistors

Resistor TypeBand RolesTypical Use
4-band resistor2 significant digits, multiplier, toleranceGeneral-purpose resistors, often 5% or 10% tolerance
5-band resistor3 significant digits, multiplier, tolerancePrecision resistors where one extra digit is needed
6-band resistor3 significant digits, multiplier, tolerance, temperature coefficientPrecision and temperature-sensitive designs

Resistor Color Code Table

ColorDigitMultiplierCommon ToleranceTemperature Coefficient
Black0×1
250 ppm/K
Brown1×10±1%100 ppm/K
Red2×100±2%50 ppm/K
Orange3×1 kΩ
15 ppm/K
Yellow4×10 kΩ
25 ppm/K
Green5×100 kΩ±0.5%20 ppm/K
Blue6×1 MΩ±0.25%10 ppm/K
Violet7×10 MΩ±0.1%5 ppm/K
Gray8×100 MΩ±0.05%1 ppm/K
White9×1 GΩ

Gold
×0.1±5%
Silver
×0.01±10%
No band

±20%

Some precision resistor series may use additional tolerance or temperature-coefficient markings. Always check the manufacturer datasheet when the resistor is part of a safety-critical, high-voltage, high-power, or precision measurement design.

4-Band Resistor Formula

A 4-band resistor is read as:

Resistance = (first digit second digit) × multiplier

For example, brown-black-orange-gold is 10 × 1000 Ω = 10000 Ω, or 10 kΩ ±5%.

5-Band Resistor Formula

A 5-band resistor adds a third significant digit:

Resistance = (first digit second digit third digit) × multiplier

For example, brown-black-black-red-brown is 100 × 100 Ω = 10000 Ω, or 10 kΩ ±1%.

6-Band Resistor Formula

A 6-band resistor is read like a 5-band resistor, but the sixth band gives the temperature coefficient. This value describes how much the resistor value changes with temperature.

For example, brown-black-black-red-brown-red is 10 kΩ ±1%, 50 ppm/K.

Examples: 10 kΩ and 100 Ω Resistor Color Codes

Target Value4-Band Example5-Band ExampleMeaning
100 ΩBrown - Black - Brown - GoldBrown - Black - Black - Black - Brown100 Ω, with tolerance set by the final band
220 ΩRed - Red - Brown - GoldRed - Red - Black - Black - Brown220 Ω, common in LED and signal circuits
1 kΩBrown - Black - Red - GoldBrown - Black - Black - Brown - Brown1000 Ω, or 1 kΩ
4.7 kΩYellow - Violet - Red - GoldYellow - Violet - Black - Brown - Brown4700 Ω, or 4.7 kΩ
10 kΩBrown - Black - Orange - GoldBrown - Black - Black - Red - Brown10000 Ω, or 10 kΩ
1 MΩBrown - Black - Green - GoldBrown - Black - Black - Yellow - Brown1000000 Ω, or 1 MΩ

100 ohm resistor color code for a 4-band resistor

100 Ω resistor color code for a 4-band resistor.

How to Read Band Direction

The tolerance band is often placed slightly farther away from the other bands, making it a useful clue for orientation. On many 4-band resistors, gold or silver appears at the tolerance end. Start reading from the opposite side.

If the resistor has a brown or red tolerance band and both directions look plausible, calculate both possible values and compare them with standard resistor values. The value that belongs to a common E-series and matches the circuit context is usually the intended reading.

Resistor Color Bands by Type

3-band 4-band 5-band and 6-band resistor color code examples

Three-band resistors omit the tolerance band, so their tolerance is commonly treated as ±20%. Four-band resistors are common in everyday electronics. Five-band and six-band resistors are often used where tighter tolerance or better temperature stability is required.

What Is a Resistor?

A resistor is a passive electronic component that limits current, divides voltage, sets bias points, terminates signals, or converts electrical energy into heat. Fixed resistors have a nominal resistance value, while variable resistors such as potentiometers allow the resistance to be adjusted.

The rated value printed or marked on a resistor is not always the exact measured value. The actual value depends on tolerance, temperature, aging, and operating conditions. In precision circuits, the tolerance and temperature coefficient can matter as much as the nominal resistance.

Tolerance and Resistance Range

Tolerance tells you the expected variation around the nominal resistance value. For example, a 10 kΩ resistor with ±5% tolerance may measure from 9.5 kΩ to 10.5 kΩ under specified conditions.

Nominal ValueToleranceMinimum ValueMaximum Value
100 Ω±5%95 Ω105 Ω
1 kΩ±1%990 Ω1010 Ω
10 kΩ±0.1%9990 Ω10010 Ω
1 MΩ±10%900 kΩ1.1 MΩ

Standard Resistor Values and E-Series

Standard resistor values are organized into E-series such as E3, E6, E12, E24, E48, E96, and E192. Each series divides a decade into a fixed number of preferred values. Lower-count series are common for general designs, while higher-count series are used for closer tolerance and precision work.

SeriesTypical Tolerance AssociationValues Per DecadeTypical Use
E3Wide tolerance3Non-critical pull-up, pull-down, and rough current limiting
E620%6General non-precision designs
E1210%12Common analog and digital circuits
E245%24General-purpose through-hole and film resistors
E482%48Closer tolerance designs
E961%96Precision analog, filters, and measurement circuits
E1920.5%, 0.25%, 0.1%, and tighter192High-precision applications

Standard EIA resistor value table

Preferred resistor values chart

Common Reading Mistakes

MistakeWhy It MattersHow to Avoid It
Reading from the tolerance endThe digits and multiplier will be reversed, giving a wrong value.Look for the wider gap or the gold/silver tolerance band first.
Confusing red, orange, brown, or gold bandsA small color difference can change the value by a factor of 10 or more.Use good lighting and compare with nearby known resistors if possible.
Ignoring toleranceA resistor may be in spec even if it does not measure exactly at the nominal value.Calculate the allowed minimum and maximum resistance range.
Measuring in-circuitParallel circuit paths can make a resistor appear lower than its true value.Lift one lead or remove the part when an accurate measurement is required.
Using color code for damaged partsHeat, age, or coating damage can discolor bands.Confirm with a multimeter and check the circuit schematic.

Applications

Resistor color code reading is useful when repairing older equipment, identifying loose components, checking bill-of-material values, learning basic electronics, and confirming whether a resistor matches a schematic. It is especially helpful for axial through-hole resistors where the color bands are still the main marking method.

For surface-mount resistors, use an SMD Resistor Code Calculator instead, because SMD parts usually use printed numeric or alphanumeric codes rather than color bands.

FAQ

What does a gold band mean on a resistor?

A gold band is commonly used as a multiplier of ×0.1 or as a tolerance band of ±5%, depending on its position.

What does a silver band mean on a resistor?

A silver band is commonly used as a multiplier of ×0.01 or as a tolerance band of ±10%, depending on its position.

Why do some resistors have five bands?

Five-band resistors use three significant digits instead of two, which allows more precise nominal resistance values.

What is ppm/K on a resistor?

ppm/K means parts per million per kelvin. It describes the expected change in resistance for each 1 K temperature change.

Can I rely only on the color code?

The color code is a fast identification method, but it should be confirmed with a multimeter when the resistor is critical, old, overheated, or difficult to read.

Related Online Calculation Tools

Frequently Asked Questions

1.How do you calculate resistor color code?

Hold the resistor with the gold or silver band to the right and read the color codes from the left to the right. Select the color codes from the bands on the resistor. Read the colors from left to right. The resistance value based on the color code provided is now displayed.

2.What is a Resistor Colour code?

A Resistor colour code or Resistor Color Code is a system for displaying information by using different colors. The earliest examples of color codes in use are for long distance communication by use of flags, as in semaphore communication.

3.How do I know if I have a 100K resistor?

100k ohm resistor color code- 4 band  
1) Brown, Black, Yellow, Gold. 
2) And tolerance considered as ==> 5% of 100K ==>5000Ω  
3) Other methods: Remove the resistor from PCB then test it with a DMM in resistance mode and note down its value. It needs to be separated from pcb so as to avoid the equivalent parallel resistance from resistors in the circuit.

4.What does a 1k resistor look like?

1k ohm resistor color code are - Brown - black - red  
1 k ohm Resistors with 5 band are 1% tolerance resistors. First three bands determine the value of the resistor.

5.What is resistor value?

A resistor is a device that opposes the flow of electrical current. The bigger the value of a resistor the more it opposes the current flow. The value of a resistor is given in ohms and is often referred to as its 'resistance'.

6.How is a 3.9 K resistor color code?

3.9K Ohm 0.5W Metal Film Resistor (MFR) with ±1% Tolerance. 3.9K Ohm Resistor Color Code: Orange, White, Black, Brown, Brown.

7.What is a 100K resistor?

Actual value of 100k Ohm resistor is calculated as:  1st band= Brown= 1 (1st digit) 2nd band= Black= 0 (2nd digit) 3rd band= Yellow= 4(multiplier)= 10000. 4th band= Gold= ±5% (tolerance) Therefore, 10×1000000±5% ==> 1000000Ω ==> 100KΩ

8.What is resistor explain?

A passive electrical component with two terminals that are used for either limiting or regulating the flow of electric current in electrical circuits. The main purpose of the resistor is to reduce the current flow and to lower the voltage in any particular portion of the circuit.

9. What is 2.2k ohm Resistor color code for 4-band?

The color code of 2.2 k resistor is Red-Red-Red-Gold. From the above resistor color code table, you will find that Red stands for 2 and Red for 2. The third band is Red, so it means a multiplier value of 2 (100). And the 4th band is Gold, which means the tolerance is 5%. Thus the value of 2k2 resistor is 56 · 102 = 56 · 100 = 5600 Ω. Thus The resistance value lies therefore between 5320 and 5880 Ω (5560 ± 5%).

10.How do I know if I have a 10k ohm resistor?

You could read its band color and get it with the online color code calculator. For example, the 4 band 10k resistor color code is brown-black-orange-silver/gold. And the tolerance of the silver band is 10% or gold for 5% tolerance. And if it is a 5 band resistor, the 10k resistor color code will be brown-black-black-red. Meanwhile the tolerance band is separated from the other 4 bands color code. Its color could be one of several depending on the resistors tolerance.

11.How can I calculate a 6-band resistor value?

Fill in the blanks using the first five colors. Resistors with six bands are essentially five-band resistors with an extra ring showing the temperature coefficient or dependability.

12. I have a resistor with only 3 bands, How to know its value?

3-band resistors have a tolerance of 20% and are widely employed by amateurs or in situations where the resistance value is not crucial. Brown, black, and gold are the colors for a 3 band 1R0 (1 ) resistor. Between 1.2 and 0.8 will be the resistance value. 
Therefore, you don't need to enter the 4th band while using our online resistor color code calculator. Because there is not a tolerance ring for 20% resistors. However, the 3 band resistor will be calculated through the 4 bands color code rule (digit, digit, multiplier).Therefore, the 4 band resitor color code calculator is 3 band resistor color code calculator too.

For example:
3 band resistor color code of a 10K resistor with 20% tolerance is Brown, black, orange.
Resistor color code 3 band for 220 ohm resistors with 20% tolerance is Red, red, brown.

13. Which is the first band for the colored-resistors?

There are a few guidelines to follow: 
1.) The color bands on certain resistors are packed together and/or near to one end. Hold the resistor to the left of the tightly clustered bars and read the resistor from left to right. 
2.) The process for reading 5% and 10% resistors is straightforward: hold the resistor with the silver or gold band to the right and read the resistance from left to right. 
3.) The first band can't be silver or gold, so if you have one, you'll know where to start right away. As fundamental resistor values vary from 0.1 Ohm to 10 Mohms, the third color for 4-band resistors will be blue (106) or less, while the fourth color for 5-band resistors will be green (105) or less.

14. How do you read a 3-band resistor?

For a 3-band resistor color codes, the first two bands always denote the first two digits of the resistance value while the third band represents the multiplier. In the example we have, the bands are brown, black and brown. The first band is the brown band closest to the edge.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

TP3420AV309TP3420AV309Texas InstrumentsInterface - Telecom20-LCC (J-Lead)IC TELECOM INTERFACE 20PLCC-

In stock

Minimum: 1

19-217/R6C-AL1M2VY/3T19-217/R6C-AL1M2VY/3TEverlight Electronics Co LtdLED Indication - Discrete0603 (1608 Metric)LED RED CLEAR 2SMD-

In stock : 6070

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock : 10000

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP
  • 1:$0.465882
  • 10:$0.439511
  • 100:$0.414633
  • 500:$0.391163

In stock : 1000

Minimum: 1

HMC588LC4BTRHMC588LC4BTRAnalog Devices Inc.RF Misc ICs and Modules24-TFQFN Exposed PadIC OSC VCO WIDEBAND 24SMD-

In stock : 5

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

DS21Q48NDS21Q48NMaxim IntegratedInterface - Telecom144-BBGAIC LIU E1/T1/J1 4X 5V LONG144BGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

EEF-CS1E150REEF-CS1E150RPanasonic Electronic ComponentsAluminum - Polymer Capacitors2917 (7343 Metric)Aluminum Organic Polymer Capacitors 15uF 25volt
  • 1:$0.593588
  • 10:$0.559988
  • 100:$0.528291
  • 500:$0.498388

In stock : 28000

Minimum: 1

AFBR-2418TZAFBR-2418TZBroadcom LimitedFiber Optics - Receivers-Fiber Optic Transmitters, Receivers, Transceivers RX DC-50MBd ML 820nm ST Thrd-

In stock : 660

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock : 6000

Minimum: 1

TZY2Z060AC01R00TZY2Z060AC01R00Murata ElectronicsTrimmers, Variable Capacitors-2.5 ~ 6pF Trimmer Capacitor 25V Top Adjustment-

In stock : 4636

Minimum: 1

SML-S13RTT86SML-S13RTT86ROHM SemiconductorInfrared, UV, Visible Emitters1206 (3216 Metric)EMITTER IR 850NM 30MA 1206-

In stock : 1

Minimum: 1

TZY2Z100AC01R00TZY2Z100AC01R00Murata ElectronicsTrimmers, Variable Capacitors-3 ~ 10pF Trimmer Capacitor 25V Top Adjustment-

In stock : 22000

Minimum: 1

DGD2136S28-13DGD2136S28-13Diodes IncorporatedPMIC - Gate Drivers28-SOIC (0.295, 7.50mm Width)HV GATE DRIVER SO-28-

In stock : 2799

Minimum: 1

TEN-HS5TEN-HS5Traco PowerAccessoriesAluminumTRACOPOWER TEN-HS5 Power Supply Accessory, Heat Sink, DC/DC Converter, TEN25, TEN25WI Series
  • 1:$3.808917
  • 10:$3.593318
  • 100:$3.389922
  • 500:$3.198040

In stock : 255

Minimum: 1

HEF4044BT,652HEF4044BT,652NXP USA Inc.Logic - Latches16-SOIC (0.154, 3.90mm Width)IC R/S LATCH 3-STATE QUAD 16SOIC-

In stock

Minimum: 1

T9GV5L14-22T9GV5L14-22TE ConnectivityRelays-Power Relays, Standard, Monostable, DC, 900 mW Coil Power Rating DC, 538 Ω Coil Resistance, UL Coil Insulation Class F, Potter & Brumfield T9G-

In stock

Minimum: 1