web counter
Capacitance Conversion

Use Utmel's capacitance conversion chart and calculator to perform conversions between code to capacitor value and capacitance units from pF, µF, nF, and F

Capacitance Conversion

Picofarad
pF
Nanofarad
nF
Microfarad
µF
Farad
F

CAPACITOR CONVERSION CHART

Introduction

Methods in converting from milli, micro, nano and pico to farad.

Capacitor Conversion

Capacitance Conversion Calculator

Use this calculator to convert capacitance values between farads, millifarads, microfarads, nanofarads, picofarads, and other supported units. It can also help decode common three-digit capacitor value codes such as 104 or 472 when the code follows the picofarad marking convention.

Unit conversion and component marking are different tasks. A capacitance unit has a defined SI scale factor, while markings printed on a capacitor may also contain tolerance, rated voltage, dielectric, series, date, or manufacturer-specific information. Verify an actual component against its datasheet whenever identification matters.

How to Use the Capacitance Converter

  1. Enter the known capacitance value.

  2. Select its current unit, such as µF, nF, or pF.

  3. Select the desired output unit.

  4. Calculate and review the converted value.

  5. When decoding a printed code, confirm that the component uses the expected pF code convention.

Unit symbols are case-sensitive. Use F for farad, mF for millifarad, µF for microfarad, nF for nanofarad, and pF for picofarad. When the micro symbol is unavailable, uF is often used informally in plain text, but µF is the SI-prefix form.

What Is Capacitance?

Capacitance describes the ratio of electric charge stored on a conductor to the potential difference associated with that charge. For an ideal capacitor:

C = Q/V

where C is capacitance, Q is electric charge, and V is voltage. The SI unit of capacitance is the farad, symbol F. One farad equals one coulomb per volt:

1 F = 1 C/V

In electronics, one farad is relatively large, so capacitor values are commonly stated in millifarads, microfarads, nanofarads, or picofarads.

Capacitance Units and SI Prefixes

UnitSymbolValue in Farads
FaradF1 F
MillifaradmF10−3 F
MicrofaradµF10−6 F
NanofaradnF10−9 F
PicofaradpF10−12 F
FemtofaradfF10−15 F
AttofaradaF10−18 F

Common Capacitance Relationships

  • 1 F = 1,000 mF

  • 1 F = 1,000,000 µF

  • 1 F = 1,000,000,000 nF

  • 1 F = 1,000,000,000,000 pF

  • 1 mF = 1,000 µF

  • 1 µF = 1,000 nF = 1,000,000 pF

  • 1 nF = 1,000 pF

Capacitance Conversion Formula

Express each unit as a factor of one farad, then use:

Target value = Source value × Source factor in F ÷ Target factor in F

Example: Convert 4.7 µF to nF and pF

4.7 µF × 1,000 = 4,700 nF

4.7 µF × 1,000,000 = 4,700,000 pF

Example: Convert 220 nF to µF

220 nF ÷ 1,000 = 0.22 µF

Example: Convert 3,300 pF to nF and µF

3,300 pF ÷ 1,000 = 3.3 nF

3,300 pF ÷ 1,000,000 = 0.0033 µF

Capacitance Conversion Chart

MicrofaradsNanofaradsPicofarads
0.000001 µF0.001 nF1 pF
0.00001 µF0.01 nF10 pF
0.0001 µF0.1 nF100 pF
0.001 µF1 nF1,000 pF
0.01 µF10 nF10,000 pF
0.1 µF100 nF100,000 pF
1 µF1,000 nF1,000,000 pF
10 µF10,000 nF10,000,000 pF
100 µF100,000 nF100,000,000 pF

How to Read a Three-Digit Capacitor Code

In the common three-digit convention, capacitance is expressed in picofarads. The first two digits are the significant figures and the third digit is the number of zeros that follow:

Capacitance in pF = First two digits × 10Third digit

For example, code 104 means 10 × 104 pF = 100,000 pF = 100 nF = 0.1 µF.

Three-Digit Capacitor Code Examples

CodeCalculationCapacitance
10010 × 100 pF10 pF
10110 × 101 pF100 pF
10210 × 102 pF1,000 pF = 1 nF
10310 × 103 pF10,000 pF = 10 nF = 0.01 µF
10410 × 104 pF100,000 pF = 100 nF = 0.1 µF
10510 × 105 pF1,000,000 pF = 1 µF
22122 × 101 pF220 pF
22222 × 102 pF2,200 pF = 2.2 nF
33133 × 101 pF330 pF
33233 × 102 pF3,300 pF = 3.3 nF
47147 × 101 pF470 pF
47247 × 102 pF4,700 pF = 4.7 nF
47347 × 103 pF47,000 pF = 47 nF = 0.047 µF
47447 × 104 pF470,000 pF = 470 nF = 0.47 µF
47547 × 105 pF4,700,000 pF = 4.7 µF

Special and Manufacturer-Specific Markings

Not every marking follows the basic three-digit rule. Some capacitor families use a letter as a decimal marker, while some low-picofarad coding systems use 9 to indicate division by ten. For example, a manufacturer may document 919 as 9.1 pF. These special cases are not universal.

A code such as 4R7 may be used by some manufacturers to represent 4.7 pF, but the same characters can have another meaning in a different component system. Very small surface-mount capacitors may have no body marking at all. Always consult the relevant series datasheet, packaging label, bill of materials, or measured value.

Capacitance Tolerance Letters

A letter following the capacitance code may indicate tolerance. Common examples include:

LetterCommon ToleranceExample
J±5%104J commonly indicates 0.1 µF ±5%
K±10%104K commonly indicates 0.1 µF ±10%
M±20%104M commonly indicates 0.1 µF ±20%

These examples are widely used, but the full marking system still depends on the capacitor family. Other letters may describe temperature characteristic, rated voltage, failure rate, or production information rather than capacitance tolerance.

Do Not Confuse Capacitor and Resistor Codes

A three-digit code can look identical on resistors and capacitors while using a different base unit. For example, 104 on a capacitor following the pF convention means 100,000 pF or 0.1 µF. On a resistor using the common ohm convention, 104 means 100,000 Ω or 100 kΩ. Identify the component type before decoding the number.

Capacitance in Circuit Calculations

Convert capacitance to farads before using it in SI-based equations unless the equation explicitly uses another unit.

QuantityFormulaUse
ChargeQ = CVCharge stored at voltage V
Stored energyE = ½CV2Ideal capacitor energy
Capacitive reactanceXC = 1/(2πfC)Ideal capacitor reactance at frequency f
RC time constantτ = RCFirst-order resistor-capacitor timing

Worked Circuit Example

A capacitor is marked 104 and is connected in an ideal RC circuit with a 10 kΩ resistor.

  1. Decode 104 as 100,000 pF.

  2. Convert 100,000 pF to 100 nF or 0.1 µF.

  3. Convert 0.1 µF to 0.0000001 F.

  4. Calculate τ = RC = 10,000 Ω × 0.0000001 F = 0.001 s.

The ideal RC time constant is 1 ms.

Accuracy and Practical Limits

  • Unit conversion is exact when the original number is exact, but a real capacitor has tolerance.

  • Capacitance can vary with temperature, frequency, DC bias, aging, and measurement conditions depending on capacitor technology.

  • Parasitic resistance and inductance affect real behavior, especially at high frequency.

  • A body code may be incomplete or manufacturer-specific.

  • Use a suitable capacitance meter and the manufacturer's test conditions when actual value matters.

  • Do not infer voltage rating, polarity, dielectric, or safety classification from capacitance alone.

Common Capacitance Conversion Mistakes

  • Using C = Q × V instead of C = Q/V.

  • Using C as the unit symbol for capacitance instead of F.

  • Confusing mF with µF; 1 mF equals 1,000 µF.

  • Moving the decimal point in the wrong direction between µF, nF, and pF.

  • Reading 104 as 104 pF instead of 100,000 pF under the standard three-digit convention.

  • Applying capacitor pF decoding to a resistor marking.

  • Assuming every printed letter is a tolerance code.

  • Using a nominal converted value as if it were a measured capacitance.

Capacitance Conversion FAQ

How many nanofarads are in one microfarad?

One microfarad equals 1,000 nanofarads.

How many picofarads are in one nanofarad?

One nanofarad equals 1,000 picofarads.

What does capacitor code 104 mean?

Under the common pF code convention, 104 means 10 followed by four zeros in picofarads: 100,000 pF = 100 nF = 0.1 µF.

What does capacitor code 472 mean?

Under the common pF code convention, 472 means 47 × 102 pF = 4,700 pF = 4.7 nF.

Is uF the same as µF?

In informal electronic text, uF is often substituted when the micro symbol is unavailable. Both are intended to represent microfarads, but µF is the proper SI-prefix symbol.

Can a capacitance code identify the voltage rating?

Not by itself. A capacitance code identifies capacitance only under its documented convention. Voltage rating and other properties require the complete manufacturer marking or datasheet.

Why can two capacitors with the same marked value measure differently?

Manufacturing tolerance and operating conditions can change the measured capacitance. The amount depends on capacitor technology, temperature, frequency, applied DC bias, aging, and the specified test method.

Capacitance Conversion Video

Watch the original capacitance conversion video on YouTube.

References

Frequently Asked Questions

What is capacitor value conversion used for?

Capacitor conversion helps resolve notation ambiguity when values overlap between units like µF/nF/pF. It ensures accurate component selection by converting between units like 0.1µF to 100nF or 100,000pF.

How do I convert microfarads (µF) to nanofarads (nF)?

Multiply the microfarad value by 1,000. For example/ 1µF = 1,000nF/ 0.01µF = 10nF. Refer to the conversion chart for common µF/nF/pF equivalents.

Why are nanofarads (nF) less commonly used?

Some regions avoid nF notation/ expressing values as fractions of µF (e.g./ 0.1µF) or large pF values (e.g./ 100,000pF). Use conversion tools to translate nF markings when needed.

What are common capacitor value conversions?

Examples include/ 1µF = 1,000nF = 1,000,000pF/ 0.001µF = 1nF = 1,000pF. The chart clarifies overlaps like 0.1µF = 100nF or 10nF = 10,000pF.

How to handle ambiguous capacitor markings?

Cross-check values using the conversion chart. For example/ a component labeled “0.1” could mean 0.1µF (100nF) or 0.1nF (100pF). Confirm units with a multimeter or datasheet if unclear.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

AD9364BBCZAD9364BBCZAnalog Devices Inc.RF Transceiver ICs144-LFBGA, CSPBGARF Transceiver 1.3V 144-Pin CSP-BGA Tray-

In stock

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock : 10000

Minimum: 1

CYBL10162-56LQXICYBL10162-56LQXICypress Semiconductor CorpRF Transceiver ICs56-UFQFN Exposed PadMCU 32-Bit CYBL10X6X ARM Cortex M0 RISC 128KB Flash 1.8V/2.5V/3.3V/5V 56-Pin QFN EP Tray-

In stock : 48

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP
  • 1:$0.519922
  • 10:$0.490493
  • 100:$0.462729
  • 500:$0.436537

In stock : 1000

Minimum: 1

HSMS-282P-TR1GHSMS-282P-TR1GBroadcom LimitedDiodes - RF6-TSSOP, SC-88, SOT-363Diode Schottky 15V 6-Pin SOT-363 T/R-

In stock

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

SI8261BBD-C-ISSI8261BBD-C-ISSilicon LabsIsolators - Gate Drivers6-SOIC (0.295, 7.50mm Width)4A Gate Driver Capacitive Coupling 5000Vrms 1 Channel 6-SDIP
  • 1:$7.581997
  • 10:$7.152827
  • 100:$6.747950
  • 500:$6.365991

In stock : 28210

Minimum: 1

SI8261BAD-C-ISSI8261BAD-C-ISSilicon LabsIsolators - Gate Drivers6-SOIC (0.295, 7.50mm Width)Gate Drivers 5kV Opto input Sgl channel 4.0A driver
  • 1:$8.435041
  • 10:$7.957586
  • 100:$7.507156
  • 500:$7.082223

In stock : 100000

Minimum: 1

CSR8510A06-ICXR-RCSR8510A06-ICXR-RQualcommRF Transceiver ICs6-XFBGAIC RF TXRX BLUETOOTH 6XFBGA-

In stock

Minimum: 1

FOD8333FOD8333ON SemiconductorIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)Optocoupler AC/DC-IN 1-CH DC-OUT 16-Pin SO Rail
  • 1:$7.808566
  • 10:$7.366572
  • 100:$6.949596
  • 500:$6.556223

In stock : 50

Minimum: 1

FOD8332R2FOD8332R2ON SemiconductorIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)OPTOISO 4.243KV GATE DRIVER 16SO-

In stock : 11

Minimum: 1

SP1004U-ULC-04UTGSP1004U-ULC-04UTGLittelfuse Inc.TVS - Diodes10-XFDFNTVS DIODE 9.2V 1004/10DFN-

In stock : 2633

Minimum: 1

ISM303DACTRISM303DACTRSTMicroelectronicsMultifunction-HIGH PERFORMANCELOW POWER COMPAC-

In stock : 4138

Minimum: 1

SLD8S36ASLD8S36ALittelfuse Inc.TVS - DiodesNonstandard SMDTVS DIODE 36.5V 58.1V SMTO-263-

In stock : 20

Minimum: 1

ACPL-302J-500EACPL-302J-500EBroadcom LimitedIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)OPTOISO 5KV 1CH GATE DRIVER 16SO
  • 1:$6.846048
  • 10:$6.458536
  • 100:$6.092958
  • 500:$5.748074

In stock : 36800

Minimum: 1

UR020-006-RAUR020-006-RATripp LiteUSB Cables-TRIPP-LITE UR020-006-RACOMPUTER CABLE, USB, 6FT, BLACK-

In stock

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock : 6000

Minimum: 1