web counter

Capacitor Basic: How do Capacitors Work?

Published: 21 July 2020 | Last Updated: 18 April 202516573
This comprehensive guide explores the fundamental principles of capacitors, explaining how they store electrical energy by accumulating charges on metal plates separated by dielectric materials. The article details the charging and discharging processes of capacitors, alongside a thorough explanation of capacitance units and practical size considerations that affect their energy storage capabilities. Additionally, it outlines twelve key applications of capacitors in electronic circuits, including filtering, coupling, tuning, and motor operation, demonstrating their essential role in modern electronics.
In this video, how a capacitor works and how the energy is stored in the capacitor is explained intuitively.

How does a capacitor work?

Catalog

  

Ⅰ Introduction

Ⅱ How do capacitors work?

Ⅲ Capacity Unit- F

V The main application of capacitors
IV Comparison of Capacitor Types

 

How do Capacitors Work

Ⅰ Introduction

The working principle of the capacitor is to store electrical energy by storing charge on the electrode, and it is usually used together with the inductor to form an LC oscillation circuit. The working principle of the capacitor is that the charge will move under the force of the electric field. When there is a medium between the conductors, it will hinder the movement of the charge and cause the charge to accumulate on the conductor, resulting in the accumulation of charge. Capacitors are one of the electronic components used in a large number of electronic equipment, so they are widely used in DC blocking, coupling, bypass, filtering, tuning loop, energy conversion, control circuit, etc.

In a sense, capacitors are a bit like batteries. Although the two work in very different ways, they can both store electrical energy. If you have learned the working principle of the battery, then you should know that the battery has two electrodes. Inside the battery, a chemical reaction causes one electrode to generate electrons, and the other electrode absorbs electrons. A capacitor is much simpler, and it cannot produce electrons-it just stores them.

Capacitors, resistors, and inductors are also called the three major passive components, and their annual output has reached about 2 trillion units worldwide. The most widely used capacitors are ceramic capacitors. At the same time, various types of capacitors such as film capacitors with excellent insulation and stability, electrolytic capacitors are known for their large capacity, etc., are also used by people with their respective advantages and characteristics.

Ⅱ How do capacitors work?

Like a battery, a capacitor also has two electrodes. Inside the capacitor, these two electrodes are connected to two metal plates separated by a dielectric. The dielectric can be air, paper, plastic, or any other material that does not conduct electricity and prevents the two metal poles from coming into contact with each other. Using two pieces of aluminum foil and a piece of paper, you can easily make a capacitor. Although the capacitor you made is not ideal in terms of storage capacity, it does work.

 

The basic structure of a capacitor 

 The basic structure of a capacitor

The basic structure of a capacitor is two electrodes (metal plates) facing each other. Applying a DC voltage (V) to the two electrodes, the electrons instantly gather on one of the electrodes, the electrode is negatively charged, and the other electrode is in a state of insufficient electrons, which is positively charged. This state still exists after removing the DC voltage. That is, electric charge (Q) is accumulated between the two electrodes. A dielectric (ceramic, plastic film, etc.) is inserted between the electrodes. The polarization of the dielectric increases the accumulated charge. The index indicating how much charge is stored in a capacitor is called capacitance (C).

The capacitor in the electronic circuit is shown in the figure:

 The capacitor in the electronic circuit

Let's see what happens when we connect the capacitor and battery together:

 

connect the capacitor and battery together 

The metal plate on the capacitor connected to the negative electrode of the battery will absorb the electrons generated by the battery; The metal plate on the capacitor connected to the positive electrode of the battery will release electrons to the battery.

In the circuit, the movement of the charge forms a current. Due to the repulsive effect of the isoelectric charge, the current is the largest at the beginning of the charge movement, and then gradually decreases; and the charge of the capacitor is the smallest at the beginning of the charge movement, which is zero. The charge capacity gradually increases, and the voltage between the two metal plates gradually increases. When it increases to be equal to the power supply voltage, the charging is completed and the current decreases to zero.

After charging, the capacitor and the battery have the same voltage (if the battery voltage is 1.5 volts, the capacitor voltage is also 1.5 volts). Small capacitors have lower capacity, but large capacitors can hold a lot of charges. For example, a soda can-sized capacitor can hold enough charge to light a flashlight bulb for a few minutes. When you see the lightning in the sky, you see a huge capacitor, one of which is the dark cloud in the sky, the other is the earth. Lightning is the charge release phenomenon between the two "poles" of the dark cloud and the earth. Obviously, such a huge capacitor can hold a lot of charges!

Next, let us assume that you connect the capacitor to the circuit as follows:

connect a battery, a light bulb and a capacitor 

You have a battery, a light bulb, and a capacitor. If the capacitor is very large, then you will see that after connecting the battery, current flows from the battery to the capacitor to charge it, and the bulb will be lit. The bulb will gradually dim, and finally, once the capacitor reaches its capacity, the bulb will immediately go out. You can then remove the battery and replace it with a piece of wire. Current will flow from one pole of the capacitor to the other. At this point, the bulb will replay brightly, but soon the bulb gradually dims. Finally, the capacitor is discharged (the number of electrons on the two poles of the capacitor is equal), and the bulb goes out again.

In the circuit, the movement of the charge forms a current. Due to the attraction of the opposite charge, the current is the largest at the beginning of the discharge process and then gradually decreases; the charge capacity of the capacitor is the largest at the beginning of the discharge process and gradually decreases afterwards. When the power is reduced to zero, the discharge is completed, and the current is reduced to zero.

After the capacitor is charged, no current flows in the circuit, so the capacitor can play a role in blocking DC. In the DC circuit, it can be regarded as an open circuit.

The charging process of the capacitor is the process of storing charge. When the capacitor is connected to the DC power supply, the charge on the metal plate connected to the positive electrode of the power supply will run toward the metal plate connected to the negative electrode of the power supply under the action of the electric field force. So that the metal plate connected to the positive pole of the power supply loses its charge and is positively charged. The metal plate connected to the negative pole of the power supply gets negatively charged (the charges of the two metal plates are equal and the signs are opposite), and the capacitor begins to charge.

The discharge process is the process of the capacitor releasing the stored charge. When the charged capacitor is located in a closed path without power, the charge on the negatively charged metal plate will be directed to the positively charged metal under the action of the electric field force. The plate runs away, so that the positive and negative charges are neutralized, and the capacitor begins to discharge.

 

The charge accumulated in the capacitor

 The charge accumulated in the capacitor

The role of the capacitor can be visually described by a water tower connected to the water pipe. The water tower can be used to "storage" water pressure-when the water supplied by the water pump of the water supply system exceeds the amount of water required by the town, the excess water will be stored in the water tower. Then, when the water demand is high, excess water will flow out of the water tower to maintain the water pressure. Capacitors store electrons in the same way.

Capacitance Calculation Formula

The fundamental relationship between capacitance, charge, and voltage is expressed by the equation:

C = Q/V

Where:

- C is the capacitance in farads (F)

- Q is the electric charge in coulombs (C)

- V is the potential difference in volts (V)

For parallel plate capacitors, the capacitance can be calculated using:

C = ε₀εᵣA/d

Where:

- ε₀ is the permittivity of free space (8.85 × 10⁻¹² F/m)

- εᵣ is the relative permittivity of the dielectric material

- A is the area of plate overlap

- d is the distance between plates

Ⅲ Capacity Unit- F

The unit of electric capacity is F. A capacitor with a capacity of 1F can store 1 coulomb of electricity at a voltage of 1 volt. 1 Coulomb is 6.25e18 (6.25*10^18, or 6.25 quintillion) electrons. 1 ampere represents the flow rate of electrons flowing through 1 coulomb of electrons per second. Therefore, a capacitor with a capacity of 1F can store 1 ampere-second of electrons at a voltage of 1 volt.

The 1F capacitor is usually quite large. Depending on the voltage tolerance of the capacitor, it may be as large as a can of tuna or a 1 liter soda bottle. Therefore, the capacitors you see are usually measured in microfarads (parts per million).

To understand how big the 1 farad is, it may be calculated like this:

A typical alkaline AA battery stores about 2.8 amp-hours of electricity. This means that an AA battery can produce a current of 2.8 amps for 1 hour at 1.5 volts (about 4.2 watt-hours, that is, an AA battery can keep a 4 watt light bulb continuously lit for a little more than an hour).

For the convenience of calculation, we simply counted the voltage of the AA battery as 1 volt. To store the energy of one AA battery in the capacitor, a capacitor with a capacity of 3,600*2.8=10,080F is needed, because 1 amp-hour is equivalent to 3600 amp-seconds.

If the capacity of 1 farad needs to be stored with a tuna-sized capacitor, then the size of an AA battery is nothing compared to the size of a 10,080 method capacitor! Obviously, unless a capacitor has a high withstand voltage, it is not practical to use a capacitor to store a large amount of energy.

Ⅳ Comparison of Capacitor Types

TypeCapacitance RangeVoltage RangeTypical Applications
Ceramic1pF-100μF50V-30kVHigh-frequency coupling, bypassing
Film1nF-100μF50V-2kVAudio equipment, timing circuits
Electrolytic1μF-100,000μF6.3V-450VPower supply filtering, audio coupling
Tantalum0.1μF-1000μF2V-50VPortable electronics, medical devices
Supercapacitors1F-3000F2.5V-5.5VEnergy storage, backup power
Variable10pF-500pF100V-1kVRadio tuning, oscillators


V The main application of capacitors

1. Filtering

The capacitor connected between the positive and negative poles of the DC output of the power module can filter out unnecessary AC components in the DC module, which can make the DC power smoother.

2. Decoupling

The capacitor connected between the positive and negative poles of the power supply of the amplifier circuit can prevent the parasitic oscillation caused by the positive feedback formed by the internal resistance of the power supply.

3. Bypassing

In the circuit of AC and DC signals, connect the capacitor in parallel with the two ends of the resistor or jump to the common potential from a certain point of the circuit. You can set a path for the AC signal or pulse signal to avoid AC signal components. The voltage drop attenuation due to the resistance.

4. Coupling

In the AC signal processing circuit, it is used to connect the signal source and the signal processing circuit or as the inter-stage connection of the two amplifiers. It is used to cut off the DC, so AC signal or the pulse signal will pass. And the DC working points of the front and rear amplifier circuits do not affect each other.

5. Tuning

A capacitor is connected at both ends of the oscillating coil of the resonant circuit, which plays the role of selecting the oscillating frequency.

6. Compensation

Auxiliary capacitors connected in parallel with the main capacitor of the resonance circuit. Adjusting this capacitor can expand the frequency range of the oscillation signal.

7. Neutralization

Capacitors connected in parallel between the base and emitter of the triode amplifier to form a negative feedback network to suppress self-oscillation caused by the capacitance between the triodes.

8. Frequency stabilization

The capacitor plays a role in stabilizing the oscillation frequency in the oscillation circuit.

9. Timing

The capacitor in series with the resistor R in the RC time constant circuit can determine the charge and discharge time.

10. Acceleration

Connecting to the oscillator feedback circuit to accelerate the positive feedback process and increase the amplitude of the oscillation signal.

11. Start-up

Connected in series with the auxiliary winding of the single-phase motor to provide the starting phase-shifted AC voltage for the motor, and disconnected from the auxiliary winding after the motor runs normally.

12. Operation

Connected in series with the secondary winding of a single-phase motor to provide phase-shifted alternating current for the secondary winding of the motor. When the motor is running normally, it is connected in series with the auxiliary winding.


Lasted updated: 2025-04-18

 

Article Recommended:

What is a Decoupling Capacitor?

Basic Introduction to Film Capacitors

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

How a capacitor works in a circuit?

Unlike a resistor, a capacitor does not dissipate energy. Instead, a capacitor stores energy in the form of an electrostatic field between its plates. ... In practice, the dielectric between the plates passes a small amount of leakage current and also has an electric field strength limit, known as the breakdown voltage.

What is the working principle of capacitor?

A capacitor works on the principle that the capacitance of a conductor increases appreciably when an earthed conductor is brought near it. Hence, a capacitor has two plates separated by a distance having equal and opposite charges.

What is the main use of capacitor?

A capacitor is a basic storage device to store electrical charges and release it as is required by the circuit. Capacitors are widely used in electronic circuits to perform variety of tasks, such as smoothing, filtering, bypassing etc…

Can a capacitor kill you?

Capacitors are not fatal, they cannot kill you. The voltage stored in the capacitor and the current during discharge can harm you.

Why do you need to discharge a capacitor?

You must discharge the capacitors before working on power supply circuits so you won't get shocked. Using a screwdriver to discharge the capacitor is not recommended because you can generate a spark and damage the printed circuit board or circuitry of the power supply. You can even blow the power section.
Related Articles

  • AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    UTMEL02 June 20263584

    Next-generation AI servers like NVIDIA's Rubin architecture require over 600,000 MLCCs per rack due to extreme power densities exceeding 120kW. This transition from GB300 demands high-capacitance, low-ESR capacitors with X7R/X7S dielectrics to handle intense transient responses and thermal loads, forcing procurement teams to navigate extended 24-week lead times for these specialized components.

    Read More
  • MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    UTMEL07 August 2026766

    Facing 2026 MLCC lead times of up to 24 weeks driven by AI server demand, hardware engineers are substituting multi-layer ceramic capacitors with conductive polymer tantalum capacitors. While Class II MLCCs suffer severe DC bias capacitance loss and acoustic noise, polymer tantalums offer voltage stability and low ESR. Implementing a division-of-labor strategy—using polymer tantalums for bulk decoupling and MLCCs for point-of-load—optimizes PDN performance and bypasses supply bottlenecks.

    Read More
  • Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    UTMEL13 August 2026644

    Modern AI hardware requires a hybrid Power Delivery Network (PDN) to maintain low-voltage stability under extreme transient currents. Deep Trench Silicon Capacitors (DTCs) integrate directly into advanced packages to deliver ultra-low ESL and stable performance for high-frequency transient suppression. Meanwhile, Multilayer Ceramic Capacitors (MLCCs) provide essential bulk energy storage on the motherboard, making both technologies complementary across the AI power stack.

    Read More
  • MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    UTMEL11 September 2026645

    Class II ceramic capacitors suffer significant capacitance loss under DC voltage due to ferroelectric domain saturation and high electric field intensity. This comprehensive engineering guide explains how to calculate true worst-case effective capacitance by compounding DC bias, temperature, tolerance, and aging. It provides multi-vendor simulation workflows, benchtop impedance measurement techniques, and practical guidelines to maintain power supply stability and avoid costly design failures.

    Read More
  • Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    UTMEL13 July 2026424

    Explore how the transition from traditional air-cooling to liquid cooling (direct-to-chip and immersion) in high-density AI server racks alters component thermal profiles. Focus on why design engineers are increasingly specifying Class 2 MLCCs (X7R and X7S dielectrics) over standard X5R variants to prevent thermal degradation near the liquid cooling microchannels. Explain how these capacitors mitigate acoustic noise and voltage bias degradation under heavy workloads. Provide sourcing advice for high-reliability passives via UTMEL during this high-demand memory and passive component super-cycle.

    Read More

Subscribe to Utmel !

Featured Parts More