web counter
Time Constant Calculator

This Capacitor Energy and Time Constant calculator help electrician to calculate the energy stored in a capacitor and compute the time constant of a capacitor for the given voltage across it. With this online calculator for the capacitor energy and time constant calculation, you are able to get the energy (E) and Time Constant (T) just by inputting 3 values: Voltage across capacitor, Capacitance and Load Resistance.

Input

Voltage (V)
Capacitance (C)
Load Resistance (R)

Output

Time Constant ()
s
Energy (E)
J

Formula

Introduction

Recorded with http://screencast-o-matic.com

RC Time Constant Circuit - Calculations

Time Constant Calculator Overview

The Time Constant Calculator determines the RC time constant of a resistor-capacitor circuit and the energy stored in a charged capacitor. Enter resistance, capacitance, and voltage to calculate the response time in seconds and stored energy in joules.

The time constant does not represent the exact time required for a capacitor to become completely charged or discharged. Instead, it describes the speed of the exponential response. After one time constant, a charging capacitor has completed about 63.2% of the voltage change, while a discharging capacitor retains about 36.8% of its initial voltage. Five time constants corresponds to about 99.3% of the total change and is commonly used as a practical settling estimate.

This calculator is useful for RC delay circuits, reset networks, sensor filtering, power-supply startup, capacitor discharge planning, pulse circuits, debounce networks, and first-order low-pass or high-pass filters.

What This Calculator Calculates

  • RC time constant: the characteristic response time of the resistor-capacitor network.

  • Stored capacitor energy: the electrical energy stored at the entered capacitance and voltage.

  • Approximate settling time: one to five time constants can be used to estimate charging or discharging progress.

Input Parameters

InputMeaningCommon Units
Voltage, VThe voltage across the capacitor used in the stored-energy calculation.V
Capacitance, CThe capacitance of the capacitor.F, mF, µF, nF, pF
Resistance, RThe effective resistance through which the capacitor charges or discharges.Ω, kΩ, MΩ

Output Parameters

OutputMeaningSI Unit
Time constant, τThe characteristic time for the RC voltage and current response.s
Stored energy, EThe ideal electrical energy stored in the capacitor at the entered voltage.J

Capacitor Energy Formula

The ideal energy stored in a capacitor is:

E = 0.5 × C × V2

Where:

  • E = stored energy in joules

  • C = capacitance in farads

  • V = voltage across the capacitor in volts

The voltage is squared, so stored energy rises quickly as voltage increases. Doubling the voltage stores four times as much energy when capacitance remains unchanged.

Capacitor stored energy formula

Capacitor Energy Example

Consider a 1000 µF capacitor charged to 10 V. First convert the capacitance to farads:

1000 µF = 0.001 F

Then calculate the stored energy:

E = 0.5 × 0.001 × 102 = 0.05 J

The ideal stored energy is 0.05 joule. Resistance affects how quickly this energy is transferred, but it does not change the ideal energy stored at a specified capacitance and voltage.

RC Time Constant Formula

For a simple RC circuit, the time constant is:

τ = R × C

Where:

  • τ = time constant in seconds

  • R = resistance in ohms

  • C = capacitance in farads

When more components are connected around the capacitor, use the effective resistance seen from the capacitor terminals rather than automatically using one labeled resistor. Independent voltage sources are set to zero when determining this resistance for a linear RC network.

Time Constant Example

Consider a 2000 µF capacitor charging or discharging through a 10 kΩ resistor:

  • C = 2000 µF = 0.002 F

  • R = 10 kΩ = 10000 Ω

τ = 10000 × 0.002 = 20 s

After 20 seconds, the capacitor has completed about 63.2% of a charging transition or retains about 36.8% of its initial voltage during discharge. A practical five-time-constant estimate is 100 seconds.

Capacitor Charging Equation

For a capacitor that starts at 0 V and charges through a resistor toward a constant supply voltage, the capacitor voltage is:

VC(t) = VS × (1 - e-t/RC)

For a capacitor with an initial voltage that is not zero, the more general equation is:

VC(t) = VF + (V0 - VF) × e-t/RC

Where V0 is the initial capacitor voltage and VF is the final steady-state voltage. The capacitor voltage changes rapidly at first, then approaches the final value more slowly.

Capacitor Discharging Equation

For a capacitor discharging through a resistor toward 0 V:

VC(t) = V0 × e-t/RC

The ideal discharge current has the same exponential decay. Its initial magnitude is approximately V0 divided by R, then it decreases as the capacitor voltage falls.

RC capacitor charging and discharging response

Charging and Discharging Percentages

Elapsed TimeCharging VoltageDischarging Voltage Remaining
0.5τ39.3% of final voltage60.7% of initial voltage
1τ63.2% of final voltage36.8% of initial voltage
2τ86.5% of final voltage13.5% of initial voltage
3τ95.0% of final voltage5.0% of initial voltage
4τ98.2% of final voltage1.8% of initial voltage
5τ99.3% of final voltage0.7% of initial voltage

A capacitor never reaches its final value in a mathematically exact sense because the response is exponential. In practical circuit work, five time constants is often treated as fully settled when an error of about 0.7% is acceptable. Precision systems may require a longer settling interval.

How to Calculate Time to a Target Voltage

One time constant is only a reference point. When a circuit must reach a specific threshold, calculate the required time directly.

Charging from 0 V

t = -R × C × ln(1 - VT / VS)

VT is the target capacitor voltage and VS is the charging supply voltage. The target must be lower than the supply voltage for this ideal equation.

Discharging toward 0 V

t = R × C × ln(V0 / VT)

V0 is the initial voltage and VT is the desired lower voltage. These equations are useful for reset thresholds, logic input thresholds, delay circuits, and capacitor safety-discharge calculations.

Useful Unit Combinations

The formula τ = RC gives seconds when resistance is in ohms and capacitance is in farads. The following combinations can reduce conversion mistakes:

Resistance UnitCapacitance UnitResulting Time Unit
ΩFs
ΩµFµs
kΩµFms
MΩµFs
kΩnFµs
MΩnFms

Capacitance and Resistance Conversions

ValueEquivalent SI Value
1 mF0.001 F
1 µF0.000001 F
1 nF0.000000001 F
1 pF0.000000000001 F
1 kΩ1000 Ω
1 MΩ1000000 Ω

How to Use the Time Constant Calculator

  1. Enter the capacitor voltage used for the energy calculation.

  2. Enter the capacitance value and select the correct capacitance unit.

  3. Enter the effective charging or discharging resistance and select its unit.

  4. Calculate the capacitor energy and RC time constant.

  5. Multiply τ by the required number of time constants to estimate settling time.

  6. For a specific threshold, use the charging or discharging logarithmic equation.

  7. Check the result against component tolerances, leakage, source resistance, and load current.

Worked RC Charging Example

A 47 µF capacitor charges from 0 V toward 5 V through a 100 kΩ resistor.

τ = 100000 × 0.000047 = 4.7 s

Elapsed TimeApproximate Capacitor Voltage
4.7 s3.16 V
9.4 s4.32 V
14.1 s4.75 V
23.5 s4.97 V

If a logic input changes state at 3.0 V, the switching delay is not exactly one time constant. Using the target-voltage equation gives approximately 4.31 seconds for an ideal circuit.

Practical Design Considerations

  • Component tolerance: the actual RC time may vary with both resistor and capacitor tolerance.

  • Capacitor leakage: leakage can prevent a high-resistance timing circuit from reaching the expected voltage.

  • Input and load resistance: connected circuitry may be parallel with the timing resistor and change the effective R value.

  • Source resistance: a power source, signal generator, switch, or transistor may add series resistance.

  • Equivalent series resistance: capacitor ESR affects pulse current, loss, and very fast transients.

  • DC bias: some ceramic capacitors lose substantial effective capacitance as applied voltage increases.

  • Temperature: resistance, capacitance, leakage, and ESR can change with temperature.

  • Initial voltage: a capacitor that is not fully discharged requires the general charging equation.

  • Voltage rating: the capacitor rating must exceed the highest voltage it will experience.

  • Stored-energy safety: large or high-voltage capacitors may remain hazardous after power is removed.

Common Calculation Mistakes

  • Entering microfarads as farads without applying the 10-6 conversion.

  • Entering kilo-ohms as ohms without applying the 103 conversion.

  • Calling one time constant a complete charge or discharge.

  • Using reactance instead of resistance in the DC transient formula.

  • Ignoring the resistance of the source, load, measurement probe, or semiconductor switch.

  • Assuming the nominal capacitor value is its exact in-circuit capacitance.

  • Using the energy formula with capacitance in µF while expecting a result directly in joules.

  • Assuming RC timing alone defines an RC filter without considering its cutoff frequency and surrounding impedances.

Time Constant and RC Filter Cutoff Frequency

For a first-order RC filter, the time constant is related to the cutoff frequency:

fC = 1 / (2 × π × R × C) = 1 / (2 × π × τ)

A larger time constant produces a lower cutoff frequency and a slower transient response. This relationship applies to ideal first-order RC networks; source and load impedances must be included when they affect the resistance seen by the capacitor.

Video References


Frequently Asked Questions

What is an RC time constant?

The RC time constant is the product of effective resistance and capacitance. It describes how quickly capacitor voltage and circuit current respond to a step change.

Why is the charge level 63.2% after one time constant?

Ideal capacitor charging follows 1 - e-t/RC. At t = RC, this becomes 1 - e-1, which is approximately 0.632.

How long does a capacitor take to charge fully?

An ideal capacitor approaches its final voltage exponentially and never reaches it exactly. Five time constants reaches about 99.3%, which is often close enough for practical estimates. Precision applications may need a stricter settling requirement.

Does resistance change the energy stored in the capacitor?

For an ideal capacitor at a fixed final voltage, stored energy depends on capacitance and voltage. Resistance changes charging and discharging speed and controls current, but not the ideal final energy.

Can I multiply kΩ by µF directly?

Yes, but the numerical result is in milliseconds. For example, 10 kΩ × 100 µF = 1000 ms, which equals 1 second.

What resistance should be used in a complex circuit?

Use the effective resistance seen by the capacitor. This may include a timing resistor, source resistance, load resistance, switch resistance, and other paths connected to the capacitor.

Is a five-time-constant estimate always sufficient?

No. Five time constants leaves about 0.7% of the transition unfinished. Systems with tighter accuracy requirements need more settling time, while threshold circuits may require less.

Can a charged capacitor be dangerous?

Yes. Large-capacitance or high-voltage capacitors can store hazardous energy. Use a suitable discharge path and verify the voltage before touching or servicing the circuit.

Related Online Calculation Tools

Frequently Asked Questions

How is time constant calculated?

The time constant, τ is found using the formula T = R x C in seconds. 

What is time constant of a capacitor?

The time constant of a resistor-capacitor series combination is defined as the time it takes for the capacitor to deplete 36.8% (for a discharging circuit) of its charge or the time it takes to reach 63.2% (for a charging circuit) of its maximum charge capacity given that it has no initial charge.

What is the time constant equal to?

The RC time constant, also called tau, the time constant (in seconds) of an RC circuit, is equal to the product of the circuit resistance (in ohms) and the circuit capacitance (in farads), i.e.

What is meant by time constant of a circuit?

So time constant is the duration in seconds during which the current through a capacities circuit becomes 36.7 percent of its initial value. This is numerically equal to the product of resistance and capacitance value of the circuit. The time constant is normally denoted by τ (tau).

What is time constant in control system?

Time Constant is the “how fast” variable. It describes the speed with which the measured Process Variable (PV) responds to changes in the Controller Output (CO). More specifically it represents the time needed for the PV to reach 63.2% of its total and final change.

How is RC calculated?

Calculating the RC is straight forward -- multiply the capacitance C, in Farads, by the resistance R, in Ohms. Remember to take care of your powers of 10 -- a micro-Farad is 10-6F, while a pico-Farad is 10-9F.

What is the unit of RC?

seconds The units of RC are seconds, units of time. This quantity is known as the time constant: τ=RC. At time t=τ=RC, the charge equal to 1−e−1=1−0.368=0.632 of the maximum charge Q=Cϵ.

Why we use RC circuit?

The RC circuit is used in camera flashes, pacemaker, timing circuit etc. The RC signal filters the signals by blocking some frequencies and allowing others to pass through it. It is also called first-order RC circuit and is used to filter the signals bypassing some frequencies and blocking others.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

TP3420AV309TP3420AV309Texas InstrumentsInterface - Telecom20-LCC (J-Lead)IC TELECOM INTERFACE 20PLCC-

In stock

Minimum: 1

19-217/R6C-AL1M2VY/3T19-217/R6C-AL1M2VY/3TEverlight Electronics Co LtdLED Indication - Discrete0603 (1608 Metric)LED RED CLEAR 2SMD-

In stock : 6070

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP-

In stock

Minimum: 1

HMC588LC4BTRHMC588LC4BTRAnalog Devices Inc.RF Misc ICs and Modules24-TFQFN Exposed PadIC OSC VCO WIDEBAND 24SMD-

In stock

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

DS21Q48NDS21Q48NMaxim IntegratedInterface - Telecom144-BBGAIC LIU E1/T1/J1 4X 5V LONG144BGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

EEF-CS1E150REEF-CS1E150RPanasonic Electronic ComponentsAluminum - Polymer Capacitors2917 (7343 Metric)Aluminum Organic Polymer Capacitors 15uF 25volt-

In stock

Minimum: 1

AFBR-2418TZAFBR-2418TZBroadcom LimitedFiber Optics - Receivers-Fiber Optic Transmitters, Receivers, Transceivers RX DC-50MBd ML 820nm ST Thrd-

In stock

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock

Minimum: 1

TZY2Z060AC01R00TZY2Z060AC01R00Murata ElectronicsTrimmers, Variable Capacitors-2.5 ~ 6pF Trimmer Capacitor 25V Top Adjustment-

In stock

Minimum: 1

SML-S13RTT86SML-S13RTT86ROHM SemiconductorInfrared, UV, Visible Emitters1206 (3216 Metric)EMITTER IR 850NM 30MA 1206-

In stock : 1

Minimum: 1

TZY2Z100AC01R00TZY2Z100AC01R00Murata ElectronicsTrimmers, Variable Capacitors-3 ~ 10pF Trimmer Capacitor 25V Top Adjustment-

In stock

Minimum: 1

DGD2136S28-13DGD2136S28-13Diodes IncorporatedPMIC - Gate Drivers28-SOIC (0.295, 7.50mm Width)HV GATE DRIVER SO-28-

In stock

Minimum: 1

TEN-HS5TEN-HS5Traco PowerAccessoriesAluminumTRACOPOWER TEN-HS5 Power Supply Accessory, Heat Sink, DC/DC Converter, TEN25, TEN25WI Series
  • 1:$3.817981
  • 10:$3.601869
  • 100:$3.397990
  • 500:$3.205651

In stock : 255

Minimum: 1

HEF4044BT,652HEF4044BT,652NXP USA Inc.Logic - Latches16-SOIC (0.154, 3.90mm Width)IC R/S LATCH 3-STATE QUAD 16SOIC-

In stock

Minimum: 1

T9GV5L14-22T9GV5L14-22TE ConnectivityRelays-Power Relays, Standard, Monostable, DC, 900 mW Coil Power Rating DC, 538 Ω Coil Resistance, UL Coil Insulation Class F, Potter & Brumfield T9G-

In stock

Minimum: 1