Tee Attenuator Calculator Overview
The Tee Attenuator Calculator helps calculate the resistor values for a symmetrical T-pad attenuator. A T-pad attenuator reduces signal level while maintaining the same input and output impedance, which is important in RF, audio, test equipment, and transmission-line applications.
Enter the desired attenuation in decibels and the characteristic impedance of the system, such as 50 Ω, 75 Ω, or 600 Ω. The calculator returns the two resistor values used in the T network: the two equal series resistors R1 and the center shunt resistor R2.

What Is a Tee Attenuator?
A tee attenuator, also called a T-pad attenuator, is a passive resistive network shaped like the letter T. In the common symmetrical version, it has two equal series resistors and one shunt resistor connected from the center node to ground.
The purpose of the network is to reduce voltage or power delivered to the load while preserving the required impedance match between the source and load. When the source impedance and load impedance are both equal to Z0, a correctly designed T-pad also presents approximately Z0 at both ports.
Tee Attenuator Formula
For a symmetrical T-pad with equal input and output impedance:
K = 10^(AdB / 20)
R1 = Z0 × (K - 1) / (K + 1)
R2 = 2 × Z0 × K / (K² - 1)

| Symbol | Meaning | Typical Unit |
|---|---|---|
| R1 | Each series resistor in the symmetrical T-pad attenuator. | Ω |
| R2 | Center shunt resistor connected from the middle node to ground. | Ω |
| Z0 | Characteristic impedance of the source, load, or transmission line. | Ω |
| AdB | Desired attenuation, entered as a positive loss value. | dB |
| K | Voltage loss ratio, equal to Vin / Vout for matched ports. | unitless |
Example Calculation
Suppose you need a 6 dB T-pad attenuator in a 50 Ω RF system.
K = 10^(6 / 20) ≈ 1.995
R1 = 50 × (1.995 - 1) / (1.995 + 1) ≈ 16.6 Ω
R2 = 2 × 50 × 1.995 / (1.995² - 1) ≈ 66.9 Ω
In practice, select the nearest available resistor values and then check the actual attenuation, return loss, and power dissipation. For RF work, resistor package parasitics and PCB layout can affect performance, especially at higher frequencies.
Common T-Pad Values for 50 Ω Systems
| Attenuation | R1, Each Series Resistor | R2, Shunt Resistor |
|---|---|---|
| 3 dB | 8.55 Ω | 141.9 Ω |
| 6 dB | 16.6 Ω | 66.9 Ω |
| 10 dB | 26.0 Ω | 35.1 Ω |
| 20 dB | 40.9 Ω | 10.1 Ω |
| 30 dB | 46.9 Ω | 3.17 Ω |
These values assume an ideal matched 50 Ω system. Use the calculator when your impedance or attenuation value is different.
How to Use the Tee Attenuator Calculator
Enter the required attenuation as a positive number in dB. Then enter the impedance value that both ports should match. For RF lab equipment this is often 50 Ω; for video and CATV systems it may be 75 Ω; for some audio systems it may be 600 Ω.
The output values are ideal resistor values. If you must use standard resistor values, choose the closest available parts or combine resistors in series or parallel. After substitution, recalculate the actual attenuation and impedance match.
Where Tee Attenuators Are Used
| Application | Why a T-Pad Helps |
|---|---|
| RF signal level control | Reduces signal amplitude without intentionally changing the system impedance. |
| Test equipment protection | Prevents excessive power from reaching a receiver, analyzer, or measurement input. |
| Impedance-sensitive measurements | Improves matching between stages and can reduce reflections in a transmission line. |
| Stage isolation | Reduces interaction between source and load by adding a controlled loss pad. |
| Thin-film RF circuits | The T topology can be convenient to implement as a compact resistive network. |
Tee Attenuator vs Pi Attenuator
| Topology | Structure | Typical Use |
|---|---|---|
| Tee attenuator | Two series resistors with one shunt resistor in the middle. | Useful when a series path is convenient in the physical layout. |
| Pi attenuator | Two shunt resistors with one series resistor between them. | Useful when shunt elements are easier to place or when converting from a T network. |
Both topologies can provide the same attenuation and impedance match when designed correctly. The best choice often depends on layout, available resistor values, power handling, frequency range, and whether the circuit is single-ended or balanced.
Power Dissipation and Resistor Selection
A passive attenuator turns part of the input signal power into heat. The resistors must be rated for the expected input power, and the power is not always shared equally among the three parts. Higher attenuation values can place significant power in the series or shunt elements depending on the design.
For RF attenuators, also check resistor parasitics, package size, voltage rating, temperature coefficient, and layout. At high frequencies, ordinary leaded resistors and long traces can introduce inductance and capacitance that change the attenuation and return loss.
Common Mistakes to Avoid
| Mistake | Why It Matters |
|---|---|
| Using dB as a direct multiplier | dB must be converted to the voltage ratio K before using the T-pad formulas. |
| Confusing voltage ratio and power ratio | For equal impedances, voltage loss uses 20 log10, while power loss uses 10 log10. |
| Using the wrong impedance | A 50 Ω pad used in a 75 Ω system will not provide the intended match. |
| Ignoring resistor power rating | The attenuator can overheat or drift if the input power exceeds resistor ratings. |
| Assuming ideal RF behavior | PCB layout, resistor package parasitics, and grounding affect high-frequency performance. |
Design Notes for RF Layout
Keep the attenuator compact and symmetrical. Use short traces, good ground connections for the shunt resistor, and controlled-impedance routing where necessary. For microwave layouts, use resistor packages and pad geometries intended for the target frequency range.
If the attenuator is part of a measurement setup, verify it with a network analyzer or calibrated RF instrument. Important checks include insertion loss, input return loss, output return loss, and usable frequency range.
FAQ
Is a T-pad attenuator directional?
A symmetrical T-pad with equal source and load impedance can be used in either direction. The two series resistors are equal, so the input and output ports are interchangeable in the ideal circuit.
Can this calculator match unequal impedances?
This calculator is for the common symmetrical case where the source and load impedances are the same. For unequal impedances, use an L-pad, unequal T-pad, or another matching network designed for the two different impedances.
Does the attenuator only reduce voltage?
It reduces both voltage and power delivered to the load. The formulas often use voltage ratio because dB voltage loss is convenient when the input and output impedances are equal.
Can I build a high-power RF attenuator from ordinary resistors?
Only if the resistor power rating, voltage rating, frequency behavior, thermal design, and layout are suitable. High-power or high-frequency attenuators usually require RF-rated resistor technology and careful heat management.
Related Online Calculation Tools
Pi Attenuator Calculator - calculates resistor values for a matched pi-pad attenuator.
dBm to Watts Calculator - converts RF power between dBm and watts.
Ohm's Law Calculator - calculates voltage, current, resistance, and power.
Parallel and Series Resistor Calculator - calculates equivalent resistance for resistor networks.


Product
Brand
Articles
Tools