web counter

Film Capacitors Explained: Types, Characteristics, and How to Choose

Published: 08 April 2020 | Last Updated: 14 July 202611995
This guide walks through what makes the family distinct, the plastic dielectrics that distinguish each variant, the two main ways the parts are built, the characteristics worth weighing, and a practical way to decide which film wins for a given design.
Find out all about the different properties of the various capacitor types.

Capacitor Types: electrolytic, ceramic, tantalum, plastic film

Film capacitors sit in a comfortable middle ground between the bulk energy storage of electrolytics and the tiny footprint of ceramics. They are the parts engineers reach for when a circuit needs a stable, low-loss, non-polarized capacitor that behaves predictably over years of service. Instead of treating them as one generic component, it helps to think of the film family as a set of dielectric materials, each with its own personality, and to match that personality to the job in front of you.


What sets film capacitors apart

A film capacitor stores charge between metal electrodes separated by a thin sheet of plastic dielectric. Because that dielectric is an insulating polymer rather than an oxide layer grown on a polarized metal, the part is non-polarized and can sit happily in an AC path or a circuit where the voltage reverses. That single property already separates the family from aluminum and tantalum electrolytics.

Film capacitor internal structure showing metal electrodes, plastic dielectric film, wound layers, and non-polarized AC operation..png
A film capacitor uses plastic dielectric film between metal electrodes, giving it stable, low-loss, non-polarized behavior for AC and precision circuits.

The reputation of film capacitors rests on a handful of behaviours that engineers value. They tend to hold their capacitance closely over temperature and time, they dissipate little energy as heat at moderate frequencies, and they show low dielectric absorption, meaning they release stored charge cleanly rather than "remembering" a previous voltage. Many film constructions also handle voltage transients and ripple current gracefully. None of this comes for free: against a ceramic of the same value, a film part is usually physically larger, and against an electrolytic, it stores far less energy per unit volume. The family wins on stability and signal integrity, not on density.

The dielectric materials inside a film capacitor

The label on the part hides the most important decision, which is the polymer doing the insulating. Each film changes the trade between stability, temperature tolerance, and size.

Polypropylene (PP) is the workhorse of high-performance film. It offers very low loss, excellent stability, and strong behaviour under high voltage and high ripple, which is why it dominates power-electronics roles. Polyester, also called PET or by the trade name Mylar, trades some of that stability for a higher dielectric constant, so a PET part is more compact and more economical for a given value. The cost is weaker capacitance stability over temperature, which is acceptable in coupling, decoupling, and general-purpose timing where precision is not critical.

The specialty films extend the family into harder conditions. Polyphenylene sulphide (PPS) is prized for capacitance that barely moves across a wide temperature span, making it a candidate for precision filtering and circuits exposed to heat. Polyethylene naphthalate (PEN) tolerates elevated temperatures better than ordinary polyester and is often chosen where a compact part must survive a warm environment. Polystyrene and polycarbonate appear in legacy and niche precision designs, valued historically for stability, though availability has narrowed over the years. The qualitative ranking below is a starting frame; the exact temperature coefficients and tolerances always belong to a specific manufacturer datasheet.

DielectricCapacitance stabilityTemperature behaviourRelative size for a given valueWhere it typically fits
Polypropylene (PP)Very highGood, with a predictable negative driftLargerDC-link, snubber, audio, EMI/safety, high ripple
Polyester / PET (Mylar)ModerateModerate, more drift than PPCompactCoupling, decoupling, general purpose
Polyphenylene sulphide (PPS)HighVery flat across a wide rangeCompactPrecision filtering, hot environments
Polyethylene naphthalate (PEN)Moderate to highBetter high-temperature tolerance than PETCompactCompact parts in warm settings
Comparison chart of film capacitor dielectric materials including polypropylene, polyester PET, PPS, and PEN with stability, temperature behavior, size, and applications..png
Different film capacitor dielectrics trade stability, temperature performance, size, and cost, so the material choice should follow the circuit role.

Treat this as a behavioural map rather than a spec sheet. Two PP parts from different makers can differ in voltage rating, ripple handling, and self-healing behaviour, so the named datasheet remains the authority on any number.

Film/foil versus metallized construction

Two parts can share the same dielectric and still behave differently because of how the electrodes are made. In a film/foil capacitor, separate sheets of metal foil act as the electrodes and are wound with the plastic film between them. In a metallized film capacitor, an extremely thin metal layer is vacuum-deposited directly onto the plastic, and that coated film is wound to form the part.

The metallized approach brings a property that genuinely changes reliability thinking: self-healing. If a localized weak spot in the dielectric breaks down, the high current density at the fault vaporizes the thin metal coating around it, isolating the defect and letting the capacitor keep working at a marginally reduced value rather than failing as a hard short. Film/foil parts cannot do this, but their thicker foil electrodes carry higher peak and pulse currents and tend to offer lower inductance, which matters in demanding pulse and high-frequency roles. The two styles therefore answer different questions, as summarized below.

ConstructionElectrodeSelf-healingPeak/pulse current handlingTypical reason to choose it
Film/foilSeparate metal foilNoHigherPulse and high-current paths, lowest inductance
Metallized filmMetal deposited on filmYesModerateReliability under occasional dielectric stress, compact size

Characteristics that matter when you specify one

When an engineer weighs a film capacitor, a few properties carry most of the decision. Capacitance stability over temperature and time decides whether the part is suitable for timing, filtering, or precision analog work. Loss, often discussed through dissipation factor and series resistance (ESR), governs how much the part heats under ripple and how it behaves at frequency. Voltage handling covers both the steady working voltage and the ability to absorb transients without damage. Ripple-current capability sets how much AC the part can pass before self-heating becomes a problem, which is central to power roles.

Physical size and mounting style round out the picture, because a stable dielectric is only useful if the part fits the board and the thermal environment. Where exact figures are needed, the relevant temperature coefficient, tolerance, voltage derating curve, and ripple rating come from the manufacturer datasheet for the specific series, not from a general rule of thumb.

Choosing the right film capacitor for the job

A good way to choose is to start from the role and let the application pull you toward a dielectric and a construction, rather than starting from a part number. The mapping below reflects where each film commonly earns its place.

ApplicationCommon film choiceWhat the role demands
DC-link in power conversionMetallized polypropyleneHigh ripple handling, stability, self-healing safety margin
Snubber across switchesPolypropylene, often film/foil for pulse dutyFast voltage edges, high peak current, low loss
Audio signal pathPolypropyleneLow loss and low dielectric absorption for clean signal
EMI and line-filtering / safety positionsPolypropylene or polyester in safety-rated seriesPredictable behaviour across line voltage; safety-rated parts only
Precision filtering and timingPPS, or polystyrene in legacy designsTight, temperature-stable capacitance
General coupling and decouplingPolyester / PETCompact, economical, stability not critical
Film capacitor selection flowchart based on application, ripple current, voltage stress, temperature stability, self-healing, and pulse-current requirements..png
Start with the circuit role, then narrow the choice by stability, ripple current, voltage stress, and whether self-healing or pulse-current handling matters more.

A short selection checklist keeps the process repeatable:

  • Start from the electrical role: energy buffering, signal coupling, snubbing, or filtering.

  • Note the temperature range and how flat the capacitance must stay across it.

  • Estimate the ripple current and peak voltage the part must survive.

  • Decide whether self-healing reliability or maximum pulse current matters more, which points you to metallized or film/foil.

  • Confirm the working voltage and any safety positioning, then read the candidate series datasheet for the exact ratings.

For any role that touches the AC line or a safety function, the part must carry the appropriate safety-rated series designation from the manufacturer, and that status should be confirmed in the datasheet rather than assumed from the dielectric alone.

Trade-offs and pitfalls to plan around

The most common surprise is size. A film capacitor is physically larger than a ceramic of the same value, so high capacitance in a small footprint is simply not the family's strength, and there is a practical ceiling on how much capacitance a single film part offers before it becomes impractical. Where bulk energy storage is the goal, an electrolytic usually carries that load while a film part handles the high-frequency or high-ripple portion alongside it.

Voltage derating deserves respect. Running a film capacitor near its rated voltage, especially at elevated temperature or with significant ripple, shortens its useful life, so designers leave headroom and follow the derating guidance in the datasheet. It is also worth remembering that a charged power capacitor holds energy after the supply is removed; treat such a part as charged until it has been safely discharged. Finally, the gradual capacitance loss that comes with metallized self-healing is normal and benign in most roles, but in a precision circuit it is one more reason to favour a stable dielectric and a generous voltage margin.

Frequently asked questions

What is the practical difference between a PP and a PET film capacitor?
Polypropylene offers lower loss and tighter stability over temperature and time, which is why it dominates power, audio, and precision roles. Polyester (PET) is more compact and more economical for the same value but drifts more with temperature, making it a better fit for general coupling and decoupling where precision is not essential.

What is a PPS capacitor and when would I use one?
A PPS capacitor uses a polyphenylene sulphide dielectric whose capacitance stays unusually flat across a wide temperature range. It suits precision filtering, timing, and circuits that run warm, in situations where the stability justifies its cost relative to ordinary polyester.

What are the common types of film capacitors?
The family is usually grouped by dielectric: polypropylene (PP), polyester/PET, polyphenylene sulphide (PPS), and polyethylene naphthalate (PEN), with polystyrene and polycarbonate appearing in legacy and niche precision designs. Within each dielectric, parts are built as either film/foil or metallized film.

How does the self-healing property actually work?
In a metallized film part, the electrode is a very thin metal layer on the plastic. If a small dielectric flaw breaks down, the concentrated current vaporizes the metal around the fault and isolates it, so the capacitor keeps working at a slightly reduced capacitance instead of failing short.

Are film capacitors long-lived?
Within their rated voltage, temperature, and ripple limits they are generally durable and age gracefully. Lifetime depends heavily on operating conditions and the specific series, so the manufacturer datasheet, not a general claim, is the right reference for any expected-life figure.

What are the main disadvantages of film capacitors?
They are larger than ceramics for the same value, they top out at modest capacitance compared with electrolytics, and the higher-performance dielectrics cost more. They are chosen for stability and clean behaviour, not for energy density or smallest size.

Sources and references

  • Panasonic Industry film capacitors confirms the dielectric families Panasonic offers and the roles they position each series for; as a manufacturer catalog it presents its own portfolio rather than a neutral cross-vendor comparison.

  • TDK film capacitors confirms construction styles and application categories such as DC-link and snubber duty; the technical detail lives in individual series datasheets linked from each product page rather than the overview itself.

  • Vishay film capacitors confirms the distinction between film/foil and metallized parts and the safety-rated line-filter categories; ratings vary by series, so the specific datasheet remains the authority on numbers.

  • WIMA film capacitors confirms how dielectric choice maps to audio, power, and pulse roles; as a specialist supplier its framing reflects its own product range and not the whole market.

  • KEMET film capacitors confirms metallized self-healing behaviour and DC-link positioning; the descriptions are product-oriented, so design limits should be verified against the relevant datasheet.

  • Digi-Key film capacitor selection guidance provides cross-vendor framing for comparing dielectric types during selection; it summarizes general behaviour and points back to manufacturer documentation for exact specifications.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Related Articles

  • AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    UTMEL02 June 20263584

    Next-generation AI servers like NVIDIA's Rubin architecture require over 600,000 MLCCs per rack due to extreme power densities exceeding 120kW. This transition from GB300 demands high-capacitance, low-ESR capacitors with X7R/X7S dielectrics to handle intense transient responses and thermal loads, forcing procurement teams to navigate extended 24-week lead times for these specialized components.

    Read More
  • MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    UTMEL07 August 2026766

    Facing 2026 MLCC lead times of up to 24 weeks driven by AI server demand, hardware engineers are substituting multi-layer ceramic capacitors with conductive polymer tantalum capacitors. While Class II MLCCs suffer severe DC bias capacitance loss and acoustic noise, polymer tantalums offer voltage stability and low ESR. Implementing a division-of-labor strategy—using polymer tantalums for bulk decoupling and MLCCs for point-of-load—optimizes PDN performance and bypasses supply bottlenecks.

    Read More
  • Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    UTMEL13 August 2026644

    Modern AI hardware requires a hybrid Power Delivery Network (PDN) to maintain low-voltage stability under extreme transient currents. Deep Trench Silicon Capacitors (DTCs) integrate directly into advanced packages to deliver ultra-low ESL and stable performance for high-frequency transient suppression. Meanwhile, Multilayer Ceramic Capacitors (MLCCs) provide essential bulk energy storage on the motherboard, making both technologies complementary across the AI power stack.

    Read More
  • MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    UTMEL11 September 2026645

    Class II ceramic capacitors suffer significant capacitance loss under DC voltage due to ferroelectric domain saturation and high electric field intensity. This comprehensive engineering guide explains how to calculate true worst-case effective capacitance by compounding DC bias, temperature, tolerance, and aging. It provides multi-vendor simulation workflows, benchtop impedance measurement techniques, and practical guidelines to maintain power supply stability and avoid costly design failures.

    Read More
  • Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    UTMEL13 July 2026424

    Explore how the transition from traditional air-cooling to liquid cooling (direct-to-chip and immersion) in high-density AI server racks alters component thermal profiles. Focus on why design engineers are increasingly specifying Class 2 MLCCs (X7R and X7S dielectrics) over standard X5R variants to prevent thermal degradation near the liquid cooling microchannels. Explain how these capacitors mitigate acoustic noise and voltage bias degradation under heavy workloads. Provide sourcing advice for high-reliability passives via UTMEL during this high-demand memory and passive component super-cycle.

    Read More

Subscribe to Utmel !

Featured Parts More