What is RF Filter?

Practical RF Filter Design and Construction
| Topics covered in this article: |
| Ⅰ. What is an RF Filter? |
| Ⅱ. The classification of RF Filter |
| Ⅲ. The technical index of RF Filter |
| Ⅳ. The application of RF Filter |
Ⅰ. What is an RF Filter?
In a radiofrequency/microwave system, it's common to have to distinguish the useful frequency signals from the worthless ones in the signal spectrum. A filter is the piece of equipment that completes this purpose.
The filter is an important radio frequency component of a wireless communication system.
Image frequency interference is filtered out, noise is reduced, and frequency division multiplexing is used.
Oscillation, amplification, frequency multiplication, and mixing circuits with excellent performance
In the passband range, a radio frequency/microwave filter refers to a filter in the radio frequency and microwave frequency bands. One of the most significant components in consumer electronics is the radio frequency filter, commonly known as a "radio frequency interference filter." The radio frequency filter is a filter circuit made up of capacitors, inductors, and resistors that are used to filter the signal frequency in communication channels. The filter allows signals that meet a specific frequency to pass while suppressing unwanted frequency signals. It is widely used in radio frequency signal processing systems for base stations and terminal equipment to solve the problem of signal interference between different frequency bands and communication systems. The filter is situated on the backside of the power amplifier in the radio frequency transmission path, and on the front side of the low noise amplifier in the radio frequency receiving path, from the perspective of the layout of the radio frequency signal processing system.
Network and coupling structure for effective broadband impedance matching
Ⅱ. The classification of RF Filter
The working attenuation LA is usually used to describe the amplitude characteristics of the filter.
According to attenuation characteristics

Low-frequency signals can be sent from the input port to the output port with a minor amount of attenuation thanks to the low-pass filter. When the signal frequency exceeds the characteristic cut-off frequency, the signal attenuation increases significantly, resulting in a reduction in signal amplitude at the output port.
A high-pass filter has the exact opposite features. When the signal frequency exceeds a particular cutoff frequency, the signal is attenuated and sent from the input port to the output port.

Specific lower and upper frequencies separate band pass and band stop filters into frequency bands. In comparison to other frequency bands, the signal attenuator in this band has low (band pass) or high (band stop) attenuation.
According to structure

Tuned electronic equipment is used in active filters. The wave device is designed to have a specified frequency-dependent transmission response, which is mostly used to suppress unwanted signal components, interference, or noise in the spectrum.
Resistors, capacitors, inductors, resonators, attenuators, and other passive structures and components make up passive filters.
Digital hardware, such as application-specific integrated circuits (ASIC), field programmable gate arrays (FPGA), or digital signal processors, are used to execute signal conditioning functions on digitized signals in radio frequency digital filters (DSP).
Low-pass and band-pass filters are the most often used filters.
Low-pass filters are commonly utilized in the mixer's image suppression and the frequency source's harmonic suppression.
Receiver front-end signal selection, spurious suppression after transmitter power amplifier, and frequency source spurious suppression all require bandpass filters.
Ⅲ. The technical index of RF Filter
Order (number of series)
The order of high-pass and low-pass filters is equal to the total of their capacitors and inductors. The order of band-pass filters is the total number of parallel resonators, whereas the order of band-stop filters is the total number of series and parallel resonators.
Absolute bandwidth / relative bandwidth
This indicator is typically used for band-pass filters to characterize the frequency range of the signal that can pass through the filter and to represent the filter's frequency selection. The relative bandwidth to the center frequency is expressed as a proportion of the absolute bandwidth.
Cut-off frequency
High-pass and low-pass filters are commonly utilized. The cutoff frequency characterizes the highest frequency range that a low-pass filter can pass, while the cutoff frequency characterizes the lowest frequency range that a high-pass filter can pass.
Standing wave
That is, the S11 value determined by the vector network represents the degree of matching between the filter port impedance and the system's needed impedance. The percentage of the input signal that does not pass through the filter and is reflected back to the input.
Out-of-band suppression
Outside of the filter passband frequency range, there is "attenuation." Describe how well the filter can select undesired frequency signals.
Ripple
The difference between the S21 curve's peak and trough in the filter's passband.
loss
Indicates how much energy is lost when the signal passes through the filter, or how much energy the filter consumes.
Passband flatness
Within the filter's passband, the absolute value of the difference between the maximum and smallest losses. The filter is used to characterize the difference in energy consumption of different frequency signals.
Phase linearity
The phase difference between a transmission line with the same time delay as the center frequency and the phase in the filter's passband frequency range. Determine the filter's dispersion properties.
Absolute group delay
Within the passband of the filter, the time it takes for the signal to travel from the input port to the output port.
Power Capacity
The maximum power of the filter's passband signal can be input.
Phase consistency
The phase difference between different filters in the same index and batch when transmitting a signal. Determine the distinction (consistency) between batch filters.
Amplitude consistency
The difference in signal transmission loss between different filters in the same index and batch. Determine the distinction (consistency) between batch filters.
Operating temperature
The filter design's operating temperature range.
Ⅳ. The application of RF Filter
The radio frequency filter is a unique technology that allows frequency band filtering to be accomplished. It can pass select frequency components in the signal while drastically attenuating or suppressing others, allowing for filtering, coexistence, duplexing, aggregation, and other radio frequency signal functions.
It can be classified into two broad categories from the standpoint of application: "civilian" and "military."
Filters are widely employed in mobile phones, tablet computers, smart homes, cars, and biological sectors for civilian usage, and the market is enormous;
In terms of military applications, filters are useful in areas such as GPS navigation and electronic countermeasures. It's fair to say that it's a crucial component of national information security.
1. What product can the RF filter applied to?
RF filters are used in unlimited products. The filters are divided into high-pass, low-pass and band-pass, which can be selected according to the needs of the circuit.
2. What is an RF Filter?
The radio frequency filter is a filter circuit made up of capacitors, inductors, and resistors that is used to filter the signal frequency in communication channels.
3. Will RF filter PCB traces cause in-band unevenness?
It will cause unevenness in the band. If the RF signal line has to be wound from the input end of the filter back to the output end, this may seriously damage the bandpass characteristics of the filter. In order to get a good isolation between the input and the output, a ground must be laid around the filter first, and then a ground must be laid in the lower layer area of the filter and connected to the main ground surrounding the filter. It is also a good way to keep the signal lines that need to pass through the filter as far away as possible from the filter pins.
What is a High-pass Filter?UTMEL10 March 202114457A high-pass filter is a combination device of capacitors, inductances, and resistors that allow signal components above a certain frequency to pass, while greatly suppressing signal components below that frequency. The high-pass filter only attenuates the frequency components below a given frequency, and allows the frequency components above the cutoff frequency to pass, and there is no phase shift filtering process. Mainly used to eliminate low-frequency noise, also called low-cut filter.
Read More
Introduction to Pi FilterUTMEL19 February 202115409A Pi filter is a type of filter with a two-port, three-terminal block consisting of three elements with two terminals in each element: the first element is connected to the GND terminal via i/p, the second terminals are connected to the terminals from i/p to o/p and the third element is connected to the terminals from o/p to GND. The circuit model is going to be like a 'Pi' symbol. Capacitors and one inductor are the elements used in the circuit.
Read More
EMI Filter: Introduction, Functions and ApplicationsUTMEL23 December 202013366Electromagnetic interference filter, also known as "EMI filter" is an electronic circuit device used to suppress electromagnetic interference, especially noise in power lines or control signal lines. The EMI filter functions as two low-pass filters: one is to attenuate common mode interference, and the other is to attenuate differential mode interference. It is top choice for electronic equipment design engineers to control conducted electromagnetic interference and radiated electromagnetic interference.
Read More
SAW Filter: Introduction, Features and ApplicationsUTMEL30 December 202010453The Surface Acoustic Wave (SAW) filter is a passive band-pass filter made by using the piezoelectric effect and the physical characteristics of surface acoustic wave propagation. Its role is to filter and delay electrical signals. It has the advantages of small size, stable performance, strong overload capacity, low phase distortion, and no need to adjust, so it is used in televisions, video recorders, wireless data transmission systems and other fields.
Read More
Introduction to Bandstop FilterUTMEL28 January 20219292There are numerous filter types, including high-pass filters, low-pass filters, bandpass filters, and filters for bandstops. The high-pass filter only allows frequencies greater than the cut-off frequency, and the low-pass filter allows frequencies smaller than the cut-off frequencies. A specific band of frequencies will be permitted by the bandpass filter and a band stop filter will reject a specific band of frequencies. An overview of the bandstop filter is discussed in this article.
Read More
Subscribe to Utmel !
BF1211RNXP
N1913A/106Agilent
NE73435CEL
NIS02D1N8TRFNippon-Chemi-Con
UP0.4SA-1R0-REaton
UPC3221GVNEC
UPG2409T6X-1CEL
VTP-01001Premier Magnetics
WHM30-2525LEToshiba
WI.232FHSS-250-FCC-CFTC-ST-RLinx Technologies


Product
Brand
Articles
Tools