Sort by
What is Resistor?02 November 2021
Hello, I am Rose. Weilcome to the new post today. Today I will introduce resistor to you. Resistor is one of the three main passive components of electronics, along with inductors and capacitors; from an energy standpoint, resistance is an energy-consuming component that turns electrical energy into heat.
How Fast is Wi-Fi 6?07 June 2021
Wi-Fi 6 ( IEEE 802.11.ax) is the sixth-generation wireless network technology and the name of the Wi-Fi standard. It is a wireless local area network technology created by the Wi-Fi Alliance based on the IEEE 802.11 standard. Wi-Fi 6 will allow communication with up to 8 devices with a maximum rate of 9.6Gbps.
7 Common Functions of MOSFET Gate Circuits22 January 2022
The gate is the MOSFET's weakest component. It is possible to cause the device or even the system to fail if the circuit is not constructed appropriately. As a result, this article organizes the most popular gate circuits for your reference and discussion, and you are also free to share your own thoughts.
What is an Encoder?20 October 2020
An encoder is a device that compiles and converts a signal (such as a bitstream) or data into a signal form that can be used for communication, transmission, and storage. The encoder converts angular displacement or linear displacement into electrical signals.
MIT Technology Review Officially Released 2022 Top 10 Breakthrough Technologies in the World26 April 2022
In the past year or two, the world we live in has undergone an unprecedented and dramatic transformation.
The Era of UFS 4.0, Announced?06 May 2022
Samsung Electronics recently announced the development of its Universal Flash Storage (UFS) 4.0 solution, the first UFS 4.0 product to comply with the recently approved JEDEC storage standard for next-generation mobile and computing systems.
A Simple Method to Build a Programmable Oscillator27 May 2022
Hello, this is Candy. Nice to meet you. Digital potentiometers (digiPOT) are versatile and can be used for a variety of tasks, including filtering and generating AC signals. However, depending on the application, the frequency must occasionally be able to fluctuate and be altered. Programmable solutions that permit frequency change through the appropriate interface are quite handy and, in some situations, extremely beneficial to the development of such designs. Using digiPOT, this article shows how to make a programmable oscillator in which the oscillation frequency and amplitude may be modified independently of one another.
What is Comparator?11 April 2022
Hello everyone, I am Rose. Welcome to the new post today. Today I will introduce comparator to you. Including its definition, working principles and applications.
What is a Motherboard Chipset? A Guide to 2026 Architecture12 June 2026
The chipset is a set of integrated circuit "chips" and is sold as a product. It is responsible for connecting the core microprocessor of the computer and other parts of the machine.
What is Chip: Definition, Classification and Design Process17 January 2026
Hi fellas. I am Rose. Today I will introduce the process of designing chips for you. Chips, also known as integrated circuits or VLSIs, are electronic circuits made up of thousands, millions, or even billions of transistors, resistors, and capacitors.
What is Low Pass Filter18 November 2021
Hello, today I will introduce low pass filter to you. A low-pass filter (LPF) is a filter that allows low-frequency signals to pass while attenuating high-frequency sounds. The frequency response of a low-pass filter is mostly determined by the low-pass filter's design.
Low-Power Design of Operational Amplifiers27 March 2025
Hello, this is Candy. With the rise in popularity of battery-powered electronics in recent years, analog circuit designers have been increasingly concerned about power usage. This article will cover how to use low-power op amps in system design, as well as low-power op amps with low supply voltage capabilities and their applications, as well as how to read and understand op amp data sheets appropriately. Circuit design with energy-saving technologies for more efficient device choices.


Product
Brand
Articles
Tools