Low-Power Design of Operational Amplifiers

Introduction to Operational Amplifier: Characteristics of Ideal Op-Amp
Topics covered in this article: |
Ⅰ. Understanding Power Dissipation in Op Amp Circuits
First, we'll look at amplifiers with low quiescent current (IQ) and how changing the feedback network's resistor value affects power dissipation.
Consider the following circuit, which uses a battery-powered sensor to generate an analog sinusoidal signal with 50mV amplitude and 50mV offset at 1kHz. For signal conditioning, the signal must be increased to the 0V to 3V range (Figure 1). To save battery power as much as possible, a noninverting amplifier architecture with a gain of 30V/V is required (Figure 2). So, how should we reduce the circuit's power consumption?

Figure. 1 Input and Output Signals in an Example Circuit

Figure. 2 Sensor Amplifier Circuit
Static power, op amp output power, and load power all contribute to the power dissipation of an op amp circuit. Quiescent power (or PQuiescent for short) is the power required to keep the amplifier turned on, and it's usually written in datasheets as IQ (quiescent current), like the one below.

Figure. 3 Quiescent Current of an Op Amp
The power utilized by the op amp output stage when driving a load is known as output power (POutput). Finally, load power (PLoad) refers to the amount of energy consumed by the load.
We have a single-supply op amp with a sinusoidal output signal with a DC voltage offset in this example. As a result, we'll apply the equation below to figure out the overall average power (Ptotal,avg). V+ is the supply voltage, Voff is the output signal's DC offset, Vamp is the output signal's amplitude, and RLoad is the op amp's total load resistance. It's worth noting that overall power is related to IQ and inversely proportional to RLoad.

Figure. 4
Ⅱ. Choose Components with the Right IQ
Because there are so many variables in Equations 5 and 6, it's preferable to focus on just one when choosing materials. The most obvious technique for reducing total power consumption is to select an amplifier with a low IQ. There are, of course, certain sacrifices in the process. Devices with a lower IQ, for example, often have less bandwidth, and more noise, and are more difficult to stabilize.
Because the IQ of different types of op amps might differ by a factor of ten, it's important to spend the time to find the perfect one. The following references are for comparison: TI TLV9042, OPA2333, OPA391, and TLV8802. The TLV8802 would be an excellent choice for applications that require maximum power efficiency based on purely numerical analysis.

Figure. 5 Comparison of Various Types Of Low-Power Op Amps
Ⅲ. Reduce the Resistance Value of the Load Network
Proceed to Equations 5 and 6 to consider the remaining terms. The Vamp terms cancel each other out, therefore Ptotal, avg, and Voff, which are normally predetermined by the application, are unaffected. In other words, the system is unable to cut power usage by using Voff.
Similarly, the V+ rail voltage is normally determined by the circuit's supply voltage. Furthermore, RLoad is determined by the program. RLoad, on the other hand, refers to any load output, not simply the load resistor RL. RLoad would contain RL and the feedback components R1 and R2 in the circuit shown in Figure 1. As a result, equations 7 and 8 will define RLoad as follows:

Figure. 6
The output power of the amplifier in the system is reduced by raising the value of the feedback resistor. This approach is very useful when Poutput outnumbers PQuiescent, but it has its drawbacks. If the feedback resistance exceeds RL by a substantial amount, RL will take control of RLoad, causing the power dissipation to plateau. The enormous feedback resistor interacts with the input capacitance of the amplifier, causing the circuit to become unstable and noisy.
It's recommended to compare the thermal noise of the corresponding resistor seen at each op amp input (see Figure 7 below) with the voltage noise spectral density of the amplifier to reduce noise contribution from these components. As a general rule, the amplifier's input voltage noise density requirements should be at least three times the voltage noise of the equivalent resistors measured from each input.

Figure. 7 Resistor Thermal Noise
Ⅳ. Real World Example
Let's return to the original challenge, which demands a signal amplification rate of 30V/V for a battery-powered sensor that provides a 0 to 100mV analog signal at 1kHz. The two designs are shown in Figure 8 below. A standard 3.3V supply, power-saving resistors, and the TLV9002 general-purpose op amp are used in the design on the left. The TLV9042 op amp is used in the design on the right, which has a bigger resistor value and lower power.
The noise spectrum density is less than one-third of the amplifier's broadband noise when the equivalent resistance at the TLV9042's inverting input is roughly 9.667kΩ, ensuring that the op amp's noise dominates any noise caused by the resistors status.

Figure. 8 Typical Design and Subtle Design
Equation 6 may be used to get Ptotal,avg for the TLV9002 and TLV9042 designs, respectively, based on the numbers in Figure 8, the design parameters, and the specifications of the two op amps. Equations 9 and 10 illustrate the outcomes for each.

Figure. 9
The power consumption of the TLV9002 design is more than four times that of the TLV9042 design, based on the preceding findings. This is due to the amplifier's greater IQ, and it also demonstrates that even when using low feedback resistor values, there are no substantial power savings with a high IQ op amp. We can use two strategies in the example above: raising the resistor value and selecting an op amp with a lower quiescent current. In most op amp applications, both techniques are possible.
Ⅴ. Use Low Voltage Rails to Save Power
Revisit Equations 1 and 6 again to define the average power dissipation for a single-supply op amp circuit with a sinusoidal signal and a DC offset voltage:

Figure. 10
Also, as shown in Equation 6, V+ is the power rail (V+) that symbolizes the line, and power dissipation is directly proportional to V+, therefore lowering V+ to the lowest attainable supply voltage in the circuit is another technique to reduce power consumption Methods.
The minimal supply voltage range for many op amps is 2.7V or 3.3V. The minimum voltage required to keep the inside transistors within the intended functioning range is the reason for this restriction. Some op amps are capable of operating at voltages as low as 1.8V or even lower. The TLV9042 general-purpose op amp. for example, may function from a 1.2V rail.
Ⅵ. Battery Powered Applications
The majority of today's sensors and smart gadgets are powered by batteries, and when they drain, their terminal voltages fall below their nominal voltage ratings. A 1.5V alkaline AA battery, for example, has a nominal voltage of 1.5V. The actual terminal voltage during the initial no-load measurement may be close to 1.6V. The voltage at this terminal will drop to 1.2V or even lower when the battery empties.
Designing using an op amp that can operate at 1.2V instead of a higher voltage op amp has the following benefits:
1. Even as the battery nears the end of its charge cycle and its terminal voltage lowers, the op amp circuit will continue to work for longer.
2. Instead of using two 1.5V batteries to generate the 3V rail, the op amp circuit can use just one 1.5V battery.
Consider the battery discharge diagram in Figure 11 to see why a lower voltage op amp can get more life out of a battery. Discharge cycles for batteries are often similar to this graph. The battery's terminal voltage will begin to approach its nominal rating. The terminal voltage will steadily decrease as the battery discharges. The terminal voltage of the battery will rapidly drop as it approaches the end of its charging cycle. The op-amp circuit's working period t1 will be short if it is only meant to operate at a voltage close to the battery's nominal voltage, say V1. Using an op amp that can operate at slightly lower voltages, such as V2, can greatly lengthen the battery's operating life, t2.

Figure. 11 Typical Discharge Curve for a Single Cell
While the effect varies depending on the type of battery, the load on the battery, and other variables, it is obvious that op amps with low operational power supply have longer working times.
Ⅶ. Low Voltage Digital Logic Levels
Low power op amps with low supply voltage capability can be used in applications that employ low voltage rails for digital and analog circuits. Standard voltage ranges for digital logic range from 5V to 1.8V and below (Figure 12). At lower voltages, digital logic, like op amp circuits, becomes more energy efficient. As a result, lower levels of digital logic are often preferred.
You might choose to use the same supply voltage levels for your analog and digital circuits to make the design process easier. An op amp with 1.8V capabilities, such as the high-precision, wide-bandwidth OPA391 or the cost-optimized TLV9001, could be useful in this situation. It's worth noting, though, that if a design must work with a 1.2V digital rail, the wiring system must clean up any noise that may escape from the digital circuitry to the analog device power supply pins.

Figure 12. Standard Logic Levels
Ⅷ. Summarize
In this post, we'll show you how to rapidly identify a low-power op amp by looking at the op amp's specifications. Picking an op amp with low quiescent current, as bandwidth allows, and selecting an op amp in a feedback circuit are two of these ways. resistors with a higher resistance value Other considerations to consider while assuring low-power op amps are the usage of low-voltage rails and low-voltage digital logic levels.
References
Analog Devices. (2003, February 7). One resistor takes heat from single-supply op amps. https://www.analog.com/en/resources/technical-articles/one-resistor-takes-heat-from-singlesupply-op-amps.html
Texas Instruments. (2014, August 8). Top questions on op amp power dissipation – Part 2. https://e2e.ti.com/blogs_/archives/b/precisionhub/posts/top-2-questions-on-op-amp-power-dissipation-part-2
All About Circuits. (2021, January 5). How much power does an op amp dissipate? https://forum.allaboutcircuits.com/threads/how-much-power-does-an-op-amp-dissipate.175561/
ELE Times. (2021, April 15). Power-saving techniques for op-amp circuits. https://www.eletimes.com/power-saving-techniques-for-op-amp-circuits
What is operational amplifier and its types?
An operational amplifier (op amp) is an analog circuit block that produces a single-ended voltage output from a differential voltage input. Two high-impedance inputs and a low-impedance output port are common on op amps.
What are the 3 main characteristics of operational amplifiers?
In summary, an ideal op-amp has the following characteristics: The op-optimal amp's gain allows for infinite bandwidth. A gain that is infinite in the open-loop The common-mode gain can be infinity or zero.
Why is it called operational amplifier?
Op-amps got their name because they were originally employed in electrical analog computers to mimic basic mathematical operations like addition, subtraction, integration, differentiation, and so on. A real operational amplifier is an ideal circuit element in this regard.
What is the difference between transistor and operational amplifier?
A transistor is a semiconductor device with a single PNP or NPN junction. An operational amplifier (op amp) is a circuit block made up of several transistors and other components that are usually combined into a single integrated circuit.
What is the difference between op amp and differential amplifier?
In electronic circuits, amplifiers play a critical role. A differential amplifier amplifies a voltage difference between its inputs, whereas an operational amplifier is a sort of differential amplifier with a large open-loop gain, high input impedance, and low output impedance.
Introduction to MD8002A Audio AmplifierUTMEL27 March 20259697The MD8002A is an audio power amplifier that uses a 5V DC power supply to provide 2.0 watts of continuous power to a BTL load with less than 10% distortion. It was created with the aim of providing high-quality o/p control with fewer components. It doesn't use any output coupling capacitors or bootstrap capacitors.
Read More
Understanding the Low Noise Amplifier (LNA)UTMEL20 March 202526384A low noise amplifier is an amplifier with a very low noise figure. It is generally used as a high-frequency or intermediate-frequency preamplifier for various types of radio receivers, as well as amplifying circuits for high-sensitivity electronic detection equipment.
Read More
Introduction to Optical AmplifierUTMEL27 March 202510369An optical amplifier is a subsystem product that can amplify optical signals in optical fiber communication systems. The principle of the optical amplifier is basically based on the stimulated radiation of the laser, which realizes the amplification effect by converting the energy of the pump light into the energy of the signal light.
Read More
What is an Inverting Amplifier?UTMEL25 April 202512274An inverting amplifier is a fundamental configuration of operational amplifiers where the output signal has opposite polarity to the input signal. This configuration uses an operational amplifier with its inverting input terminal receiving the input signal, while the non-inverting terminal is typically connected to ground. The primary function of this circuit is to amplify the input signal while inverting its phase by 180 degrees.
Read More
Low-Power Design of Operational AmplifiersUTMEL27 March 20257623Hello, this is Candy. With the rise in popularity of battery-powered electronics in recent years, analog circuit designers have been increasingly concerned about power usage. This article will cover how to use low-power op amps in system design, as well as low-power op amps with low supply voltage capabilities and their applications, as well as how to read and understand op amp data sheets appropriately. Circuit design with energy-saving technologies for more efficient device choices.
Read More
Subscribe to Utmel !
SP2555NUTGLittelfuse Inc.
ETP01-1621RLSTMicroelectronics
SMBJ10CAe3/TR13Microchip Technology
MQ1N8152Microchip Technology
MQ1N8155Microchip Technology
MQ1N8159Microchip Technology
MQ1N8157Microchip Technology
P1300SCLRPLittelfuse Inc.
SMBJ28CAe3/TR13Microchip Technology
MART100KP280CAMicrochip Technology


Product
Brand
Articles
Tools