The History of Thermometers

Fahrenheit to Celsius: History of the thermometer
Quick answer
No single person invented the modern thermometer in one step. Ancient pneumatic experiments showed that heated air could move a liquid. Around the end of the 16th century and the beginning of the 17th, several European experimenters developed air thermoscopes that made warming and cooling visible. Galileo is strongly associated with this stage, but Museo Galileo notes that the invention has also been attributed to Santorio Santorio, Robert Fludd, and Cornelis Drebbel.
A thermoscope indicates that temperature has changed; a thermometer adds a scale and a repeatable measurement method. Santorio described thermometric apparatus for medical measurement, Florentine instrument makers developed sealed spirit-in-glass thermometers, and Fahrenheit and Celsius helped establish reproducible scales. Kelvin later provided an absolute thermodynamic scale. Modern instruments may use electrical resistance, thermoelectric voltage, semiconductor junctions, or emitted infrared radiation instead of liquid expansion.
Thermoscope vs thermometer
The distinction is important because many popular histories call every early temperature-sensitive device a thermometer. A thermoscope shows that a body or the surrounding air has become warmer or cooler. It may move a liquid column, but without a calibrated scale it cannot report a standardized numerical temperature.
A thermometer combines a temperature-sensitive element with a scale, readout, or conversion function. The instrument also needs a defined procedure if measurements are to be compared across locations and over time. Modern thermometry adds calibration, traceability, measurement uncertainty, and controls for environmental effects.
| Feature | Thermoscope | Thermometer |
|---|---|---|
| Primary purpose | Shows relative warming or cooling | Reports a numerical temperature |
| Scale | Absent or not standardized | Calibrated or electronically converted |
| Comparability | Usually limited to observations with the same device | Can be compared when calibration and method are controlled |
| Examples | Open air bulb-and-tube device | Liquid-in-glass, RTD, thermistor, thermocouple, digital, or infrared instrument |
Who invented the first thermometer?
Ancient pneumatic experiments
Devices described in antiquity by writers such as Philo of Byzantium and Hero of Alexandria used the expansion and contraction of air to move liquid. These demonstrations were not calibrated thermometers, but they established the physical behavior that later thermoscopes used.
Galileo and a shared historical attribution
Galileo is commonly connected with a bulb-and-tube air thermoscope. Museo Galileo reports that Vincenzo Viviani's later biography placed Galileo's development of such an instrument in Padua in 1597. That is historical testimony, not a surviving dated instrument or proof that no one else developed a similar device independently.
Museo Galileo's broader account explicitly says that the thermoscope has been attributed to Galileo, Santorio Santorio, Robert Fludd, and Cornelis Drebbel. The evidence therefore supports a cautious conclusion: Galileo played an important role in the early thermoscope tradition, but the modern thermometer was a cumulative invention.

Santorio and quantitative medical use
Santorio Santorio was a physician who promoted physical measurement in medicine. Museo Galileo states that he published descriptions of thermometric apparatus that were probably inspired by Galileo's thermoscope. Adding graduations and using a repeatable procedure allowed changes in a patient's temperature to be compared, although the early apparatus was bulky and still affected by atmospheric conditions.
It is therefore more accurate to describe Santorio as a pioneer of quantitative clinical thermometry than to assign him or Galileo sole ownership of the complete modern thermometer.

How sealed liquid thermometers improved measurement
Why an open air thermoscope was limited
In a typical open air thermoscope, warming the bulb expands the trapped air and moves liquid in the tube. Cooling reverses the movement. Because the system communicates with the atmosphere, changes in barometric pressure can also move the liquid. The reading is therefore not a response to temperature alone.
Florentine spirit-in-glass instruments
By the middle of the 17th century, Florentine instrument makers associated with the Medici court and the Accademia del Cimento were producing sealed thermometers filled with alcohol or another spirit. Sealing the liquid and removing the open air-pressure path made the indication more useful and repeatable.
These instruments were not yet governed by one universal scale. Museo Galileo documents several Accademia del Cimento scales, including 30-, 50-, 60-, 100-, and 180-division versions. Their reference procedures were not fully homogeneous, so measurements from different instruments could still disagree.

Why fixed points mattered
A useful scale requires reproducible reference conditions. Melting ice and boiling water became important reference points because other instrument makers could reproduce them more readily than an arbitrary mark on one thermometer. Pressure, water purity, thermometer construction, and the exact procedure still matter, so modern metrology defines reference conditions and uncertainty much more carefully.
How Fahrenheit and Celsius scales developed
Fahrenheit: reproducible instruments and a lasting scale
Daniel Gabriel Fahrenheit was an instrument maker and experimental physicist. Royal Society records document his thermometric research and papers in the 1720s. His contribution was not merely choosing numbers for a scale; he also worked on making liquid-in-glass instruments that could agree more closely with one another.
The modern Fahrenheit scale is related exactly to Celsius by °F = (°C × 9/5) + 32. Under the common water fixed-point convention, freezing is 32 °F and boiling is 212 °F at one standard atmosphere. Actual phase-change temperatures depend on pressure and sample conditions.
Celsius: a 100-division interval
Anders Celsius proposed his scale in 1742 after comparing existing thermometers and investigating reproducible reference points. Uppsala University records that his original orientation placed 100 at the freezing point of water and 0 at the boiling point. The direction was reversed in subsequent use, producing the familiar modern orientation of 0 °C for freezing and 100 °C for boiling under the stated reference conditions.
Popular accounts sometimes credit the inversion to a single named person. The historical record is less tidy, so the safer statement is that the modern orientation was adopted after Celsius's original proposal.
Réaumur and Rankine
Other scales remain relevant in historical documents or specialized calculations. Réaumur used an 80-division interval between the water fixed points. Rankine is an absolute scale with Fahrenheit-sized intervals. Neither replaces the SI kelvin in scientific measurement.
| Scale | Symbol | Water freezing reference | Water boiling reference | Typical context |
|---|---|---|---|---|
| Celsius | °C | 0 °C | 100 °C | Everyday and technical use in most countries |
| Fahrenheit | °F | 32 °F | 212 °F | Everyday use in the United States and some related contexts |
| Kelvin | K | 273.15 K | 373.15 K | SI thermodynamic temperature |
| Réaumur | °Ré or °Re | 0 °Ré | 80 °Ré | Historical records and limited specialist use |
| Rankine | °R | 491.67 °R | 671.67 °R | Some engineering calculations using Fahrenheit-sized intervals |
The water values in this table are conventional reference values. Boiling point varies with pressure, and high-accuracy work must state the realization method rather than relying on a household water test.

Kelvin and the current SI definition
From an absolute scale to an SI base unit
William Thomson, later Lord Kelvin, proposed a thermodynamic temperature scale in 1848. Its zero is absolute zero: 0 K = -273.15 °C = -459.67 °F. Its interval has the same magnitude as the Celsius interval. A difference of 1 K therefore equals a difference of 1 °C, while the zero points differ by 273.15.
The relationship is exact: t/°C = T/K - 273.15. A temperature of 0 °C is therefore 273.15 K. It is correct to write 300 K, not 300 °K or 300 degrees Kelvin.
The kelvin changed definition in 2019
The old article states that the triple point of water defines the kelvin as exactly 273.16 K. That was the earlier SI definition, but it is no longer current. Since 20 May 2019, the kelvin has been defined by fixing the numerical value of the Boltzmann constant, k, at 1.380 649 × 10-23 J K-1.
This change connects the unit to a fundamental constant and allows primary thermometry to be realized through more than one physical method. It did not make existing calibrated thermometers suddenly change their readings.
What happened to the triple point of water?
The triple point of water remains an important calibration reference near 273.16 K, but its thermodynamic temperature is now measured rather than used to define the kelvin. NIST explains that the International Temperature Scale of 1990, ITS-90, continues to use reproducible fixed points and specified instruments to disseminate practical temperature measurements.
Clinical and electronic thermometers
Smaller clinical instruments
Clinical thermometry became practical when instruments were made compact enough for routine use and their response time was reduced. Mercury-in-glass clinical thermometers were widely used because a constriction could retain the maximum reading after removal. They also carried breakage and mercury-exposure risks, so many health systems and laboratories later moved to safer alternatives.
Electronic thermometers appeared before the 1980s
The old article says the first digital thermometers appeared in the 1980s. That is too late as a general milestone. The Smithsonian catalogs a LaBarge electronic clinical thermometer made in 1972, with related work documented in 1971. Electronic temperature measurement existed earlier in laboratories and industry; later integrated electronics made compact digital readouts cheaper and more common.
A digital display does not identify the sensing principle. A digital thermometer may use a thermistor, RTD, thermocouple, semiconductor sensor, or infrared detector. Accuracy depends on the complete instrument, probe, calibration, placement, and use method.
Modern temperature sensor types
Resistance thermometers and RTDs
A resistance thermometer infers temperature from the predictable change in electrical resistance of a sensing element. Platinum resistance thermometers are important in precision and industrial work. Lead resistance, self-heating, mechanical strain, immersion depth, and readout quality can all affect the result.
Thermistors and semiconductor sensors
A thermistor offers a large resistance change over a defined range, which can provide high sensitivity. Its response is nonlinear, and self-heating or poor thermal coupling can introduce error. Semiconductor temperature ICs can add signal conditioning, calibration data, alarms, and digital communication, but their useful range and package-dependent thermal response are device-specific.
Thermocouples
A thermocouple produces a small voltage related to the temperature difference between its measuring junction and reference junction. Different alloy combinations cover different ranges. The measurement system must account for the reference junction, wiring, electrical noise, inhomogeneity, drift, and calibration. A thermocouple is valuable for broad-range or rugged measurements, but it is not automatically more accurate than an RTD or thermistor.
Infrared and radiation thermometers
An infrared thermometer estimates surface temperature from emitted thermal radiation. It can measure moving, hazardous, very hot, or inaccessible targets without contact. The result depends on emissivity, wavelength band, field of view, spot size, focus, reflections, intervening windows or atmosphere, surface condition, and instrument calibration.
A forehead scanner is therefore not universally more accurate than a contact thermometer, and an industrial infrared instrument does not directly measure internal temperature unless the application model supports that inference.

| Sensor type | Measured property | Useful strengths | Important limitations to control |
|---|---|---|---|
| Liquid-in-glass | Thermal expansion of a liquid | Local reading, no electrical power | Fragility, response time, immersion, reading angle, liquid safety |
| Platinum RTD / PRT | Electrical resistance | Stability and precision | Lead resistance, self-heating, strain, readout, range |
| Thermistor | Electrical resistance | High sensitivity in a designed range | Nonlinearity, self-heating, aging, limited range |
| Thermocouple | Thermoelectric voltage | Wide range, rugged probes, small junctions | Reference junction, drift, small signal, wire condition |
| Semiconductor / digital IC | Temperature-dependent semiconductor behavior | System integration and digital functions | Package coupling, device range, latency, supply and interface errors |
| Infrared / radiation | Emitted thermal radiation | Fast, non-contact surface measurement | Emissivity, optics, field of view, reflections, atmosphere |
Accuracy, calibration, and ITS-90
A sensor does not measure temperature directly
Each thermometer observes a physical property that changes with temperature: liquid volume, resistance, voltage, semiconductor behavior, or radiation. A mathematical relationship and calibration convert that property into a temperature indication. The uncertainty belongs to the complete measurement chain, not just the sensing element.
Traceability and practical temperature scales
National metrology institutes maintain standards and calibration services that link working instruments to the SI. NIST calibrates resistance thermometers, thermistors, thermocouples, digital readouts with probes, and radiation thermometry standards across appropriate ranges. Many high-accuracy measurements are disseminated through ITS-90 fixed points, specified interpolation instruments, and defined equations.
Common sources of measurement error
Poor thermal contact: the sensor has not reached the target temperature.
Heat conduction: the probe stem or wires carry heat away from the measurement point.
Self-heating: excitation current raises a resistance sensor's temperature.
Response time: the reading is taken before the sensor settles.
Environmental influence: airflow, radiation, pressure, humidity, or electrical noise changes the result.
Infrared setup: emissivity, reflections, spot size, or an intervening window is not controlled.
Calibration drift: the instrument has changed since its last calibration.
How to choose a thermometer
Define the expected temperature range, required uncertainty, resolution, and response time.
Decide whether the sensor can contact the target or must measure remotely.
Identify the target material, surface, dimensions, motion, pressure, and surrounding environment.
Check probe construction, chemical compatibility, electrical isolation, safety, and installation method.
For resistance sensors, account for wiring and self-heating; for thermocouples, account for reference-junction and extension-wire errors.
For infrared instruments, verify emissivity, spectral band, spot size, focus distance, reflections, and any window material.
Use the manufacturer's specified accuracy over the required range, not only the display resolution.
Define calibration interval, traceability, acceptance limits, and an in-process verification method.
For medical diagnosis, food safety, regulated production, and other critical applications, use an instrument approved for that purpose and follow the applicable procedure. A consumer wearable or general-purpose sensor should not be treated as a diagnostic instrument unless its labeling and evidence support that use.
Thermometer history timeline
| Period | Development | Why it mattered | Historical caution |
|---|---|---|---|
| Ancient period | Pneumatic demonstrations linked heat with air expansion | Established an observable temperature-dependent effect | These were demonstrations, not calibrated thermometers |
| Late 1500s to early 1600s | Air thermoscopes associated with Galileo and other experimenters | Made relative warming and cooling visible | No single uncontested inventor or surviving first device |
| Early 1600s | Santorio described thermometric apparatus for medical measurement | Connected scales and procedures with clinical observation | Early devices remained cumbersome and pressure-sensitive |
| Mid-1600s | Florentine sealed spirit-in-glass thermometers | Reduced atmospheric-pressure interference | Different instruments still used different scales |
| Early 1700s | Fahrenheit improved instrument reproducibility and established his scale | Supported comparison between instruments | The modern fixed-point convention evolved over time |
| 1742 | Celsius proposed a 100-division water fixed-point scale | Provided a simple centigrade interval | His original orientation was opposite to modern Celsius |
| 1848 onward | Thomson proposed an absolute thermodynamic scale | Linked temperature measurement to thermodynamics | The kelvin's formal definition changed again in 2019 |
| 20th century onward | Resistance, thermoelectric, semiconductor, digital, and radiation instruments expanded | Enabled remote, fast, automated, and extreme-range measurement | No one sensor type is best for every application |
Frequently asked questions
Did Galileo invent the thermometer?
Galileo is strongly associated with an early air thermoscope, but the invention is also attributed to other experimenters. The modern thermometer resulted from later additions including a scale, a sealed sensing medium, reproducible fixed points, and calibration methods.
What is the difference between a thermoscope and a thermometer?
A thermoscope shows relative temperature change. A thermometer reports a numerical temperature using a calibrated scale or conversion function.
Did Fahrenheit invent the mercury thermometer?
Fahrenheit made major advances in liquid-in-glass thermometry, instrument reproducibility, and the scale that bears his name. It is safer to describe those documented contributions than to frame the entire mercury thermometer as a one-person invention.
Was the Celsius scale originally reversed?
Yes. Uppsala University states that Celsius's original 1742 orientation used 100 at the freezing point and 0 at the boiling point. The familiar orientation was adopted afterward.
Is the kelvin still defined by the triple point of water?
No. Since 2019, the kelvin has been defined by the fixed numerical value of the Boltzmann constant. The triple point of water remains a useful calibration reference but no longer defines the unit.
Why is Kelvin written without a degree sign?
The SI unit name is kelvin and its symbol is K. Write 300 K, not 300 °K. Celsius and Fahrenheit use degree symbols: 27 °C and 80.6 °F.
Are infrared thermometers more accurate than contact thermometers?
Not inherently. Infrared instruments are valuable for fast non-contact surface measurements, but emissivity, optics, spot size, reflections, atmosphere, and calibration can dominate the error. The best method depends on the target and uncertainty requirement.
Does a digital display guarantee accuracy?
No. Display resolution is not the same as measurement accuracy. Sensor quality, calibration, probe placement, thermal coupling, environmental effects, electronics, and the specified operating range all matter.
Official sources
How to Use the Oscilloscope's X-Y Display CorrectlyUTMEL19 September 202216496Hello everyone, I am Rose. Welcome to the new post today. This post will tell you how to use the oscilloscope's X-Y display directly.
Read More
The History of ThermometersUTMEL12 August 202619892Hello everyone, I am Rose. Today I will introduce you thermometers. Thermometers are tools that can accurately judge and measure temperature and are divided into pointer thermometers and digital thermometers. According to the difference of the purpose of use, a variety of thermometers have been designed and manufactured.
Read More
The Introduction of Oscilloscope ProbesUTMEL11 January 20228272Hello everyone, I am Rose. Welcome to the new post today. The oscilloscope probe is critical to the accuracy and correctness of the measurement results. It is the electronic component that connects the circuit under test to the input of the oscilloscope.
Read More
50 Frequently Asked Questions about OscilloscopeUTMEL22 November 202113847Hello everyone, I am Rose. Welcome to the new post today. Today I collected some frequently asked questions about oscilloscope to you. hope these will help you solve the problems you meet in dailylife.
Read More
What is Oscilloscope?UTMEL24 September 20218321An oscilloscope, formerly known as an oscillograph, is an instrument that graphically displays electrical signals and shows how those signals change over time. This article will introduce it in four aspects.
Read More
Subscribe to Utmel !
B66343GX127EPC
B65813JR97EPC
B65807JR97EPC
![B65887E1000J41]()
B65813JR87EPC
B67345B1X87EPC
B65701DR48EPC
![B65684A630A27]()
![B65807J250A41]()
![B66367G200X187]()


Product
Brand
Articles
Tools