Diode Basis: Symbol, Types and Applications

Diodes Explained - The basics how diodes work working principle pn junction
Executive Summary: Diode Technology in 2026
What is a Diode? A diode is a two-terminal electronic component that acts as a one-way valve for electric current, allowing it to flow easily in one direction (forward bias) while blocking it in the opposite direction (reverse bias). In 2026, diodes remain fundamental to modern electronics, ranging from power rectification in EVs to signal processing in 5G networks.
Key Takeaway: Modern diodes, including Silicon, Silicon Carbide (SiC), and Gallium Nitride (GaN) variants, are critical for rectification, voltage regulation, and circuit protection (TVS). Understanding package types (SMD vs. Through-hole) and operating principles is essential for efficient PCB design.
Ⅰ. What is a Diode? (Definition & Basics)
A diode is a fundamental semiconductor device that essentially acts as a one-way switch for current. It allows electricity to flow easily in one direction (forward direction) but severely restricts current from flowing in the opposite direction (reverse direction).
Structurally, a modern diode consists of a die (the semiconductor chip), a protective casing, and two electrodes. As illustrated below, the core is a P-N junction where P-type and N-type materials meet.
Anode (+): The positive electrode connected to the P-region.
Cathode (-): The negative electrode connected to the N-region.

Internal Structure of a Diode
Ⅱ. Diode Packaging Standards (2026)
Diode packaging determines how the component is mounted onto a circuit board and its heat dissipation capabilities. In 2026, while Surface Mount Devices (SMD) dominate consumer electronics, Plug-in (Through-hole) packages remain vital for high-power industrial applications.
1) Plug-in / Through-Hole Packages
These are typically used in power supplies and legacy hardware where mechanical durability is required.
DO-41: Common for 1A rectifiers (e.g., 1N4007, 1N47 series Zener).
DO-35 / DO-34: Glass packaging for signal diodes (e.g., 1N4148).
DO-15: Medium power rectifiers (e.g., SR240, SR260).
DO-201AD: Higher current handling (e.g., SR340, SR540).
TO-220 / TO-251 / TO-126: High-power packages with heatsink tabs (e.g., Schottky MBR10100CT).
Bridge Rectifiers: KBP, KBL, GBU series for AC-to-DC conversion.

Common Through-Hole Packages
2) SMD (Surface Mount Device) Packages
SMD packages are the standard for modern, compact electronics (Smartphones, IoT).
SOT-23 / SOT-89: Small outline transistors, often used for arrays (e.g., MMBT3904).
SOD-123 / SOD-323 / SOD-523: Ultra-compact packages for signal diodes (e.g., 1N4148W).
SMA (DO-214AC): Standard for 1A surface mount rectifiers (e.g., M7).
SMB (DO-214AA) / SMC (DO-214AB): Medium to high power surface mount (e.g., SK24, SK34).
MELF (LL-34): Cylindrical glass surface mount (e.g., LL4148).
Mini-Bridges: ABS, MB-S series for compact power supplies.

Common SMD Packages
Ⅲ. How does a Diode Work? (Physics Explained)
To understand how a diode works, we must look at the atomic level of the semiconductor material, typically Silicon (Si).

Atomic Bond Architecture of Pure Silicon
1. N-Type Doping: When pure silicon is doped with Phosphorus (5 valence electrons), it creates an excess of "free electrons."

Generation of Free Electrons (N-Type)
2. P-Type Doping: When silicon is doped with Boron (3 valence electrons), it creates "electron holes" (an absence of electrons).

Creation of Holes (P-Type)
3. The Depletion Region: When N-type and P-type materials are joined, electrons and holes near the junction recombine. This creates a "depletion region"—an internal electric field or potential barrier that stops further current flow. In this state, the diode is OFF.

Electron-Hole Recombination (Depletion Zone)
4. Reverse Bias (Blocked Current): If we connect the positive voltage to the N-side and negative to the P-side, the internal barrier widens. No current flows.

Reverse Bias: Current Blocked
5. Forward Bias (Conduction): If the external voltage (Anode + / Cathode -) is strong enough to overcome the internal barrier (typically 0.7V for Silicon), electrons cross the junction. The diode turns ON.

Forward Bias: Current Flows
Ⅳ. Key Types of Diodes in 2026
1. Classification by Semiconductor Material
Silicon Diodes (Si): The industry standard for general-purpose rectification (0.7V drop).
Germanium Diodes (Ge): Legacy tech, used in low-voltage detection (0.3V drop).
Silicon Carbide (SiC) & Gallium Nitride (GaN): Modern wide-bandgap materials used in 2026 for high-efficiency EV chargers and 5G power systems.
2. Classification by Installation
Plug-in (Through-hole): High mechanical strength.
SMD (Surface Mount): High density, automated assembly.
3. Classification by Internal Structure
Point Contact Diode: Uses a thin metal wire for a small PN junction. Low capacitance, ideal for high-frequency detection.

Surface Contact Diode: Large PN junction area allowing high current (Amps). Used primarily for rectification.

Planar Diode: High stability and reliability, used in switching and pulse circuits.

4. Functional Classification (Usage)
(1) TVS Diode (Transient Voltage Suppressor)
Critical for protecting sensitive electronics (like USB ports and microprocessors) from voltage spikes and ESD. They react in picoseconds to clamp overvoltage.

Typical Application: TVS Surge Protection
(2) Ultrafast Recovery Diode (FRED)
Essential for high-frequency inverters and UPS systems. These diodes minimize switching losses due to their rapid reverse recovery time (Trr).

(3) Switching Diode
Designed for rapid on/off cycling in digital logic, pulse circuits, and high-speed data processing.

(4) Fast Recovery Diode (FRD)
Used in DC-DC converters and reverse battery protection. They prevent current backflow when the power source is connected incorrectly.

(5) Zener Diode
Operates in reverse breakdown mode to maintain a constant voltage. It is the core component of simple voltage regulators and reference circuits.

(6) Schottky Diode (SBD)
Known for extremely low forward voltage drop (0.15V–0.45V) and fast switching. Ideal for solar bypass, battery management, and high-efficiency power supplies.

(7) Rectifier Diode
The workhorse of power conversion, transforming AC to DC. Found in every wall adapter and power supply unit.

Ⅴ. Comparison of Diodes
Schottky Diodes vs. Ordinary Silicon Diodes
Voltage Drop: Schottky diodes have a much lower forward voltage drop (approx. 0.4V) compared to standard Silicon diodes (approx. 0.7V). This makes Schottky diodes more efficient for battery-powered devices.
Speed: Schottky diodes have near-zero reverse recovery time, making them faster than standard diodes.
Leakage: However, Schottky diodes typically have higher reverse leakage current than standard silicon diodes.
TVS (Transient Voltage Suppressor) vs. ESD Diodes
TVS: Built to absorb high-energy transients (surges) across a circuit. They have higher capacitance.
ESD Protection: Designed specifically for electrostatic discharge. They must have very low capacitance (<3.5pF) to avoid distorting high-speed data signals (e.g., HDMI, USB 4.0).
LED (Light Emitting Diode) vs. Laser Diode (LD)
Emission: LEDs emit incoherent (random phase) light with a wide angle. Laser Diodes emit coherent (in-phase), highly directional light.
Applications: LEDs are for illumination and indicators. LDs are for fiber optics, barcode scanners, and precision measurement.
Ⅵ. Modern Diode Applications
1. Rectification (AC to DC)
Converting alternating mains power (AC) into direct current (DC) for laptops, chargers, and LED drivers.
2. Logic & Signal Switching
Using the "One-Way" property to create logic gates (AND/OR) or to route signals in microcontrollers.
3. Voltage Clipping & Limiting
Protecting inputs by shaving off signal peaks that exceed a safe voltage (e.g., in audio equipment or sensor inputs).
4. Freewheeling (Snubber)
Protecting transistors from high-voltage spikes generated by inductive loads like motors and relay coils when they turn off.
5. Light Emission & Display
From simple power indicators to massive OLED screens and automotive lighting.
Ⅶ. Frequently Asked Questions (FAQ)
1. What is the simple definition of a diode?
A diode is an electronic component that allows current to flow in only one direction. Think of it as a "check valve" for electricity. It conducts when forward-biased and blocks current when reverse-biased.
2. What are the main types of diodes used today?
The most common types in 2026 include Rectifier Diodes (power conversion), Zener Diodes (voltage regulation), Schottky Diodes (high efficiency), LEDs (lighting), and TVS Diodes (circuit protection).
3. How do you identify a Schottky Diode?
Physically, the cathode band may be different, but electrically, you measure the forward voltage drop. A Schottky diode will read between 0.15V and 0.45V, whereas a standard silicon diode reads around 0.6V to 0.7V.
4. What materials are diodes made from?
Most commercial diodes are made from Silicon (Si). Specialized diodes use Germanium (Ge) for low voltage detection, or Silicon Carbide (SiC) and Gallium Nitride (GaN) for high-power applications like electric vehicles.
5. What is the function of a diode in a circuit?
Diodes serve multiple roles: Rectification (AC to DC), Protection (blocking reverse polarity), Regulation (Zener voltage fixing), and Signal Modulation (clipping/clamping).
All You Need to Know About Rectifier CircuitUTMEL24 April 202517208All You Need to Know About Rectifier Circuit
Read More
15 Key Elements of Diode SelectionUTMEL26 November 202118673Hello everyone, I am Rose. Welcome back to the new post today. Diodes are one of the most common components in our circuit boards. So, what factors should be considered when selecting models?
Read More
What is a PIN Diode?UTMEL04 February 20219885While diodes with a simple PN junction are by far the most common type of diode in operation, in a variety of applications, other forms of diode may be used. The PIN diode is one type that is used for a number of circuits. In a variety of places, this diode type is used. For RF switching, the PIN diode is very fine, and the PIN structure in photodiodes is very useful as well.
Read More
Microwave Diode: Introduction and TypesUTMEL07 January 202125171Microwave diodes are diodes that work in the microwave frequency band. It is a solid-state microwave device. Microwave band usually refers to the frequency from 300 MHz to 3000 GHz. After the discovery of the point contact diode effect at the end of the 19th century, microwave diodes such as PIN diodes, varactor diodes, and Schottky diode tubes appeared one after another. Microwave diodes have the advantages of small size and high reliability, and are used in microwave oscillation, amplification, frequency conversion, switching, phase shifting and modulation.
Read More
What Determines the Maximum Operating Frequency of a Diode?UTMEL29 June 202212620Hello, wish you a wonderful day. In this essay, we first pose the following query: what determines the diode's maximum operating frequency? In regards to the solution, the first thing we need to understand is that the junction capacitance and the reverse recovery time of the diode are two distinct concepts. The charging and discharging times of the junction capacitance cannot match the reverse recovery time. You say that, why? Let's start by taking a look at these facts.
Read More
Subscribe to Utmel !
BLM18BB220SN1DMurata Electronics
BLM15BD221SN1DMurata Electronics
MPZ1608S601ATD25TDK Corporation
BLM15BB470SN1DMurata Electronics
NFM21CC471R1H3DMurata Electronics
BLM18HG471SN1DMurata Electronics
ST1284-01A8RLSTMicroelectronics
MMZ2012R102AT000TDK Corporation
MMZ2012Y102BTD25TDK Corporation
BKP1005HS221-TTaiyo Yuden


Product
Brand
Articles
Tools