Introduction to Optical Amplifier

Optical Amplifier Basics, Types, Working & Applications
Topics covered in this post: |
What is an optical amplifier?
The optical amplifier is to amplify the optical signal. Before that, the amplification of the transmission signal was to realize the photoelectric conversion and the electro-optical conversion, that is, the O/E/O conversion. With the optical amplifier, the optical signal can be amplified directly. Since its commercialization in the 1990s, optical amplifiers have profoundly changed the status quo of the optical fiber communications industry. The successful development and industrialization of optical amplifiers is a very important achievement in optical fiber communication technology, which has greatly promoted the development of optical multiplexing technology, optical soliton communication, and all-optical networks.
Optical amplifiers have a wide range of applications in optical fiber communications, consumer electronics, power systems, commercial advertising, medicine, and life sciences. In recent years, with the rapid development of information and communication technology, the research and development of optical fiber amplifiers have further expanded the gain bandwidth and pushed the optical fiber communication system to the direction of high speed, large capacity, and long-distance. Due to the unique performance of optical fiber amplifiers, it has a wide range of applications in DWDM transmission systems, optical fiber CATV, and optical fiber access networks.

optical fiber amplifier
In the optical fiber communication system, the optical amplifier can be used as the power booster amplifier of the transmitter to increase the transmission power. It can also be used as the preamplifier of the receiver to improve the receiving sensitivity, extend the transmission distance and realize all-optical communication. Optical amplifiers can be used not only in long-distance trunk systems but also in optical fiber distribution networks, especially in WDM systems, capable of simultaneous amplification of multiple channels.
Optical amplifier classification
At present, there are three main types of optical amplifier technologies: rare earth-doped optical amplifiers (such as erbium-doped fiber amplifiers EDFA, praseodymium-doped fiber amplifiers PDFA, niobium-doped fiber amplifiers NDFA, etc.); semiconductor optical amplifiers SOA; non-linear optical amplifiers (such as Raman amplifiers FRA, Brillouin amplifier, etc.).
(1) Optical fiber amplifier
It is to dope rare-earth ions (such as erbium, praseodymium, thulium, etc.) in the optical fiber as laser-active materials. The gain bandwidth of each dopant is different. The gain band of the erbium-doped fiber amplifier is wide, covering the S, C, and L bands. The gain band of the thulium-doped fiber amplifier is S-band; the gain band of praseodymium-doped fiber amplifier is around 1310nm.
(2) Raman optical amplifier
It is an optical amplifier made by using the Raman scattering effect, that is after a high-power laser is injected into the fiber, the non-linear effect of Raman scattering will occur. In the process of continuous scattering, the energy is transferred to the signal light, so that the signal light is amplified. Therefore, it is not difficult to understand that Raman amplification is a distributed amplification process. Its working bandwidth can be said to be very wide, almost unlimited. This optical amplifier has begun to be commercialized, but it is quite expensive.
(3) Semiconductor optical amplifier
Its working principle is similar to that of a semiconductor laser. Its working bandwidth is very wide. However, the gain range is slightly smaller, making it more difficult to manufacture. Although this optical amplifier has been practical, the output is small. In a WDM optical transmission system that uses an optical amplifier in its transmission path, a monitoring signal channel is used to monitor and control the operation of the amplifier and spectrally separate from data transmission can be multiplexed with data.
Optical amplifier functions
An optical fiber amplifier is an optical device that can amplify the power of optical signals. It is used in optical fiber communication lines to achieve signal amplification. According to its position and function in the optical fiber line, it is generally divided into three types: relay amplification, pre-amplification, and power amplification. Compared with the traditional semiconductor laser amplifier (SOA), OFA does not need to go through complicated processes such as photoelectric conversion, electro-optical conversion, and signal regeneration. It can directly perform all-optical amplification of the signal. It has good "transparency" and is especially suitable for long distances.

Optical amplifier structure
To expand the capacity of communication lines while minimizing the cost, optical fiber amplification is one of the preferred options. When a wavelength division multiplexed optical signal is transmitted in an optical fiber, there is inevitably a certain loss and dispersion. Loss leads to a reduction in the energy of the optical signal, and dispersion causes the optical pulse to expand. Therefore, a repeater needs to be set every certain distance to continue to transmit after amplifying and regenerating the signal.
The conventional method to solve this problem is to use an optical/electrical/optical repeater. Its working principle is to first convert the received weak optical signal into an electrical signal through a PIN or APD, and then amplify, equalize, regenerate in order to obtain a good performance electrical signal, and finally through the semiconductor laser (LtD) to complete the electrical/optical conversion, and then send it to the lower section of the optical fiber.

Schematic diagram of the optical amplifier
This kind of optical/electrical/optical conversion and the processing method can no longer meet the requirements of modern telecommunication transmission. Since wavelength division multiplexing is a multi-wavelength transmission on a single fiber core, to perform electrical regenerative relaying, each wavelength must be performed one by one. This complicates the electrical relay equipment, and the transmission distance is limited by attenuation, and the cost is higher. The optical fiber amplifier can amplify the fuse time of all wavelengths in the band, that is, use the same one. One amplifier provides gain to multiple channels, and the gain is not affected by signal polarization. Crosstalk will not occur in high-speed, multi-channel transmission systems, and pulse distortion will not occur in high-speed transmission systems. Therefore, the fiber amplifier is a key component of the wavelength division multiplexing system. So far, almost all WDM systems, whether they are test systems or commercial systems, use optical fiber amplifiers.
F1TH (fiber to the home), FTTO (fiber to the office), FTTB (fiber to the building), FTTC (fiber to the roadside), and other methods have appeared in the optical fiber access network. Among them, FTTH is the most widely used, and the difficulty is an optical fiber. There are too many terminal branches. For passive networks, after several branches, the optical power received by the user is very low (the optical power drops by 3dB for every doubling of the branch), making the terminal unable to work. After adopting the optical fiber amplifier, the emitted power increases. After multiple branches, the user end can still receive normally, so the realization of FTTH will become possible. Therefore, the emergence and development of optical fiber amplifiers have overcome the biggest obstacle of high-speed transmission lease distance transmission-the limitation of optical power budget and is an important milestone in the history of optical communication.
The development direction of the optical amplifier
Due to the development of ultra-high-speed, large-capacity, and long-distance optical fiber communication systems, new requirements have been put forward for optical fiber amplifiers, which are key components in the field of optical fiber communication, in terms of power, bandwidth, and gain flatness. Therefore, in the future optical fiber communication network Among them, the development direction of optical fiber amplifiers mainly includes the following aspects:
(1) EDFA develops from C-Band to L-Band;
(2) Broad-spectrum, high-power fiber Raman amplifier;
(3) Use the locally flat EDFA in series with the fiber Raman amplifier to obtain an ultra-wideband flat gain amplifier;
(4) Develop strain-compensated non-polarization, monolithic integrated, optical laterally connected semiconductor optical amplifier optical switches;
(5) Research and develop fiber amplifiers with dynamic gain flattening technology;
(6) Miniaturized and integrated optical fiber amplifier.
With the continuous breakthrough of new materials and new technologies, it will not be a dream for the optical fiber amplifier to obtain an ultra-wideband bandwidth of 300nm in the wavelength range of 1292~1660nm. The Tbit/s DWDM optical network transmission system will surely be realized.
Reference
Scholarpedia. (2011, October 20). Optical amplification. http://www.scholarpedia.org/article/Optical_amplification
Wikipedia. (n.d.) Optical amplifier. https://en.wikipedia.org/wiki/Optical_amplifier
Paschotta, R. (n.d.). Optical amplifiers. RP Photonics. https://www.rp-photonics.com/optical_amplifiers.html
Lightyear.ai. (n.d.). What are optical amplifiers? https://lightyear.ai/tips/what-are-optical-amplifiers
1.Which optical amplifier has more advantages?
As compared to all the amplifications, Raman amplification is more advantageous. It has self-phase matching between pump of signal together with broad gain bandwidth as compared to other nonlinear processes.
2.How can you classify optical amplifiers?
Optical amplifiers are basically classified into 3 categories namely: Semiconductor optical amplifier. Doped fiber amplifier. Raman amplifier.
3.What is amplifier in optical fiber communication?
An optical fiber amplifier is used in transmitting data in fiber optic communication systems. Amplifiers are inserted at specific places to boost optical signals in a system where the signals are weak. This boost allows the signals to be successfully transmitted through the remaining cable length.
Introduction to MD8002A Audio AmplifierUTMEL27 March 20259696The MD8002A is an audio power amplifier that uses a 5V DC power supply to provide 2.0 watts of continuous power to a BTL load with less than 10% distortion. It was created with the aim of providing high-quality o/p control with fewer components. It doesn't use any output coupling capacitors or bootstrap capacitors.
Read More
Understanding the Low Noise Amplifier (LNA)UTMEL20 March 202526384A low noise amplifier is an amplifier with a very low noise figure. It is generally used as a high-frequency or intermediate-frequency preamplifier for various types of radio receivers, as well as amplifying circuits for high-sensitivity electronic detection equipment.
Read More
Introduction to Optical AmplifierUTMEL27 March 202510369An optical amplifier is a subsystem product that can amplify optical signals in optical fiber communication systems. The principle of the optical amplifier is basically based on the stimulated radiation of the laser, which realizes the amplification effect by converting the energy of the pump light into the energy of the signal light.
Read More
What is an Inverting Amplifier?UTMEL25 April 202512274An inverting amplifier is a fundamental configuration of operational amplifiers where the output signal has opposite polarity to the input signal. This configuration uses an operational amplifier with its inverting input terminal receiving the input signal, while the non-inverting terminal is typically connected to ground. The primary function of this circuit is to amplify the input signal while inverting its phase by 180 degrees.
Read More
Low-Power Design of Operational AmplifiersUTMEL27 March 20257622Hello, this is Candy. With the rise in popularity of battery-powered electronics in recent years, analog circuit designers have been increasingly concerned about power usage. This article will cover how to use low-power op amps in system design, as well as low-power op amps with low supply voltage capabilities and their applications, as well as how to read and understand op amp data sheets appropriately. Circuit design with energy-saving technologies for more efficient device choices.
Read More
Subscribe to Utmel !
JANTX1N6037A/TRMicrochip Technology
LTC4368HMS-1#PBFLinear Technology/Analog Devices
TBU-CA025-050-WHBourns Inc.
01550900MLittelfuse Inc.
SN65240PWRG4Texas Instruments
LT4363MPS-1#PBFLinear Technology/Analog Devices
M15KP30CA/TRMicrochip Technology
TPD13S523RSVRTexas Instruments
1N5665A/TRMicrochip Technology
P40-G240-WHBourns Inc.


Product
Brand
Articles
Tools