Sort by
Revolutionizing Automotive Traction: A Comprehensive Review of Multiphase Drives for Next-Generation Vehicles04 May 2023
In recent years, the revolutionary development of power electronics and converters paved the way for more scope for research in multiphase drives.
Electric Car Rechargeable Batteries: How Long Do They Last?13 April 2023
According to the most recent estimations, the average lifespan of rechargeable batteries of electric cars and vehicles is between 15 and 20 years before it has to be replaced. However, to provide a deeper and more meaningful response, let's read the whole article.
The Different Types of Circuit Breakers and Their Applications11 April 2023
Electricity, electrical equipment, electronics and powered devices have become an integral part of modern society. From getting a cup of coffee from the coffee machine to running an entire plant, electricity is used. Electricity can thus be defined as an energy that enables us to power many devices and systems that we heavily depend on in the day to day lives.
The Rapid Design of Active Filters29 March 2023
This article briefly introduces the advantages, basic principles, rapid design, and applications of active filters.
Understanding UARTs: The Basics and Benefits of Serial Communication06 March 2023
In this article, we'll take a closer look at what UARTs are, how they work, and why they're so important in modern electronics.
L298N: A Motor Driver That Accepts High Voltages24 February 2023
As more automation is used across industries, the demand for servo motors increases accordingly. Their ability to combine precise motion control with high torque levels makes them ideally suited to automation and robotics. The article focuses on the L298N motor driver and the knowledge content related to motor drive control.
Using ESP32 to Make an IoT Weather Station24 February 2023
ESP32 is a powerful microcontroller that is commonly used for IoT projects. In this article, we will show you how to build an IoT-based weather station using ESP32. This weather station will be able to measure temperature, humidity, and pressure, and then send the data to the cloud using Wi-Fi.
FPGA: A Highly Customised Type of Chip Based on Digital Circuits22 February 2023
Field programmable gate arrays are divided into three categories based on application, such as low-end FPGAs, mid-range FPGAs, and high-end FPGAs.
BYD Semiconductor Terminates IPO Application for the Fourth Time22 February 2023
In response, BYD responded to the media that the withdrawal was a prudent decision based on the judgment of the market situation, the urgency of the project construction and other factors to make full justification.
SIA's Latest Report: Status and Challenges of US Semiconductors22 February 2023
Recently, because of the US embargo on Huawei, domestic readers, and even global stakeholders, have been highly concerned about the strength of US semiconductors and the semiconductor strife between China and the US. The US has even seen a semiconductor manufacturing renaissance in the last month, with several legislators suggesting that the US itself should introduce relevant policies and funding to support the development of semiconductors. In response, the SIA has released this report, which provides an in-depth look at the current state of the US semiconductor industry and the challenges it faces.
PMIC - Gate Drivers: A Purpose-Built Integrated Circuit22 February 2023
A PMIC (Power Management IC), also known as a power management IC, is a purpose-built integrated circuit whose function is to manage power for the main system, for example.
Global Semiconductor Market Expected to Shrink by 4.1 Percent in 202322 February 2023
On 29 November, the World Semiconductor Trade Statistics (WSTS), an organization made up of major semiconductor manufacturers, released its forecast that the semiconductor market will decrease by 4.1% year-on-year to US$556.5 billion in 2023.


Product
Brand
Articles
Tools