web counter

Understanding UARTs: The Basics and Benefits of Serial Communication

Published: 06 March 2023 | Last Updated: 06 March 20233207
In this article, we'll take a closer look at what UARTs are, how they work, and why they're so important in modern electronics.
UART is one of the many ways that computers communicate with each other. In this video I explain how UART transmission works. It all comes down to how voltages represent bits that make up binary data. In my demonstration I am using an Arduino board to generate The data signal and a RIGOL DS 1102E oscilloscope to visualize that signal. Comments, questions, and concerns are welcome. Thanks for watching!

how does UART work??? (explained clearly)


If you've ever used a computer, you've probably heard of UARTs or Universal Asynchronous Receiver-Transmitters. These small devices play an important role in many modern communication systems, from computers and smartphones to industrial control systems and automotive electronics. In this article, we'll take a closer look at what UARTs are, how they work, and why they're so important in modern electronics.

What Are Uarts?

A UART is a type of electronic circuit that allows for serial communication between two devices. It's called "universal" because it can be used to connect almost any two devices, regardless of their manufacturer or specific communication protocols. The term "asynchronous" refers to the fact that UARTs don't rely on a fixed clock signal to regulate communication between devices. Instead, they use to start and stop bits to signal the beginning and end of each data packet.


Figure 1. Communication between two arduino using UART.png 

Figure 1. Communication between two Arduino using UART

How Do Uarts Work?

At a high level, a UART works by converting parallel data (bits transmitted in parallel, or all at once) into serial data (bits transmitted one at a time) and vice versa. The process begins when the transmitting device sends a start bit to the receiving device. The start bit signals to the receiver that a new data packet is beginning. After the start bit, the data bits are transmitted in a specific order, with the least significant bit (LSB) being sent first. Once all the data bits have been sent, a stop bit is transmitted to signal the end of the packet.

UARTs use a fixed baud rate, which determines the speed at which data is transmitted. The baud rate is determined by dividing the clock frequency by a divisor, with the divisor being set by the user. For example, if the clock frequency is 16 MHz and the user sets the divisor to 8, the resulting baud rate would be 2 Mbps.

Why Are Uarts Important?

UARTs are important because they're an essential component of many modern communication systems. They're used in everything from computer peripherals (like keyboards and mice) to smartphones, industrial control systems, and automotive electronics. Because UARTs are universal, they can be used to connect almost any two devices, regardless of their manufacturer or specific communication protocols. This makes them a highly versatile and widely used component in modern electronics.

In addition to their versatility, UARTs are also highly reliable. Because they don't rely on a fixed clock signal to regulate communication, they're less susceptible to timing issues and synchronization problems than other communication protocols. This makes them an ideal choice for systems that require high levels of reliability and robustness.

The Basics and Benefits of UART Communication

The UART has been around for decades and has proved to be a reliable and efficient way of transmitting data between devices. Although it has been largely replaced by higher-level protocols like USB, Ethernet, and Bluetooth, UARTs are still widely used in many applications, including embedded systems, serial communication, and automation. In this article, we have discussed the basic principles of UART communication, including how data is transmitted and received, and the different modes of operation.

A Comparison of UART and Other Serial Communication Protocols

We also looked at some of the important features of UARTs, including the baud rate, parity, and stop bits, and how they affect the performance of the UART. Finally, we discussed some of the common challenges that can arise when working with UARTs, such as timing issues, buffer overflows, and communication errors.

Tips and Best Practices for Implementing UART Communication

UARTs are an important and reliable way of transmitting data between devices. They offer a simple and efficient way of communicating over a serial interface and are still widely used in many applications. While they may not be as fast or versatile as higher-level protocols like USB, Ethernet, or Bluetooth, UARTs remain an important part of many embedded systems and industrial applications. With a solid understanding of the principles of UART communication and some basic troubleshooting skills, engineers and developers can successfully use UARTs in a variety of applications.

Conclusion

In summary, UARTs are an essential component of many modern communication systems. They allow for serial communication between two devices, using start and stop bits to signal the beginning and end of each data packet. UARTs are universal and highly reliable, making them a highly versatile and widely used component in modern electronics. Whether you're using a computer peripheral, a smartphone, or an industrial control system, chances are that you're using a UART to communicate.


Related News

1、Chip Packaging Lead Time Has Grown to 50 Weeks

2、Eight Internet of Things (IoT) Trends for 2022

3、Demand for Automotive Chips Will Surge 300%

4、Volkswagen CFO: Chip Supply Shortage Will Continue Until 2024

5、BMW CEO: The Car Chip Problem Will Not Be Solved Until 2023

6、Shenzhen: This Year Will Focus on Promoting SMIC and CR Micro 12-inch Project



UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Related Articles

Subscribe to Utmel !

Featured Parts More