DVI Connector: Types, Advantages, Distiguishment And Development

Published: 18 November 2020 | Last Updated: 18 November 202015430
A DVI connector, that is, digital video interface connector, is an interface standard launched in 1999 by the DDWG (Digital Display Working Group) formed by Silicon Image, Intel, Compaq, IBM, HP, NEC, Fujitsu and other companies.
Today we’ll be taking a look at the different styles of DVI.  DVI is a common video type used on many computers and monitors.

What's The Difference Between DVI Types?

Catalog

I. Types
II. Advantages1. Fast speed
2. Clear picture
3. Supporting HDCP protocol
III. Distinguishment
IV. Future Development

 

A DVI connector is based on TMDS, which converts the smallest differential signal technology to transmit digital signals. TMDS uses advanced coding algorithms to encode 8bit data (each of the primary color signals in R, G, B) into 10bit data (including horizontal and vertical synchronization information) through minimum conversion, Clock information, data DE, error correction, etc.). After DC balance, it adopts a differential signal to transmit data. Compared with LVDS and TTL, it has better electromagnetic compatibility performance. It can use low-cost dedicated cables to achieve long-distance and high-Quality digital signal transmission.

I. Types

DVI connectors include DVI-A (DVI-Analog), DVI-D (DVI-Digital), and DVI-I (DVI-Integrated).

DVI-A is an analog signal connector, which can only transmit analog signals. Its essence is the VGA analog transmission interface specification, which is barely put into use now.

DVI-A

The DVI-D connector is a pure digital connector, which can only transmit digital signals and is not compatible with analog signals.

DVI-D

The DVI-I connector is compatible with digital and analog connectors. In order to be compatible with VGA analog signals, it has 4 more signal pins than DVI-D to transmit analog signals.

DVI-I

The difference between DVI-D and DVI-I

DVI-D can only transmit digital signals, and a complete DVI-I is compatible with both digital and analog signals. In fact, DVI-I is a combination of DVI-A and DVI-D. In terms of manifestation, the DVI-D connector has 24 pins in 3 rows and 3 columns, one of the pins in the upper right corner is empty, and this "missing" empty pin corresponds to analog I/O. The DVI-D/I is divided into two types, namely single-link and dual-link versions. Among them, the form of DVI-I is also 3 rows, 3 columns, and 24 pins, but there are 5 more on the right to support analog I/ O pin. As for the difference between single and dual-link DVI-D/I, single-link DVI-D/I actually has only 18 pins defined, so its transmission rate and refresh capability are only half of dual-link DVI-D/I.

In terms of actual performance, dual-link DVI-I is the most powerful, but the cost is higher, while ordinary LCDs mostly use DVI-D and single-link DVI-I. Generally, the dual-link LCD configuration that retains the VGA connector is DVI-D, and some single-link DVI LCDs use the DVI-I connector.

In terms of compatibility, DVI-A and DVI-D are not compatible with each other, and DVI-I can be compatible with DVI-D (including cable), but DVI-D is not compatible with DVI-I cable. In addition, the maximum refresh rate of a single-link DVI-I connector can only support 1920*1080@60Hz or 1600*1200@60Hz, so it is more difficult to deal with LCDs over 22 inches, and the display quality may decrease. When purchasing large-screen LCDs, this detail must be examined clearly. Currently, on the market, the DVI for most graphics cards is still a single-link DVI-D or DVI-I.

II. Advantages

1. Fast speed

DVI transmits digital signals, and digital image information will be directly transmitted to the display device without any conversion. Therefore, the cumbersome conversion process of digital → analog → digital is reduced, which greatly saves time. Therefore, It is faster, effectively eliminates the smear phenomenon. The signal is not attenuated by using DVI for data transmission, and the color is purer and more realistic.

2. Clear picture

the computer transmits a binary digital signal. If you use the VGA connector to connect to the LCD display, you need to first convert the signal to the R, G, and B three primary color signals through the D/A (digital/analog) converter in the graphics card And line and field synchronization signals, these signals are transmitted to the inside of the liquid crystal through the analog signal line, and the corresponding A/D (analog/digital) converter is needed to convert the analog signal into a digital signal again to display an image on the liquid crystal. In the above-mentioned D/A, A/D conversion, and signal transmission process, signal loss and interference will inevitably occur, resulting in image distortion and even display errors. The DVI connector does not need to perform these conversions, avoiding signal loss and making The image clarity and detail expression have been greatly improved.

3. Supporting HDCP protocol

The DVI connector supports the HDCP protocol, laying the foundation for watching copyrighted HD videos. However, if you want the graphics card to support HDCP, the DVI connector alone is not enough. You need to install a dedicated chip and pay a high HDCP certification fee. Therefore, there are not many graphics cards that really support the HDCP protocol.

Compared with the existing DVI connector, which is also a digital connector, the biggest change of HDMI is the integration of video and audio transmission, and the connector is small in size, and its flexibility and convenience are more advantageous. The HDMI interface can solve two problems with only one line. The output will greatly simplify the connection of the device and make the desktop more tidy.

III. Distinguishment

The DVI-D connector

The DVI-I connector

As mentioned above, the current DVI connectors are mainly DVI-D and DVI-I connectors, and these two specifications are further divided into "dual link" and "single link". Of the two types, what we usually see is the single-link version. The dual-link version is expensive, so it is usually used in some professional equipment.

Distinguish between different DVI standards

Among the common DVI connectors, the DVI-D connector can only receive digital signals. The connector has only 3 rows and 8 columns with a total of 24 pins, and one of the pins in the upper right corner is empty. Not compatible with analog signals.

The DVI-I connector is compatible with both analog and digital signals. Generally, the graphics card using this connector will have a related conversion connector.

The difference between an 18-pin and a 24-pin DVI connector

In fact, the 18-pin DVI is single-link, while the 24-pin is dual-link. That is to say, the transmission rate of the 18-pin DVI connector is only half of that of the 24-pin, which is 165MHz. The on-screen display, the resolution supported by a single-link DVI connector is exactly the same as that of a dual-link connector, but the refresh rate is only about half of that of a dual-link, which will impair the display quality. Generally speaking, the maximum refresh rate of a single-channel DVI connector can only support 1920*1080*60hz or 1600*1200*60hz, that is, the normal display of the existing 23-inch widescreen monitor and 20-inch normal ratio monitor, if it is higher it will impair the display effect.

IV. Future development

Although the DVI connector is a fully digital transmission technology, at the beginning of its development, its initial goal is to achieve high-definition, lossless compression of digital signal transmission. Because the making of it did not take the trend of IT products and AV products integration into consideration, the DVI standard puts too much emphasis on the support of computer display devices while ignoring the support of AV devices such as digital flat-panel TVs. At the same time, for Hollywood publishers who have been concerned about piracy issues, the DVI connector does not provide the copyright anti-theft function they care about. Therefore, from the final result, although the DVI connector has successfully achieved the goal of lossless HD transmission, the over-specific positioning has also caused the overall performance to lag to a considerable extent. Let's look at the main problems of the DVI connector:

- DVI connector is mainly used in PC, which is generally compatible with flat-panel TVs.

- DVI connector lacks support for image copyright protection.

- DVI connector only supports RGB digital signals in the computer field, and unable to support digital color difference signals.

- The DVI interface only supports 8bit RGB signal transmission, which cannot allow a wide color gamut display terminal to exert its best performance.

- For compatibility reasons, the DVI interface reserves a lot of pins to support analog devices, causing the mouth volume to be large and the efficiency is very low.

- DVI connectors can only transmit image signals, and the support for digital audio signals is completely ignored in consideration.

- Due to the above disadvantages, the DVI connector can no longer better meet the development needs of the entire industry. Therefore, whether it is IT manufacturers, flat-panel TV manufacturers, or many publishers in Hollywood, there is an urgent need for a better connector technology that can meet the future development of the high-definition video industry. It is for these reasons that the HDMI standard has been promoted.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

Is DVI as good as HDMI?

HDMI is the best choice if you are just connecting a gaming console, blu-ray player or streaming device to your TV. DVI is a good choice if you're looking to get the most out your high frame rate on a 1080p monitor. With the latest graphics cards, gaming at 4K resolution and a 120Hz refresh rate is possible.

What does a DVI connector look like?

A DVI connector is characteristically colored white (as opposed to a VGA connector which is colored blue)

What is the most common DVI port?

The most common use of DVI-A is connecting to a VGA device, since DVI-A and VGAcarry the same signal. There is some quality loss involved in the digital to analog conversion, which is why a digital signal is recommended whenever possible.
Related Articles

  • The Introduction to USB Type-C Pin Signal and PCB Layout
    The Introduction to USB Type-C Pin Signal and PCB Layout
    UTMEL03 December 202126185

    Hello everyone. Welcome to the new post today. USB Type-C is a smaller-volume USB interface standard than Type-A and Type-B. It can be used on a PC (master device) as well as external devices (slave devices, such as mobile phones).

    Read More
  • Everything You Need to Know about Connectors
    Everything You Need to Know about Connectors
    UTMEL07 September 20218139

    Electrical connectors, as key components for current or signal connections, are also an important part of the industrial system. Connectors can be as huge as airplanes and rockets or as small as mobile phones and televisions, forming bridges between circuits or other components and serving as electric current or signal links.

    Read More
  • Network Interface Card: Types, Functions and Buying Guide
    Network Interface Card: Types, Functions and Buying Guide
    UTMEL17 August 202110448

    Network Interface Card (NIC, also known as a network interface controller) is one of the most basic components in the local area network. It is the hardware device connecting the computer and the network. Whether it is a twisted pair connection, a coaxial cable connection, or an optical fiber connection, data communication must be realized with the help of a network interface card.

    Read More
  • What is Universal Serial Bus (USB)?
    What is Universal Serial Bus (USB)?
    UTMEL19 January 202612411

    Universal Serial Bus (USB) is a serial bus standard and a technical specification for input and output interfaces. It is widely used in information communication devices. The latest generation is USB4, and its transmission speed is 40Gbit/s, the three-stage voltage is 5V/12V/20V, the maximum power supply is 100W.

    Read More
  • Classification and Selection of Industrial Connectors
    Classification and Selection of Industrial Connectors
    UTMEL11 February 20225802

    This article mainly introduces a very important component-connector in the modern industrial system, including its definition, classification, and selection.

    Read More